![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Data Structures | |
| struct | sai_edma_handle_t |
| SAI DMA transfer handle, users should not touch the content of the handle. More... | |
Typedefs | |
| typedef void(* | sai_edma_callback_t )(I2S_Type *base, sai_edma_handle_t *handle, status_t status, void *userData) |
| SAI eDMA transfer callback function for finish and error. | |
Driver version | |
| #define | FSL_SAI_EDMA_DRIVER_VERSION (MAKE_VERSION(2, 3, 1)) |
| Version 2.3.1. | |
eDMA Transactional | |
| void | SAI_TransferTxCreateHandleEDMA (I2S_Type *base, sai_edma_handle_t *handle, sai_edma_callback_t callback, void *userData, edma_handle_t *txDmaHandle) |
| Initializes the SAI eDMA handle. More... | |
| void | SAI_TransferRxCreateHandleEDMA (I2S_Type *base, sai_edma_handle_t *handle, sai_edma_callback_t callback, void *userData, edma_handle_t *rxDmaHandle) |
| Initializes the SAI Rx eDMA handle. More... | |
| void | SAI_TransferTxSetFormatEDMA (I2S_Type *base, sai_edma_handle_t *handle, sai_transfer_format_t *format, uint32_t mclkSourceClockHz, uint32_t bclkSourceClockHz) |
| Configures the SAI Tx audio format. More... | |
| void | SAI_TransferRxSetFormatEDMA (I2S_Type *base, sai_edma_handle_t *handle, sai_transfer_format_t *format, uint32_t mclkSourceClockHz, uint32_t bclkSourceClockHz) |
| Configures the SAI Rx audio format. More... | |
| void | SAI_TransferTxSetConfigEDMA (I2S_Type *base, sai_edma_handle_t *handle, sai_transceiver_t *saiConfig) |
| Configures the SAI Tx. More... | |
| void | SAI_TransferRxSetConfigEDMA (I2S_Type *base, sai_edma_handle_t *handle, sai_transceiver_t *saiConfig) |
| Configures the SAI Rx. More... | |
| status_t | SAI_TransferSendEDMA (I2S_Type *base, sai_edma_handle_t *handle, sai_transfer_t *xfer) |
| Performs a non-blocking SAI transfer using DMA. More... | |
| status_t | SAI_TransferReceiveEDMA (I2S_Type *base, sai_edma_handle_t *handle, sai_transfer_t *xfer) |
| Performs a non-blocking SAI receive using eDMA. More... | |
| void | SAI_TransferTerminateSendEDMA (I2S_Type *base, sai_edma_handle_t *handle) |
| Terminate all SAI send. More... | |
| void | SAI_TransferTerminateReceiveEDMA (I2S_Type *base, sai_edma_handle_t *handle) |
| Terminate all SAI receive. More... | |
| void | SAI_TransferAbortSendEDMA (I2S_Type *base, sai_edma_handle_t *handle) |
| Aborts a SAI transfer using eDMA. More... | |
| void | SAI_TransferAbortReceiveEDMA (I2S_Type *base, sai_edma_handle_t *handle) |
| Aborts a SAI receive using eDMA. More... | |
| status_t | SAI_TransferGetSendCountEDMA (I2S_Type *base, sai_edma_handle_t *handle, size_t *count) |
| Gets byte count sent by SAI. More... | |
| status_t | SAI_TransferGetReceiveCountEDMA (I2S_Type *base, sai_edma_handle_t *handle, size_t *count) |
| Gets byte count received by SAI. More... | |
| struct sai_edma_handle |
Data Fields | |
| edma_handle_t * | dmaHandle |
| DMA handler for SAI send. | |
| uint8_t | nbytes |
| eDMA minor byte transfer count initially configured. More... | |
| uint8_t | bytesPerFrame |
| Bytes in a frame. | |
| uint8_t | channel |
| Which data channel. | |
| uint8_t | count |
| The transfer data count in a DMA request. | |
| uint32_t | state |
| Internal state for SAI eDMA transfer. | |
| sai_edma_callback_t | callback |
| Callback for users while transfer finish or error occurs. | |
| void * | userData |
| User callback parameter. | |
| uint8_t | tcd [(SAI_XFER_QUEUE_SIZE+1U)*sizeof(edma_tcd_t)] |
| TCD pool for eDMA transfer. More... | |
| sai_transfer_t | saiQueue [SAI_XFER_QUEUE_SIZE] |
| Transfer queue storing queued transfer. More... | |
| size_t | transferSize [SAI_XFER_QUEUE_SIZE] |
| Data bytes need to transfer. | |
| volatile uint8_t | queueUser |
| Index for user to queue transfer. More... | |
| volatile uint8_t | queueDriver |
| Index for driver to get the transfer data and size. | |
| uint8_t sai_edma_handle_t::nbytes |
| uint8_t sai_edma_handle_t::tcd[(SAI_XFER_QUEUE_SIZE+1U)*sizeof(edma_tcd_t)] |
| sai_transfer_t sai_edma_handle_t::saiQueue[SAI_XFER_QUEUE_SIZE] |
| volatile uint8_t sai_edma_handle_t::queueUser |
| void SAI_TransferTxCreateHandleEDMA | ( | I2S_Type * | base, |
| sai_edma_handle_t * | handle, | ||
| sai_edma_callback_t | callback, | ||
| void * | userData, | ||
| edma_handle_t * | txDmaHandle | ||
| ) |
This function initializes the SAI master DMA handle, which can be used for other SAI master transactional APIs. Usually, for a specified SAI instance, call this API once to get the initialized handle.
| base | SAI base pointer. |
| handle | SAI eDMA handle pointer. |
| base | SAI peripheral base address. |
| callback | Pointer to user callback function. |
| userData | User parameter passed to the callback function. |
| txDmaHandle | eDMA handle pointer, this handle shall be static allocated by users. |
| void SAI_TransferRxCreateHandleEDMA | ( | I2S_Type * | base, |
| sai_edma_handle_t * | handle, | ||
| sai_edma_callback_t | callback, | ||
| void * | userData, | ||
| edma_handle_t * | rxDmaHandle | ||
| ) |
This function initializes the SAI slave DMA handle, which can be used for other SAI master transactional APIs. Usually, for a specified SAI instance, call this API once to get the initialized handle.
| base | SAI base pointer. |
| handle | SAI eDMA handle pointer. |
| base | SAI peripheral base address. |
| callback | Pointer to user callback function. |
| userData | User parameter passed to the callback function. |
| rxDmaHandle | eDMA handle pointer, this handle shall be static allocated by users. |
| void SAI_TransferTxSetFormatEDMA | ( | I2S_Type * | base, |
| sai_edma_handle_t * | handle, | ||
| sai_transfer_format_t * | format, | ||
| uint32_t | mclkSourceClockHz, | ||
| uint32_t | bclkSourceClockHz | ||
| ) |
The audio format can be changed at run-time. This function configures the sample rate and audio data format to be transferred. This function also sets the eDMA parameter according to formatting requirements.
| base | SAI base pointer. |
| handle | SAI eDMA handle pointer. |
| format | Pointer to SAI audio data format structure. |
| mclkSourceClockHz | SAI master clock source frequency in Hz. |
| bclkSourceClockHz | SAI bit clock source frequency in Hz. If bit clock source is master clock, this value should equals to masterClockHz in format. |
| kStatus_Success | Audio format set successfully. |
| kStatus_InvalidArgument | The input argument is invalid. |
| void SAI_TransferRxSetFormatEDMA | ( | I2S_Type * | base, |
| sai_edma_handle_t * | handle, | ||
| sai_transfer_format_t * | format, | ||
| uint32_t | mclkSourceClockHz, | ||
| uint32_t | bclkSourceClockHz | ||
| ) |
The audio format can be changed at run-time. This function configures the sample rate and audio data format to be transferred. This function also sets the eDMA parameter according to formatting requirements.
| base | SAI base pointer. |
| handle | SAI eDMA handle pointer. |
| format | Pointer to SAI audio data format structure. |
| mclkSourceClockHz | SAI master clock source frequency in Hz. |
| bclkSourceClockHz | SAI bit clock source frequency in Hz. If a bit clock source is the master clock, this value should equal to masterClockHz in format. |
| kStatus_Success | Audio format set successfully. |
| kStatus_InvalidArgument | The input argument is invalid. |
| void SAI_TransferTxSetConfigEDMA | ( | I2S_Type * | base, |
| sai_edma_handle_t * | handle, | ||
| sai_transceiver_t * | saiConfig | ||
| ) |
| base | SAI base pointer. |
| handle | SAI eDMA handle pointer. |
| saiConfig | sai configurations. |
| void SAI_TransferRxSetConfigEDMA | ( | I2S_Type * | base, |
| sai_edma_handle_t * | handle, | ||
| sai_transceiver_t * | saiConfig | ||
| ) |
| base | SAI base pointer. |
| handle | SAI eDMA handle pointer. |
| saiConfig | sai configurations. |
| status_t SAI_TransferSendEDMA | ( | I2S_Type * | base, |
| sai_edma_handle_t * | handle, | ||
| sai_transfer_t * | xfer | ||
| ) |
| base | SAI base pointer. |
| handle | SAI eDMA handle pointer. |
| xfer | Pointer to the DMA transfer structure. |
| kStatus_Success | Start a SAI eDMA send successfully. |
| kStatus_InvalidArgument | The input argument is invalid. |
| kStatus_TxBusy | SAI is busy sending data. |
| status_t SAI_TransferReceiveEDMA | ( | I2S_Type * | base, |
| sai_edma_handle_t * | handle, | ||
| sai_transfer_t * | xfer | ||
| ) |
| base | SAI base pointer |
| handle | SAI eDMA handle pointer. |
| xfer | Pointer to DMA transfer structure. |
| kStatus_Success | Start a SAI eDMA receive successfully. |
| kStatus_InvalidArgument | The input argument is invalid. |
| kStatus_RxBusy | SAI is busy receiving data. |
| void SAI_TransferTerminateSendEDMA | ( | I2S_Type * | base, |
| sai_edma_handle_t * | handle | ||
| ) |
This function will clear all transfer slots buffered in the sai queue. If users only want to abort the current transfer slot, please call SAI_TransferAbortSendEDMA.
| base | SAI base pointer. |
| handle | SAI eDMA handle pointer. |
| void SAI_TransferTerminateReceiveEDMA | ( | I2S_Type * | base, |
| sai_edma_handle_t * | handle | ||
| ) |
This function will clear all transfer slots buffered in the sai queue. If users only want to abort the current transfer slot, please call SAI_TransferAbortReceiveEDMA.
| base | SAI base pointer. |
| handle | SAI eDMA handle pointer. |
| void SAI_TransferAbortSendEDMA | ( | I2S_Type * | base, |
| sai_edma_handle_t * | handle | ||
| ) |
This function only aborts the current transfer slots, the other transfer slots' information still kept in the handler. If users want to terminate all transfer slots, just call SAI_TransferTerminateSendEDMA.
| base | SAI base pointer. |
| handle | SAI eDMA handle pointer. |
| void SAI_TransferAbortReceiveEDMA | ( | I2S_Type * | base, |
| sai_edma_handle_t * | handle | ||
| ) |
This function only aborts the current transfer slots, the other transfer slots' information still kept in the handler. If users want to terminate all transfer slots, just call SAI_TransferTerminateReceiveEDMA.
| base | SAI base pointer |
| handle | SAI eDMA handle pointer. |
| status_t SAI_TransferGetSendCountEDMA | ( | I2S_Type * | base, |
| sai_edma_handle_t * | handle, | ||
| size_t * | count | ||
| ) |
| base | SAI base pointer. |
| handle | SAI eDMA handle pointer. |
| count | Bytes count sent by SAI. |
| kStatus_Success | Succeed get the transfer count. |
| kStatus_NoTransferInProgress | There is no non-blocking transaction in progress. |
| status_t SAI_TransferGetReceiveCountEDMA | ( | I2S_Type * | base, |
| sai_edma_handle_t * | handle, | ||
| size_t * | count | ||
| ) |
| base | SAI base pointer |
| handle | SAI eDMA handle pointer. |
| count | Bytes count received by SAI. |
| kStatus_Success | Succeed get the transfer count. |
| kStatus_NoTransferInProgress | There is no non-blocking transaction in progress. |