|
| enum | lin_lpuart_stop_bit_count_t {
kLPUART_OneStopBit = 0U,
kLPUART_TwoStopBit = 1U
} |
| |
| enum | _lin_lpuart_flags {
kLPUART_TxDataRegEmptyFlag = (LPUART_STAT_TDRE_MASK),
kLPUART_TransmissionCompleteFlag = (LPUART_STAT_TC_MASK),
kLPUART_RxDataRegFullFlag = (LPUART_STAT_RDRF_MASK),
kLPUART_IdleLineFlag = (LPUART_STAT_IDLE_MASK),
kLPUART_RxOverrunFlag = (LPUART_STAT_OR_MASK),
kLPUART_NoiseErrorFlag = (LPUART_STAT_NF_MASK),
kLPUART_FramingErrorFlag = (LPUART_STAT_FE_MASK),
kLPUART_ParityErrorFlag = (LPUART_STAT_PF_MASK),
kLPUART_LinBreakFlag = (LPUART_STAT_LBKDIF_MASK),
kLPUART_RxActiveEdgeFlag = (LPUART_STAT_RXEDGIF_MASK),
kLPUART_RxActiveFlag = (LPUART_STAT_RAF_MASK),
kLPUART_DataMatch1Flag = LPUART_STAT_MA1F_MASK,
kLPUART_DataMatch2Flag = LPUART_STAT_MA2F_MASK,
kLPUART_NoiseErrorInRxDataRegFlag = (LPUART_DATA_NOISY_MASK >> 10),
kLPUART_ParityErrorInRxDataRegFlag = (LPUART_DATA_PARITYE_MASK >> 10)
} |
| |
| enum | _lin_lpuart_interrupt_enable {
kLPUART_LinBreakInterruptEnable = (LPUART_BAUD_LBKDIE_MASK >> 8),
kLPUART_RxActiveEdgeInterruptEnable = (LPUART_BAUD_RXEDGIE_MASK >> 8),
kLPUART_TxDataRegEmptyInterruptEnable = (LPUART_CTRL_TIE_MASK),
kLPUART_TransmissionCompleteInterruptEnable = (LPUART_CTRL_TCIE_MASK),
kLPUART_RxDataRegFullInterruptEnable = (LPUART_CTRL_RIE_MASK),
kLPUART_IdleLineInterruptEnable = (LPUART_CTRL_ILIE_MASK),
kLPUART_RxOverrunInterruptEnable = (LPUART_CTRL_ORIE_MASK),
kLPUART_NoiseErrorInterruptEnable = (LPUART_CTRL_NEIE_MASK),
kLPUART_FramingErrorInterruptEnable = (LPUART_CTRL_FEIE_MASK),
kLPUART_ParityErrorInterruptEnable = (LPUART_CTRL_PEIE_MASK)
} |
| |
| enum | _lin_lpuart_status {
kStatus_LPUART_TxBusy = MAKE_STATUS(kStatusGroup_LPUART, 0),
kStatus_LPUART_RxBusy = MAKE_STATUS(kStatusGroup_LPUART, 1),
kStatus_LPUART_TxIdle = MAKE_STATUS(kStatusGroup_LPUART, 2),
kStatus_LPUART_RxIdle = MAKE_STATUS(kStatusGroup_LPUART, 3),
kStatus_LPUART_TxWatermarkTooLarge = MAKE_STATUS(kStatusGroup_LPUART, 4),
kStatus_LPUART_RxWatermarkTooLarge = MAKE_STATUS(kStatusGroup_LPUART, 5),
kStatus_LPUART_FlagCannotClearManually,
kStatus_LPUART_Error = MAKE_STATUS(kStatusGroup_LPUART, 7),
kStatus_LPUART_RxRingBufferOverrun,
kStatus_LPUART_RxHardwareOverrun = MAKE_STATUS(kStatusGroup_LPUART, 9),
kStatus_LPUART_NoiseError = MAKE_STATUS(kStatusGroup_LPUART, 10),
kStatus_LPUART_FramingError = MAKE_STATUS(kStatusGroup_LPUART, 11),
kStatus_LPUART_ParityError = MAKE_STATUS(kStatusGroup_LPUART, 12)
} |
| |
| enum | lin_lpuart_bit_count_per_char_t {
LPUART_8_BITS_PER_CHAR = 0x0U,
LPUART_9_BITS_PER_CHAR = 0x1U,
LPUART_10_BITS_PER_CHAR = 0x2U
} |
| |
|
| static bool | LIN_LPUART_GetRxDataPolarity (const LPUART_Type *base) |
| | Initializes an LIN_LPUART instance for LIN Network. More...
|
| |
| lin_status_t | LIN_LPUART_Deinit (LPUART_Type *base) |
| | Shuts down the LIN_LPUART by disabling interrupts and transmitter/receiver. More...
|
| |
| lin_status_t | LIN_LPUART_SendFrameDataBlocking (LPUART_Type *base, const uint8_t *txBuff, uint8_t txSize, uint32_t timeoutMSec) |
| | Sends Frame data out through the LIN_LPUART module using blocking method. More...
|
| |
| lin_status_t | LIN_LPUART_SendFrameData (LPUART_Type *base, const uint8_t *txBuff, uint8_t txSize) |
| | Sends frame data out through the LIN_LPUART module using non-blocking method. More...
|
| |
| lin_status_t | LIN_LPUART_GetTransmitStatus (LPUART_Type *base, uint8_t *bytesRemaining) |
| | Get status of an on-going non-blocking transmission While sending frame data using non-blocking method, users can use this function to get status of that transmission. More...
|
| |
| lin_status_t | LIN_LPUART_RecvFrmDataBlocking (LPUART_Type *base, uint8_t *rxBuff, uint8_t rxSize, uint32_t timeoutMSec) |
| | Receives frame data through the LIN_LPUART module using blocking method. More...
|
| |
| lin_status_t | LIN_LPUART_RecvFrmData (LPUART_Type *base, uint8_t *rxBuff, uint8_t rxSize) |
| | Receives frame data through the LIN_LPUART module using non- blocking method. More...
|
| |
| lin_status_t | LIN_LPUART_AbortTransferData (LPUART_Type *base) |
| | Aborts an on-going non-blocking transmission/reception. More...
|
| |
| lin_status_t | LIN_LPUART_GetReceiveStatus (LPUART_Type *base, uint8_t *bytesRemaining) |
| | Get status of an on-going non-blocking reception While receiving frame data using non-blocking method, users can use this function to get status of that receiving. More...
|
| |
| lin_status_t | LIN_LPUART_GoToSleepMode (LPUART_Type *base) |
| | This function puts current node to sleep mode This function changes current node state to LIN_NODE_STATE_SLEEP_MODE. More...
|
| |
| lin_status_t | LIN_LPUART_GotoIdleState (LPUART_Type *base) |
| | Puts current LIN node to Idle state This function changes current node state to LIN_NODE_STATE_IDLE. More...
|
| |
| lin_status_t | LIN_LPUART_SendWakeupSignal (LPUART_Type *base) |
| | Sends a wakeup signal through the LIN_LPUART interface. More...
|
| |
| lin_status_t | LIN_LPUART_MasterSendHeader (LPUART_Type *base, uint8_t id) |
| | Sends frame header out through the LIN_LPUART module using a non-blocking method. More...
|
| |
| lin_status_t | LIN_LPUART_EnableIRQ (LPUART_Type *base) |
| | Enables LIN_LPUART hardware interrupts. More...
|
| |
| lin_status_t | LIN_LPUART_DisableIRQ (LPUART_Type *base) |
| | Disables LIN_LPUART hardware interrupts. More...
|
| |
| lin_status_t | LIN_LPUART_AutoBaudCapture (uint32_t instance) |
| | This function capture bits time to detect break char, calculate baudrate from sync bits and enable transceiver if autobaud successful. More...
|
| |
| void | LIN_LPUART_IRQHandler (LPUART_Type *base) |
| | LIN_LPUART RX TX interrupt handler. More...
|
| |
| static bool LIN_LPUART_GetRxDataPolarity |
( |
const LPUART_Type * |
base | ) |
|
|
inlinestatic |
The caller provides memory for the driver state structures during initialization. The user must select the LIN_LPUART clock source in the application to initialize the LIN_LPUART. This function initializes a LPUART instance for operation. This function will initialize the run-time state structure to keep track of the on-going transfers, initialize the module to user defined settings and default settings, set break field length to be 13 bit times minimum, enable the break detect interrupt, Rx complete interrupt, frame error detect interrupt, and enable the LPUART module transmitter and receiver
- Parameters
-
| instance | LIN_LPUART instance number |
| linUserConfig | user configuration structure of type lin_user_config_t |
| linCurrentState | pointer to the LIN_LPUART driver state structure |
- Returns
- An error code or lin_status_t