MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages

Overview

ECSPI driver includes functional APIs and transactional APIs.

Functional APIs are feature/property target low level APIs. Functional APIs can be used for ECSPI initialization/configuration/operation for optimization/customization purpose. Using the functional API requires the knowledge of the SPI peripheral and how to organize functional APIs to meet the application requirements. All functional API use the peripheral base address as the first parameter. ECSPI functional operation groups provide the functional API set.

Transactional APIs are transaction target high level APIs. Transactional APIs can be used to enable the peripheral and in the application if the code size and performance of transactional APIs satisfy the requirements. If the code size and performance are a critical requirement, see the transactional API implementation and write a custom code. All transactional APIs use the spi_handle_t as the first parameter. Initialize the handle by calling the SPI_MasterTransferCreateHandle() or SPI_SlaveTransferCreateHandle() API.

Transactional APIs support asynchronous transfer. This means that the functions SPI_MasterTransferNonBlocking() and SPI_SlaveTransferNonBlocking() set up the interrupt for data transfer. When the transfer completes, the upper layer is notified through a callback function with the kStatus_SPI_Idle status.

Typical use case

SPI master transfer using polling method

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/ecspi

SPI master transfer using an interrupt method

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/ecspi

Data Structures

struct  ecspi_channel_config_t
 ECSPI user channel configure structure. More...
 
struct  ecspi_master_config_t
 ECSPI master configure structure. More...
 
struct  ecspi_slave_config_t
 ECSPI slave configure structure. More...
 
struct  ecspi_transfer_t
 ECSPI transfer structure. More...
 
struct  ecspi_master_handle_t
 ECSPI master handle structure. More...
 

Macros

#define ECSPI_DUMMYDATA   (0xFFFFFFFFU)
 ECSPI dummy transfer data, the data is sent while txBuff is NULL. More...
 
#define SPI_RETRY_TIMES   0U /* Define to zero means keep waiting until the flag is assert/deassert. */
 Retry times for waiting flag. More...
 

Typedefs

typedef ecspi_master_handle_t ecspi_slave_handle_t
 Slave handle is the same with master handle.
 
typedef void(* ecspi_master_callback_t )(ECSPI_Type *base, ecspi_master_handle_t *handle, status_t status, void *userData)
 ECSPI master callback for finished transmit.
 
typedef void(* ecspi_slave_callback_t )(ECSPI_Type *base, ecspi_slave_handle_t *handle, status_t status, void *userData)
 ECSPI slave callback for finished transmit.
 

Enumerations

enum  {
  kStatus_ECSPI_Busy = MAKE_STATUS(kStatusGroup_ECSPI, 0),
  kStatus_ECSPI_Idle = MAKE_STATUS(kStatusGroup_ECSPI, 1),
  kStatus_ECSPI_Error = MAKE_STATUS(kStatusGroup_ECSPI, 2),
  kStatus_ECSPI_HardwareOverFlow = MAKE_STATUS(kStatusGroup_ECSPI, 3),
  kStatus_ECSPI_Timeout = MAKE_STATUS(kStatusGroup_ECSPI, 4)
}
 Return status for the ECSPI driver. More...
 
enum  ecspi_clock_polarity_t {
  kECSPI_PolarityActiveHigh = 0x0U,
  kECSPI_PolarityActiveLow
}
 ECSPI clock polarity configuration. More...
 
enum  ecspi_clock_phase_t {
  kECSPI_ClockPhaseFirstEdge,
  kECSPI_ClockPhaseSecondEdge
}
 ECSPI clock phase configuration. More...
 
enum  {
  kECSPI_TxfifoEmptyInterruptEnable = ECSPI_INTREG_TEEN_MASK,
  kECSPI_TxFifoDataRequstInterruptEnable = ECSPI_INTREG_TDREN_MASK,
  kECSPI_TxFifoFullInterruptEnable = ECSPI_INTREG_TFEN_MASK,
  kECSPI_RxFifoReadyInterruptEnable = ECSPI_INTREG_RREN_MASK,
  kECSPI_RxFifoDataRequstInterruptEnable = ECSPI_INTREG_RDREN_MASK,
  kECSPI_RxFifoFullInterruptEnable = ECSPI_INTREG_RFEN_MASK,
  kECSPI_RxFifoOverFlowInterruptEnable = ECSPI_INTREG_ROEN_MASK,
  kECSPI_TransferCompleteInterruptEnable = ECSPI_INTREG_TCEN_MASK,
  kECSPI_AllInterruptEnable
}
 ECSPI interrupt sources. More...
 
enum  {
  kECSPI_TxfifoEmptyFlag = ECSPI_STATREG_TE_MASK,
  kECSPI_TxFifoDataRequstFlag = ECSPI_STATREG_TDR_MASK,
  kECSPI_TxFifoFullFlag = ECSPI_STATREG_TF_MASK,
  kECSPI_RxFifoReadyFlag = ECSPI_STATREG_RR_MASK,
  kECSPI_RxFifoDataRequstFlag = ECSPI_STATREG_RDR_MASK,
  kECSPI_RxFifoFullFlag = ECSPI_STATREG_RF_MASK,
  kECSPI_RxFifoOverFlowFlag = ECSPI_STATREG_RO_MASK,
  kECSPI_TransferCompleteFlag = ECSPI_STATREG_TC_MASK
}
 ECSPI status flags. More...
 
enum  {
  kECSPI_TxDmaEnable = ECSPI_DMAREG_TEDEN_MASK,
  kECSPI_RxDmaEnable = ECSPI_DMAREG_RXDEN_MASK,
  kECSPI_DmaAllEnable = (ECSPI_DMAREG_TEDEN_MASK | ECSPI_DMAREG_RXDEN_MASK)
}
 ECSPI DMA enable. More...
 
enum  ecspi_Data_ready_t {
  kECSPI_DataReadyIgnore = 0x0U,
  kECSPI_DataReadyFallingEdge,
  kECSPI_DataReadyLowLevel
}
 ECSPI SPI_RDY signal configuration. More...
 
enum  ecspi_channel_source_t {
  kECSPI_Channel0 = 0x0U,
  kECSPI_Channel1,
  kECSPI_Channel2,
  kECSPI_Channel3
}
 ECSPI channel select source. More...
 
enum  ecspi_master_slave_mode_t {
  kECSPI_Slave = 0U,
  kECSPI_Master
}
 ECSPI master or slave mode configuration. More...
 
enum  ecspi_data_line_inactive_state_t {
  kECSPI_DataLineInactiveStateHigh = 0x0U,
  kECSPI_DataLineInactiveStateLow
}
 ECSPI data line inactive state configuration. More...
 
enum  ecspi_clock_inactive_state_t {
  kECSPI_ClockInactiveStateLow = 0x0U,
  kECSPI_ClockInactiveStateHigh
}
 ECSPI clock inactive state configuration. More...
 
enum  ecspi_chip_select_active_state_t {
  kECSPI_ChipSelectActiveStateLow = 0x0U,
  kECSPI_ChipSelectActiveStateHigh
}
 ECSPI active state configuration. More...
 
enum  ecspi_sample_period_clock_source_t {
  kECSPI_spiClock = 0x0U,
  kECSPI_lowFreqClock
}
 ECSPI sample period clock configuration. More...
 

Functions

uint32_t ECSPI_GetInstance (ECSPI_Type *base)
 Get the instance for ECSPI module. More...
 

Driver version

#define FSL_ECSPI_DRIVER_VERSION   (MAKE_VERSION(2, 2, 0))
 ECSPI driver version. More...
 

Initialization and deinitialization

void ECSPI_MasterGetDefaultConfig (ecspi_master_config_t *config)
 Sets the ECSPI configuration structure to default values. More...
 
void ECSPI_MasterInit (ECSPI_Type *base, const ecspi_master_config_t *config, uint32_t srcClock_Hz)
 Initializes the ECSPI with configuration. More...
 
void ECSPI_SlaveGetDefaultConfig (ecspi_slave_config_t *config)
 Sets the ECSPI configuration structure to default values. More...
 
void ECSPI_SlaveInit (ECSPI_Type *base, const ecspi_slave_config_t *config)
 Initializes the ECSPI with configuration. More...
 
void ECSPI_Deinit (ECSPI_Type *base)
 De-initializes the ECSPI. More...
 
static void ECSPI_Enable (ECSPI_Type *base, bool enable)
 Enables or disables the ECSPI. More...
 

Status

static uint32_t ECSPI_GetStatusFlags (ECSPI_Type *base)
 Gets the status flag. More...
 
static void ECSPI_ClearStatusFlags (ECSPI_Type *base, uint32_t mask)
 Clear the status flag. More...
 

Interrupts

static void ECSPI_EnableInterrupts (ECSPI_Type *base, uint32_t mask)
 Enables the interrupt for the ECSPI. More...
 
static void ECSPI_DisableInterrupts (ECSPI_Type *base, uint32_t mask)
 Disables the interrupt for the ECSPI. More...
 

Software Reset

static void ECSPI_SoftwareReset (ECSPI_Type *base)
 Software reset. More...
 

Channel mode check

static bool ECSPI_IsMaster (ECSPI_Type *base, ecspi_channel_source_t channel)
 Mode check. More...
 

DMA Control

static void ECSPI_EnableDMA (ECSPI_Type *base, uint32_t mask, bool enable)
 Enables the DMA source for ECSPI. More...
 

FIFO Operation

static uint8_t ECSPI_GetTxFifoCount (ECSPI_Type *base)
 Get the Tx FIFO data count. More...
 
static uint8_t ECSPI_GetRxFifoCount (ECSPI_Type *base)
 Get the Rx FIFO data count. More...
 

Bus Operations

static void ECSPI_SetChannelSelect (ECSPI_Type *base, ecspi_channel_source_t channel)
 Set channel select for transfer. More...
 
void ECSPI_SetChannelConfig (ECSPI_Type *base, ecspi_channel_source_t channel, const ecspi_channel_config_t *config)
 Set channel select configuration for transfer. More...
 
void ECSPI_SetBaudRate (ECSPI_Type *base, uint32_t baudRate_Bps, uint32_t srcClock_Hz)
 Sets the baud rate for ECSPI transfer. More...
 
status_t ECSPI_WriteBlocking (ECSPI_Type *base, uint32_t *buffer, size_t size)
 Sends a buffer of data bytes using a blocking method. More...
 
static void ECSPI_WriteData (ECSPI_Type *base, uint32_t data)
 Writes a data into the ECSPI data register. More...
 
static uint32_t ECSPI_ReadData (ECSPI_Type *base)
 Gets a data from the ECSPI data register. More...
 

Transactional

void ECSPI_MasterTransferCreateHandle (ECSPI_Type *base, ecspi_master_handle_t *handle, ecspi_master_callback_t callback, void *userData)
 Initializes the ECSPI master handle. More...
 
status_t ECSPI_MasterTransferBlocking (ECSPI_Type *base, ecspi_transfer_t *xfer)
 Transfers a block of data using a polling method. More...
 
status_t ECSPI_MasterTransferNonBlocking (ECSPI_Type *base, ecspi_master_handle_t *handle, ecspi_transfer_t *xfer)
 Performs a non-blocking ECSPI interrupt transfer. More...
 
status_t ECSPI_MasterTransferGetCount (ECSPI_Type *base, ecspi_master_handle_t *handle, size_t *count)
 Gets the bytes of the ECSPI interrupt transferred. More...
 
void ECSPI_MasterTransferAbort (ECSPI_Type *base, ecspi_master_handle_t *handle)
 Aborts an ECSPI transfer using interrupt. More...
 
void ECSPI_MasterTransferHandleIRQ (ECSPI_Type *base, ecspi_master_handle_t *handle)
 Interrupts the handler for the ECSPI. More...
 
void ECSPI_SlaveTransferCreateHandle (ECSPI_Type *base, ecspi_slave_handle_t *handle, ecspi_slave_callback_t callback, void *userData)
 Initializes the ECSPI slave handle. More...
 
static status_t ECSPI_SlaveTransferNonBlocking (ECSPI_Type *base, ecspi_slave_handle_t *handle, ecspi_transfer_t *xfer)
 Performs a non-blocking ECSPI slave interrupt transfer. More...
 
static status_t ECSPI_SlaveTransferGetCount (ECSPI_Type *base, ecspi_slave_handle_t *handle, size_t *count)
 Gets the bytes of the ECSPI interrupt transferred. More...
 
static void ECSPI_SlaveTransferAbort (ECSPI_Type *base, ecspi_slave_handle_t *handle)
 Aborts an ECSPI slave transfer using interrupt. More...
 
void ECSPI_SlaveTransferHandleIRQ (ECSPI_Type *base, ecspi_slave_handle_t *handle)
 Interrupts a handler for the ECSPI slave. More...
 

Data Structure Documentation

struct ecspi_channel_config_t

Data Fields

ecspi_master_slave_mode_t channelMode
 Channel mode.
 
ecspi_clock_inactive_state_t clockInactiveState
 Clock line (SCLK) inactive state.
 
ecspi_data_line_inactive_state_t dataLineInactiveState
 Data line (MOSI&MISO) inactive state.
 
ecspi_chip_select_active_state_t chipSlectActiveState
 Chip select(SS) line active state.
 
ecspi_clock_polarity_t polarity
 Clock polarity.
 
ecspi_clock_phase_t phase
 Clock phase.
 
struct ecspi_master_config_t

Data Fields

ecspi_channel_source_t channel
 Channel number.
 
ecspi_channel_config_t channelConfig
 Channel configuration.
 
ecspi_sample_period_clock_source_t samplePeriodClock
 Sample period clock source.
 
uint8_t burstLength
 Burst length.
 
uint8_t chipSelectDelay
 SS delay time.
 
uint16_t samplePeriod
 Sample period.
 
uint8_t txFifoThreshold
 TX Threshold.
 
uint8_t rxFifoThreshold
 RX Threshold.
 
uint32_t baudRate_Bps
 ECSPI baud rate for master mode.
 
bool enableLoopback
 Enable the ECSPI loopback test. More...
 

Field Documentation

bool ecspi_master_config_t::enableLoopback
struct ecspi_slave_config_t

Data Fields

uint8_t burstLength
 Burst length.
 
uint8_t txFifoThreshold
 TX Threshold.
 
uint8_t rxFifoThreshold
 RX Threshold.
 
ecspi_channel_config_t channelConfig
 Channel configuration.
 
struct ecspi_transfer_t

Data Fields

uint32_t * txData
 Send buffer.
 
uint32_t * rxData
 Receive buffer.
 
size_t dataSize
 Transfer bytes.
 
ecspi_channel_source_t channel
 ECSPI channel select.
 
struct _ecspi_master_handle

Data Fields

ecspi_channel_source_t channel
 Channel number.
 
uint32_t *volatile txData
 Transfer buffer.
 
uint32_t *volatile rxData
 Receive buffer.
 
volatile size_t txRemainingBytes
 Send data remaining in bytes.
 
volatile size_t rxRemainingBytes
 Receive data remaining in bytes.
 
volatile uint32_t state
 ECSPI internal state.
 
size_t transferSize
 Bytes to be transferred.
 
ecspi_master_callback_t callback
 ECSPI callback.
 
void * userData
 Callback parameter.
 

Macro Definition Documentation

#define FSL_ECSPI_DRIVER_VERSION   (MAKE_VERSION(2, 2, 0))
#define ECSPI_DUMMYDATA   (0xFFFFFFFFU)
#define SPI_RETRY_TIMES   0U /* Define to zero means keep waiting until the flag is assert/deassert. */

Enumeration Type Documentation

anonymous enum
Enumerator
kStatus_ECSPI_Busy 

ECSPI bus is busy.

kStatus_ECSPI_Idle 

ECSPI is idle.

kStatus_ECSPI_Error 

ECSPI error.

kStatus_ECSPI_HardwareOverFlow 

ECSPI hardware overflow.

kStatus_ECSPI_Timeout 

ECSPI timeout polling status flags.

Enumerator
kECSPI_PolarityActiveHigh 

Active-high ECSPI polarity high (idles low).

kECSPI_PolarityActiveLow 

Active-low ECSPI polarity low (idles high).

Enumerator
kECSPI_ClockPhaseFirstEdge 

First edge on SPSCK occurs at the middle of the first cycle of a data transfer.

kECSPI_ClockPhaseSecondEdge 

First edge on SPSCK occurs at the start of the first cycle of a data transfer.

anonymous enum
Enumerator
kECSPI_TxfifoEmptyInterruptEnable 

Transmit FIFO buffer empty interrupt.

kECSPI_TxFifoDataRequstInterruptEnable 

Transmit FIFO data requst interrupt.

kECSPI_TxFifoFullInterruptEnable 

Transmit FIFO full interrupt.

kECSPI_RxFifoReadyInterruptEnable 

Receiver FIFO ready interrupt.

kECSPI_RxFifoDataRequstInterruptEnable 

Receiver FIFO data requst interrupt.

kECSPI_RxFifoFullInterruptEnable 

Receiver FIFO full interrupt.

kECSPI_RxFifoOverFlowInterruptEnable 

Receiver FIFO buffer overflow interrupt.

kECSPI_TransferCompleteInterruptEnable 

Transfer complete interrupt.

kECSPI_AllInterruptEnable 

All interrupt.

anonymous enum
Enumerator
kECSPI_TxfifoEmptyFlag 

Transmit FIFO buffer empty flag.

kECSPI_TxFifoDataRequstFlag 

Transmit FIFO data requst flag.

kECSPI_TxFifoFullFlag 

Transmit FIFO full flag.

kECSPI_RxFifoReadyFlag 

Receiver FIFO ready flag.

kECSPI_RxFifoDataRequstFlag 

Receiver FIFO data requst flag.

kECSPI_RxFifoFullFlag 

Receiver FIFO full flag.

kECSPI_RxFifoOverFlowFlag 

Receiver FIFO buffer overflow flag.

kECSPI_TransferCompleteFlag 

Transfer complete flag.

anonymous enum
Enumerator
kECSPI_TxDmaEnable 

Tx DMA request source.

kECSPI_RxDmaEnable 

Rx DMA request source.

kECSPI_DmaAllEnable 

All DMA request source.

Enumerator
kECSPI_DataReadyIgnore 

SPI_RDY signal is ignored.

kECSPI_DataReadyFallingEdge 

SPI_RDY signal will be triggerd by the falling edge.

kECSPI_DataReadyLowLevel 

SPI_RDY signal will be triggerd by a low level.

Enumerator
kECSPI_Channel0 

Channel 0 is selectd.

kECSPI_Channel1 

Channel 1 is selectd.

kECSPI_Channel2 

Channel 2 is selectd.

kECSPI_Channel3 

Channel 3 is selectd.

Enumerator
kECSPI_Slave 

ECSPI peripheral operates in slave mode.

kECSPI_Master 

ECSPI peripheral operates in master mode.

Enumerator
kECSPI_DataLineInactiveStateHigh 

The data line inactive state stays high.

kECSPI_DataLineInactiveStateLow 

The data line inactive state stays low.

Enumerator
kECSPI_ClockInactiveStateLow 

The SCLK inactive state stays low.

kECSPI_ClockInactiveStateHigh 

The SCLK inactive state stays high.

Enumerator
kECSPI_ChipSelectActiveStateLow 

The SS signal line active stays low.

kECSPI_ChipSelectActiveStateHigh 

The SS signal line active stays high.

Enumerator
kECSPI_spiClock 

The sample period clock source is SCLK.

kECSPI_lowFreqClock 

The sample seriod clock source is low_frequency reference clock(32.768 kHz).

Function Documentation

uint32_t ECSPI_GetInstance ( ECSPI_Type *  base)
Parameters
baseECSPI base address
void ECSPI_MasterGetDefaultConfig ( ecspi_master_config_t *  config)

The purpose of this API is to get the configuration structure initialized for use in ECSPI_MasterInit(). User may use the initialized structure unchanged in ECSPI_MasterInit, or modify some fields of the structure before calling ECSPI_MasterInit. After calling this API, the master is ready to transfer. Example:

Parameters
configpointer to config structure
void ECSPI_MasterInit ( ECSPI_Type *  base,
const ecspi_master_config_t *  config,
uint32_t  srcClock_Hz 
)

The configuration structure can be filled by user from scratch, or be set with default values by ECSPI_MasterGetDefaultConfig(). After calling this API, the slave is ready to transfer. Example

.baudRate_Bps = 400000,
...
};
ECSPI_MasterInit(ECSPI0, &config);
Parameters
baseECSPI base pointer
configpointer to master configuration structure
srcClock_HzSource clock frequency.
void ECSPI_SlaveGetDefaultConfig ( ecspi_slave_config_t *  config)

The purpose of this API is to get the configuration structure initialized for use in ECSPI_SlaveInit(). User may use the initialized structure unchanged in ECSPI_SlaveInit(), or modify some fields of the structure before calling ECSPI_SlaveInit(). After calling this API, the master is ready to transfer. Example:

ecspi_Slaveconfig_t config;
Parameters
configpointer to config structure
void ECSPI_SlaveInit ( ECSPI_Type *  base,
const ecspi_slave_config_t *  config 
)

The configuration structure can be filled by user from scratch, or be set with default values by ECSPI_SlaveGetDefaultConfig(). After calling this API, the slave is ready to transfer. Example

ecspi_Salveconfig_t config = {
.baudRate_Bps = 400000,
...
};
ECSPI_SlaveInit(ECSPI1, &config);
Parameters
baseECSPI base pointer
configpointer to master configuration structure
void ECSPI_Deinit ( ECSPI_Type *  base)

Calling this API resets the ECSPI module, gates the ECSPI clock. The ECSPI module can't work unless calling the ECSPI_MasterInit/ECSPI_SlaveInit to initialize module.

Parameters
baseECSPI base pointer
static void ECSPI_Enable ( ECSPI_Type *  base,
bool  enable 
)
inlinestatic
Parameters
baseECSPI base pointer
enablepass true to enable module, false to disable module
static uint32_t ECSPI_GetStatusFlags ( ECSPI_Type *  base)
inlinestatic
Parameters
baseECSPI base pointer
Returns
ECSPI Status, use status flag to AND _ecspi_flags could get the related status.
static void ECSPI_ClearStatusFlags ( ECSPI_Type *  base,
uint32_t  mask 
)
inlinestatic
Parameters
baseECSPI base pointer
maskECSPI Status, use status flag to AND _ecspi_flags could get the related status.
static void ECSPI_EnableInterrupts ( ECSPI_Type *  base,
uint32_t  mask 
)
inlinestatic
Parameters
baseECSPI base pointer
maskECSPI interrupt source. The parameter can be any combination of the following values:
  • kECSPI_TxfifoEmptyInterruptEnable
  • kECSPI_TxFifoDataRequstInterruptEnable
  • kECSPI_TxFifoFullInterruptEnable
  • kECSPI_RxFifoReadyInterruptEnable
  • kECSPI_RxFifoDataRequstInterruptEnable
  • kECSPI_RxFifoFullInterruptEnable
  • kECSPI_RxFifoOverFlowInterruptEnable
  • kECSPI_TransferCompleteInterruptEnable
  • kECSPI_AllInterruptEnable
static void ECSPI_DisableInterrupts ( ECSPI_Type *  base,
uint32_t  mask 
)
inlinestatic
Parameters
baseECSPI base pointer
maskECSPI interrupt source. The parameter can be any combination of the following values:
  • kECSPI_TxfifoEmptyInterruptEnable
  • kECSPI_TxFifoDataRequstInterruptEnable
  • kECSPI_TxFifoFullInterruptEnable
  • kECSPI_RxFifoReadyInterruptEnable
  • kECSPI_RxFifoDataRequstInterruptEnable
  • kECSPI_RxFifoFullInterruptEnable
  • kECSPI_RxFifoOverFlowInterruptEnable
  • kECSPI_TransferCompleteInterruptEnable
  • kECSPI_AllInterruptEnable
static void ECSPI_SoftwareReset ( ECSPI_Type *  base)
inlinestatic
Parameters
baseECSPI base pointer
static bool ECSPI_IsMaster ( ECSPI_Type *  base,
ecspi_channel_source_t  channel 
)
inlinestatic
Parameters
baseECSPI base pointer
channelECSPI channel source
Returns
mode of channel
static void ECSPI_EnableDMA ( ECSPI_Type *  base,
uint32_t  mask,
bool  enable 
)
inlinestatic
Parameters
baseECSPI base pointer
maskECSPI DMA source. The parameter can be any of the following values:
  • kECSPI_TxDmaEnable
  • kECSPI_RxDmaEnable
  • kECSPI_DmaAllEnable
enableTrue means enable DMA, false means disable DMA
static uint8_t ECSPI_GetTxFifoCount ( ECSPI_Type *  base)
inlinestatic
Parameters
baseECSPI base pointer.
Returns
the number of words in Tx FIFO buffer.
static uint8_t ECSPI_GetRxFifoCount ( ECSPI_Type *  base)
inlinestatic
Parameters
baseECSPI base pointer.
Returns
the number of words in Rx FIFO buffer.
static void ECSPI_SetChannelSelect ( ECSPI_Type *  base,
ecspi_channel_source_t  channel 
)
inlinestatic
Parameters
baseECSPI base pointer
channelChannel source.
void ECSPI_SetChannelConfig ( ECSPI_Type *  base,
ecspi_channel_source_t  channel,
const ecspi_channel_config_t *  config 
)

The purpose of this API is to set the channel will be use to transfer. User may use this API after instance has been initialized or before transfer start. The configuration structure ecspi_channel_config can be filled by user from scratch. After calling this API, user can select this channel as transfer channel.

Parameters
baseECSPI base pointer
channelChannel source.
configConfiguration struct of channel
void ECSPI_SetBaudRate ( ECSPI_Type *  base,
uint32_t  baudRate_Bps,
uint32_t  srcClock_Hz 
)

This is only used in master.

Parameters
baseECSPI base pointer
baudRate_Bpsbaud rate needed in Hz.
srcClock_HzECSPI source clock frequency in Hz.
status_t ECSPI_WriteBlocking ( ECSPI_Type *  base,
uint32_t *  buffer,
size_t  size 
)
Note
This function blocks via polling until all bytes have been sent.
Parameters
baseECSPI base pointer
bufferThe data bytes to send
sizeThe number of data bytes to send
Return values
kStatus_SuccessSuccessfully start a transfer.
kStatus_ECSPI_TimeoutThe transfer timed out and was aborted.
static void ECSPI_WriteData ( ECSPI_Type *  base,
uint32_t  data 
)
inlinestatic
Parameters
baseECSPI base pointer
dataData needs to be write.
static uint32_t ECSPI_ReadData ( ECSPI_Type *  base)
inlinestatic
Parameters
baseECSPI base pointer
Returns
Data in the register.
void ECSPI_MasterTransferCreateHandle ( ECSPI_Type *  base,
ecspi_master_handle_t *  handle,
ecspi_master_callback_t  callback,
void *  userData 
)

This function initializes the ECSPI master handle which can be used for other ECSPI master transactional APIs. Usually, for a specified ECSPI instance, call this API once to get the initialized handle.

Parameters
baseECSPI peripheral base address.
handleECSPI handle pointer.
callbackCallback function.
userDataUser data.
status_t ECSPI_MasterTransferBlocking ( ECSPI_Type *  base,
ecspi_transfer_t *  xfer 
)
Parameters
baseSPI base pointer
xferpointer to spi_xfer_config_t structure
Return values
kStatus_SuccessSuccessfully start a transfer.
kStatus_InvalidArgumentInput argument is invalid.
kStatus_ECSPI_TimeoutThe transfer timed out and was aborted.
status_t ECSPI_MasterTransferNonBlocking ( ECSPI_Type *  base,
ecspi_master_handle_t *  handle,
ecspi_transfer_t *  xfer 
)
Note
The API immediately returns after transfer initialization is finished.
If ECSPI transfer data frame size is 16 bits, the transfer size cannot be an odd number.
Parameters
baseECSPI peripheral base address.
handlepointer to ecspi_master_handle_t structure which stores the transfer state
xferpointer to ecspi_transfer_t structure
Return values
kStatus_SuccessSuccessfully start a transfer.
kStatus_InvalidArgumentInput argument is invalid.
kStatus_ECSPI_BusyECSPI is not idle, is running another transfer.
status_t ECSPI_MasterTransferGetCount ( ECSPI_Type *  base,
ecspi_master_handle_t *  handle,
size_t *  count 
)
Parameters
baseECSPI peripheral base address.
handlePointer to ECSPI transfer handle, this should be a static variable.
countTransferred bytes of ECSPI master.
Return values
kStatus_ECSPI_SuccessSucceed get the transfer count.
kStatus_NoTransferInProgressThere is not a non-blocking transaction currently in progress.
void ECSPI_MasterTransferAbort ( ECSPI_Type *  base,
ecspi_master_handle_t *  handle 
)
Parameters
baseECSPI peripheral base address.
handlePointer to ECSPI transfer handle, this should be a static variable.
void ECSPI_MasterTransferHandleIRQ ( ECSPI_Type *  base,
ecspi_master_handle_t *  handle 
)
Parameters
baseECSPI peripheral base address.
handlepointer to ecspi_master_handle_t structure which stores the transfer state.
void ECSPI_SlaveTransferCreateHandle ( ECSPI_Type *  base,
ecspi_slave_handle_t *  handle,
ecspi_slave_callback_t  callback,
void *  userData 
)

This function initializes the ECSPI slave handle which can be used for other ECSPI slave transactional APIs. Usually, for a specified ECSPI instance, call this API once to get the initialized handle.

Parameters
baseECSPI peripheral base address.
handleECSPI handle pointer.
callbackCallback function.
userDataUser data.
static status_t ECSPI_SlaveTransferNonBlocking ( ECSPI_Type *  base,
ecspi_slave_handle_t *  handle,
ecspi_transfer_t *  xfer 
)
inlinestatic
Note
The API returns immediately after the transfer initialization is finished.
Parameters
baseECSPI peripheral base address.
handlepointer to ecspi_master_handle_t structure which stores the transfer state
xferpointer to ecspi_transfer_t structure
Return values
kStatus_SuccessSuccessfully start a transfer.
kStatus_InvalidArgumentInput argument is invalid.
kStatus_ECSPI_BusyECSPI is not idle, is running another transfer.
static status_t ECSPI_SlaveTransferGetCount ( ECSPI_Type *  base,
ecspi_slave_handle_t *  handle,
size_t *  count 
)
inlinestatic
Parameters
baseECSPI peripheral base address.
handlePointer to ECSPI transfer handle, this should be a static variable.
countTransferred bytes of ECSPI slave.
Return values
kStatus_ECSPI_SuccessSucceed get the transfer count.
kStatus_NoTransferInProgressThere is not a non-blocking transaction currently in progress.
static void ECSPI_SlaveTransferAbort ( ECSPI_Type *  base,
ecspi_slave_handle_t *  handle 
)
inlinestatic
Parameters
baseECSPI peripheral base address.
handlePointer to ECSPI transfer handle, this should be a static variable.
void ECSPI_SlaveTransferHandleIRQ ( ECSPI_Type *  base,
ecspi_slave_handle_t *  handle 
)
Parameters
baseECSPI peripheral base address.
handlepointer to ecspi_slave_handle_t structure which stores the transfer state