![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Data Structures | |
struct | ecspi_sdma_handle_t |
ECSPI SDMA transfer handle, users should not touch the content of the handle. More... | |
Typedefs | |
typedef void(* | ecspi_sdma_callback_t )(ECSPI_Type *base, ecspi_sdma_handle_t *handle, status_t status, void *userData) |
ECSPI SDMA callback called at the end of transfer. More... | |
Driver version | |
#define | FSL_ECSPI_FREERTOS_DRIVER_VERSION (MAKE_VERSION(2, 2, 0)) |
ECSPI FreeRTOS driver version. More... | |
DMA Transactional | |
void | ECSPI_MasterTransferCreateHandleSDMA (ECSPI_Type *base, ecspi_sdma_handle_t *handle, ecspi_sdma_callback_t callback, void *userData, sdma_handle_t *txHandle, sdma_handle_t *rxHandle, uint32_t eventSourceTx, uint32_t eventSourceRx, uint32_t TxChannel, uint32_t RxChannel) |
Initialize the ECSPI master SDMA handle. More... | |
void | ECSPI_SlaveTransferCreateHandleSDMA (ECSPI_Type *base, ecspi_sdma_handle_t *handle, ecspi_sdma_callback_t callback, void *userData, sdma_handle_t *txHandle, sdma_handle_t *rxHandle, uint32_t eventSourceTx, uint32_t eventSourceRx, uint32_t TxChannel, uint32_t RxChannel) |
Initialize the ECSPI Slave SDMA handle. More... | |
status_t | ECSPI_MasterTransferSDMA (ECSPI_Type *base, ecspi_sdma_handle_t *handle, ecspi_transfer_t *xfer) |
Perform a non-blocking ECSPI master transfer using SDMA. More... | |
status_t | ECSPI_SlaveTransferSDMA (ECSPI_Type *base, ecspi_sdma_handle_t *handle, ecspi_transfer_t *xfer) |
Perform a non-blocking ECSPI slave transfer using SDMA. More... | |
void | ECSPI_MasterTransferAbortSDMA (ECSPI_Type *base, ecspi_sdma_handle_t *handle) |
Abort a ECSPI master transfer using SDMA. More... | |
void | ECSPI_SlaveTransferAbortSDMA (ECSPI_Type *base, ecspi_sdma_handle_t *handle) |
Abort a ECSPI slave transfer using SDMA. More... | |
struct _ecspi_sdma_handle |
Data Fields | |
bool | txInProgress |
Send transfer finished. | |
bool | rxInProgress |
Receive transfer finished. | |
sdma_handle_t * | txSdmaHandle |
DMA handler for ECSPI send. | |
sdma_handle_t * | rxSdmaHandle |
DMA handler for ECSPI receive. | |
ecspi_sdma_callback_t | callback |
Callback for ECSPI SDMA transfer. | |
void * | userData |
User Data for ECSPI SDMA callback. | |
uint32_t | state |
Internal state of ECSPI SDMA transfer. | |
uint32_t | ChannelTx |
Channel for send handle. | |
uint32_t | ChannelRx |
Channel for receive handler. | |
#define FSL_ECSPI_FREERTOS_DRIVER_VERSION (MAKE_VERSION(2, 2, 0)) |
typedef void(* ecspi_sdma_callback_t)(ECSPI_Type *base, ecspi_sdma_handle_t *handle, status_t status, void *userData) |
void ECSPI_MasterTransferCreateHandleSDMA | ( | ECSPI_Type * | base, |
ecspi_sdma_handle_t * | handle, | ||
ecspi_sdma_callback_t | callback, | ||
void * | userData, | ||
sdma_handle_t * | txHandle, | ||
sdma_handle_t * | rxHandle, | ||
uint32_t | eventSourceTx, | ||
uint32_t | eventSourceRx, | ||
uint32_t | TxChannel, | ||
uint32_t | RxChannel | ||
) |
This function initializes the ECSPI master SDMA handle which can be used for other SPI master transactional APIs. Usually, for a specified ECSPI instance, user need only call this API once to get the initialized handle.
base | ECSPI peripheral base address. |
handle | ECSPI handle pointer. |
callback | User callback function called at the end of a transfer. |
userData | User data for callback. |
txHandle | SDMA handle pointer for ECSPI Tx, the handle shall be static allocated by users. |
rxHandle | SDMA handle pointer for ECSPI Rx, the handle shall be static allocated by users. |
eventSourceTx | event source for ECSPI send, which can be found in SDMA mapping. |
eventSourceRx | event source for ECSPI receive, which can be found in SDMA mapping. |
TxChannel | SDMA channel for ECSPI send. |
RxChannel | SDMA channel for ECSPI receive. |
void ECSPI_SlaveTransferCreateHandleSDMA | ( | ECSPI_Type * | base, |
ecspi_sdma_handle_t * | handle, | ||
ecspi_sdma_callback_t | callback, | ||
void * | userData, | ||
sdma_handle_t * | txHandle, | ||
sdma_handle_t * | rxHandle, | ||
uint32_t | eventSourceTx, | ||
uint32_t | eventSourceRx, | ||
uint32_t | TxChannel, | ||
uint32_t | RxChannel | ||
) |
This function initializes the ECSPI Slave SDMA handle which can be used for other SPI Slave transactional APIs. Usually, for a specified ECSPI instance, user need only call this API once to get the initialized handle.
base | ECSPI peripheral base address. |
handle | ECSPI handle pointer. |
callback | User callback function called at the end of a transfer. |
userData | User data for callback. |
txHandle | SDMA handle pointer for ECSPI Tx, the handle shall be static allocated by users. |
rxHandle | SDMA handle pointer for ECSPI Rx, the handle shall be static allocated by users. |
eventSourceTx | event source for ECSPI send, which can be found in SDMA mapping. |
eventSourceRx | event source for ECSPI receive, which can be found in SDMA mapping. |
TxChannel | SDMA channel for ECSPI send. |
RxChannel | SDMA channel for ECSPI receive. |
status_t ECSPI_MasterTransferSDMA | ( | ECSPI_Type * | base, |
ecspi_sdma_handle_t * | handle, | ||
ecspi_transfer_t * | xfer | ||
) |
base | ECSPI peripheral base address. |
handle | ECSPI SDMA handle pointer. |
xfer | Pointer to sdma transfer structure. |
kStatus_Success | Successfully start a transfer. |
kStatus_InvalidArgument | Input argument is invalid. |
kStatus_ECSPI_Busy | EECSPI is not idle, is running another transfer. |
status_t ECSPI_SlaveTransferSDMA | ( | ECSPI_Type * | base, |
ecspi_sdma_handle_t * | handle, | ||
ecspi_transfer_t * | xfer | ||
) |
base | ECSPI peripheral base address. |
handle | ECSPI SDMA handle pointer. |
xfer | Pointer to sdma transfer structure. |
kStatus_Success | Successfully start a transfer. |
kStatus_InvalidArgument | Input argument is invalid. |
kStatus_ECSPI_Busy | EECSPI is not idle, is running another transfer. |
void ECSPI_MasterTransferAbortSDMA | ( | ECSPI_Type * | base, |
ecspi_sdma_handle_t * | handle | ||
) |
base | ECSPI peripheral base address. |
handle | ECSPI SDMA handle pointer. |
void ECSPI_SlaveTransferAbortSDMA | ( | ECSPI_Type * | base, |
ecspi_sdma_handle_t * | handle | ||
) |
base | ECSPI peripheral base address. |
handle | ECSPI SDMA handle pointer. |