![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Data Structures | |
| struct | pdm_sdma_handle_t |
| PDM DMA transfer handle, users should not touch the content of the handle. More... | |
Typedefs | |
| typedef void(* | pdm_sdma_callback_t )(PDM_Type *base, pdm_sdma_handle_t *handle, status_t status, void *userData) |
| PDM eDMA transfer callback function for finish and error. | |
Driver version | |
| #define | FSL_PDM_SDMA_DRIVER_VERSION (MAKE_VERSION(2, 5, 0)) |
| Version 2.5.0. | |
eDMA Transactional | |
| void | PDM_TransferCreateHandleSDMA (PDM_Type *base, pdm_sdma_handle_t *handle, pdm_sdma_callback_t callback, void *userData, sdma_handle_t *dmaHandle, uint32_t eventSource) |
| Initializes the PDM eDMA handle. More... | |
| status_t | PDM_TransferReceiveSDMA (PDM_Type *base, pdm_sdma_handle_t *handle, pdm_transfer_t *xfer) |
| Performs a non-blocking PDM receive using eDMA. More... | |
| void | PDM_TransferAbortReceiveSDMA (PDM_Type *base, pdm_sdma_handle_t *handle) |
| Aborts a PDM receive using eDMA. More... | |
| void | PDM_SetChannelConfigSDMA (PDM_Type *base, pdm_sdma_handle_t *handle, uint32_t channel, const pdm_channel_config_t *config) |
| PDM channel configurations. More... | |
| struct _pdm_sdma_handle |
Data Fields | |
| sdma_handle_t * | dmaHandle |
| DMA handler for PDM send. | |
| uint8_t | nbytes |
| eDMA minor byte transfer count initially configured. More... | |
| uint8_t | fifoWidth |
| fifo width | |
| uint8_t | endChannel |
| The last enabled channel. | |
| uint8_t | channelNums |
| total channel numbers | |
| uint8_t | count |
| The transfer data count in a DMA request. | |
| uint32_t | state |
| Internal state for PDM eDMA transfer. | |
| uint32_t | eventSource |
| PDM event source number. | |
| pdm_sdma_callback_t | callback |
| Callback for users while transfer finish or error occurs. | |
| void * | userData |
| User callback parameter. | |
| sdma_buffer_descriptor_t | bdPool [PDM_XFER_QUEUE_SIZE] |
| BD pool for SDMA transfer. More... | |
| pdm_transfer_t | pdmQueue [PDM_XFER_QUEUE_SIZE] |
| Transfer queue storing queued transfer. More... | |
| size_t | transferSize [PDM_XFER_QUEUE_SIZE] |
| Data bytes need to transfer. | |
| volatile uint8_t | queueUser |
| Index for user to queue transfer. More... | |
| volatile uint8_t | queueDriver |
| Index for driver to get the transfer data and size. | |
| uint8_t pdm_sdma_handle_t::nbytes |
| sdma_buffer_descriptor_t pdm_sdma_handle_t::bdPool[PDM_XFER_QUEUE_SIZE] |
| pdm_transfer_t pdm_sdma_handle_t::pdmQueue[PDM_XFER_QUEUE_SIZE] |
| volatile uint8_t pdm_sdma_handle_t::queueUser |
| void PDM_TransferCreateHandleSDMA | ( | PDM_Type * | base, |
| pdm_sdma_handle_t * | handle, | ||
| pdm_sdma_callback_t | callback, | ||
| void * | userData, | ||
| sdma_handle_t * | dmaHandle, | ||
| uint32_t | eventSource | ||
| ) |
This function initializes the PDM DMA handle, which can be used for other PDM master transactional APIs. Usually, for a specified PDM instance, call this API once to get the initialized handle.
| base | PDM base pointer. |
| handle | PDM eDMA handle pointer. |
| callback | Pointer to user callback function. |
| userData | User parameter passed to the callback function. |
| dmaHandle | eDMA handle pointer, this handle shall be static allocated by users. |
| eventSource | PDM event source number. |
| status_t PDM_TransferReceiveSDMA | ( | PDM_Type * | base, |
| pdm_sdma_handle_t * | handle, | ||
| pdm_transfer_t * | xfer | ||
| ) |
| base | PDM base pointer |
| handle | PDM eDMA handle pointer. |
| xfer | Pointer to DMA transfer structure. |
| kStatus_Success | Start a PDM eDMA receive successfully. |
| kStatus_InvalidArgument | The input argument is invalid. |
| kStatus_RxBusy | PDM is busy receiving data. |
| void PDM_TransferAbortReceiveSDMA | ( | PDM_Type * | base, |
| pdm_sdma_handle_t * | handle | ||
| ) |
| base | PDM base pointer |
| handle | PDM eDMA handle pointer. |
| void PDM_SetChannelConfigSDMA | ( | PDM_Type * | base, |
| pdm_sdma_handle_t * | handle, | ||
| uint32_t | channel, | ||
| const pdm_channel_config_t * | config | ||
| ) |
| base | PDM base pointer. |
| handle | PDM eDMA handle pointer. |
| channel | channel number. |
| config | channel configurations. |