![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Data Structures | |
struct | uart_sdma_handle_t |
UART sDMA handle. More... | |
Typedefs | |
typedef void(* | uart_sdma_transfer_callback_t )(UART_Type *base, uart_sdma_handle_t *handle, status_t status, void *userData) |
UART transfer callback function. More... | |
Driver version | |
#define | FSL_UART_SDMA_DRIVER_VERSION (MAKE_VERSION(2, 1, 1)) |
UART SDMA driver version 2.1.1. More... | |
sDMA transactional | |
void | UART_TransferCreateHandleSDMA (UART_Type *base, uart_sdma_handle_t *handle, uart_sdma_transfer_callback_t callback, void *userData, sdma_handle_t *txSdmaHandle, sdma_handle_t *rxSdmaHandle, uint32_t eventSourceTx, uint32_t eventSourceRx) |
Initializes the UART handle which is used in transactional functions. More... | |
status_t | UART_SendSDMA (UART_Type *base, uart_sdma_handle_t *handle, uart_transfer_t *xfer) |
Sends data using sDMA. More... | |
status_t | UART_ReceiveSDMA (UART_Type *base, uart_sdma_handle_t *handle, uart_transfer_t *xfer) |
Receives data using sDMA. More... | |
void | UART_TransferAbortSendSDMA (UART_Type *base, uart_sdma_handle_t *handle) |
Aborts the sent data using sDMA. More... | |
void | UART_TransferAbortReceiveSDMA (UART_Type *base, uart_sdma_handle_t *handle) |
Aborts the receive data using sDMA. More... | |
struct _uart_sdma_handle |
Data Fields | |
uart_sdma_transfer_callback_t | callback |
Callback function. More... | |
void * | userData |
UART callback function parameter. More... | |
size_t | rxDataSizeAll |
Size of the data to receive. More... | |
size_t | txDataSizeAll |
Size of the data to send out. More... | |
sdma_handle_t * | txSdmaHandle |
The sDMA TX channel used. More... | |
sdma_handle_t * | rxSdmaHandle |
The sDMA RX channel used. More... | |
volatile uint8_t | txState |
TX transfer state. More... | |
volatile uint8_t | rxState |
RX transfer state. | |
uart_sdma_transfer_callback_t uart_sdma_handle_t::callback |
void* uart_sdma_handle_t::userData |
size_t uart_sdma_handle_t::rxDataSizeAll |
size_t uart_sdma_handle_t::txDataSizeAll |
sdma_handle_t* uart_sdma_handle_t::txSdmaHandle |
sdma_handle_t* uart_sdma_handle_t::rxSdmaHandle |
volatile uint8_t uart_sdma_handle_t::txState |
#define FSL_UART_SDMA_DRIVER_VERSION (MAKE_VERSION(2, 1, 1)) |
typedef void(* uart_sdma_transfer_callback_t)(UART_Type *base, uart_sdma_handle_t *handle, status_t status, void *userData) |
void UART_TransferCreateHandleSDMA | ( | UART_Type * | base, |
uart_sdma_handle_t * | handle, | ||
uart_sdma_transfer_callback_t | callback, | ||
void * | userData, | ||
sdma_handle_t * | txSdmaHandle, | ||
sdma_handle_t * | rxSdmaHandle, | ||
uint32_t | eventSourceTx, | ||
uint32_t | eventSourceRx | ||
) |
base | UART peripheral base address. |
handle | Pointer to the uart_sdma_handle_t structure. |
callback | UART callback, NULL means no callback. |
userData | User callback function data. |
rxSdmaHandle | User-requested DMA handle for RX DMA transfer. |
txSdmaHandle | User-requested DMA handle for TX DMA transfer. |
eventSourceTx | Eventsource for TX DMA transfer. |
eventSourceRx | Eventsource for RX DMA transfer. |
status_t UART_SendSDMA | ( | UART_Type * | base, |
uart_sdma_handle_t * | handle, | ||
uart_transfer_t * | xfer | ||
) |
This function sends data using sDMA. This is a non-blocking function, which returns right away. When all data is sent, the send callback function is called.
base | UART peripheral base address. |
handle | UART handle pointer. |
xfer | UART sDMA transfer structure. See uart_transfer_t. |
kStatus_Success | if succeeded; otherwise failed. |
kStatus_UART_TxBusy | Previous transfer ongoing. |
kStatus_InvalidArgument | Invalid argument. |
status_t UART_ReceiveSDMA | ( | UART_Type * | base, |
uart_sdma_handle_t * | handle, | ||
uart_transfer_t * | xfer | ||
) |
This function receives data using sDMA. This is a non-blocking function, which returns right away. When all data is received, the receive callback function is called.
base | UART peripheral base address. |
handle | Pointer to the uart_sdma_handle_t structure. |
xfer | UART sDMA transfer structure. See uart_transfer_t. |
kStatus_Success | if succeeded; otherwise failed. |
kStatus_UART_RxBusy | Previous transfer ongoing. |
kStatus_InvalidArgument | Invalid argument. |
void UART_TransferAbortSendSDMA | ( | UART_Type * | base, |
uart_sdma_handle_t * | handle | ||
) |
This function aborts sent data using sDMA.
base | UART peripheral base address. |
handle | Pointer to the uart_sdma_handle_t structure. |
void UART_TransferAbortReceiveSDMA | ( | UART_Type * | base, |
uart_sdma_handle_t * | handle | ||
) |
This function aborts receive data using sDMA.
base | UART peripheral base address. |
handle | Pointer to the uart_sdma_handle_t structure. |