This document consists of sections titled with Driver Overview, Data Structures, Enumerations, Functions, etc., each with an overview list and detailed documentation. It is recommended to read the Driver Overview first for it includes a comprehensive description of the peripheral, driver and driver changes. Other sections give detailed information for APIs, enums, macros, etc., for your further reference. 
|  | 
| static void | PMC_EnableInterrupts (PMC_Type *base, uint16_t u16Interrupts) | 
|  | Enables the interrups, including 2.2V high voltage interrupt, 2.7V high voltage interrupt, 2.2V low voltage interrupt, 2.7V low voltage interrupt.  More... 
 | 
|  | 
| static void | PMC_DisableInterrupts (PMC_Type *base, uint16_t u16Interrupts) | 
|  | Disables the interrups, including 2.2V high voltage interrupt, 2.7V high voltage interrupt, 2.2V low voltage interrupt, 2.7V low voltage interrupt.  More... 
 | 
|  | 
|  | 
| static uint16_t | PMC_GetStatusFlags (PMC_Type *base) | 
|  | Gets the status flags of PMC module, such as low voltage interrpt flag, small regulator 2.7 active flag, etc.  More... 
 | 
|  | 
| static void | PMC_ClearStatusFlags (PMC_Type *base, uint16_t u16StatusFlags) | 
|  | Clears the status flags of PMC module, only low voltage interrupt flag, sticky 2.7V low voltage flag, and sticky 2.2V low voltage flag can be cleared.  More... 
 | 
|  | 
| Enumerator | 
|---|
| kPMC_2P2VLowVoltageInterruptEnable | If the input supply is currently dropped below the 2.2V level, generate the low voltage interrupt.  | 
| kPMC_2P7VLowVoltageInterruptEnable | If the input supply is currently dropped below the 2.7V level, generate the low voltage interrupt.  | 
| kPMC_2P2VHighVoltageInterruptEnable | If the input supply is currently raised above the 2.2V level, generate the low voltage interrupt.  | 
| kPMC_2P7VHighVoltageInterruptEnable | If the input supply is currently raised above the 2.2V level, generate the low voltage interrupt.  | 
 
 
| Enumerator | 
|---|
| kPMC_SmallRegulator2P7VActiveFlag | The small regulator 2.7V supply is ready to be used.  | 
| kPMC_LowVoltageInterruptFlag | The low voltage interrupt flag, used to indicate whether the low voltage interrupt is asserted.  | 
| kPMC_Sticky2P7VLowVoltageFlag | Input supply has dropped below the 2.7V threshold.  This sticky flag indicates that the input supply dropped below the 2.7V level at some point.  | 
| kPMC_Sticky2P2VLowVoltageFlag | Input supply has dropped below the 2.2V threshold.  This sticky flag indicates that the input supply dropped below the 2.2V threshold at some point.  | 
| kPMC_2P7VLowVoltageFlag | Input supply is below the 2.7V threshold.  | 
| kPMC_2P2VLowVoltageFlag | Input supply is below the 2.2V threshold.  | 
 
 
  
  | 
        
          | static void PMC_SetBandgapTrim | ( | PMC_Type * | base, |  
          |  |  | uint8_t | u8TrimValue |  
          |  | ) |  |  |  | inlinestatic | 
 
- Parameters
- 
  
    | base | PMC peripheral base address. |  | u8TrimValue | The bandgap's trim value, ranges from 0 to 15. |  
 
 
 
  
  | 
        
          | static void PMC_EnableVoltageReferenceBuffer | ( | PMC_Type * | base, |  
          |  |  | bool | bEnable |  
          |  | ) |  |  |  | inlinestatic | 
 
If the users want to calibrate the ADC using the 1.2V reference voltage, then the voltage reference buffer should be enabled. When ADC calibration is not being performed, the voltage reference buffer should be disabled to save power.
- Parameters
- 
  
    | base | PMC peripheral base address. |  | bEnable | Used to control the behaviour of voltage reference buffer. 
true Enable voltage reference buffer.false Disable voltage reference buffer.  |  
 
 
 
  
  | 
        
          | static void PMC_EnableInterrupts | ( | PMC_Type * | base, |  
          |  |  | uint16_t | u16Interrupts |  
          |  | ) |  |  |  | inlinestatic | 
 
- Parameters
- 
  
    | base | PMC peripheral base address. |  | u16Interrupts | The interupts to be enabled, should be the OR'ed value of _pmc_interrupt_enable. |  
 
 
 
  
  | 
        
          | static void PMC_DisableInterrupts | ( | PMC_Type * | base, |  
          |  |  | uint16_t | u16Interrupts |  
          |  | ) |  |  |  | inlinestatic | 
 
- Parameters
- 
  
    | base | PMC peripheral base address. |  | u16Interrupts | The interupts to be disabled, should be the OR'ed value of _pmc_interrupt_enable. |  
 
 
 
  
  | 
        
          | static uint16_t PMC_GetStatusFlags | ( | PMC_Type * | base | ) |  |  | inlinestatic | 
 
- Parameters
- 
  
    | base | PMC peripheral base address. |  
 
- Returns
- The status flags of PMC module, should be the OR'ed value of _pmc_status_flags. 
 
 
  
  | 
        
          | static void PMC_ClearStatusFlags | ( | PMC_Type * | base, |  
          |  |  | uint16_t | u16StatusFlags |  
          |  | ) |  |  |  | inlinestatic |