![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Data Structures | |
| struct | enet_qos_rx_bd_struct_t |
| Defines the receive descriptor structure has the read-format and write-back format structure. More... | |
| struct | enet_qos_tx_bd_struct_t |
| Defines the transmit descriptor structure has the read-format and write-back format structure. More... | |
| struct | enet_qos_ptp_time_t |
| Defines the ENET PTP time stamp structure. More... | |
| struct | enet_qos_frame_info_t |
| Defines the frame info structure. More... | |
| struct | enet_qos_tx_dirty_ring_t |
| Defines the ENET transmit dirty addresses ring/queue structure. More... | |
| struct | enet_qos_ptp_config_t |
| Defines the ENET PTP configuration structure. More... | |
| struct | enet_qos_est_gate_op_t |
| Defines the EST gate operation structure. More... | |
| struct | enet_qos_est_gcl_t |
| Defines the EST gate control list structure. More... | |
| struct | enet_qos_rxp_config_t |
| Defines the ENET_QOS Rx parser configuration structure. More... | |
| struct | enet_qos_buffer_config_t |
| Defines the buffer descriptor configure structure. More... | |
| struct | enet_qos_cbs_config_t |
| Defines the CBS configuration for queue. More... | |
| struct | enet_qos_queue_tx_config_t |
| Defines the queue configuration structure. More... | |
| struct | enet_qos_queue_rx_config_t |
| Defines the queue configuration structure. More... | |
| struct | enet_qos_multiqueue_config_t |
| Defines the configuration when multi-queue is used. More... | |
| struct | enet_qos_config_t |
| Defines the basic configuration structure for the ENET device. More... | |
| struct | enet_qos_tx_bd_ring_t |
| Defines the ENET transmit buffer descriptor ring/queue structure. More... | |
| struct | enet_qos_rx_bd_ring_t |
| Defines the ENET receive buffer descriptor ring/queue structure. More... | |
| struct | enet_qos_handle_t |
| Defines the ENET handler structure. More... | |
Typedefs | |
| typedef void(* | enet_qos_callback_t )(ENET_QOS_Type *base, enet_qos_handle_t *handle, enet_qos_event_t event, uint8_t channel, void *userData) |
| ENET callback function. More... | |
Driver version | |
| #define | FSL_ENET_QOS_DRIVER_VERSION (MAKE_VERSION(2, 3, 0)) |
| Defines the driver version. More... | |
Control and status region bit masks of the receive buffer descriptor. | |
| #define | ENET_QOS_RXDESCRIP_RD_BUFF1VALID_MASK (1UL << 24U) |
| Defines for read format. More... | |
| #define | ENET_QOS_RXDESCRIP_RD_BUFF2VALID_MASK (1UL << 25U) |
| Buffer2 address valid. More... | |
| #define | ENET_QOS_RXDESCRIP_RD_IOC_MASK (1UL << 30U) |
| Interrupt enable on complete. More... | |
| #define | ENET_QOS_RXDESCRIP_RD_OWN_MASK (1UL << 31U) |
| Own bit. More... | |
| #define | ENET_QOS_RXDESCRIP_WR_ERR_MASK ((1UL << 3U) | (1UL << 7U)) |
| Defines for write back format. More... | |
| #define | ENET_QOS_RXDESCRIP_WR_PYLOAD_MASK (0x7UL) |
| #define | ENET_QOS_RXDESCRIP_WR_PTPMSGTYPE_MASK (0xF00UL) |
| #define | ENET_QOS_RXDESCRIP_WR_PTPTYPE_MASK (1UL << 12U) |
| #define | ENET_QOS_RXDESCRIP_WR_PTPVERSION_MASK (1UL << 13U) |
| #define | ENET_QOS_RXDESCRIP_WR_PTPTSA_MASK (1UL << 14U) |
| #define | ENET_QOS_RXDESCRIP_WR_PACKETLEN_MASK (0x7FFFUL) |
| #define | ENET_QOS_RXDESCRIP_WR_ERRSUM_MASK (1UL << 15U) |
| #define | ENET_QOS_RXDESCRIP_WR_TYPE_MASK (0x30000UL) |
| #define | ENET_QOS_RXDESCRIP_WR_DE_MASK (1UL << 19U) |
| #define | ENET_QOS_RXDESCRIP_WR_RE_MASK (1UL << 20U) |
| #define | ENET_QOS_RXDESCRIP_WR_OE_MASK (1UL << 21U) |
| #define | ENET_QOS_RXDESCRIP_WR_RS0V_MASK (1UL << 25U) |
| #define | ENET_QOS_RXDESCRIP_WR_RS1V_MASK (1UL << 26U) |
| #define | ENET_QOS_RXDESCRIP_WR_RS2V_MASK (1UL << 27U) |
| #define | ENET_QOS_RXDESCRIP_WR_LD_MASK (1UL << 28U) |
| #define | ENET_QOS_RXDESCRIP_WR_FD_MASK (1UL << 29U) |
| #define | ENET_QOS_RXDESCRIP_WR_CTXT_MASK (1UL << 30U) |
| #define | ENET_QOS_RXDESCRIP_WR_OWN_MASK (1UL << 31U) |
Control and status bit masks of the transmit buffer descriptor. | |
| #define | ENET_QOS_TXDESCRIP_RD_BL1_MASK (0x3fffUL) |
| Defines for read format. More... | |
| #define | ENET_QOS_TXDESCRIP_RD_BL2_MASK (ENET_QOS_TXDESCRIP_RD_BL1_MASK << 16U) |
| #define | ENET_QOS_TXDESCRIP_RD_BL1(n) ((uint32_t)(n)&ENET_QOS_TXDESCRIP_RD_BL1_MASK) |
| #define | ENET_QOS_TXDESCRIP_RD_BL2(n) (((uint32_t)(n)&ENET_QOS_TXDESCRIP_RD_BL1_MASK) << 16) |
| #define | ENET_QOS_TXDESCRIP_RD_TTSE_MASK (1UL << 30UL) |
| #define | ENET_QOS_TXDESCRIP_RD_IOC_MASK (1UL << 31UL) |
| #define | ENET_QOS_TXDESCRIP_RD_FL_MASK (0x7FFFUL) |
| #define | ENET_QOS_TXDESCRIP_RD_FL(n) ((uint32_t)(n)&ENET_QOS_TXDESCRIP_RD_FL_MASK) |
| #define | ENET_QOS_TXDESCRIP_RD_CIC(n) (((uint32_t)(n)&0x3U) << 16U) |
| #define | ENET_QOS_TXDESCRIP_RD_TSE_MASK (1UL << 18U) |
| #define | ENET_QOS_TXDESCRIP_RD_SLOT(n) (((uint32_t)(n)&0x0fU) << 19U) |
| #define | ENET_QOS_TXDESCRIP_RD_SAIC(n) (((uint32_t)(n)&0x07U) << 23U) |
| #define | ENET_QOS_TXDESCRIP_RD_CPC(n) (((uint32_t)(n)&0x03U) << 26U) |
| #define | ENET_QOS_TXDESCRIP_RD_LDFD(n) (((uint32_t)(n)&0x03U) << 28U) |
| #define | ENET_QOS_TXDESCRIP_RD_LD_MASK (1UL << 28U) |
| #define | ENET_QOS_TXDESCRIP_RD_FD_MASK (1UL << 29U) |
| #define | ENET_QOS_TXDESCRIP_RD_CTXT_MASK (1UL << 30U) |
| #define | ENET_QOS_TXDESCRIP_RD_OWN_MASK (1UL << 31U) |
| #define | ENET_QOS_TXDESCRIP_WB_TTSS_MASK (1UL << 17U) |
| Defines for write back format. More... | |
Bit mask for interrupt enable type. | |
| #define | ENET_QOS_ABNORM_INT_MASK |
| #define | ENET_QOS_NORM_INT_MASK |
Defines some Ethernet parameters. | |
| #define | ENET_QOS_RING_NUM_MAX (5U) |
| The Maximum number of tx/rx descriptor rings. More... | |
| #define | ENET_QOS_FRAME_MAX_FRAMELEN (1518U) |
| Default maximum Ethernet frame size. More... | |
| #define | ENET_QOS_FCS_LEN (4U) |
| Ethernet FCS length. More... | |
| #define | ENET_QOS_ADDR_ALIGNMENT (0x3U) |
| Recommended Ethernet buffer alignment. More... | |
| #define | ENET_QOS_BUFF_ALIGNMENT (8U) |
| Receive buffer alignment shall be 4bytes-aligned. More... | |
| #define | ENET_QOS_MTL_RXFIFOSIZE (8192U) |
| The rx fifo size. More... | |
| #define | ENET_QOS_MTL_TXFIFOSIZE (8192U) |
| The tx fifo size. More... | |
| #define | ENET_QOS_MACINT_ENUM_OFFSET (16U) |
| The offest for mac interrupt in enum type. More... | |
| #define | ENET_QOS_RXP_ENTRY_COUNT (256U) |
| RXP table entry count, implied by FRPES in MAC_HW_FEATURE3. | |
| #define | ENET_QOS_RXP_BUFFER_SIZE (256U) |
| RXP Buffer size, implied by FRPBS in MAC_HW_FEATURE3. | |
| #define | ENET_QOS_EST_WID (24U) |
| Width of the time interval in Gate Control List. | |
| #define | ENET_QOS_EST_DEP (512U) |
| Maxmimum depth of Gate Control List. | |
Initialization and De-initialization | |
| void | ENET_QOS_GetDefaultConfig (enet_qos_config_t *config) |
| Gets the ENET default configuration structure. More... | |
| status_t | ENET_QOS_Up (ENET_QOS_Type *base, const enet_qos_config_t *config, uint8_t *macAddr, uint8_t macCount, uint32_t refclkSrc_Hz) |
| Initializes the ENET module. More... | |
| status_t | ENET_QOS_Init (ENET_QOS_Type *base, const enet_qos_config_t *config, uint8_t *macAddr, uint8_t macCount, uint32_t refclkSrc_Hz) |
| Initializes the ENET module. More... | |
| void | ENET_QOS_Down (ENET_QOS_Type *base) |
| brief Stops the ENET module. More... | |
| void | ENET_QOS_Deinit (ENET_QOS_Type *base) |
| Deinitializes the ENET module. More... | |
| uint32_t | ENET_QOS_GetInstance (ENET_QOS_Type *base) |
| Get the ENET instance from peripheral base address. More... | |
| status_t | ENET_QOS_DescriptorInit (ENET_QOS_Type *base, enet_qos_config_t *config, enet_qos_buffer_config_t *bufferConfig) |
| Initialize for all ENET descriptors. More... | |
| void | ENET_QOS_StartRxTx (ENET_QOS_Type *base, uint8_t txRingNum, uint8_t rxRingNum) |
| Starts the ENET rx/tx. More... | |
MII interface operation | |
| static void | ENET_QOS_SetMII (ENET_QOS_Type *base, enet_qos_mii_speed_t speed, enet_qos_mii_duplex_t duplex) |
| Sets the ENET MII speed and duplex. More... | |
| void | ENET_QOS_SetSMI (ENET_QOS_Type *base, uint32_t csrClock_Hz) |
| Sets the ENET SMI(serial management interface)- MII management interface. More... | |
| static bool | ENET_QOS_IsSMIBusy (ENET_QOS_Type *base) |
| Checks if the SMI is busy. More... | |
| static uint16_t | ENET_QOS_ReadSMIData (ENET_QOS_Type *base) |
| Reads data from the PHY register through SMI interface. More... | |
| void | ENET_QOS_StartSMIRead (ENET_QOS_Type *base, uint32_t phyAddr, uint32_t phyReg) |
| Starts an SMI read command. More... | |
| void | ENET_QOS_StartSMIWrite (ENET_QOS_Type *base, uint32_t phyAddr, uint32_t phyReg, uint32_t data) |
| Starts a SMI write command. More... | |
Other basic operation | |
| static void | ENET_QOS_SetMacAddr (ENET_QOS_Type *base, uint8_t *macAddr, uint8_t index) |
| Sets the ENET module Mac address. More... | |
| void | ENET_QOS_GetMacAddr (ENET_QOS_Type *base, uint8_t *macAddr, uint8_t index) |
| Gets the ENET module Mac address. More... | |
| void | ENET_QOS_AddMulticastGroup (ENET_QOS_Type *base, uint8_t *address) |
| Adds the ENET_QOS device to a multicast group. More... | |
| void | ENET_QOS_LeaveMulticastGroup (ENET_QOS_Type *base, uint8_t *address) |
| brief Moves the ENET_QOS device from a multicast group. More... | |
| static void | ENET_QOS_AcceptAllMulticast (ENET_QOS_Type *base) |
| Enable ENET device to accept all multicast frames. More... | |
| static void | ENET_QOS_RejectAllMulticast (ENET_QOS_Type *base) |
| ENET device reject to accept all multicast frames. More... | |
| void | ENET_QOS_EnterPowerDown (ENET_QOS_Type *base, uint32_t *wakeFilter) |
| Set the MAC to enter into power down mode. More... | |
| static void | ENET_QOS_ExitPowerDown (ENET_QOS_Type *base) |
| Set the MAC to exit power down mode. More... | |
| status_t | ENET_QOS_EnableRxParser (ENET_QOS_Type *base, bool enable) |
| Enable/Disable Rx parser,please notice that for enable/disable Rx Parser, should better disable Receive first. More... | |
Interrupts. | |
| void | ENET_QOS_EnableInterrupts (ENET_QOS_Type *base, uint32_t mask) |
| Enables the ENET DMA and MAC interrupts. More... | |
| void | ENET_QOS_DisableInterrupts (ENET_QOS_Type *base, uint32_t mask) |
| Disables the ENET DMA and MAC interrupts. More... | |
| static uint32_t | ENET_QOS_GetDmaInterruptStatus (ENET_QOS_Type *base, uint8_t channel) |
| Gets the ENET DMA interrupt status flag. More... | |
| static void | ENET_QOS_ClearDmaInterruptStatus (ENET_QOS_Type *base, uint8_t channel, uint32_t mask) |
| Clear the ENET DMA interrupt status flag. More... | |
| static uint32_t | ENET_QOS_GetMacInterruptStatus (ENET_QOS_Type *base) |
| Gets the ENET MAC interrupt status flag. More... | |
| void | ENET_QOS_ClearMacInterruptStatus (ENET_QOS_Type *base, uint32_t mask) |
| Clears the ENET mac interrupt events status flag. More... | |
Functional operation. | |
| static bool | ENET_QOS_IsTxDescriptorDmaOwn (enet_qos_tx_bd_struct_t *txDesc) |
| Get the tx descriptor DMA Own flag. More... | |
| void | ENET_QOS_SetupTxDescriptor (enet_qos_tx_bd_struct_t *txDesc, void *buffer1, uint32_t bytes1, void *buffer2, uint32_t bytes2, uint32_t framelen, bool intEnable, bool tsEnable, enet_qos_desc_flag flag, uint8_t slotNum) |
| Setup a given tx descriptor. More... | |
| static void | ENET_QOS_UpdateTxDescriptorTail (ENET_QOS_Type *base, uint8_t channel, uint32_t txDescTailAddrAlign) |
| Update the tx descriptor tail pointer. More... | |
| static void | ENET_QOS_UpdateRxDescriptorTail (ENET_QOS_Type *base, uint8_t channel, uint32_t rxDescTailAddrAlign) |
| Update the rx descriptor tail pointer. More... | |
| static uint32_t | ENET_QOS_GetRxDescriptor (enet_qos_rx_bd_struct_t *rxDesc) |
| Gets the context in the ENET rx descriptor. More... | |
| void | ENET_QOS_UpdateRxDescriptor (enet_qos_rx_bd_struct_t *rxDesc, void *buffer1, void *buffer2, bool intEnable, bool doubleBuffEnable) |
| Updates the buffers and the own status for a given rx descriptor. More... | |
| status_t | ENET_QOS_ConfigureRxParser (ENET_QOS_Type *base, enet_qos_rxp_config_t *rxpConfig, uint16_t entryCount) |
| Configure flexible rx parser. More... | |
| status_t | ENET_QOS_ReadRxParser (ENET_QOS_Type *base, enet_qos_rxp_config_t *rxpConfig, uint16_t entryIndex) |
| Read flexible rx parser configuration at specified index. More... | |
| status_t | ENET_QOS_EstProgramGcl (ENET_QOS_Type *base, enet_qos_est_gcl_t *gcl, uint32_t ptpClk_Hz) |
| Program Gate Control List. More... | |
| status_t | ENET_QOS_EstReadGcl (ENET_QOS_Type *base, enet_qos_est_gcl_t *gcl, uint32_t listLen, bool hwList) |
| Read Gate Control List. More... | |
| static void | ENET_QOS_FpeEnable (ENET_QOS_Type *base) |
| Enable Frame Preemption. More... | |
| static void | ENET_QOS_FpeDisable (ENET_QOS_Type *base) |
| Disable Frame Preemption. More... | |
| static void | ENET_QOS_FpeConfigPreemptable (ENET_QOS_Type *base, uint8_t queueMask) |
| Configure preemptable transmit queues. More... | |
| void | ENET_QOS_AVBConfigure (ENET_QOS_Type *base, const enet_qos_cbs_config_t *config, uint8_t queueIndex) |
| Sets the ENET AVB feature. More... | |
Transactional operation | |
| void | ENET_QOS_CreateHandler (ENET_QOS_Type *base, enet_qos_handle_t *handle, enet_qos_config_t *config, enet_qos_buffer_config_t *bufferConfig, enet_qos_callback_t callback, void *userData) |
| Create ENET Handler. More... | |
| status_t | ENET_QOS_GetRxFrameSize (ENET_QOS_Type *base, enet_qos_handle_t *handle, uint32_t *length, uint8_t channel) |
| Gets the size of the read frame. More... | |
| status_t | ENET_QOS_ReadFrame (ENET_QOS_Type *base, enet_qos_handle_t *handle, uint8_t *data, uint32_t length, uint8_t channel, enet_qos_ptp_time_t *ts) |
| Reads a frame from the ENET device. More... | |
| status_t | ENET_QOS_SendFrame (ENET_QOS_Type *base, enet_qos_handle_t *handle, uint8_t *data, uint32_t length, uint8_t channel, bool isNeedTs, void *context) |
| Transmits an ENET frame. More... | |
| void | ENET_QOS_ReclaimTxDescriptor (ENET_QOS_Type *base, enet_qos_handle_t *handle, uint8_t channel) |
| Reclaim tx descriptors. More... | |
| void | ENET_QOS_CommonIRQHandler (ENET_QOS_Type *base, enet_qos_handle_t *handle) |
| The ENET IRQ handler. More... | |
| void | ENET_QOS_SetISRHandler (ENET_QOS_Type *base, enet_qos_isr_t ISRHandler) |
| Set the second level IRQ handler, allow user to overwrite the default second level weak IRQ handler. More... | |
ENET Enhanced function operation | |
| status_t | ENET_QOS_Ptp1588CorrectTimerInCoarse (ENET_QOS_Type *base, enet_qos_systime_op operation, uint32_t second, uint32_t nanosecond) |
| Correct the ENET PTP 1588 timer in coarse method. More... | |
| status_t | ENET_QOS_Ptp1588CorrectTimerInFine (ENET_QOS_Type *base, uint32_t addend) |
| Correct the ENET PTP 1588 timer in fine method. More... | |
| static uint32_t | ENET_QOS_Ptp1588GetAddend (ENET_QOS_Type *base) |
| Get the ENET Time stamp current addend value. More... | |
| void | ENET_QOS_Ptp1588GetTimerNoIRQDisable (ENET_QOS_Type *base, uint64_t *second, uint32_t *nanosecond) |
| Gets the current ENET time from the PTP 1588 timer without IRQ disable. More... | |
| static status_t | ENET_Ptp1588PpsControl (ENET_QOS_Type *base, enet_qos_ptp_pps_instance_t instance, enet_qos_ptp_pps_trgt_mode_t trgtMode, enet_qos_ptp_pps_cmd_t cmd) |
| Sets the ENET PTP 1588 PPS control. More... | |
| status_t | ENET_QOS_Ptp1588PpsSetTrgtTime (ENET_QOS_Type *base, enet_qos_ptp_pps_instance_t instance, uint32_t seconds, uint32_t nanoseconds) |
| Sets the ENET OQS PTP 1588 PPS target time registers. More... | |
| static void | ENET_QOS_Ptp1588PpsSetWidth (ENET_QOS_Type *base, enet_qos_ptp_pps_instance_t instance, uint32_t width) |
| Sets the ENET OQS PTP 1588 PPS output signal interval. More... | |
| static void | ENET_QOS_Ptp1588PpsSetInterval (ENET_QOS_Type *base, enet_qos_ptp_pps_instance_t instance, uint32_t interval) |
| Sets the ENET OQS PTP 1588 PPS output signal width. More... | |
| void | ENET_QOS_Ptp1588GetTimer (ENET_QOS_Type *base, uint64_t *second, uint32_t *nanosecond) |
| Gets the current ENET time from the PTP 1588 timer. More... | |
| void | ENET_QOS_GetTxFrame (enet_qos_handle_t *handle, enet_qos_frame_info_t *txFrame, uint8_t channel) |
| Gets the time stamp of the transmit frame. More... | |
| struct enet_qos_rx_bd_struct_t |
They both has the same size with different region definition. so we define the read-format region as the recive descriptor structure Use the read-format region mask bits in the descriptor initialization Use the write-back format region mask bits in the receive data process.
Data Fields | |
| __IO uint32_t | buff1Addr |
| Buffer 1 address. | |
| __IO uint32_t | reserved |
| Reserved. | |
| __IO uint32_t | buff2Addr |
| Buffer 2 or next descriptor address. | |
| __IO uint32_t | control |
| Buffer 1/2 byte counts and control. | |
| struct enet_qos_tx_bd_struct_t |
They both has the same size with different region definition. so we define the read-format region as the transmit descriptor structure Use the read-format region mask bits in the descriptor initialization Use the write-back format region mask bits in the transmit data process.
Data Fields | |
| __IO uint32_t | buff1Addr |
| Buffer 1 address. | |
| __IO uint32_t | buff2Addr |
| Buffer 2 address. | |
| __IO uint32_t | buffLen |
| Buffer 1/2 byte counts. | |
| __IO uint32_t | controlStat |
| TDES control and status word. | |
| struct enet_qos_ptp_time_t |
Data Fields | |
| uint64_t | second |
| Second. More... | |
| uint32_t | nanosecond |
| Nanosecond. More... | |
| uint64_t enet_qos_ptp_time_t::second |
| uint32_t enet_qos_ptp_time_t::nanosecond |
| struct enet_qos_frame_info_t |
Data Fields | |
| void * | context |
| User specified data, could be buffer address for free. | |
| bool | isTsAvail |
| Flag indicates timestamp available status. | |
| enet_qos_ptp_time_t | timeStamp |
| Timestamp of frame. | |
| struct enet_qos_tx_dirty_ring_t |
Data Fields | |
| enet_qos_frame_info_t * | txDirtyBase |
| Dirty buffer descriptor base address pointer. More... | |
| uint16_t | txGenIdx |
| tx generate index. More... | |
| uint16_t | txConsumIdx |
| tx consume index. More... | |
| uint16_t | txRingLen |
| tx ring length. More... | |
| bool | isFull |
| tx ring is full flag, add this parameter to avoid waste one element. More... | |
| enet_qos_frame_info_t* enet_qos_tx_dirty_ring_t::txDirtyBase |
| uint16_t enet_qos_tx_dirty_ring_t::txGenIdx |
| uint16_t enet_qos_tx_dirty_ring_t::txConsumIdx |
| uint16_t enet_qos_tx_dirty_ring_t::txRingLen |
| bool enet_qos_tx_dirty_ring_t::isFull |
| struct enet_qos_ptp_config_t |
Data Fields | |
| bool | fineUpdateEnable |
| Use the fine update. More... | |
| uint32_t | defaultAddend |
| Default addend value when fine update is enable, could be 2^32 / (refClk_Hz / ENET_QOS_MICRSECS_ONESECOND / ENET_QOS_SYSTIME_REQUIRED_CLK_MHZ). More... | |
| bool | ptp1588V2Enable |
| The desired system time frequency. More... | |
| enet_qos_ts_rollover_type | tsRollover |
| 1588 time nanosecond rollover. More... | |
| bool enet_qos_ptp_config_t::fineUpdateEnable |
| uint32_t enet_qos_ptp_config_t::defaultAddend |
| bool enet_qos_ptp_config_t::ptp1588V2Enable |
Must be lower than reference clock. (Only used with fine correction method). ptp 1588 version 2 is used.
| enet_qos_ts_rollover_type enet_qos_ptp_config_t::tsRollover |
| struct enet_qos_est_gate_op_t |
| struct enet_qos_est_gcl_t |
Data Fields | |
| bool | enable |
| Enable or disable EST. | |
| uint64_t | cycleTime |
| Base Time 32 bits seconds 32 bits nanoseconds. | |
| uint32_t | extTime |
| Cycle Time 32 bits seconds 32 bits nanoseconds. | |
| uint32_t | numEntries |
| Time Extension 32 bits seconds 32 bits nanoseconds. | |
| enet_qos_est_gate_op_t * | opList |
| Number of entries. | |
| struct enet_qos_rxp_config_t |
Data Fields | |
| uint32_t | matchEnable |
| 4-byte match data used for comparing with incoming packet | |
| uint8_t | acceptFrame: 1 |
| When matchEnable is set to 1, the matchData is used for comparing. | |
| uint8_t | rejectFrame: 1 |
| When acceptFrame = 1 and data is matched, the frame will be sent to DMA channel. | |
| uint8_t | inverseMatch: 1 |
| When rejectFrame = 1 and data is matched, the frame will be dropped. | |
| uint8_t | nextControl: 1 |
| Inverse match. | |
| uint8_t | reserved: 4 |
| Next instruction indexing control. | |
| uint8_t | frameOffset |
| Reserved control fields. | |
| uint8_t | okIndex |
| Frame offset in the packet data to be compared for match, in terms of 4 bytes. More... | |
| uint8_t | dmaChannel |
| Memory Index to be used next. More... | |
| uint32_t | reserved2 |
| The DMA channel enet_qos_rxp_dma_chn_t used for receiving the frame when frame match and acceptFrame = 1. | |
| uint8_t enet_qos_rxp_config_t::okIndex |
| uint8_t enet_qos_rxp_config_t::dmaChannel |
| struct enet_qos_buffer_config_t |
Notes:
Data Fields | |
| uint8_t | rxRingLen |
| The length of receive buffer descriptor ring. More... | |
| uint8_t | txRingLen |
| The length of transmit buffer descriptor ring. More... | |
| enet_qos_tx_bd_struct_t * | txDescStartAddrAlign |
| Aligned transmit descriptor start address. More... | |
| enet_qos_tx_bd_struct_t * | txDescTailAddrAlign |
| Aligned transmit descriptor tail address. More... | |
| enet_qos_frame_info_t * | txDirtyStartAddr |
| Start address of the dirty tx frame information. More... | |
| enet_qos_rx_bd_struct_t * | rxDescStartAddrAlign |
| Aligned receive descriptor start address. More... | |
| enet_qos_rx_bd_struct_t * | rxDescTailAddrAlign |
| Aligned receive descriptor tail address. More... | |
| uint32_t * | rxBufferStartAddr |
| Start address of the rx buffers. More... | |
| uint32_t | rxBuffSizeAlign |
| Aligned receive data buffer size. More... | |
| bool | rxBuffNeedMaintain |
| Whether receive data buffer need cache maintain. More... | |
| uint8_t enet_qos_buffer_config_t::rxRingLen |
| uint8_t enet_qos_buffer_config_t::txRingLen |
| enet_qos_tx_bd_struct_t* enet_qos_buffer_config_t::txDescStartAddrAlign |
| enet_qos_tx_bd_struct_t* enet_qos_buffer_config_t::txDescTailAddrAlign |
| enet_qos_frame_info_t* enet_qos_buffer_config_t::txDirtyStartAddr |
| enet_qos_rx_bd_struct_t* enet_qos_buffer_config_t::rxDescStartAddrAlign |
| enet_qos_rx_bd_struct_t* enet_qos_buffer_config_t::rxDescTailAddrAlign |
| uint32_t* enet_qos_buffer_config_t::rxBufferStartAddr |
| uint32_t enet_qos_buffer_config_t::rxBuffSizeAlign |
| bool enet_qos_buffer_config_t::rxBuffNeedMaintain |
| struct enet_qos_cbs_config_t |
Data Fields | |
| uint16_t | sendSlope |
| Send slope configuration. More... | |
| uint16_t | idleSlope |
| Idle slope configuration. More... | |
| uint32_t | highCredit |
| High credit. More... | |
| uint32_t | lowCredit |
| Low credit. More... | |
| uint16_t enet_qos_cbs_config_t::sendSlope |
| uint16_t enet_qos_cbs_config_t::idleSlope |
| uint32_t enet_qos_cbs_config_t::highCredit |
| uint32_t enet_qos_cbs_config_t::lowCredit |
| struct enet_qos_queue_tx_config_t |
Data Fields | |
| enet_qos_queue_mode_t | mode |
| tx queue mode configuration. More... | |
| uint32_t | weight |
| Refer to the MTL TxQ Quantum Weight register. More... | |
| uint32_t | priority |
| Refer to Transmit Queue Priority Mapping register. More... | |
| enet_qos_cbs_config_t * | cbsConfig |
| CBS configuration if queue use AVB mode. More... | |
| enet_qos_queue_mode_t enet_qos_queue_tx_config_t::mode |
| uint32_t enet_qos_queue_tx_config_t::weight |
| uint32_t enet_qos_queue_tx_config_t::priority |
| enet_qos_cbs_config_t* enet_qos_queue_tx_config_t::cbsConfig |
| struct enet_qos_queue_rx_config_t |
Data Fields | |
| enet_qos_queue_mode_t | mode |
| rx queue mode configuration. More... | |
| uint8_t | mapChannel |
| tx queue map dma channel. More... | |
| uint32_t | priority |
| Rx queue priority. More... | |
| enet_qos_rx_queue_route_t | packetRoute |
| Receive packet routing. More... | |
| enet_qos_queue_mode_t enet_qos_queue_rx_config_t::mode |
| uint8_t enet_qos_queue_rx_config_t::mapChannel |
| uint32_t enet_qos_queue_rx_config_t::priority |
| enet_qos_rx_queue_route_t enet_qos_queue_rx_config_t::packetRoute |
| struct enet_qos_multiqueue_config_t |
Data Fields | |
| enet_qos_dma_burstlen | burstLen |
| Burst len for the multi-queue. More... | |
| uint8_t | txQueueUse |
| Used Tx queue count. More... | |
| enet_qos_mtl_multiqueue_txsche | mtltxSche |
| Transmit schedule for multi-queue. More... | |
| enet_qos_queue_tx_config_t | txQueueConfig [ENET_QOS_RING_NUM_MAX] |
| Tx Queue configuration. More... | |
| uint8_t | rxQueueUse |
| Used Rx queue count. More... | |
| enet_qos_mtl_multiqueue_rxsche | mtlrxSche |
| Receive schedule for multi-queue. More... | |
| enet_qos_queue_rx_config_t | rxQueueConfig [ENET_QOS_RING_NUM_MAX] |
| Rx Queue configuration. More... | |
| enet_qos_dma_burstlen enet_qos_multiqueue_config_t::burstLen |
| uint8_t enet_qos_multiqueue_config_t::txQueueUse |
| enet_qos_mtl_multiqueue_txsche enet_qos_multiqueue_config_t::mtltxSche |
| enet_qos_queue_tx_config_t enet_qos_multiqueue_config_t::txQueueConfig[ENET_QOS_RING_NUM_MAX] |
| uint8_t enet_qos_multiqueue_config_t::rxQueueUse |
| enet_qos_mtl_multiqueue_rxsche enet_qos_multiqueue_config_t::mtlrxSche |
| enet_qos_queue_rx_config_t enet_qos_multiqueue_config_t::rxQueueConfig[ENET_QOS_RING_NUM_MAX] |
| struct enet_qos_config_t |
Note:
Data Fields | |
| uint16_t | specialControl |
| The logic or of enet_qos_special_config_t. | |
| enet_qos_multiqueue_config_t * | multiqueueCfg |
| Use multi-queue. More... | |
| enet_qos_mii_mode_t | miiMode |
| MII mode. More... | |
| enet_qos_mii_speed_t | miiSpeed |
| MII Speed. More... | |
| enet_qos_mii_duplex_t | miiDuplex |
| MII duplex. More... | |
| uint16_t | pauseDuration |
| Used in the tx flow control frame, only valid when kENET_QOS_FlowControlEnable is set. More... | |
| enet_qos_ptp_config_t * | ptpConfig |
| PTP 1588 feature configuration. | |
| uint32_t | csrClock_Hz |
| CSR clock frequency in HZ. More... | |
| enet_qos_multiqueue_config_t* enet_qos_config_t::multiqueueCfg |
| enet_qos_mii_mode_t enet_qos_config_t::miiMode |
| enet_qos_mii_speed_t enet_qos_config_t::miiSpeed |
| enet_qos_mii_duplex_t enet_qos_config_t::miiDuplex |
| uint16_t enet_qos_config_t::pauseDuration |
| uint32_t enet_qos_config_t::csrClock_Hz |
| struct enet_qos_tx_bd_ring_t |
Data Fields | |
| enet_qos_tx_bd_struct_t * | txBdBase |
| Buffer descriptor base address pointer. More... | |
| uint16_t | txGenIdx |
| tx generate index. More... | |
| uint16_t | txConsumIdx |
| tx consume index. More... | |
| volatile uint16_t | txDescUsed |
| tx descriptor used number. More... | |
| uint16_t | txRingLen |
| tx ring length. More... | |
| enet_qos_tx_bd_struct_t* enet_qos_tx_bd_ring_t::txBdBase |
| uint16_t enet_qos_tx_bd_ring_t::txGenIdx |
| uint16_t enet_qos_tx_bd_ring_t::txConsumIdx |
| volatile uint16_t enet_qos_tx_bd_ring_t::txDescUsed |
| uint16_t enet_qos_tx_bd_ring_t::txRingLen |
| struct enet_qos_rx_bd_ring_t |
Data Fields | |
| enet_qos_rx_bd_struct_t * | rxBdBase |
| Buffer descriptor base address pointer. More... | |
| uint16_t | rxGenIdx |
| The current available receive buffer descriptor pointer. More... | |
| uint16_t | rxRingLen |
| Receive ring length. More... | |
| uint32_t | rxBuffSizeAlign |
| Receive buffer size. More... | |
| enet_qos_rx_bd_struct_t* enet_qos_rx_bd_ring_t::rxBdBase |
| uint16_t enet_qos_rx_bd_ring_t::rxGenIdx |
| uint16_t enet_qos_rx_bd_ring_t::rxRingLen |
| uint32_t enet_qos_rx_bd_ring_t::rxBuffSizeAlign |
| struct _enet_qos_handle |
Data Fields | |
| uint8_t | txQueueUse |
| Used tx queue count. More... | |
| uint8_t | rxQueueUse |
| Used rx queue count. More... | |
| bool | doubleBuffEnable |
| The double buffer is used in the descriptor. More... | |
| bool | rxintEnable |
| Rx interrupt enabled. More... | |
| bool | rxMaintainEnable [ENET_QOS_RING_NUM_MAX] |
| Rx buffer cache maintain enabled. More... | |
| enet_qos_rx_bd_ring_t | rxBdRing [ENET_QOS_RING_NUM_MAX] |
| Receive buffer descriptor. More... | |
| enet_qos_tx_bd_ring_t | txBdRing [ENET_QOS_RING_NUM_MAX] |
| Transmit buffer descriptor. More... | |
| enet_qos_tx_dirty_ring_t | txDirtyRing [ENET_QOS_RING_NUM_MAX] |
| Transmit dirty buffers addresses. More... | |
| uint32_t * | rxBufferStartAddr [ENET_QOS_RING_NUM_MAX] |
| Rx buffer start address for reInitialize. More... | |
| enet_qos_callback_t | callback |
| Callback function. More... | |
| void * | userData |
| Callback function parameter. More... | |
| uint8_t | multicastCount [64] |
| Multicast collisions counter. | |
| uint8_t enet_qos_handle_t::txQueueUse |
| uint8_t enet_qos_handle_t::rxQueueUse |
| bool enet_qos_handle_t::doubleBuffEnable |
| bool enet_qos_handle_t::rxintEnable |
| bool enet_qos_handle_t::rxMaintainEnable[ENET_QOS_RING_NUM_MAX] |
| enet_qos_rx_bd_ring_t enet_qos_handle_t::rxBdRing[ENET_QOS_RING_NUM_MAX] |
| enet_qos_tx_bd_ring_t enet_qos_handle_t::txBdRing[ENET_QOS_RING_NUM_MAX] |
| enet_qos_tx_dirty_ring_t enet_qos_handle_t::txDirtyRing[ENET_QOS_RING_NUM_MAX] |
| uint32_t* enet_qos_handle_t::rxBufferStartAddr[ENET_QOS_RING_NUM_MAX] |
| enet_qos_callback_t enet_qos_handle_t::callback |
| void* enet_qos_handle_t::userData |
| #define FSL_ENET_QOS_DRIVER_VERSION (MAKE_VERSION(2, 3, 0)) |
| #define ENET_QOS_RXDESCRIP_RD_BUFF1VALID_MASK (1UL << 24U) |
Buffer1 address valid.
| #define ENET_QOS_RXDESCRIP_RD_BUFF2VALID_MASK (1UL << 25U) |
| #define ENET_QOS_RXDESCRIP_RD_IOC_MASK (1UL << 30U) |
| #define ENET_QOS_RXDESCRIP_RD_OWN_MASK (1UL << 31U) |
| #define ENET_QOS_RXDESCRIP_WR_ERR_MASK ((1UL << 3U) | (1UL << 7U)) |
| #define ENET_QOS_TXDESCRIP_RD_BL1_MASK (0x3fffUL) |
| #define ENET_QOS_TXDESCRIP_WB_TTSS_MASK (1UL << 17U) |
| #define ENET_QOS_RING_NUM_MAX (5U) |
| #define ENET_QOS_FRAME_MAX_FRAMELEN (1518U) |
| #define ENET_QOS_FCS_LEN (4U) |
| #define ENET_QOS_ADDR_ALIGNMENT (0x3U) |
| #define ENET_QOS_BUFF_ALIGNMENT (8U) |
| #define ENET_QOS_MTL_RXFIFOSIZE (8192U) |
| #define ENET_QOS_MTL_TXFIFOSIZE (8192U) |
| #define ENET_QOS_MACINT_ENUM_OFFSET (16U) |
| typedef void(* enet_qos_callback_t)(ENET_QOS_Type *base, enet_qos_handle_t *handle, enet_qos_event_t event, uint8_t channel, void *userData) |
| anonymous enum |
| enum enet_qos_mii_mode_t |
| enum enet_qos_mii_speed_t |
| enum enet_qos_desc_flag |
| enum enet_qos_systime_op |
These control flags are provided for special user requirements. Normally, these is no need to set this control flags for ENET initialization. But if you have some special requirements, set the flags to specialControl in the enet_qos_config_t.
This enumeration uses one-bot encoding to allow a logical OR of multiple members.
This enumeration uses one-bot encoding to allow a logical OR of multiple members.
| enum enet_qos_event_t |
| void ENET_QOS_GetDefaultConfig | ( | enet_qos_config_t * | config | ) |
The purpose of this API is to get the default ENET configure structure for ENET_QOS_Init(). User may use the initialized structure unchanged in ENET_QOS_Init(), or modify some fields of the structure before calling ENET_QOS_Init(). Example:
| config | The ENET mac controller configuration structure pointer. |
| status_t ENET_QOS_Up | ( | ENET_QOS_Type * | base, |
| const enet_qos_config_t * | config, | ||
| uint8_t * | macAddr, | ||
| uint8_t | macCount, | ||
| uint32_t | refclkSrc_Hz | ||
| ) |
This function initializes it with the ENET basic configuration.
| base | ENET peripheral base address. |
| config | ENET mac configuration structure pointer. The "enet_qos_config_t" type mac configuration return from ENET_QOS_GetDefaultConfig can be used directly. It is also possible to verify the Mac configuration using other methods. |
| macAddr | Pointer to ENET mac address array of Ethernet device. This MAC address should be provided. |
| macCount | Count of macAddr in the ENET mac address array |
| refclkSrc_Hz | ENET input reference clock. |
| status_t ENET_QOS_Init | ( | ENET_QOS_Type * | base, |
| const enet_qos_config_t * | config, | ||
| uint8_t * | macAddr, | ||
| uint8_t | macCount, | ||
| uint32_t | refclkSrc_Hz | ||
| ) |
This function ungates the module clock and initializes it with the ENET basic configuration.
| base | ENET peripheral base address. |
| config | ENET mac configuration structure pointer. The "enet_qos_config_t" type mac configuration return from ENET_QOS_GetDefaultConfig can be used directly. It is also possible to verify the Mac configuration using other methods. |
| macAddr | Pointer to ENET mac address array of Ethernet device. This MAC address should be provided. |
| macCount | Count of macAddr in the ENET mac address array |
| refclkSrc_Hz | ENET input reference clock. |
| void ENET_QOS_Down | ( | ENET_QOS_Type * | base | ) |
This function disables the ENET module.
param base ENET peripheral base address.
| void ENET_QOS_Deinit | ( | ENET_QOS_Type * | base | ) |
This function gates the module clock and disables the ENET module.
| base | ENET peripheral base address. |
| uint32_t ENET_QOS_GetInstance | ( | ENET_QOS_Type * | base | ) |
| base | ENET peripheral base address. |
| status_t ENET_QOS_DescriptorInit | ( | ENET_QOS_Type * | base, |
| enet_qos_config_t * | config, | ||
| enet_qos_buffer_config_t * | bufferConfig | ||
| ) |
| base | ENET peripheral base address. |
| config | The configuration for ENET. |
| bufferConfig | All buffers configuration. |
| void ENET_QOS_StartRxTx | ( | ENET_QOS_Type * | base, |
| uint8_t | txRingNum, | ||
| uint8_t | rxRingNum | ||
| ) |
This function enable the tx/rx and starts the rx/tx DMA. This shall be set after ENET initialization and before starting to receive the data.
| base | ENET peripheral base address. |
| rxRingNum | The number of the used rx rings. It shall not be larger than the ENET_QOS_RING_NUM_MAX(2). If the ringNum is set with 1, the ring 0 will be used. |
| txRingNum | The number of the used tx rings. It shall not be larger than the ENET_QOS_RING_NUM_MAX(2). If the ringNum is set with 1, the ring 0 will be used. |
|
inlinestatic |
This API is provided to dynamically change the speed and duplex for MAC.
| base | ENET peripheral base address. |
| speed | The speed of the RMII mode. |
| duplex | The duplex of the RMII mode. |
| void ENET_QOS_SetSMI | ( | ENET_QOS_Type * | base, |
| uint32_t | csrClock_Hz | ||
| ) |
| base | ENET peripheral base address. |
| csrClock_Hz | CSR clock frequency in HZ |
|
inlinestatic |
| base | ENET peripheral base address. |
|
inlinestatic |
| base | ENET peripheral base address. |
| void ENET_QOS_StartSMIRead | ( | ENET_QOS_Type * | base, |
| uint32_t | phyAddr, | ||
| uint32_t | phyReg | ||
| ) |
support both MDIO IEEE802.3 Clause 22 and clause 45.
| base | ENET peripheral base address. |
| phyAddr | The PHY address. |
| phyReg | The PHY register. |
| void ENET_QOS_StartSMIWrite | ( | ENET_QOS_Type * | base, |
| uint32_t | phyAddr, | ||
| uint32_t | phyReg, | ||
| uint32_t | data | ||
| ) |
support both MDIO IEEE802.3 Clause 22 and clause 45.
| base | ENET peripheral base address. |
| phyAddr | The PHY address. |
| phyReg | The PHY register. |
| data | The data written to PHY. |
|
inlinestatic |
| base | ENET peripheral base address. |
| macAddr | The six-byte Mac address pointer. The pointer is allocated by application and input into the API. |
| index | Configure macAddr to MAC_ADDRESS[index] register. |
| void ENET_QOS_GetMacAddr | ( | ENET_QOS_Type * | base, |
| uint8_t * | macAddr, | ||
| uint8_t | index | ||
| ) |
| base | ENET peripheral base address. |
| macAddr | The six-byte Mac address pointer. The pointer is allocated by application and input into the API. |
| index | Get macAddr from MAC_ADDRESS[index] register. |
| void ENET_QOS_AddMulticastGroup | ( | ENET_QOS_Type * | base, |
| uint8_t * | address | ||
| ) |
| base | ENET_QOS peripheral base address. |
| address | The six-byte multicast group address which is provided by application. |
| void ENET_QOS_LeaveMulticastGroup | ( | ENET_QOS_Type * | base, |
| uint8_t * | address | ||
| ) |
param base ENET_QOS peripheral base address. param address The six-byte multicast group address which is provided by application.
|
inlinestatic |
| base | ENET peripheral base address. |
|
inlinestatic |
| base | ENET peripheral base address. |
| void ENET_QOS_EnterPowerDown | ( | ENET_QOS_Type * | base, |
| uint32_t * | wakeFilter | ||
| ) |
the remote power wake up frame and magic frame can wake up the ENET from the power down mode.
| base | ENET peripheral base address. |
| wakeFilter | The wakeFilter provided to configure the wake up frame filter. Set the wakeFilter to NULL is not required. But if you have the filter requirement, please make sure the wakeFilter pointer shall be eight continuous 32-bits configuration. |
|
inlinestatic |
Exit from the power down mode and recover to normal work mode.
| base | ENET peripheral base address. |
| status_t ENET_QOS_EnableRxParser | ( | ENET_QOS_Type * | base, |
| bool | enable | ||
| ) |
| base | ENET_QOS peripheral base address. |
| enable | Enable/Disable Rx parser function |
| kStatus_Success | Configure rx parser success. |
| kStatus_ENET_QOS_Timeout | Poll status flag timeout. |
| void ENET_QOS_EnableInterrupts | ( | ENET_QOS_Type * | base, |
| uint32_t | mask | ||
| ) |
This function enables the ENET interrupt according to the provided mask. The mask is a logical OR of enet_qos_dma_interrupt_enable_t and enet_qos_mac_interrupt_enable_t. For example, to enable the dma and mac interrupt, do the following.
| base | ENET peripheral base address. |
| mask | ENET interrupts to enable. This is a logical OR of both enumeration :: enet_qos_dma_interrupt_enable_t and enet_qos_mac_interrupt_enable_t. |
| void ENET_QOS_DisableInterrupts | ( | ENET_QOS_Type * | base, |
| uint32_t | mask | ||
| ) |
This function disables the ENET interrupt according to the provided mask. The mask is a logical OR of enet_qos_dma_interrupt_enable_t and enet_qos_mac_interrupt_enable_t. For example, to disable the dma and mac interrupt, do the following.
| base | ENET peripheral base address. |
| mask | ENET interrupts to disables. This is a logical OR of both enumeration :: enet_qos_dma_interrupt_enable_t and enet_qos_mac_interrupt_enable_t. |
|
inlinestatic |
| base | ENET peripheral base address. |
| channel | The DMA Channel. Shall not be larger than ENET_QOS_RING_NUM_MAX. |
|
inlinestatic |
| base | ENET peripheral base address. |
| channel | The DMA Channel. Shall not be larger than ENET_QOS_RING_NUM_MAX. |
| mask | The interrupt status to be cleared. This is the logical OR of members of the enumeration :: enet_qos_dma_interrupt_enable_t. |
|
inlinestatic |
| base | ENET peripheral base address. |
| void ENET_QOS_ClearMacInterruptStatus | ( | ENET_QOS_Type * | base, |
| uint32_t | mask | ||
| ) |
This function clears enabled ENET interrupts according to the provided mask. The mask is a logical OR of enumeration members. See the enet_qos_mac_interrupt_enable_t. For example, to clear the TX frame interrupt and RX frame interrupt, do the following.
| base | ENET peripheral base address. |
| mask | ENET interrupt source to be cleared. This is the logical OR of members of the enumeration :: enet_qos_mac_interrupt_enable_t. |
|
inlinestatic |
| txDesc | The given tx descriptor. |
| True | the dma own tx descriptor, false application own tx descriptor. |
| void ENET_QOS_SetupTxDescriptor | ( | enet_qos_tx_bd_struct_t * | txDesc, |
| void * | buffer1, | ||
| uint32_t | bytes1, | ||
| void * | buffer2, | ||
| uint32_t | bytes2, | ||
| uint32_t | framelen, | ||
| bool | intEnable, | ||
| bool | tsEnable, | ||
| enet_qos_desc_flag | flag, | ||
| uint8_t | slotNum | ||
| ) |
This function is a low level functional API to setup or prepare a given tx descriptor.
| txDesc | The given tx descriptor. |
| buffer1 | The first buffer address in the descriptor. |
| bytes1 | The bytes in the fist buffer. |
| buffer2 | The second buffer address in the descriptor. |
| bytes2 | The bytes in the second buffer. |
| framelen | The length of the frame to be transmitted. |
| intEnable | Interrupt enable flag. |
| tsEnable | The timestamp enable. |
| flag | The flag of this tx descriptor, enet_qos_desc_flag . |
| slotNum | The slot num used for AV only. |
|
inlinestatic |
This function is a low level functional API to update the the tx descriptor tail. This is called after you setup a new tx descriptor to update the tail pointer to make the new descriptor accessible by DMA.
| base | ENET peripheral base address. |
| channel | The tx DMA channel. |
| txDescTailAddrAlign | The new tx tail pointer address. |
|
inlinestatic |
This function is a low level functional API to update the the rx descriptor tail. This is called after you setup a new rx descriptor to update the tail pointer to make the new descriptor accessible by DMA and to anouse the rx poll command for DMA.
| base | ENET peripheral base address. |
| channel | The rx DMA channel. |
| rxDescTailAddrAlign | The new rx tail pointer address. |
|
inlinestatic |
This function is a low level functional API to get the the status flag from a given rx descriptor.
| rxDesc | The given rx descriptor. |
| The | RDES3 regions for write-back format rx buffer descriptor. |
| void ENET_QOS_UpdateRxDescriptor | ( | enet_qos_rx_bd_struct_t * | rxDesc, |
| void * | buffer1, | ||
| void * | buffer2, | ||
| bool | intEnable, | ||
| bool | doubleBuffEnable | ||
| ) |
This function is a low level functional API to Updates the buffers and the own status for a given rx descriptor.
| rxDesc | The given rx descriptor. |
| buffer1 | The first buffer address in the descriptor. |
| buffer2 | The second buffer address in the descriptor. |
| intEnable | Interrupt enable flag. |
| doubleBuffEnable | The double buffer enable flag. |
| status_t ENET_QOS_ConfigureRxParser | ( | ENET_QOS_Type * | base, |
| enet_qos_rxp_config_t * | rxpConfig, | ||
| uint16_t | entryCount | ||
| ) |
This function is used to configure the flexible rx parser table.
| base | ENET peripheral base address.. |
| rxpConfig | The rx parser configuration pointer. |
| entryCount | The rx parser entry count. |
| kStatus_Success | Configure rx parser success. |
| kStatus_ENET_QOS_Timeout | Poll status flag timeout. |
| status_t ENET_QOS_ReadRxParser | ( | ENET_QOS_Type * | base, |
| enet_qos_rxp_config_t * | rxpConfig, | ||
| uint16_t | entryIndex | ||
| ) |
This function is used to read flexible rx parser configuration at specified index.
| base | ENET peripheral base address.. |
| rxpConfig | The rx parser configuration pointer. |
| entryIndex | The rx parser entry index to read, start from 0. |
| kStatus_Success | Configure rx parser success. |
| kStatus_ENET_QOS_Timeout | Poll status flag timeout. |
| status_t ENET_QOS_EstProgramGcl | ( | ENET_QOS_Type * | base, |
| enet_qos_est_gcl_t * | gcl, | ||
| uint32_t | ptpClk_Hz | ||
| ) |
This function is used to program the Enhanced Scheduled Transmisson. (IEEE802.1Qbv)
| base | ENET peripheral base address.. |
| gcl | Pointer to the Gate Control List structure. |
| ptpClk_Hz | frequency of the PTP clock. |
| status_t ENET_QOS_EstReadGcl | ( | ENET_QOS_Type * | base, |
| enet_qos_est_gcl_t * | gcl, | ||
| uint32_t | listLen, | ||
| bool | hwList | ||
| ) |
This function is used to read the Enhanced Scheduled Transmisson list. (IEEE802.1Qbv)
| base | ENET peripheral base address.. |
| gcl | Pointer to the Gate Control List structure. |
| listLen | length of the provided opList array in gcl structure. |
| hwList | Boolean if True read HW list, false read SW list. |
|
inlinestatic |
This function is used to enable frame preemption. (IEEE802.1Qbu)
| base | ENET peripheral base address.. |
|
inlinestatic |
This function is used to disable frame preemption. (IEEE802.1Qbu)
| base | ENET peripheral base address.. |
|
inlinestatic |
This function is used to configure the preemptable queues. (IEEE802.1Qbu)
| base | ENET peripheral base address.. |
| queueMask | bitmask representing queues to set in preemptable mode. The N-th bit represents the queue N. |
| void ENET_QOS_AVBConfigure | ( | ENET_QOS_Type * | base, |
| const enet_qos_cbs_config_t * | config, | ||
| uint8_t | queueIndex | ||
| ) |
ENET_QOS AVB feature configuration, set transmit bandwidth. This API is called when the AVB feature is required.
| base | ENET_QOS peripheral base address. |
| config | The ENET_QOS AVB feature configuration structure. |
| queueIndex | ENET_QOS queue index. |
| void ENET_QOS_CreateHandler | ( | ENET_QOS_Type * | base, |
| enet_qos_handle_t * | handle, | ||
| enet_qos_config_t * | config, | ||
| enet_qos_buffer_config_t * | bufferConfig, | ||
| enet_qos_callback_t | callback, | ||
| void * | userData | ||
| ) |
This is a transactional API and it's provided to store all data which are needed during the whole transactional process. This API should not be used when you use functional APIs to do data tx/rx. This is function will store many data/flag for transactional use, so all configure API such as ENET_QOS_Init(), ENET_QOS_DescriptorInit(), ENET_QOS_EnableInterrupts() etc.
| base | ENET peripheral base address. |
| handle | ENET handler. |
| config | ENET configuration. |
| bufferConfig | ENET buffer configuration. |
| callback | The callback function. |
| userData | The application data. |
| status_t ENET_QOS_GetRxFrameSize | ( | ENET_QOS_Type * | base, |
| enet_qos_handle_t * | handle, | ||
| uint32_t * | length, | ||
| uint8_t | channel | ||
| ) |
This function gets a received frame size from the ENET buffer descriptors.
| base | ENET peripheral base address. |
| handle | The ENET handler structure. This is the same handler pointer used in the ENET_QOS_Init. |
| length | The length of the valid frame received. |
| channel | The DMAC channel for the rx. |
| kStatus_ENET_QOS_RxFrameEmpty | No frame received. Should not call ENET_QOS_ReadFrame to read frame. |
| kStatus_ENET_QOS_RxFrameError | Data error happens. ENET_QOS_ReadFrame should be called with NULL data and NULL length to update the receive buffers. |
| kStatus_Success | Receive a frame Successfully then the ENET_QOS_ReadFrame should be called with the right data buffer and the captured data length input. |
| status_t ENET_QOS_ReadFrame | ( | ENET_QOS_Type * | base, |
| enet_qos_handle_t * | handle, | ||
| uint8_t * | data, | ||
| uint32_t | length, | ||
| uint8_t | channel, | ||
| enet_qos_ptp_time_t * | ts | ||
| ) |
This function reads a frame from the ENET DMA descriptors. The ENET_QOS_GetRxFrameSize should be used to get the size of the prepared data buffer. For example use rx dma channel 0:
| base | ENET peripheral base address. |
| handle | The ENET handler structure. This is the same handler pointer used in the ENET_QOS_Init. |
| data | The data buffer provided by user to store the frame which memory size should be at least "length". |
| length | The size of the data buffer which is still the length of the received frame. |
| channel | The rx DMA channel. shall not be larger than 2. |
| ts | Pointer to the structure enet_qos_ptp_time_t to save frame timestamp. |
| status_t ENET_QOS_SendFrame | ( | ENET_QOS_Type * | base, |
| enet_qos_handle_t * | handle, | ||
| uint8_t * | data, | ||
| uint32_t | length, | ||
| uint8_t | channel, | ||
| bool | isNeedTs, | ||
| void * | context | ||
| ) |
| base | ENET peripheral base address. |
| handle | The ENET handler pointer. This is the same handler pointer used in the ENET_QOS_Init. |
| data | The data buffer provided by user to be send. |
| length | The length of the data to be send. |
| channel | Channel to send the frame, same with queue index. |
| isNeedTs | True to enable timestamp save for the frame |
| context | pointer to user context to be kept in the tx dirty frame information. |
| kStatus_Success | Send frame succeed. |
| kStatus_ENET_QOS_TxFrameBusy | Transmit buffer descriptor is busy under transmission. The transmit busy happens when the data send rate is over the MAC capacity. The waiting mechanism is recommended to be added after each call return with kStatus_ENET_QOS_TxFrameBusy. |
| void ENET_QOS_ReclaimTxDescriptor | ( | ENET_QOS_Type * | base, |
| enet_qos_handle_t * | handle, | ||
| uint8_t | channel | ||
| ) |
This function is used to update the tx descriptor status and store the tx timestamp when the 1588 feature is enabled. This is called by the transmit interrupt IRQ handler after the complete of a frame transmission.
| base | ENET peripheral base address. |
| handle | The ENET handler pointer. This is the same handler pointer used in the ENET_QOS_Init. |
| channel | The tx DMA channel. |
| void ENET_QOS_CommonIRQHandler | ( | ENET_QOS_Type * | base, |
| enet_qos_handle_t * | handle | ||
| ) |
| base | ENET peripheral base address. |
| handle | The ENET handler pointer. |
| void ENET_QOS_SetISRHandler | ( | ENET_QOS_Type * | base, |
| enet_qos_isr_t | ISRHandler | ||
| ) |
| base | ENET peripheral base address. |
| ISRHandler | The handler to install. |
| status_t ENET_QOS_Ptp1588CorrectTimerInCoarse | ( | ENET_QOS_Type * | base, |
| enet_qos_systime_op | operation, | ||
| uint32_t | second, | ||
| uint32_t | nanosecond | ||
| ) |
| base | ENET peripheral base address. |
| operation | The system time operation, refer to "enet_qos_systime_op" |
| second | The correction second. |
| nanosecond | The correction nanosecond. |
| status_t ENET_QOS_Ptp1588CorrectTimerInFine | ( | ENET_QOS_Type * | base, |
| uint32_t | addend | ||
| ) |
| base | ENET peripheral base address. |
| addend | The addend value to be set in the fine method |
|
inlinestatic |
| base | ENET peripheral base address. |
| void ENET_QOS_Ptp1588GetTimerNoIRQDisable | ( | ENET_QOS_Type * | base, |
| uint64_t * | second, | ||
| uint32_t * | nanosecond | ||
| ) |
| base | ENET peripheral base address. |
| second | The PTP 1588 system timer second. |
| nanosecond | The PTP 1588 system timer nanosecond. For the unit of the nanosecond is 1ns. so the nanosecond is the real nanosecond. |
|
inlinestatic |
All channels operate in flexible PPS output mode.
| base | ENET peripheral base address. |
| instance | The ENET QOS PTP PPS instance. |
| trgtMode | The target time register mode. |
| cmd | The target flexible PPS output control command. |
| status_t ENET_QOS_Ptp1588PpsSetTrgtTime | ( | ENET_QOS_Type * | base, |
| enet_qos_ptp_pps_instance_t | instance, | ||
| uint32_t | seconds, | ||
| uint32_t | nanoseconds | ||
| ) |
| base | ENET QOS peripheral base address. |
| instance | The ENET QOS PTP PPS instance. |
| seconds | The target seconds. |
| nanoseconds | The target nanoseconds. |
|
inlinestatic |
param base ENET QOS peripheral base address. param instance The ENET QOS PTP PPS instance. param width Signal Width. It is stored in terms of number of units of sub-second increment value. The width value must be lesser than interval value.
|
inlinestatic |
param base ENET QOS peripheral base address. param instance The ENET QOS PTP PPS instance. param interval Signal Interval. It is stored in terms of number of units of sub-second increment value.
| void ENET_QOS_Ptp1588GetTimer | ( | ENET_QOS_Type * | base, |
| uint64_t * | second, | ||
| uint32_t * | nanosecond | ||
| ) |
| base | ENET peripheral base address. |
| second | The PTP 1588 system timer second. |
| nanosecond | The PTP 1588 system timer nanosecond. For the unit of the nanosecond is 1ns.so the nanosecond is the real nanosecond. |
| void ENET_QOS_GetTxFrame | ( | enet_qos_handle_t * | handle, |
| enet_qos_frame_info_t * | txFrame, | ||
| uint8_t | channel | ||
| ) |
This function is used for PTP stack to get the timestamp captured by the ENET driver.
| handle | The ENET handler pointer.This is the same state pointer used in ENET_QOS_Init. |
| txFrame | Input parameter, pointer to enet_qos_frame_info_t for saving read out frame information. |
| channel | Channel for searching the tx frame. |