![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Data Structures | |
struct | flexio_camera_edma_handle_t |
Camera eDMA handle. More... | |
Typedefs | |
typedef void(* | flexio_camera_edma_transfer_callback_t )(FLEXIO_CAMERA_Type *base, flexio_camera_edma_handle_t *handle, status_t status, void *userData) |
Camera transfer callback function. More... | |
Driver version | |
#define | FSL_FLEXIO_CAMERA_EDMA_DRIVER_VERSION (MAKE_VERSION(2, 1, 3)) |
FlexIO Camera EDMA driver version 2.1.3. More... | |
eDMA transactional | |
status_t | FLEXIO_CAMERA_TransferCreateHandleEDMA (FLEXIO_CAMERA_Type *base, flexio_camera_edma_handle_t *handle, flexio_camera_edma_transfer_callback_t callback, void *userData, edma_handle_t *rxEdmaHandle) |
Initializes the Camera handle, which is used in transactional functions. More... | |
status_t | FLEXIO_CAMERA_TransferReceiveEDMA (FLEXIO_CAMERA_Type *base, flexio_camera_edma_handle_t *handle, flexio_camera_transfer_t *xfer) |
Receives data using eDMA. More... | |
void | FLEXIO_CAMERA_TransferAbortReceiveEDMA (FLEXIO_CAMERA_Type *base, flexio_camera_edma_handle_t *handle) |
Aborts the receive data which used the eDMA. More... | |
status_t | FLEXIO_CAMERA_TransferGetReceiveCountEDMA (FLEXIO_CAMERA_Type *base, flexio_camera_edma_handle_t *handle, size_t *count) |
Gets the remaining bytes to be received. More... | |
struct _flexio_camera_edma_handle |
Forward declaration of the handle typedef.
Data Fields | |
flexio_camera_edma_transfer_callback_t | callback |
Callback function. More... | |
void * | userData |
Camera callback function parameter. More... | |
size_t | rxSize |
Total bytes to be received. More... | |
edma_handle_t * | rxEdmaHandle |
The eDMA RX channel used. More... | |
uint8_t | nbytes |
eDMA minor byte transfer count initially configured. More... | |
volatile uint8_t | rxState |
RX transfer state. | |
flexio_camera_edma_transfer_callback_t flexio_camera_edma_handle_t::callback |
void* flexio_camera_edma_handle_t::userData |
size_t flexio_camera_edma_handle_t::rxSize |
edma_handle_t* flexio_camera_edma_handle_t::rxEdmaHandle |
uint8_t flexio_camera_edma_handle_t::nbytes |
#define FSL_FLEXIO_CAMERA_EDMA_DRIVER_VERSION (MAKE_VERSION(2, 1, 3)) |
typedef void(* flexio_camera_edma_transfer_callback_t)(FLEXIO_CAMERA_Type *base, flexio_camera_edma_handle_t *handle, status_t status, void *userData) |
status_t FLEXIO_CAMERA_TransferCreateHandleEDMA | ( | FLEXIO_CAMERA_Type * | base, |
flexio_camera_edma_handle_t * | handle, | ||
flexio_camera_edma_transfer_callback_t | callback, | ||
void * | userData, | ||
edma_handle_t * | rxEdmaHandle | ||
) |
base | Pointer to the FLEXIO_CAMERA_Type. |
handle | Pointer to flexio_camera_edma_handle_t structure. |
callback | The callback function. |
userData | The parameter of the callback function. |
rxEdmaHandle | User requested DMA handle for RX DMA transfer. |
kStatus_Success | Successfully create the handle. |
kStatus_OutOfRange | The FlexIO Camera eDMA type/handle table out of range. |
status_t FLEXIO_CAMERA_TransferReceiveEDMA | ( | FLEXIO_CAMERA_Type * | base, |
flexio_camera_edma_handle_t * | handle, | ||
flexio_camera_transfer_t * | xfer | ||
) |
This function receives data using eDMA. This is a non-blocking function, which returns right away. When all data is received, the receive callback function is called.
base | Pointer to the FLEXIO_CAMERA_Type. |
handle | Pointer to the flexio_camera_edma_handle_t structure. |
xfer | Camera eDMA transfer structure, see flexio_camera_transfer_t. |
kStatus_Success | if succeeded, others failed. |
kStatus_CAMERA_RxBusy | Previous transfer on going. |
void FLEXIO_CAMERA_TransferAbortReceiveEDMA | ( | FLEXIO_CAMERA_Type * | base, |
flexio_camera_edma_handle_t * | handle | ||
) |
This function aborts the receive data which used the eDMA.
base | Pointer to the FLEXIO_CAMERA_Type. |
handle | Pointer to the flexio_camera_edma_handle_t structure. |
status_t FLEXIO_CAMERA_TransferGetReceiveCountEDMA | ( | FLEXIO_CAMERA_Type * | base, |
flexio_camera_edma_handle_t * | handle, | ||
size_t * | count | ||
) |
This function gets the number of bytes still not received.
base | Pointer to the FLEXIO_CAMERA_Type. |
handle | Pointer to the flexio_camera_edma_handle_t structure. |
count | Number of bytes sent so far by the non-blocking transaction. |
kStatus_Success | Succeed get the transfer count. |
kStatus_InvalidArgument | The count parameter is invalid. |