![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
The MCUXpresso SDK provides a driver for the MECC module of MCUXpresso SDK devices.
The MECC64 module supports Single Error Correction and Double Error Detection(SECDED) ECC function to provide reliability for 4 banks On-Chip RAM(OCRAM) access.
This example code shows how to correct single error and detect multiple error using the MECC driver.
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/mecc
Data Structures | |
| struct | mecc_config_t |
| MECC user configuration. More... | |
| struct | mecc_single_error_info_t |
| MECC ocram single error information, including single error address, ECC code, error data and error bit position. More... | |
| struct | mecc_multi_error_info_t |
| MECC ocram multiple error information, including multiple error address, ECC code, error data. More... | |
Variables | |
| bool | mecc_config_t::enableMecc |
| Enable the MECC function. More... | |
| uint32_t | mecc_config_t::Ocram1StartAddress |
| Ocram 1 start address. More... | |
| uint32_t | mecc_config_t::Ocram1EndAddress |
| Ocram 1 end address. More... | |
| uint32_t | mecc_config_t::Ocram2StartAddress |
| Ocram 2 start address. More... | |
| uint32_t | mecc_config_t::Ocram2EndAddress |
| Ocram 2 end address. More... | |
| uint32_t | mecc_single_error_info_t::singleErrorAddress |
| Single error address on Ocram bank n. | |
| uint32_t | mecc_single_error_info_t::singleErrorDataLow |
| Single error low 32 bits uncorrected read data on Ocram bank n. | |
| uint32_t | mecc_single_error_info_t::singleErrorDataHigh |
| Single error high 32 bits uncorrected read data on Ocram bank n. | |
| uint32_t | mecc_single_error_info_t::singleErrorPosLow |
| Single error bit postion of low 32 bits read data on Ocram bank n. | |
| uint32_t | mecc_single_error_info_t::singleErrorPosHigh |
| Single error bit postion of high 32 bits read data on Ocram bank n. | |
| uint8_t | mecc_single_error_info_t::singleErrorEccCode |
| Single error ECC code on Ocram bank n. | |
| uint32_t | mecc_multi_error_info_t::multiErrorAddress |
| Multiple error address on Ocram bank n. | |
| uint32_t | mecc_multi_error_info_t::multiErrorDataLow |
| Multiple error low 32 bits read data on Ocram bank n. | |
| uint32_t | mecc_multi_error_info_t::multiErrorDataHigh |
| Multiple error high 32 bits read data on Ocram bank n. | |
| uint8_t | mecc_multi_error_info_t::multiErrorEccCode |
| Multiple error ECC code on Ocram bank n. | |
Driver version | |
| #define | FSL_MECC_DRIVER_VERSION (MAKE_VERSION(2U, 0U, 1U)) |
| Driver version 2.0.1. More... | |
Initialization and deinitialization | |
| void | MECC_Init (MECC_Type *base, mecc_config_t *config) |
| MECC module initialization function. More... | |
| void | MECC_Deinit (MECC_Type *base) |
| Deinitializes the MECC. More... | |
| void | MECC_GetDefaultConfig (mecc_config_t *config) |
| Sets the MECC configuration structure to default values. More... | |
Status | |
| static uint32_t | MECC_GetStatusFlags (MECC_Type *base) |
| Gets MECC status flags. More... | |
| static void | MECC_ClearStatusFlags (MECC_Type *base, uint32_t mask) |
| MECC module clear interrupt status. More... | |
| static void | MECC_EnableInterruptStatus (MECC_Type *base, uint32_t mask) |
| MECC module enable interrupt status. More... | |
| static void | MECC_DisableInterruptStatus (MECC_Type *base, uint32_t mask) |
| MECC module disable interrupt status. More... | |
Interrupts | |
| static void | MECC_EnableInterrupts (MECC_Type *base, uint32_t mask) |
| MECC module enable interrupt. More... | |
| static void | MECC_DisableInterrupts (MECC_Type *base, uint32_t mask) |
| MECC module disable interrupt. More... | |
functional | |
| status_t | MECC_ErrorInjection (MECC_Type *base, uint32_t lowerrordata, uint32_t higherrordata, uint8_t eccdata, uint8_t banknumber) |
| MECC module error injection. More... | |
| status_t | MECC_GetSingleErrorInfo (MECC_Type *base, mecc_single_error_info_t *info, uint8_t banknumber) |
| MECC module get single error information. More... | |
| status_t | MECC_GetMultiErrorInfo (MECC_Type *base, mecc_multi_error_info_t *info, uint8_t banknumber) |
| MECC module get multiple error information. More... | |
| struct mecc_config_t |
Data Fields | |
| bool | enableMecc |
| Enable the MECC function. More... | |
| uint32_t | Ocram1StartAddress |
| Ocram 1 start address. More... | |
| uint32_t | Ocram1EndAddress |
| Ocram 1 end address. More... | |
| uint32_t | Ocram2StartAddress |
| Ocram 2 start address. More... | |
| uint32_t | Ocram2EndAddress |
| Ocram 2 end address. More... | |
| struct mecc_single_error_info_t |
Data Fields | |
| uint32_t | singleErrorAddress |
| Single error address on Ocram bank n. | |
| uint32_t | singleErrorDataLow |
| Single error low 32 bits uncorrected read data on Ocram bank n. | |
| uint32_t | singleErrorDataHigh |
| Single error high 32 bits uncorrected read data on Ocram bank n. | |
| uint32_t | singleErrorPosLow |
| Single error bit postion of low 32 bits read data on Ocram bank n. | |
| uint32_t | singleErrorPosHigh |
| Single error bit postion of high 32 bits read data on Ocram bank n. | |
| uint8_t | singleErrorEccCode |
| Single error ECC code on Ocram bank n. | |
| struct mecc_multi_error_info_t |
Data Fields | |
| uint32_t | multiErrorAddress |
| Multiple error address on Ocram bank n. | |
| uint32_t | multiErrorDataLow |
| Multiple error low 32 bits read data on Ocram bank n. | |
| uint32_t | multiErrorDataHigh |
| Multiple error high 32 bits read data on Ocram bank n. | |
| uint8_t | multiErrorEccCode |
| Multiple error ECC code on Ocram bank n. | |
| #define FSL_MECC_DRIVER_VERSION (MAKE_VERSION(2U, 0U, 1U)) |
| anonymous enum |
This structure contains the settings for all of the MECC interrupt configurations.
| anonymous enum |
This structure contains the settings for all of the MECC interrupt status configurations.
| anonymous enum |
This provides constants for the MECC status flags for use in the MECC functions.
| anonymous enum |
| anonymous enum |
| void MECC_Init | ( | MECC_Type * | base, |
| mecc_config_t * | config | ||
| ) |
| base | MECC base address. |
| config | pointer to the MECC configuration structure. |
| void MECC_Deinit | ( | MECC_Type * | base | ) |
| base | MECC base address. |
| void MECC_GetDefaultConfig | ( | mecc_config_t * | config | ) |
| config | pointer to the MECC configuration structure. |
|
inlinestatic |
| base | MECC peripheral base address. |
|
inlinestatic |
| base | MECC base address. |
| mask | status to clear. |
|
inlinestatic |
| base | MECC base address. |
| mask | status to enable. |
|
inlinestatic |
| base | MECC base address. |
| mask | status to disable. |
|
inlinestatic |
| base | MECC base address. |
| mask | The interrupts to enable. |
|
inlinestatic |
| base | MECC base address. |
| mask | The interrupts to disable. |
| status_t MECC_ErrorInjection | ( | MECC_Type * | base, |
| uint32_t | lowerrordata, | ||
| uint32_t | higherrordata, | ||
| uint8_t | eccdata, | ||
| uint8_t | banknumber | ||
| ) |
| base | MECC base address. |
| lowerrordata | low 32 bits data. |
| higherrordata | high 32 bits data. |
| eccdata | ecc code. |
| banknumber | ocram bank number. |
| kStatus_Success. | Bank0: ocram_base_address+0x20*i Bank1: ocram_base_address+0x20*i+0x8 Bank2: ocram_base_address+0x20*i+0x10 Bank3: ocram_base_address+0x20*i+0x18 i = 0,1,2,3,4..... |
| status_t MECC_GetSingleErrorInfo | ( | MECC_Type * | base, |
| mecc_single_error_info_t * | info, | ||
| uint8_t | banknumber | ||
| ) |
| base | MECC base address. |
| info | single error information. |
| banknumber | ocram bank number. |
| kStatus_Success. | |
| kStatus_MECC_BankMiss. | Bank0: ocram_base_address+0x20*i Bank1: ocram_base_address+0x20*i+0x8 Bank2: ocram_base_address+0x20*i+0x10 Bank3: ocram_base_address+0x20*i+0x18 i = 0,1,2,3,4..... |
| status_t MECC_GetMultiErrorInfo | ( | MECC_Type * | base, |
| mecc_multi_error_info_t * | info, | ||
| uint8_t | banknumber | ||
| ) |
| base | MECC base address. |
| info | multiple error information. |
| banknumber | ocram bank number. |
| kStatus_Success. | |
| kStatus_MECC_BankMiss. | Bank0: ocram_base_address+0x20*i Bank1: ocram_base_address+0x20*i+0x8 Bank2: ocram_base_address+0x20*i+0x10 Bank3: ocram_base_address+0x20*i+0x18 i = 0,1,2,3,4..... |
| bool mecc_config_t::enableMecc |
| uint32_t mecc_config_t::Ocram1StartAddress |
| uint32_t mecc_config_t::Ocram1EndAddress |
| uint32_t mecc_config_t::Ocram2StartAddress |
| uint32_t mecc_config_t::Ocram2EndAddress |