![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Data Structures | |
struct | sgtl_audio_format_t |
Audio format configuration. More... | |
struct | sgtl_config_t |
Initailize structure of sgtl5000. More... | |
struct | sgtl_handle_t |
SGTL codec handler. More... | |
Macros | |
#define | CHIP_ID 0x0000U |
Define the register address of sgtl5000. More... | |
#define | SGTL5000_HEADPHONE_MAX_VOLUME_VALUE 0x7FU |
SGTL5000 volume setting range. | |
#define | SGTL5000_I2C_ADDR 0x0A |
SGTL5000 I2C address. More... | |
#define | SGTL_I2C_HANDLER_SIZE CODEC_I2C_MASTER_HANDLER_SIZE |
sgtl handle size | |
#define | SGTL_I2C_BITRATE 100000U |
sgtl i2c baudrate | |
Functions | |
status_t | SGTL_Init (sgtl_handle_t *handle, sgtl_config_t *config) |
sgtl5000 initialize function. More... | |
status_t | SGTL_SetDataRoute (sgtl_handle_t *handle, sgtl_route_t route) |
Set audio data route in sgtl5000. More... | |
status_t | SGTL_SetProtocol (sgtl_handle_t *handle, sgtl_protocol_t protocol) |
Set the audio transfer protocol. More... | |
void | SGTL_SetMasterSlave (sgtl_handle_t *handle, bool master) |
Set sgtl5000 as master or slave. More... | |
status_t | SGTL_SetVolume (sgtl_handle_t *handle, sgtl_module_t module, uint32_t volume) |
Set the volume of different modules in sgtl5000. More... | |
uint32_t | SGTL_GetVolume (sgtl_handle_t *handle, sgtl_module_t module) |
Get the volume of different modules in sgtl5000. More... | |
status_t | SGTL_SetMute (sgtl_handle_t *handle, sgtl_module_t module, bool mute) |
Mute/unmute modules in sgtl5000. More... | |
status_t | SGTL_EnableModule (sgtl_handle_t *handle, sgtl_module_t module) |
Enable expected devices. More... | |
status_t | SGTL_DisableModule (sgtl_handle_t *handle, sgtl_module_t module) |
Disable expected devices. More... | |
status_t | SGTL_Deinit (sgtl_handle_t *handle) |
Deinit the sgtl5000 codec. More... | |
status_t | SGTL_ConfigDataFormat (sgtl_handle_t *handle, uint32_t mclk, uint32_t sample_rate, uint32_t bits) |
Configure the data format of audio data. More... | |
status_t | SGTL_SetPlay (sgtl_handle_t *handle, uint32_t playSource) |
select SGTL codec play source. More... | |
status_t | SGTL_SetRecord (sgtl_handle_t *handle, uint32_t recordSource) |
select SGTL codec record source. More... | |
status_t | SGTL_WriteReg (sgtl_handle_t *handle, uint16_t reg, uint16_t val) |
Write register to sgtl using I2C. More... | |
status_t | SGTL_ReadReg (sgtl_handle_t *handle, uint16_t reg, uint16_t *val) |
Read register from sgtl using I2C. More... | |
status_t | SGTL_ModifyReg (sgtl_handle_t *handle, uint16_t reg, uint16_t clr_mask, uint16_t val) |
Modify some bits in the register using I2C. More... | |
Driver version | |
#define | FSL_SGTL5000_DRIVER_VERSION (MAKE_VERSION(2, 1, 1)) |
CLOCK driver version 2.1.1. More... | |
struct sgtl_audio_format_t |
Data Fields | |
uint32_t | mclk_HZ |
master clock | |
uint32_t | sampleRate |
Sample rate. | |
uint32_t | bitWidth |
Bit width. | |
sgtl_sclk_edge_t | sclkEdge |
sclk valid edge | |
struct sgtl_config_t |
Data Fields | |
sgtl_route_t | route |
Audio data route. More... | |
sgtl_protocol_t | bus |
Audio transfer protocol. | |
bool | master_slave |
Master or slave. More... | |
sgtl_audio_format_t | format |
audio format | |
uint8_t | slaveAddress |
code device slave address | |
codec_i2c_config_t | i2cConfig |
i2c bus configuration | |
sgtl_route_t sgtl_config_t::route |
bool sgtl_config_t::master_slave |
True means master, false means slave.
struct sgtl_handle_t |
Data Fields | |
sgtl_config_t * | config |
sgtl config pointer | |
uint8_t | i2cHandle [SGTL_I2C_HANDLER_SIZE] |
i2c handle | |
#define FSL_SGTL5000_DRIVER_VERSION (MAKE_VERSION(2, 1, 1)) |
#define CHIP_ID 0x0000U |
#define SGTL5000_I2C_ADDR 0x0A |
enum sgtl_module_t |
enum sgtl_route_t |
enum sgtl_protocol_t |
anonymous enum |
anonymous enum |
anonymous enum |
enum sgtl_sclk_edge_t |
status_t SGTL_Init | ( | sgtl_handle_t * | handle, |
sgtl_config_t * | config | ||
) |
This function calls SGTL_I2CInit(), and in this function, some configurations are fixed. The second parameter can be NULL. If users want to change the SGTL5000 settings, a configure structure should be prepared.
handle | Sgtl5000 handle structure. |
config | sgtl5000 configuration structure. If this pointer equals to NULL, it means using the default configuration. |
status_t SGTL_SetDataRoute | ( | sgtl_handle_t * | handle, |
sgtl_route_t | route | ||
) |
This function would set the data route according to route. The route cannot be combined, as all route would enable different modules.
handle | Sgtl5000 handle structure. |
route | Audio data route in sgtl5000. |
status_t SGTL_SetProtocol | ( | sgtl_handle_t * | handle, |
sgtl_protocol_t | protocol | ||
) |
Sgtl5000 only supports I2S, I2S left, I2S right, PCM A, PCM B format.
handle | Sgtl5000 handle structure. |
protocol | Audio data transfer protocol. |
void SGTL_SetMasterSlave | ( | sgtl_handle_t * | handle, |
bool | master | ||
) |
handle | Sgtl5000 handle structure. |
master | 1 represent master, 0 represent slave. |
status_t SGTL_SetVolume | ( | sgtl_handle_t * | handle, |
sgtl_module_t | module, | ||
uint32_t | volume | ||
) |
This function would set the volume of sgtl5000 modules. This interface set module volume. The function assume that left channel and right channel has the same volume.
kSGTL_ModuleADC volume range: 0 - 0xF, 0dB - 22.5dB kSGTL_ModuleDAC volume range: 0x3C - 0xF0, 0dB - -90dB kSGTL_ModuleHP volume range: 0 - 0x7F, 12dB - -51.5dB kSGTL_ModuleLineOut volume range: 0 - 0x1F, 0.5dB steps
handle | Sgtl5000 handle structure. |
module | Sgtl5000 module, such as DAC, ADC and etc. |
volume | Volume value need to be set. The value is the exact value in register. |
uint32_t SGTL_GetVolume | ( | sgtl_handle_t * | handle, |
sgtl_module_t | module | ||
) |
This function gets the volume of sgtl5000 modules. This interface get DAC module volume. The function assume that left channel and right channel has the same volume.
handle | Sgtl5000 handle structure. |
module | Sgtl5000 module, such as DAC, ADC and etc. |
status_t SGTL_SetMute | ( | sgtl_handle_t * | handle, |
sgtl_module_t | module, | ||
bool | mute | ||
) |
handle | Sgtl5000 handle structure. |
module | Sgtl5000 module, such as DAC, ADC and etc. |
mute | True means mute, and false means unmute. |
status_t SGTL_EnableModule | ( | sgtl_handle_t * | handle, |
sgtl_module_t | module | ||
) |
handle | Sgtl5000 handle structure. |
module | Module expected to enable. |
status_t SGTL_DisableModule | ( | sgtl_handle_t * | handle, |
sgtl_module_t | module | ||
) |
handle | Sgtl5000 handle structure. |
module | Module expected to enable. |
status_t SGTL_Deinit | ( | sgtl_handle_t * | handle | ) |
Shut down Sgtl5000 modules.
handle | Sgtl5000 handle structure pointer. |
status_t SGTL_ConfigDataFormat | ( | sgtl_handle_t * | handle, |
uint32_t | mclk, | ||
uint32_t | sample_rate, | ||
uint32_t | bits | ||
) |
This function would configure the registers about the sample rate, bit depths.
handle | Sgtl5000 handle structure pointer. |
mclk | Master clock frequency of I2S. |
sample_rate | Sample rate of audio file running in sgtl5000. Sgtl5000 now supports 8k, 11.025k, 12k, 16k, 22.05k, 24k, 32k, 44.1k, 48k and 96k sample rate. |
bits | Bit depth of audio file (Sgtl5000 only supports 16bit, 20bit, 24bit and 32 bit in HW). |
status_t SGTL_SetPlay | ( | sgtl_handle_t * | handle, |
uint32_t | playSource | ||
) |
handle | Sgtl5000 handle structure pointer. |
playSource | play source value, reference _sgtl_play_source. |
status_t SGTL_SetRecord | ( | sgtl_handle_t * | handle, |
uint32_t | recordSource | ||
) |
handle | Sgtl5000 handle structure pointer. |
recordSource | record source value, reference _sgtl_record_source. |
status_t SGTL_WriteReg | ( | sgtl_handle_t * | handle, |
uint16_t | reg, | ||
uint16_t | val | ||
) |
handle | Sgtl5000 handle structure. |
reg | The register address in sgtl. |
val | Value needs to write into the register. |
status_t SGTL_ReadReg | ( | sgtl_handle_t * | handle, |
uint16_t | reg, | ||
uint16_t * | val | ||
) |
handle | Sgtl5000 handle structure. |
reg | The register address in sgtl. |
val | Value written to. |
status_t SGTL_ModifyReg | ( | sgtl_handle_t * | handle, |
uint16_t | reg, | ||
uint16_t | clr_mask, | ||
uint16_t | val | ||
) |
handle | Sgtl5000 handle structure. |
reg | The register address in sgtl. |
clr_mask | The mask code for the bits want to write. The bit you want to write should be 0. |
val | Value needs to write into the register. |