The MCUXpresso SDK provides a driver for the General Purpose Timer Module (GPT) of MCUXpresso SDK devices.
Function groups
The GPT driver supports the generation of one-shot pulse/edge, PWM signals, and input capture modes.
Initialization and deinitialization
The function GPT_Init() initializes the GPT with specified configurations. The function GPT_GetDefaultConfig() gets the default configurations. The initialization function configures the GPT for the requested parameters.
The function GPT_Deinit() disables the GPT counter and turns off the module clock.
Input capture operations
The function GPT_SetupInputCapture() sets up a GPT channel for the input capture. The user can specify the capture edge and a filter value to be used when processing the input signal.
The function GPT_TriggerInputCapture() can be used to trigger the capture by software.
One-shot operations
The function GPT_SetupOneshotPulse() sets up a GPT channel for one-shot pulse generation on the output pin.
The function GPT_SetupOneshotEdge() sets up a GPT channel for one-shot edge toggle on the output pin.
PWM Operations
The function GPT_SetupPwm() sets up GPT channels for the PWM output. The function sets up the PWM signal properties for 1 of 6 channels. Each channel has its own period, duty cycle and polarity specified. However, the same counter is applied to all channels requesting the PWM output. The signal duty cycle is provided as a percentage of the PWM period. Its value should be between 0 and 100 0=inactive signal (0% duty cycle) and 100=always active signal (100% duty cycle).
The function GPT_UpdatePwmDutycycle() updates the PWM signal duty cycle of a particular GPT channel. The update will take effect on the end of PWM period. If it's called again before last update doesn't take effect, error will be returned.
The function GPT_PausePwm() pauses the PWM signal on particular GPT channel. This can be used to disable the PWM output when making changes to the PWM signal. Pause will also take effect on the end of PWM period, so check the return value to see if it's set correctly.
Typical use case
PWM output
Output a PWM signal on two GPT channels with different duty cycles. Periodically update the PWM signal duty cycle. Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/gpt
|
| enum | gpt_chnl_t {
kGPT_Chnl_0 = 0U,
kGPT_Chnl_1,
kGPT_Chnl_2,
kGPT_Chnl_3,
kGPT_Chnl_4,
kGPT_Chnl_5
} |
| | List of GPT channels. More...
|
| |
| enum | gpt_chnl_pol_t {
kGPT_ChnlPol_Low = 0U,
kGPT_ChnlPol_High
} |
| | GPT channel polarity. More...
|
| |
| enum | gpt_pwm_mode_t {
kGPT_EdgeAlignedPwm = 0U,
kGPT_CenterAlignedPwm
} |
| | GPT PWM operation modes. More...
|
| |
| enum | gpt_input_capture_edge_t {
kGPT_RisingEdge = 0U,
kGPT_FallingEdge
} |
| | GPT input capture edge. More...
|
| |
| enum | gpt_input_capture_filter_t {
kGPT_InputCapFilter_None = 0U,
kGPT_InputCapFilter_2Cycles,
kGPT_InputCapFilter_3Cycles,
kGPT_InputCapFilter_4Cycles,
kGPT_InputCapFilter_5Cycles,
kGPT_InputCapFilter_6Cycles,
kGPT_InputCapFilter_7Cycles
} |
| | GPT input capture edge. More...
|
| |
| enum | gpt_clock_source_t {
kGPT_SystemClock = 0U,
kGPT_ExternalClock
} |
| | GPT clock source selection. More...
|
| |
| enum | gpt_clock_div_t {
kGPT_ClkDiv_Divide_1 = 0U,
kGPT_ClkDiv_Divide_2,
kGPT_ClkDiv_Divide_4,
kGPT_ClkDiv_Divide_8,
kGPT_ClkDiv_Divide_16,
kGPT_ClkDiv_Divide_32,
kGPT_ClkDiv_Divide_64,
kGPT_ClkDiv_Divide_128,
kGPT_ClkDiv_Divide_256,
kGPT_ClkDiv_Divide_512,
kGPT_ClkDiv_Divide_1024,
kGPT_ClkDiv_Divide_2048,
kGPT_ClkDiv_Divide_4096,
kGPT_ClkDiv_Divide_8192,
kGPT_ClkDiv_Divide_16384,
kGPT_ClkDiv_Divide_32768
} |
| | GPT clock divider factor selection for the clock source. More...
|
| |
| enum | gpt_interrupt_enable_t {
kGPT_Chnl0InterruptEnable = (1U << 0),
kGPT_Chnl1InterruptEnable = (1U << 1),
kGPT_Chnl2InterruptEnable = (1U << 2),
kGPT_Chnl3InterruptEnable = (1U << 3),
kGPT_Chnl4InterruptEnable = (1U << 4),
kGPT_Chnl5InterruptEnable = (1U << 5),
kGPT_Chnl0ErrInterruptEnable = (1U << 8),
kGPT_Chnl1ErrInterruptEnable = (1U << 9),
kGPT_Chnl2ErrInterruptEnable = (1U << 10),
kGPT_Chnl3ErrInterruptEnable = (1U << 11),
kGPT_Chnl4ErrInterruptEnable = (1U << 12),
kGPT_Chnl5ErrInterruptEnable = (1U << 13),
kGPT_TimeOverflowInterruptEnable = (1U << 16),
kGPT_Dma0OverflowInterruptEnable = (1U << 24),
kGPT_Dma1OverflowInterruptEnable = (1U << 25),
kGPT_AllInterruptsEnable = 0x3013F3FUL
} |
| | List of GPT interrupts. More...
|
| |
| enum | gpt_status_flags_t {
kGPT_Chnl0Flag = (1U << 0),
kGPT_Chnl1Flag = (1U << 1),
kGPT_Chnl2Flag = (1U << 2),
kGPT_Chnl3Flag = (1U << 3),
kGPT_Chnl4Flag = (1U << 4),
kGPT_Chnl5Flag = (1U << 5),
kGPT_Chnl0ErrFlag = (1U << 8),
kGPT_Chnl1ErrFlag = (1U << 9),
kGPT_Chnl2ErrFlag = (1U << 10),
kGPT_Chnl3ErrFlag = (1U << 11),
kGPT_Chnl4ErrFlag = (1U << 12),
kGPT_Chnl5ErrFlag = (1U << 13),
kGPT_TimeOverflowFlag = (1U << 16),
kGPT_Dma0OverflowFlag = (1U << 24),
kGPT_Dma1OverflowFlag = (1U << 25),
kGPT_AllFlags = 0x3013F3FUL
} |
| | List of GPT flags. More...
|
| |
| enum | gpt_cnt_update_mode_t {
kGPT_CntUpdateMode_Normal = 0U,
kGPT_CntUpdateMode_Fast = 1U,
kGPT_CntUpdateMode_Off = 3U
} |
| | GPT counter update mode. More...
|
| |
| enum | gpt_input_capture_div_t {
kGPT_SampClkDiv_Divide_1 = 0U,
kGPT_SampClkDiv_Divide_2,
kGPT_SampClkDiv_Divide_4,
kGPT_SampClkDiv_Divide_8,
kGPT_SampClkDiv_Divide_16,
kGPT_SampClkDiv_Divide_32,
kGPT_SampClkDiv_Divide_64,
kGPT_SampClkDiv_Divide_128
} |
| | GPT sample clock divider factor selection. More...
|
| |
|
| void | GPT_SetupInputCapture (GPT_Type *base, gpt_chnl_t chnlNumber, gpt_input_capture_edge_t captureMode) |
| | Enables capturing an input signal on the channel using the function parameters. More...
|
| |
| void | GPT_TriggerInputCapture (GPT_Type *base, gpt_chnl_t chnlNumber) |
| | Trigger input capturing by software. More...
|
| |
| uint32_t | GPT_GetCapturedValue (GPT_Type *base, gpt_chnl_t chnlNumber) |
| | Get captured value. More...
|
| |
| void | GPT_SetupOneshotPulse (GPT_Type *base, gpt_chnl_t chnlNumber, gpt_chnl_pol_t pol, uint32_t delayTicks, uint32_t dutyTicks) |
| | Configures one-shot pulse on the channel. More...
|
| |
| void | GPT_SetupOneshotEdge (GPT_Type *base, gpt_chnl_t chnlNumber, gpt_chnl_pol_t pol, uint32_t delayTicks) |
| | Configures one-shot edge on the channel. More...
|
| |
| status_t | GPT_SetupPwm (GPT_Type *base, gpt_chnl_t chnlNumber, gpt_chnl_pol_t pol, uint32_t dutyPercent, gpt_pwm_mode_t mode, uint32_t pwmFreq_Hz, uint32_t srcClock_Hz) |
| | Configures the PWM signal parameters. More...
|
| |
| status_t | GPT_SetupPwmMode (GPT_Type *base, gpt_chnl_t chnlNumber, gpt_chnl_pol_t pol, uint32_t periodTicks, uint32_t dutyTicks, gpt_pwm_mode_t mode) |
| | Configures the PWM mode parameters. More...
|
| |
| status_t | GPT_UpdatePwmDutycycle (GPT_Type *base, gpt_chnl_t chnlNumber, uint8_t dutyPercent) |
| | Updates the duty cycle of an active PWM signal. More...
|
| |
| status_t | GPT_PausePwm (GPT_Type *base, gpt_chnl_t chnlNumber) |
| | Pause the PWM signal. More...
|
| |
This structure holds the configuration settings for the GPT peripheral. To initialize this structure to reasonable defaults, call the GPT_GetDefaultConfig() function and pass a pointer to the configuration structure instance.
The configuration structure can be made constant so as to reside in flash.
| bool gpt_config_t::stopCntInDebug |
false: In debug mode, counters are not affected.
| uint32_t gpt_config_t::cntUppVal |
- Note
- Actual number of available channels is SoC dependent
| Enumerator |
|---|
| kGPT_Chnl_0 |
GPT channel number 0.
|
| kGPT_Chnl_1 |
GPT channel number 1.
|
| kGPT_Chnl_2 |
GPT channel number 2.
|
| kGPT_Chnl_3 |
GPT channel number 3.
|
| kGPT_Chnl_4 |
GPT channel number 4.
|
| kGPT_Chnl_5 |
GPT channel number 5.
|
| Enumerator |
|---|
| kGPT_ChnlPol_Low |
Output state reset to 0.
|
| kGPT_ChnlPol_High |
Output state reset to 1.
|
| Enumerator |
|---|
| kGPT_EdgeAlignedPwm |
Edge-aligned PWM.
|
| kGPT_CenterAlignedPwm |
Center-aligned PWM.
|
| Enumerator |
|---|
| kGPT_RisingEdge |
Capture on rising edge only.
|
| kGPT_FallingEdge |
Capture on falling edge only.
|
| Enumerator |
|---|
| kGPT_InputCapFilter_None |
No filter.
|
| kGPT_InputCapFilter_2Cycles |
Filter 2 consecutive cycles.
|
| kGPT_InputCapFilter_3Cycles |
Filter 3 consecutive cycles.
|
| kGPT_InputCapFilter_4Cycles |
Filter 4 consecutive cycles.
|
| kGPT_InputCapFilter_5Cycles |
Filter 5 consecutive cycles.
|
| kGPT_InputCapFilter_6Cycles |
Filter 6 consecutive cycles.
|
| kGPT_InputCapFilter_7Cycles |
Filter 7 consecutive cycles.
|
| Enumerator |
|---|
| kGPT_SystemClock |
System clock from PMU selected.
|
| kGPT_ExternalClock |
External clock from pad.
|
| Enumerator |
|---|
| kGPT_ClkDiv_Divide_1 |
Divide by 1.
|
| kGPT_ClkDiv_Divide_2 |
Divide by 2.
|
| kGPT_ClkDiv_Divide_4 |
Divide by 4.
|
| kGPT_ClkDiv_Divide_8 |
Divide by 8.
|
| kGPT_ClkDiv_Divide_16 |
Divide by 16.
|
| kGPT_ClkDiv_Divide_32 |
Divide by 32.
|
| kGPT_ClkDiv_Divide_64 |
Divide by 64.
|
| kGPT_ClkDiv_Divide_128 |
Divide by 128.
|
| kGPT_ClkDiv_Divide_256 |
Divide by 256.
|
| kGPT_ClkDiv_Divide_512 |
Divide by 512.
|
| kGPT_ClkDiv_Divide_1024 |
Divide by 1024.
|
| kGPT_ClkDiv_Divide_2048 |
Divide by 2048.
|
| kGPT_ClkDiv_Divide_4096 |
Divide by 4096.
|
| kGPT_ClkDiv_Divide_8192 |
Divide by 8192.
|
| kGPT_ClkDiv_Divide_16384 |
Divide by 16384.
|
| kGPT_ClkDiv_Divide_32768 |
Divide by 32768.
|
| Enumerator |
|---|
| kGPT_Chnl0InterruptEnable |
Channel 0 interrupt.
|
| kGPT_Chnl1InterruptEnable |
Channel 1 interrupt.
|
| kGPT_Chnl2InterruptEnable |
Channel 2 interrupt.
|
| kGPT_Chnl3InterruptEnable |
Channel 3 interrupt.
|
| kGPT_Chnl4InterruptEnable |
Channel 4 interrupt.
|
| kGPT_Chnl5InterruptEnable |
Channel 5 interrupt.
|
| kGPT_Chnl0ErrInterruptEnable |
Channel 0 error interrupt.
|
| kGPT_Chnl1ErrInterruptEnable |
Channel 1 error interrupt.
|
| kGPT_Chnl2ErrInterruptEnable |
Channel 2 error interrupt.
|
| kGPT_Chnl3ErrInterruptEnable |
Channel 3 error interrupt.
|
| kGPT_Chnl4ErrInterruptEnable |
Channel 4 error interrupt.
|
| kGPT_Chnl5ErrInterruptEnable |
Channel 5 error interrupt.
|
| kGPT_TimeOverflowInterruptEnable |
Time overflow interrupt.
|
| kGPT_Dma0OverflowInterruptEnable |
DMA0 overflow interrupt.
|
| kGPT_Dma1OverflowInterruptEnable |
DMA1 overflow interrupt.
|
| kGPT_AllInterruptsEnable |
All interrupts.
|
| Enumerator |
|---|
| kGPT_Chnl0Flag |
Channel 0 flag.
|
| kGPT_Chnl1Flag |
Channel 1 flag.
|
| kGPT_Chnl2Flag |
Channel 2 flag.
|
| kGPT_Chnl3Flag |
Channel 3 flag.
|
| kGPT_Chnl4Flag |
Channel 4 flag.
|
| kGPT_Chnl5Flag |
Channel 5 flag.
|
| kGPT_Chnl0ErrFlag |
Channel 0 error flag.
|
| kGPT_Chnl1ErrFlag |
Channel 1 error flag.
|
| kGPT_Chnl2ErrFlag |
Channel 2 error flag.
|
| kGPT_Chnl3ErrFlag |
Channel 3 error flag.
|
| kGPT_Chnl4ErrFlag |
Channel 4 error flag.
|
| kGPT_Chnl5ErrFlag |
Channel 5 error flag.
|
| kGPT_TimeOverflowFlag |
Time overflow flag.
|
| kGPT_Dma0OverflowFlag |
DMA0 overflow flag.
|
| kGPT_Dma1OverflowFlag |
DMA1 overflow flag.
|
| kGPT_AllFlags |
All flags.
|
| Enumerator |
|---|
| kGPT_CntUpdateMode_Normal |
Used in any ratio between counter clock and APB clock.
Every 3-4 counter ticks are updated to CNT_VAL
|
| kGPT_CntUpdateMode_Fast |
Used when counter clock is at least 5 times slower than APB clock.
Every counter tick is updated to CNT_VAL
|
| kGPT_CntUpdateMode_Off |
Do not update to CNT_VAL.
|
| Enumerator |
|---|
| kGPT_SampClkDiv_Divide_1 |
Divide by 1.
|
| kGPT_SampClkDiv_Divide_2 |
Divide by 2.
|
| kGPT_SampClkDiv_Divide_4 |
Divide by 4.
|
| kGPT_SampClkDiv_Divide_8 |
Divide by 8.
|
| kGPT_SampClkDiv_Divide_16 |
Divide by 16.
|
| kGPT_SampClkDiv_Divide_32 |
Divide by 32.
|
| kGPT_SampClkDiv_Divide_64 |
Divide by 64.
|
| kGPT_SampClkDiv_Divide_128 |
Divide by 128.
|
- Note
- This API should be called at the beginning of the application which is using the GPT driver. If the GPT instance has only TPM features, please use the TPM driver.
- Parameters
-
| base | GPT peripheral base address |
| config | Pointer to the user configuration structure. |
- Returns
- kStatus_Success indicates success; Else indicates failure.
| void GPT_Deinit |
( |
GPT_Type * |
base | ) |
|
- Parameters
-
| base | GPT peripheral base address |
The default values are:
* config->prescale = 0U;
* config->stopCntInDebug = true;
* config->cntUppVal = 0xFFFFFFFFU;
*
- Parameters
-
| config | Pointer to the user configuration structure. |
When the edge specified in the captureMode argument occurs on the channel, the GPT counter is captured into the CMR0 register. The user has to read the CMR0 register separately to get this value.
- Parameters
-
| base | GPT peripheral base address |
| chnlNumber | The channel number |
| captureMode | Specifies which edge to capture |
| void GPT_TriggerInputCapture |
( |
GPT_Type * |
base, |
|
|
gpt_chnl_t |
chnlNumber |
|
) |
| |
Edge and filter is ignored.
- Parameters
-
| base | GPT peripheral base address |
| chnlNumber | The channel number |
| uint32_t GPT_GetCapturedValue |
( |
GPT_Type * |
base, |
|
|
gpt_chnl_t |
chnlNumber |
|
) |
| |
- Parameters
-
| base | GPT peripheral base address |
| chnlNumber | The channel number |
- Returns
- The captured counter value.
| void GPT_SetupOneshotPulse |
( |
GPT_Type * |
base, |
|
|
gpt_chnl_t |
chnlNumber, |
|
|
gpt_chnl_pol_t |
pol, |
|
|
uint32_t |
delayTicks, |
|
|
uint32_t |
dutyTicks |
|
) |
| |
- Parameters
-
| base | GPT peripheral base address |
| chnlNumber | The channel number |
| pol | Channel output polarity reset value. |
| delayTicks | Delay width before triggering the pulse, the uint of this value is timer ticks. |
| dutyTicks | Pulse width, the uint of this value is timer ticks. |
- Parameters
-
| base | GPT peripheral base address |
| chnlNumber | The channel number |
| pol | Channel output polarity reset value. |
| delayTicks | Delay width before changing the edge, the uint of this value is timer ticks. |
Call this function to configure the PWM signal period, mode, duty cycle, and edge. Use this function to configure all GPT channels that are used to output a PWM signal.
- Parameters
-
| base | GPT peripheral base address |
| chnlNumber | The channel number. |
| pol | PWM output polarity reset value. |
| dutyPercent | PWM pulse width, value should be between 0 to 100 |
| mode | PWM operation mode, options available in enumeration gpt_pwm_mode_t |
| pwmFreq_Hz | PWM signal frequency in Hz |
| srcClock_Hz | GPT counter clock in Hz |
- Returns
- kStatus_Success if the PWM setup was successful kStatus_Error on failure
Call this function to configure the PWM signal mode, duty cycle in ticks, and edge. Use this function to configure all GPT channels that are used to output a PWM signal. Please note that: This API is similar with GPT_SetupPwm() API, but will not set the timer period, and this API will set channel match value in timer ticks, not period percent.
- Parameters
-
| base | GPT peripheral base address |
| chnlNumber | The channel number. |
| pol | PWM output polarity reset value. |
| periodTicks | PWM period width, the uint of this value is timer ticks. |
| dutyTicks | PWM pulse width, the uint of this value is timer ticks. |
| mode | PWM operation mode, options available in enumeration gpt_pwm_mode_t |
- Returns
- kStatus_Success if the PWM setup was successful kStatus_Error on failure
| status_t GPT_UpdatePwmDutycycle |
( |
GPT_Type * |
base, |
|
|
gpt_chnl_t |
chnlNumber, |
|
|
uint8_t |
dutyPercent |
|
) |
| |
- Parameters
-
| base | GPT peripheral base address |
| chnlNumber | The channel number. |
| dutyPercent | New PWM pulse width; The value should be between 0 to 100 0=inactive signal(0% duty cycle)... 100=active signal (100% duty cycle) |
- Returns
- kStatus_Success if the PWM update was successful kStatus_Error on failure
- Parameters
-
| base | GPT peripheral base address |
| chnlNumber | The channel number. |
- Returns
- kStatus_Success if the PWM update was successful kStatus_Error on failure
| void GPT_EnableInterrupts |
( |
GPT_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
- Parameters
-
| base | GPT peripheral base address |
| mask | The interrupts to enable. This is a logical OR of members of the enumeration gpt_interrupt_enable_t |
| void GPT_DisableInterrupts |
( |
GPT_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
- Parameters
-
| base | GPT peripheral base address |
| mask | The interrupts to enable. This is a logical OR of members of the enumeration gpt_interrupt_enable_t |
| uint32_t GPT_GetEnabledInterrupts |
( |
GPT_Type * |
base | ) |
|
- Parameters
-
| base | GPT peripheral base address |
- Returns
- The enabled interrupts. This is the logical OR of members of the enumeration gpt_interrupt_enable_t
| uint32_t GPT_GetStatusFlags |
( |
GPT_Type * |
base | ) |
|
- Parameters
-
| base | GPT peripheral base address |
- Returns
- The status flags. This is the logical OR of members of the enumeration gpt_status_flags_t
| void GPT_ClearStatusFlags |
( |
GPT_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
- Parameters
-
| base | GPT peripheral base address |
| mask | The status flags to clear. This is a logical OR of members of the enumeration gpt_status_flags_t |
| void GPT_SetTimerPeriod |
( |
GPT_Type * |
base, |
|
|
uint32_t |
ticks |
|
) |
| |
Timers counts from 0 until it equals the count value set here. The count value is written to the CNT_UPP_VAL register. The period update take effects during the next counter-reach-upper event. To guarantee an immediate update, use GPT_ResetTimer() after setting the period.
- Note
- Call the utility macros provided in the fsl_common.h to convert usec or msec to ticks.
- Parameters
-
| base | GPT peripheral base address |
| ticks | A timer period in units of ticks, which should be equal or greater than 1. |
| uint32_t GPT_GetCurrentTimerCount |
( |
GPT_Type * |
base | ) |
|
This function returns the real-time timer counting value in a range from 0 to a timer period.
- Note
- Call the utility macros provided in the fsl_common.h to convert ticks to usec or msec.
- Parameters
-
| base | GPT peripheral base address |
- Returns
- The current counter value in ticks
| void GPT_StartTimer |
( |
GPT_Type * |
base | ) |
|
- Parameters
-
| base | GPT peripheral base address |
| void GPT_StopTimer |
( |
GPT_Type * |
base | ) |
|
- Parameters
-
| base | GPT peripheral base address |
| void GPT_ResetTimer |
( |
GPT_Type * |
base | ) |
|
- Parameters
-
| base | GPT peripheral base address |