![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Functions | |
| void | FSP_CorrelateF32 (FSP_Type *base, float32_t *p_src_a, uint32_t srcALen, float32_t *p_src_b, uint32_t srcBLen, float32_t *p_dst) |
| Correlation of floating-point sequences. More... | |
| void | FSP_CorrelateQ31 (FSP_Type *base, q31_t *p_src_a, uint32_t srcALen, q31_t *p_src_b, uint32_t srcBLen, q31_t *p_dst) |
| Correlation of q31 sequences. More... | |
| void FSP_CorrelateF32 | ( | FSP_Type * | base, |
| float32_t * | p_src_a, | ||
| uint32_t | srcALen, | ||
| float32_t * | p_src_b, | ||
| uint32_t | srcBLen, | ||
| float32_t * | p_dst | ||
| ) |
| base | FSP peripheral base address |
| *p_src_a | points to the long input sequence. |
| srcALen | length of the long input sequence, srcALen < 2 ^(Kx). |
| *p_src_b | points to the short input sequence. |
| srcBLen | length of the short input sequence, srcALen < 2 ^(Ky). |
| *p_dst | points to the location where the output result is written, Length = srcALen - srcBLen + 1. |
| void FSP_CorrelateQ31 | ( | FSP_Type * | base, |
| q31_t * | p_src_a, | ||
| uint32_t | srcALen, | ||
| q31_t * | p_src_b, | ||
| uint32_t | srcBLen, | ||
| q31_t * | p_dst | ||
| ) |
| base | FSP peripheral base address |
| *p_src_a | points to the long input sequence. |
| srcALen | length of the long input sequence, srcALen < 2 ^(Kx). |
| *p_src_b | points to the short input sequence. |
| srcBLen | length of the short input sequence, srcALen < 2 ^(Ky). |
| *p_dst | points to the location where the output result is written, Length = srcALen - srcBLen + 1. |