This section describes the programming interface of the SPI FreeRTOS driver.
Data Fields |
|
SPI_Type * | base |
| | SPI base address.
|
| |
|
spi_master_handle_t | drv_handle |
| | Handle of the underlying driver, treated as opaque by the RTOS layer.
|
| |
|
SemaphoreHandle_t | mutex |
| | Mutex to lock the handle during a trasfer.
|
| |
|
SemaphoreHandle_t | event |
| | Semaphore to notify and unblock task when transfer ends.
|
| |
This function initializes the SPI module and related RTOS context.
- Parameters
-
| handle | The RTOS SPI handle, the pointer to an allocated space for RTOS context. |
| base | The pointer base address of the SPI instance to initialize. |
| masterConfig | Configuration structure to set-up SPI in master mode. |
| srcClock_Hz | Frequency of input clock of the SPI module. |
- Returns
- status of the operation.
This function deinitializes the SPI module and related RTOS context.
- Parameters
-
| handle | The RTOS SPI handle. |
This function performs an SPI transfer according to data given in the transfer structure.
- Parameters
-
| handle | The RTOS SPI handle. |
| transfer | Structure specifying the transfer parameters. |
- Returns
- status of the operation.