![]() |
Kinetis SDK v.2.0 API Reference Manual
Rev. 0
NXP Semiconductors
|
SHA Functional Operation | |
| status_t | SHA_Init (SHA_Type *base, sha_ctx_t *ctx, sha_algo_t algo) |
| Initialize HASH context. More... | |
| status_t | SHA_Update (SHA_Type *base, sha_ctx_t *ctx, const uint8_t *message, size_t messageSize) |
| Add data to current HASH. More... | |
| status_t | SHA_Finish (SHA_Type *base, sha_ctx_t *ctx, uint8_t *output, size_t *outputSize) |
| Finalize hashing. More... | |
| void | SHA_ClkInit (SHA_Type *base) |
| Start SHA clock. More... | |
| void | SHA_ClkDeinit (SHA_Type *base) |
| Stop SHA clock. More... | |
| status_t SHA_Init | ( | SHA_Type * | base, |
| sha_ctx_t * | ctx, | ||
| sha_algo_t | algo | ||
| ) |
This function initializes new hash context.
| base | SHA peripheral base address | |
| [out] | ctx | Output hash context |
| algo | Underlaying algorithm to use for hash computation. Either SHA-1 or SHA-256. |
| status_t SHA_Update | ( | SHA_Type * | base, |
| sha_ctx_t * | ctx, | ||
| const uint8_t * | message, | ||
| size_t | messageSize | ||
| ) |
Add data to current HASH. This can be called repeatedly with an arbitrary amount of data to be hashed.
| base | SHA peripheral base address | |
| [in,out] | ctx | HASH context |
| message | Input message | |
| messageSize | Size of input message in bytes |
Outputs the final hash and erases the context. SHA-1 or SHA-256 padding bits are automatically added by this function.
| base | SHA peripheral base address | |
| [in,out] | ctx | HASH context |
| [out] | output | Output hash data |
| [in,out] | outputSize | On input, determines the size of bytes of the output array. On output, tells how many bytes have been written to output. |
| void SHA_ClkInit | ( | SHA_Type * | base | ) |
Start SHA clock
| base | SHA peripheral base address |
| void SHA_ClkDeinit | ( | SHA_Type * | base | ) |
Stop SHA clock
| base | SHA peripheral base address |