![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
The MCUXpresso SDK provides a driver for the Input multiplexing (INPUTMUX).
It configures the inputs to the pin interrupt block, DMA trigger, and frequency measure function. Once configured, the clock is not needed for the inputmux.
INPUTMUX_AttachSignal function configures the specified input
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/inputmux
Files | |
| file | fsl_inputmux.h |
| file | fsl_inputmux_connections.h |
Functions | |
| void | INPUTMUX_Init (INPUTMUX_Type *base) |
| Initialize INPUTMUX peripheral. More... | |
| void | INPUTMUX_AttachSignal (INPUTMUX_Type *base, uint32_t index, inputmux_connection_t connection) |
| Attaches a signal. More... | |
| void | INPUTMUX_Deinit (INPUTMUX_Type *base) |
| Deinitialize INPUTMUX peripheral. More... | |
Input multiplexing connections | |
| enum | inputmux_connection_t { kINPUTMUX_SctGpi0ToSct0 = 0U + (SCT0_INMUX0 << PMUX_SHIFT) , kINPUTMUX_DebugHaltedToSct0 = 23U + (SCT0_INMUX0 << PMUX_SHIFT) , kINPUTMUX_I2sSharedWs1ToTimer0Captsel = 24U + (TIMER0CAPTSEL0 << PMUX_SHIFT) , kINPUTMUX_I2sSharedWs1ToTimer1Captsel = 24U + (TIMER1CAPTSEL0 << PMUX_SHIFT) , kINPUTMUX_I2sSharedWs1ToTimer2Captsel = 24U + (TIMER2CAPTSEL0 << PMUX_SHIFT) , kINPUTMUX_GpioPort1Pin31ToPintsel = 63U + (PINTSEL0 << PMUX_SHIFT) , kINPUTMUX_HashDmaRxToDma0 = 21U + (DMA0_ITRIG_INMUX0 << PMUX_SHIFT) , kINPUTMUX_Dma0Adc0Ch1TrigoutToTriginChannels = 22U + (DMA0_OTRIG_INMUX0 << PMUX_SHIFT) , kINPUTMUX_FreqmeGpioClk_bRef = 7u + (FREQMEAS_REF_REG << PMUX_SHIFT) , kINPUTMUX_FreqmeGpioClk_bTarget = 7u + (FREQMEAS_TARGET_REG << PMUX_SHIFT) , kINPUTMUX_I2sSharedWs1ToTimer3Captsel = 24U + (TIMER3CAPTSEL0 << PMUX_SHIFT) , kINPUTMUX_GpioPort0Pin31ToPintSecsel = 31U + (PINTSECSEL0 << PMUX_SHIFT) , kINPUTMUX_HashDmaRxToDma1 = 14U + (DMA1_ITRIG_INMUX0 << PMUX_SHIFT) } |
| INPUTMUX connections type. More... | |
| enum | inputmux_signal_t { kINPUTMUX_HashCryptToDmac0Ch0RequestEna = 0U + (DMA0_REQ_ENA_ID << ENA_SHIFT) , kINPUTMUX_Adc0FIFO1ToDmac0Ch22RequestEna = 22U + (DMA0_REQ_ENA_ID << ENA_SHIFT) , kINPUTMUX_Flexcomm3TxToDmac1Ch9RequestEna = 9U + (DMA1_REQ_ENA_ID << ENA_SHIFT) , kINPUTMUX_Dmac0InputTriggerHashOutEna = 21U + (DMA0_ITRIG_ENA_ID << ENA_SHIFT) } |
| INPUTMUX signal enable/disable type. More... | |
| #define | SCT0_INMUX0 0x00U |
| Periphinmux IDs. | |
| #define | TIMER0CAPTSEL0 0x20U |
| #define | TIMER1CAPTSEL0 0x40U |
| #define | TIMER2CAPTSEL0 0x60U |
| #define | PINTSEL_PMUX_ID 0xC0U |
| #define | PINTSEL0 0xC0U |
| #define | DMA0_ITRIG_INMUX0 0xE0U |
| #define | DMA0_OTRIG_INMUX0 0x160U |
| #define | FREQMEAS_REF_REG 0x180U |
| #define | FREQMEAS_TARGET_REG 0x184U |
| #define | TIMER3CAPTSEL0 0x1A0U |
| #define | TIMER4CAPTSEL0 0x1C0U |
| #define | PINTSECSEL0 0x1E0U |
| #define | DMA1_ITRIG_INMUX0 0x200U |
| #define | DMA1_OTRIG_INMUX0 0x240U |
| #define | DMA0_REQ_ENA_ID 0x740U |
| #define | DMA1_REQ_ENA_ID 0x760U |
| #define | DMA0_ITRIG_ENA_ID 0x780U |
| #define | DMA1_ITRIG_ENA_ID 0x7A0U |
| #define | ENA_SHIFT 8U |
| #define | PMUX_SHIFT 20U |
Driver version | |
| #define | FSL_INPUTMUX_DRIVER_VERSION (MAKE_VERSION(2, 0, 3)) |
| Group interrupt driver version for SDK. | |
| enum inputmux_signal_t |
| void INPUTMUX_Init | ( | INPUTMUX_Type * | base | ) |
This function enables the INPUTMUX clock.
| base | Base address of the INPUTMUX peripheral. |
| None. |
| void INPUTMUX_AttachSignal | ( | INPUTMUX_Type * | base, |
| uint32_t | index, | ||
| inputmux_connection_t | connection | ||
| ) |
This function gates the INPUTPMUX clock.
| base | Base address of the INPUTMUX peripheral. |
| index | Destination peripheral to attach the signal to. |
| connection | Selects connection. |
| None. |
| void INPUTMUX_Deinit | ( | INPUTMUX_Type * | base | ) |
This function disables the INPUTMUX clock.
| base | Base address of the INPUTMUX peripheral. |
| None. |