![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
The MMCCARD driver provide card initialization/read/write/erase interface.
Not support yet
MMCCARD driver has added mutual exclusive access support for init/deinit/write/read/erase function. Please note that the card init function will create the mutex lock dynamically by default, so to avoid the mutex create redundantly, application must follow bellow sequence for card re-initialization.
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/sdmmc_examples/
Data Structures | |
struct | mmc_usr_param_t |
card user parameter More... | |
struct | mmc_card_t |
mmc card state More... | |
Macros | |
#define | FSL_MMC_DRIVER_VERSION (MAKE_VERSION(2U, 5U, 0U)) /*2.5.0*/ |
Middleware mmc version. More... | |
Typedefs | |
typedef void(* | mmc_io_strength_t )(uint32_t busFreq) |
card io strength control | |
Enumerations | |
enum | { kMMC_SupportHighSpeed26MHZFlag = (1U << 0U), kMMC_SupportHighSpeed52MHZFlag = (1U << 1U), kMMC_SupportHighSpeedDDR52MHZ180V300VFlag = (1 << 2U), kMMC_SupportHighSpeedDDR52MHZ120VFlag = (1 << 3U), kMMC_SupportHS200200MHZ180VFlag = (1 << 4U), kMMC_SupportHS200200MHZ120VFlag = (1 << 5U), kMMC_SupportHS400DDR200MHZ180VFlag = (1 << 6U), kMMC_SupportHS400DDR200MHZ120VFlag = (1 << 7U), kMMC_SupportHighCapacityFlag = (1U << 8U), kMMC_SupportAlternateBootFlag = (1U << 9U), kMMC_SupportDDRBootFlag = (1U << 10U), kMMC_SupportHighSpeedBootFlag = (1U << 11U), kMMC_SupportEnhanceHS400StrobeFlag = (1U << 12U) } |
MMC card flags. More... | |
enum | mmc_sleep_awake_t { kMMC_Sleep = 1U, kMMC_Awake = 0U } |
mmccard sleep/awake state More... | |
MMCCARD Function | |
status_t | MMC_Init (mmc_card_t *card) |
Initializes the MMC card and host. More... | |
void | MMC_Deinit (mmc_card_t *card) |
Deinitializes the card and host. More... | |
status_t | MMC_CardInit (mmc_card_t *card) |
Initializes the card. More... | |
void | MMC_CardDeinit (mmc_card_t *card) |
Deinitializes the card. More... | |
status_t | MMC_HostInit (mmc_card_t *card) |
initialize the host. More... | |
void | MMC_HostDeinit (mmc_card_t *card) |
Deinitializes the host. More... | |
void | MMC_HostDoReset (mmc_card_t *card) |
Resets the host. More... | |
void | MMC_HostReset (SDMMCHOST_CONFIG *host) |
Resets the host. More... | |
void | MMC_SetCardPower (mmc_card_t *card, bool enable) |
Sets card power. More... | |
bool | MMC_CheckReadOnly (mmc_card_t *card) |
Checks if the card is read-only. More... | |
status_t | MMC_ReadBlocks (mmc_card_t *card, uint8_t *buffer, uint32_t startBlock, uint32_t blockCount) |
Reads data blocks from the card. More... | |
status_t | MMC_WriteBlocks (mmc_card_t *card, const uint8_t *buffer, uint32_t startBlock, uint32_t blockCount) |
Writes data blocks to the card. More... | |
status_t | MMC_EraseGroups (mmc_card_t *card, uint32_t startGroup, uint32_t endGroup) |
Erases groups of the card. More... | |
status_t | MMC_SelectPartition (mmc_card_t *card, mmc_access_partition_t partitionNumber) |
Selects the partition to access. More... | |
status_t | MMC_SetBootConfig (mmc_card_t *card, const mmc_boot_config_t *config) |
Configures the boot activity of the card. More... | |
status_t | MMC_StartBoot (mmc_card_t *card, const mmc_boot_config_t *mmcConfig, uint8_t *buffer, sdmmchost_boot_config_t *hostConfig) |
MMC card start boot. More... | |
status_t | MMC_SetBootConfigWP (mmc_card_t *card, uint8_t wp) |
MMC card set boot configuration write protect. More... | |
status_t | MMC_ReadBootData (mmc_card_t *card, uint8_t *buffer, sdmmchost_boot_config_t *hostConfig) |
MMC card continuous read boot data. More... | |
status_t | MMC_StopBoot (mmc_card_t *card, uint32_t bootMode) |
MMC card stop boot mode. More... | |
status_t | MMC_SetBootPartitionWP (mmc_card_t *card, mmc_boot_partition_wp_t bootPartitionWP) |
MMC card set boot partition write protect. More... | |
status_t | MMC_EnableCacheControl (mmc_card_t *card, bool enable) |
MMC card cache control function. More... | |
status_t | MMC_FlushCache (mmc_card_t *card) |
MMC card cache flush function. More... | |
status_t | MMC_SetSleepAwake (mmc_card_t *card, mmc_sleep_awake_t state) |
MMC sets card sleep awake state. More... | |
status_t | MMC_PollingCardStatusBusy (mmc_card_t *card, bool checkStatus, uint32_t timeoutMs) |
Polling card idle status. More... | |
struct mmc_usr_param_t |
Data Fields | |
mmc_io_strength_t | ioStrength |
switch sd io strength | |
uint32_t | maxFreq |
board support maximum frequency | |
uint32_t | capability |
board capability flag | |
struct mmc_card_t |
Defines the card structure including the necessary fields to identify and describe the card.
Data Fields | |
sdmmchost_t * | host |
Host information. | |
mmc_usr_param_t | usrParam |
user parameter | |
bool | isHostReady |
Use this flag to indicate if host re-init needed or not. | |
bool | noInteralAlign |
Use this flag to disable sdmmc align. More... | |
uint32_t | busClock_Hz |
MMC bus clock united in Hz. | |
uint32_t | relativeAddress |
Relative address of the card. | |
bool | enablePreDefinedBlockCount |
Enable PRE-DEFINED block count when read/write. | |
uint32_t | flags |
Capability flag in _mmc_card_flag. | |
uint8_t | internalBuffer [FSL_SDMMC_CARD_INTERNAL_BUFFER_SIZE] |
raw buffer used for mmc driver internal | |
uint32_t | ocr |
Raw OCR content. | |
mmc_cid_t | cid |
CID. | |
mmc_csd_t | csd |
CSD. | |
mmc_extended_csd_t | extendedCsd |
Extended CSD. | |
uint32_t | blockSize |
Card block size. | |
uint32_t | userPartitionBlocks |
Card total block number in user partition. | |
uint32_t | bootPartitionBlocks |
Boot partition size united as block size. | |
uint32_t | eraseGroupBlocks |
Erase group size united as block size. | |
mmc_access_partition_t | currentPartition |
Current access partition. | |
mmc_voltage_window_t | hostVoltageWindowVCCQ |
application must set this value according to board specific | |
mmc_voltage_window_t | hostVoltageWindowVCC |
application must set this value according to board specific | |
mmc_high_speed_timing_t | busTiming |
indicates the current work timing mode | |
mmc_data_bus_width_t | busWidth |
indicates the current work bus width | |
sdmmc_osa_mutex_t | lock |
card access lock | |
bool mmc_card_t::noInteralAlign |
If disabled, sdmmc will not make sure the data buffer address is word align, otherwise all the transfer are aligned to low level driver.
#define FSL_MMC_DRIVER_VERSION (MAKE_VERSION(2U, 5U, 0U)) /*2.5.0*/ |
anonymous enum |
enum mmc_sleep_awake_t |
status_t MMC_Init | ( | mmc_card_t * | card | ) |
card | Card descriptor. |
Thread safe function, please note that the function will create the mutex lock dynamically by default, so to avoid the mutex to be created redundantly, application must follow bellow sequence for card re-initialization:
kStatus_SDMMC_HostNotReady | Host is not ready. |
kStatus_SDMMC_GoIdleFailed | Going idle failed. |
kStatus_SDMMC_HandShakeOperationConditionFailed | Sending operation condition failed. |
kStatus_SDMMC_AllSendCidFailed | Sending CID failed. |
kStatus_SDMMC_SetRelativeAddressFailed | Setging relative address failed. |
kStatus_SDMMC_SendCsdFailed | Sending CSD failed. |
kStatus_SDMMC_CardNotSupport | Card not support. |
kStatus_SDMMC_SelectCardFailed | Sending SELECT_CARD command failed. |
kStatus_SDMMC_SendExtendedCsdFailed | Sending EXT_CSD failed. |
kStatus_SDMMC_SetDataBusWidthFailed | Setting bus width failed. |
kStatus_SDMMC_SwitchBusTimingFailed | Switching high speed failed. |
kStatus_SDMMC_SetCardBlockSizeFailed | Setting card block size failed. |
kStatus_SDMMC_SetPowerClassFail | Setting card power class failed. |
kStatus_Success | Operation succeeded. |
void MMC_Deinit | ( | mmc_card_t * | card | ) |
card | Card descriptor. |
status_t MMC_CardInit | ( | mmc_card_t * | card | ) |
Thread safe function, please note that the function will create the mutex lock dynamically by default, so to avoid the mutex to be created redundantly, application must follow bellow sequence for card re-initialization:
card | Card descriptor. |
kStatus_SDMMC_HostNotReady | Host is not ready. |
kStatus_SDMMC_GoIdleFailed | Going idle failed. |
kStatus_SDMMC_HandShakeOperationConditionFailed | Sending operation condition failed. |
kStatus_SDMMC_AllSendCidFailed | Sending CID failed. |
kStatus_SDMMC_SetRelativeAddressFailed | Setting relative address failed. |
kStatus_SDMMC_SendCsdFailed | Sending CSD failed. |
kStatus_SDMMC_CardNotSupport | Card not support. |
kStatus_SDMMC_SelectCardFailed | Sending SELECT_CARD command failed. |
kStatus_SDMMC_SendExtendedCsdFailed | Sending EXT_CSD failed. |
kStatus_SDMMC_SetDataBusWidthFailed | Setting bus width failed. |
kStatus_SDMMC_SwitchBusTimingFailed | Switching high speed failed. |
kStatus_SDMMC_SetCardBlockSizeFailed | Setting card block size failed. |
kStatus_SDMMC_SetPowerClassFail | Setting card power class failed. |
kStatus_Success | Operation succeeded. |
void MMC_CardDeinit | ( | mmc_card_t * | card | ) |
card | Card descriptor. |
status_t MMC_HostInit | ( | mmc_card_t * | card | ) |
This function deinitializes the specific host.
card | Card descriptor. |
void MMC_HostDeinit | ( | mmc_card_t * | card | ) |
This function deinitializes the host.
card | Card descriptor. |
void MMC_HostDoReset | ( | mmc_card_t * | card | ) |
This function resets the specific host.
card | Card descriptor. |
void MMC_HostReset | ( | SDMMCHOST_CONFIG * | host | ) |
host | Host descriptor. |
void MMC_SetCardPower | ( | mmc_card_t * | card, |
bool | enable | ||
) |
card | Card descriptor. |
enable | True is powering on, false is powering off. |
bool MMC_CheckReadOnly | ( | mmc_card_t * | card | ) |
card | Card descriptor. |
true | Card is read only. |
false | Card isn't read only. |
status_t MMC_ReadBlocks | ( | mmc_card_t * | card, |
uint8_t * | buffer, | ||
uint32_t | startBlock, | ||
uint32_t | blockCount | ||
) |
card | Card descriptor. |
buffer | The buffer to save data. |
startBlock | The start block index. |
blockCount | The number of blocks to read. |
kStatus_InvalidArgument | Invalid argument. |
kStatus_SDMMC_CardNotSupport | Card not support. |
kStatus_SDMMC_SetBlockCountFailed | Setting block count failed. |
kStatus_SDMMC_TransferFailed | Transfer failed. |
kStatus_SDMMC_StopTransmissionFailed | Stopping transmission failed. |
kStatus_Success | Operation succeeded. |
status_t MMC_WriteBlocks | ( | mmc_card_t * | card, |
const uint8_t * | buffer, | ||
uint32_t | startBlock, | ||
uint32_t | blockCount | ||
) |
card | Card descriptor. |
buffer | The buffer to save data blocks. |
startBlock | Start block number to write. |
blockCount | Block count. |
kStatus_InvalidArgument | Invalid argument. |
kStatus_SDMMC_NotSupportYet | Not support now. |
kStatus_SDMMC_SetBlockCountFailed | Setting block count failed. |
kStatus_SDMMC_WaitWriteCompleteFailed | Sending status failed. |
kStatus_SDMMC_TransferFailed | Transfer failed. |
kStatus_SDMMC_StopTransmissionFailed | Stop transmission failed. |
kStatus_Success | Operation succeeded. |
status_t MMC_EraseGroups | ( | mmc_card_t * | card, |
uint32_t | startGroup, | ||
uint32_t | endGroup | ||
) |
The erase command is best used to erase the entire device or a partition. Erase group is the smallest erase unit in MMC card. The erase range is [startGroup, endGroup].
card | Card descriptor. |
startGroup | Start group number. |
endGroup | End group number. |
kStatus_InvalidArgument | Invalid argument. |
kStatus_SDMMC_WaitWriteCompleteFailed | Send status failed. |
kStatus_SDMMC_TransferFailed | Transfer failed. |
kStatus_Success | Operation succeeded. |
status_t MMC_SelectPartition | ( | mmc_card_t * | card, |
mmc_access_partition_t | partitionNumber | ||
) |
card | Card descriptor. |
partitionNumber | The partition number. |
kStatus_SDMMC_ConfigureExtendedCsdFailed | Configuring EXT_CSD failed. |
kStatus_Success | Operation succeeded. |
status_t MMC_SetBootConfig | ( | mmc_card_t * | card, |
const mmc_boot_config_t * | config | ||
) |
card | Card descriptor. |
config | Boot configuration structure. |
kStatus_SDMMC_NotSupportYet | Not support now. |
kStatus_SDMMC_ConfigureExtendedCsdFailed | Configuring EXT_CSD failed. |
kStatus_SDMMC_ConfigureBootFailed | Configuring boot failed. |
kStatus_Success | Operation succeeded. |
status_t MMC_StartBoot | ( | mmc_card_t * | card, |
const mmc_boot_config_t * | mmcConfig, | ||
uint8_t * | buffer, | ||
sdmmchost_boot_config_t * | hostConfig | ||
) |
card | Card descriptor. |
mmcConfig | The mmc Boot configuration structure. |
buffer | Address to receive data. |
hostConfig | Host boot configurations. |
kStatus_Fail | Failed. |
kStatus_SDMMC_TransferFailed | Transfer failed. |
kStatus_SDMMC_GoIdleFailed | Resetting card failed. |
kStatus_Success | Operation succeeded. |
status_t MMC_SetBootConfigWP | ( | mmc_card_t * | card, |
uint8_t | wp | ||
) |
card | Card descriptor. |
wp | Write protect value. |
status_t MMC_ReadBootData | ( | mmc_card_t * | card, |
uint8_t * | buffer, | ||
sdmmchost_boot_config_t * | hostConfig | ||
) |
card | Card descriptor. |
buffer | Buffer address. |
hostConfig | Host boot configurations. |
status_t MMC_StopBoot | ( | mmc_card_t * | card, |
uint32_t | bootMode | ||
) |
card | Card descriptor. |
bootMode | Boot mode. |
status_t MMC_SetBootPartitionWP | ( | mmc_card_t * | card, |
mmc_boot_partition_wp_t | bootPartitionWP | ||
) |
card | Card descriptor. |
bootPartitionWP | Boot partition write protect value. |
status_t MMC_EnableCacheControl | ( | mmc_card_t * | card, |
bool | enable | ||
) |
The mmc device's cache is enabled by the driver by default. The cache should in typical case reduce the access time (compared to an access to the main nonvolatile storage) for both write and read.
card | Card descriptor. |
enable | True is enabling the cache, false is disabling the cache. |
status_t MMC_FlushCache | ( | mmc_card_t * | card | ) |
A Flush operation refers to the requirement, from the host to the device, to write the cached data to the nonvolatile memory. Prior to a flush, the device may autonomously write data to the nonvolatile memory, but after the flush operation all data in the volatile area must be written to nonvolatile memory. There is no requirement for flush due to switching between the partitions. (Note: This also implies that the cache data shall not be lost when switching between partitions). Cached data may be lost in SLEEP state, so host should flush the cache before placing the device into SLEEP state.
card | Card descriptor. |
status_t MMC_SetSleepAwake | ( | mmc_card_t * | card, |
mmc_sleep_awake_t | state | ||
) |
The Sleep/Awake command is used to initiate the state transition between Standby state and Sleep state. The memory device indicates the transition phase busy by pulling down the DAT0 line. The Sleep/Standby state is reached when the memory device stops pulling down the DAT0 line, then the function returns.
card | Card descriptor. |
state | The sleep/awake command argument, refer to mmc_sleep_awake_t. |
kStatus_SDMMC_NotSupportYet | Indicates the memory device doesn't support the Sleep/Awake command. |
kStatus_SDMMC_TransferFailed | Indicates command transferred fail. |
kStatus_SDMMC_PollingCardIdleFailed | Indicates polling DAT0 busy timeout. |
kStatus_SDMMC_DeselectCardFailed | Indicates deselect card command failed. |
kStatus_SDMMC_SelectCardFailed | Indicates select card command failed. |
kStatus_Success | Indicates the card state switched successfully. |
status_t MMC_PollingCardStatusBusy | ( | mmc_card_t * | card, |
bool | checkStatus, | ||
uint32_t | timeoutMs | ||
) |
This function can be used to poll the status from busy to idle, the function will return with the card status being idle or timeout or command failed.
card | Card descriptor. |
checkStatus | True is send CMD and read DAT0 status to check card status, false is read DAT0 status only. |
timeoutMs | Polling card status timeout value. |
kStatus_SDMMC_CardStatusIdle | Card is idle. |
kStatus_SDMMC_CardStatusBusy | Card is busy. |
kStatus_SDMMC_TransferFailed | Command tranfer failed. |
kStatus_SDMMC_SwitchFailed | Status command reports switch error. |