MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
SDHC: Secure Digital Host Controller Driver

Overview

The MCUXpresso SDK provides a peripheral driver for the Secure Digital Host Controller (SDHC) module of MCUXpresso SDK devices.

Typical use case

SDHC Operation

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/sdhc

Data Structures

struct  sdhc_adma2_descriptor_t
 Defines the ADMA2 descriptor structure. More...
 
struct  sdhc_capability_t
 SDHC capability information. More...
 
struct  sdhc_transfer_config_t
 Card transfer configuration. More...
 
struct  sdhc_boot_config_t
 Data structure to configure the MMC boot feature. More...
 
struct  sdhc_config_t
 Data structure to initialize the SDHC. More...
 
struct  sdhc_data_t
 Card data descriptor. More...
 
struct  sdhc_command_t
 Card command descriptor. More...
 
struct  sdhc_transfer_t
 Transfer state. More...
 
struct  sdhc_transfer_callback_t
 SDHC callback functions. More...
 
struct  sdhc_handle_t
 SDHC handle. More...
 
struct  sdhc_host_t
 SDHC host descriptor. More...
 

Macros

#define SDHC_MAX_BLOCK_COUNT   (SDHC_BLKATTR_BLKCNT_MASK >> SDHC_BLKATTR_BLKCNT_SHIFT)
 Maximum block count can be set one time.
 
#define SDHC_ADMA1_ADDRESS_ALIGN   (4096U)
 The alignment size for ADDRESS filed in ADMA1's descriptor.
 
#define SDHC_ADMA1_LENGTH_ALIGN   (4096U)
 The alignment size for LENGTH field in ADMA1's descriptor.
 
#define SDHC_ADMA2_ADDRESS_ALIGN   (4U)
 The alignment size for ADDRESS field in ADMA2's descriptor.
 
#define SDHC_ADMA2_LENGTH_ALIGN   (4U)
 The alignment size for LENGTH filed in ADMA2's descriptor.
 
#define SDHC_ADMA1_DESCRIPTOR_ADDRESS_SHIFT   (12U)
 The bit shift for ADDRESS filed in ADMA1's descriptor.
 
#define SDHC_ADMA1_DESCRIPTOR_ADDRESS_MASK   (0xFFFFFU)
 The bit mask for ADDRESS field in ADMA1's descriptor.
 
#define SDHC_ADMA1_DESCRIPTOR_LENGTH_SHIFT   (12U)
 The bit shift for LENGTH filed in ADMA1's descriptor.
 
#define SDHC_ADMA1_DESCRIPTOR_LENGTH_MASK   (0xFFFFU)
 The mask for LENGTH field in ADMA1's descriptor.
 
#define SDHC_ADMA1_DESCRIPTOR_MAX_LENGTH_PER_ENTRY   (SDHC_ADMA1_DESCRIPTOR_LENGTH_MASK + 1U)
 The maximum value of LENGTH filed in ADMA1's descriptor.
 
#define SDHC_ADMA2_DESCRIPTOR_LENGTH_SHIFT   (16U)
 The bit shift for LENGTH field in ADMA2's descriptor.
 
#define SDHC_ADMA2_DESCRIPTOR_LENGTH_MASK   (0xFFFFU)
 The bit mask for LENGTH field in ADMA2's descriptor.
 
#define SDHC_ADMA2_DESCRIPTOR_MAX_LENGTH_PER_ENTRY   (SDHC_ADMA2_DESCRIPTOR_LENGTH_MASK)
 The maximum value of LENGTH field in ADMA2's descriptor.
 

Typedefs

typedef uint32_t sdhc_adma1_descriptor_t
 Defines the adma1 descriptor structure. More...
 
typedef status_t(* sdhc_transfer_function_t )(SDHC_Type *base, sdhc_transfer_t *content)
 SDHC transfer function. More...
 

Enumerations

enum  _sdhc_status {
  kStatus_SDHC_BusyTransferring = MAKE_STATUS(kStatusGroup_SDHC, 0U),
  kStatus_SDHC_PrepareAdmaDescriptorFailed = MAKE_STATUS(kStatusGroup_SDHC, 1U),
  kStatus_SDHC_SendCommandFailed = MAKE_STATUS(kStatusGroup_SDHC, 2U),
  kStatus_SDHC_TransferDataFailed = MAKE_STATUS(kStatusGroup_SDHC, 3U),
  kStatus_SDHC_DMADataBufferAddrNotAlign
}
 SDHC status. More...
 
enum  _sdhc_capability_flag {
  kSDHC_SupportAdmaFlag = SDHC_HTCAPBLT_ADMAS_MASK,
  kSDHC_SupportHighSpeedFlag = SDHC_HTCAPBLT_HSS_MASK,
  kSDHC_SupportDmaFlag = SDHC_HTCAPBLT_DMAS_MASK,
  kSDHC_SupportSuspendResumeFlag = SDHC_HTCAPBLT_SRS_MASK,
  kSDHC_SupportV330Flag = SDHC_HTCAPBLT_VS33_MASK,
  kSDHC_Support4BitFlag = (SDHC_HTCAPBLT_MBL_SHIFT << 0U),
  kSDHC_Support8BitFlag = (SDHC_HTCAPBLT_MBL_SHIFT << 1U)
}
 Host controller capabilities flag mask. More...
 
enum  _sdhc_wakeup_event {
  kSDHC_WakeupEventOnCardInt = SDHC_PROCTL_WECINT_MASK,
  kSDHC_WakeupEventOnCardInsert = SDHC_PROCTL_WECINS_MASK,
  kSDHC_WakeupEventOnCardRemove = SDHC_PROCTL_WECRM_MASK,
  kSDHC_WakeupEventsAll
}
 Wakeup event mask. More...
 
enum  _sdhc_reset {
  kSDHC_ResetAll = SDHC_SYSCTL_RSTA_MASK,
  kSDHC_ResetCommand = SDHC_SYSCTL_RSTC_MASK,
  kSDHC_ResetData = SDHC_SYSCTL_RSTD_MASK,
  kSDHC_ResetsAll = (kSDHC_ResetAll | kSDHC_ResetCommand | kSDHC_ResetData)
}
 Reset type mask. More...
 
enum  _sdhc_transfer_flag {
  kSDHC_EnableDmaFlag = SDHC_XFERTYP_DMAEN_MASK,
  kSDHC_CommandTypeSuspendFlag = (SDHC_XFERTYP_CMDTYP(1U)),
  kSDHC_CommandTypeResumeFlag = (SDHC_XFERTYP_CMDTYP(2U)),
  kSDHC_CommandTypeAbortFlag = (SDHC_XFERTYP_CMDTYP(3U)),
  kSDHC_EnableBlockCountFlag = SDHC_XFERTYP_BCEN_MASK,
  kSDHC_EnableAutoCommand12Flag = SDHC_XFERTYP_AC12EN_MASK,
  kSDHC_DataReadFlag = SDHC_XFERTYP_DTDSEL_MASK,
  kSDHC_MultipleBlockFlag = SDHC_XFERTYP_MSBSEL_MASK,
  kSDHC_ResponseLength136Flag = SDHC_XFERTYP_RSPTYP(1U),
  kSDHC_ResponseLength48Flag = SDHC_XFERTYP_RSPTYP(2U),
  kSDHC_ResponseLength48BusyFlag = SDHC_XFERTYP_RSPTYP(3U),
  kSDHC_EnableCrcCheckFlag = SDHC_XFERTYP_CCCEN_MASK,
  kSDHC_EnableIndexCheckFlag = SDHC_XFERTYP_CICEN_MASK,
  kSDHC_DataPresentFlag = SDHC_XFERTYP_DPSEL_MASK
}
 Transfer flag mask. More...
 
enum  _sdhc_present_status_flag {
  kSDHC_CommandInhibitFlag = SDHC_PRSSTAT_CIHB_MASK,
  kSDHC_DataInhibitFlag = SDHC_PRSSTAT_CDIHB_MASK,
  kSDHC_DataLineActiveFlag = SDHC_PRSSTAT_DLA_MASK,
  kSDHC_SdClockStableFlag = SDHC_PRSSTAT_SDSTB_MASK,
  kSDHC_WriteTransferActiveFlag = SDHC_PRSSTAT_WTA_MASK,
  kSDHC_ReadTransferActiveFlag = SDHC_PRSSTAT_RTA_MASK,
  kSDHC_BufferWriteEnableFlag = SDHC_PRSSTAT_BWEN_MASK,
  kSDHC_BufferReadEnableFlag = SDHC_PRSSTAT_BREN_MASK,
  kSDHC_CardInsertedFlag = SDHC_PRSSTAT_CINS_MASK,
  kSDHC_CommandLineLevelFlag = SDHC_PRSSTAT_CLSL_MASK,
  kSDHC_Data0LineLevelFlag = (1U << 24U),
  kSDHC_Data1LineLevelFlag = (1U << 25U),
  kSDHC_Data2LineLevelFlag = (1U << 26U),
  kSDHC_Data3LineLevelFlag = (1U << 27U),
  kSDHC_Data4LineLevelFlag = (1U << 28U),
  kSDHC_Data5LineLevelFlag = (1U << 29U),
  kSDHC_Data6LineLevelFlag = (1U << 30U),
  kSDHC_Data7LineLevelFlag = (1U << 31U)
}
 Present status flag mask. More...
 
enum  _sdhc_interrupt_status_flag {
  kSDHC_CommandCompleteFlag = SDHC_IRQSTAT_CC_MASK,
  kSDHC_DataCompleteFlag = SDHC_IRQSTAT_TC_MASK,
  kSDHC_BlockGapEventFlag = SDHC_IRQSTAT_BGE_MASK,
  kSDHC_DmaCompleteFlag = SDHC_IRQSTAT_DINT_MASK,
  kSDHC_BufferWriteReadyFlag = SDHC_IRQSTAT_BWR_MASK,
  kSDHC_BufferReadReadyFlag = SDHC_IRQSTAT_BRR_MASK,
  kSDHC_CardInsertionFlag = SDHC_IRQSTAT_CINS_MASK,
  kSDHC_CardRemovalFlag = SDHC_IRQSTAT_CRM_MASK,
  kSDHC_CardInterruptFlag = SDHC_IRQSTAT_CINT_MASK,
  kSDHC_CommandTimeoutFlag = SDHC_IRQSTAT_CTOE_MASK,
  kSDHC_CommandCrcErrorFlag = SDHC_IRQSTAT_CCE_MASK,
  kSDHC_CommandEndBitErrorFlag = SDHC_IRQSTAT_CEBE_MASK,
  kSDHC_CommandIndexErrorFlag = SDHC_IRQSTAT_CIE_MASK,
  kSDHC_DataTimeoutFlag = SDHC_IRQSTAT_DTOE_MASK,
  kSDHC_DataCrcErrorFlag = SDHC_IRQSTAT_DCE_MASK,
  kSDHC_DataEndBitErrorFlag = SDHC_IRQSTAT_DEBE_MASK,
  kSDHC_AutoCommand12ErrorFlag = SDHC_IRQSTAT_AC12E_MASK,
  kSDHC_DmaErrorFlag = SDHC_IRQSTAT_DMAE_MASK,
  kSDHC_CommandErrorFlag,
  kSDHC_DataErrorFlag,
  kSDHC_ErrorFlag = (kSDHC_CommandErrorFlag | kSDHC_DataErrorFlag | kSDHC_DmaErrorFlag),
  kSDHC_DataFlag,
  kSDHC_CommandFlag = (kSDHC_CommandErrorFlag | kSDHC_CommandCompleteFlag),
  kSDHC_CardDetectFlag = (kSDHC_CardInsertionFlag | kSDHC_CardRemovalFlag),
  kSDHC_AllInterruptFlags
}
 Interrupt status flag mask. More...
 
enum  _sdhc_auto_command12_error_status_flag {
  kSDHC_AutoCommand12NotExecutedFlag = SDHC_AC12ERR_AC12NE_MASK,
  kSDHC_AutoCommand12TimeoutFlag = SDHC_AC12ERR_AC12TOE_MASK,
  kSDHC_AutoCommand12EndBitErrorFlag = SDHC_AC12ERR_AC12EBE_MASK,
  kSDHC_AutoCommand12CrcErrorFlag = SDHC_AC12ERR_AC12CE_MASK,
  kSDHC_AutoCommand12IndexErrorFlag = SDHC_AC12ERR_AC12IE_MASK,
  kSDHC_AutoCommand12NotIssuedFlag = SDHC_AC12ERR_CNIBAC12E_MASK
}
 Auto CMD12 error status flag mask. More...
 
enum  _sdhc_adma_error_status_flag {
  kSDHC_AdmaLenghMismatchFlag = SDHC_ADMAES_ADMALME_MASK,
  kSDHC_AdmaDescriptorErrorFlag = SDHC_ADMAES_ADMADCE_MASK
}
 ADMA error status flag mask. More...
 
enum  sdhc_adma_error_state_t {
  kSDHC_AdmaErrorStateStopDma = 0x00U,
  kSDHC_AdmaErrorStateFetchDescriptor = 0x01U,
  kSDHC_AdmaErrorStateChangeAddress = 0x02U,
  kSDHC_AdmaErrorStateTransferData = 0x03U
}
 ADMA error state. More...
 
enum  _sdhc_force_event {
  kSDHC_ForceEventAutoCommand12NotExecuted = SDHC_FEVT_AC12NE_MASK,
  kSDHC_ForceEventAutoCommand12Timeout = SDHC_FEVT_AC12TOE_MASK,
  kSDHC_ForceEventAutoCommand12CrcError = SDHC_FEVT_AC12CE_MASK,
  kSDHC_ForceEventEndBitError = SDHC_FEVT_AC12EBE_MASK,
  kSDHC_ForceEventAutoCommand12IndexError = SDHC_FEVT_AC12IE_MASK,
  kSDHC_ForceEventAutoCommand12NotIssued = SDHC_FEVT_CNIBAC12E_MASK,
  kSDHC_ForceEventCommandTimeout = SDHC_FEVT_CTOE_MASK,
  kSDHC_ForceEventCommandCrcError = SDHC_FEVT_CCE_MASK,
  kSDHC_ForceEventCommandEndBitError = SDHC_FEVT_CEBE_MASK,
  kSDHC_ForceEventCommandIndexError = SDHC_FEVT_CIE_MASK,
  kSDHC_ForceEventDataTimeout = SDHC_FEVT_DTOE_MASK,
  kSDHC_ForceEventDataCrcError = SDHC_FEVT_DCE_MASK,
  kSDHC_ForceEventDataEndBitError = SDHC_FEVT_DEBE_MASK,
  kSDHC_ForceEventAutoCommand12Error = SDHC_FEVT_AC12E_MASK,
  kSDHC_ForceEventCardInt = SDHC_FEVT_CINT_MASK,
  kSDHC_ForceEventDmaError = SDHC_FEVT_DMAE_MASK,
  kSDHC_ForceEventsAll
}
 Force event mask. More...
 
enum  sdhc_data_bus_width_t {
  kSDHC_DataBusWidth1Bit = 0U,
  kSDHC_DataBusWidth4Bit = 1U,
  kSDHC_DataBusWidth8Bit = 2U
}
 Data transfer width. More...
 
enum  sdhc_endian_mode_t {
  kSDHC_EndianModeBig = 0U,
  kSDHC_EndianModeHalfWordBig = 1U,
  kSDHC_EndianModeLittle = 2U
}
 Endian mode. More...
 
enum  sdhc_dma_mode_t {
  kSDHC_DmaModeNo = 0U,
  kSDHC_DmaModeAdma1 = 1U,
  kSDHC_DmaModeAdma2 = 2U
}
 DMA mode. More...
 
enum  _sdhc_sdio_control_flag {
  kSDHC_StopAtBlockGapFlag = 0x01,
  kSDHC_ReadWaitControlFlag = 0x02,
  kSDHC_InterruptAtBlockGapFlag = 0x04,
  kSDHC_ExactBlockNumberReadFlag = 0x08
}
 SDIO control flag mask. More...
 
enum  sdhc_boot_mode_t {
  kSDHC_BootModeNormal = 0U,
  kSDHC_BootModeAlternative = 1U
}
 MMC card boot mode. More...
 
enum  sdhc_card_command_type_t {
  kCARD_CommandTypeNormal = 0U,
  kCARD_CommandTypeSuspend = 1U,
  kCARD_CommandTypeResume = 2U,
  kCARD_CommandTypeAbort = 3U
}
 The command type. More...
 
enum  sdhc_card_response_type_t {
  kCARD_ResponseTypeNone = 0U,
  kCARD_ResponseTypeR1 = 1U,
  kCARD_ResponseTypeR1b = 2U,
  kCARD_ResponseTypeR2 = 3U,
  kCARD_ResponseTypeR3 = 4U,
  kCARD_ResponseTypeR4 = 5U,
  kCARD_ResponseTypeR5 = 6U,
  kCARD_ResponseTypeR5b = 7U,
  kCARD_ResponseTypeR6 = 8U,
  kCARD_ResponseTypeR7 = 9U
}
 The command response type. More...
 
enum  _sdhc_adma1_descriptor_flag {
  kSDHC_Adma1DescriptorValidFlag = (1U << 0U),
  kSDHC_Adma1DescriptorEndFlag = (1U << 1U),
  kSDHC_Adma1DescriptorInterrupFlag = (1U << 2U),
  kSDHC_Adma1DescriptorActivity1Flag = (1U << 4U),
  kSDHC_Adma1DescriptorActivity2Flag = (1U << 5U),
  kSDHC_Adma1DescriptorTypeNop = (kSDHC_Adma1DescriptorValidFlag),
  kSDHC_Adma1DescriptorTypeTransfer,
  kSDHC_Adma1DescriptorTypeLink,
  kSDHC_Adma1DescriptorTypeSetLength
}
 The mask for the control/status field in ADMA1 descriptor. More...
 
enum  _sdhc_adma2_descriptor_flag {
  kSDHC_Adma2DescriptorValidFlag = (1U << 0U),
  kSDHC_Adma2DescriptorEndFlag = (1U << 1U),
  kSDHC_Adma2DescriptorInterruptFlag = (1U << 2U),
  kSDHC_Adma2DescriptorActivity1Flag = (1U << 4U),
  kSDHC_Adma2DescriptorActivity2Flag = (1U << 5U),
  kSDHC_Adma2DescriptorTypeNop = (kSDHC_Adma2DescriptorValidFlag),
  kSDHC_Adma2DescriptorTypeReserved,
  kSDHC_Adma2DescriptorTypeTransfer,
  kSDHC_Adma2DescriptorTypeLink
}
 ADMA1 descriptor control and status mask. More...
 

Driver version

#define FSL_SDHC_DRIVER_VERSION   (MAKE_VERSION(2U, 1U, 6U))
 Driver version 2.1.6. More...
 

Initialization and deinitialization

void SDHC_Init (SDHC_Type *base, const sdhc_config_t *config)
 SDHC module initialization function. More...
 
void SDHC_Deinit (SDHC_Type *base)
 Deinitializes the SDHC. More...
 
bool SDHC_Reset (SDHC_Type *base, uint32_t mask, uint32_t timeout)
 Resets the SDHC. More...
 

DMA Control

status_t SDHC_SetAdmaTableConfig (SDHC_Type *base, sdhc_dma_mode_t dmaMode, uint32_t *table, uint32_t tableWords, const uint32_t *data, uint32_t dataBytes)
 Sets the ADMA descriptor table configuration. More...
 

Interrupts

static void SDHC_EnableInterruptStatus (SDHC_Type *base, uint32_t mask)
 Enables the interrupt status. More...
 
static void SDHC_DisableInterruptStatus (SDHC_Type *base, uint32_t mask)
 Disables the interrupt status. More...
 
static void SDHC_EnableInterruptSignal (SDHC_Type *base, uint32_t mask)
 Enables the interrupt signal corresponding to the interrupt status flag. More...
 
static void SDHC_DisableInterruptSignal (SDHC_Type *base, uint32_t mask)
 Disables the interrupt signal corresponding to the interrupt status flag. More...
 

Status

static uint32_t SDHC_GetInterruptStatusFlags (SDHC_Type *base)
 Gets the current interrupt status. More...
 
static void SDHC_ClearInterruptStatusFlags (SDHC_Type *base, uint32_t mask)
 Clears a specified interrupt status. More...
 
static uint32_t SDHC_GetAutoCommand12ErrorStatusFlags (SDHC_Type *base)
 Gets the status of auto command 12 error. More...
 
static uint32_t SDHC_GetAdmaErrorStatusFlags (SDHC_Type *base)
 Gets the status of the ADMA error. More...
 
static uint32_t SDHC_GetPresentStatusFlags (SDHC_Type *base)
 Gets a present status. More...
 

Bus Operations

void SDHC_GetCapability (SDHC_Type *base, sdhc_capability_t *capability)
 Gets the capability information. More...
 
static void SDHC_EnableSdClock (SDHC_Type *base, bool enable)
 Enables or disables the SD bus clock. More...
 
uint32_t SDHC_SetSdClock (SDHC_Type *base, uint32_t srcClock_Hz, uint32_t busClock_Hz)
 Sets the SD bus clock frequency. More...
 
bool SDHC_SetCardActive (SDHC_Type *base, uint32_t timeout)
 Sends 80 clocks to the card to set it to the active state. More...
 
static void SDHC_SetDataBusWidth (SDHC_Type *base, sdhc_data_bus_width_t width)
 Sets the data transfer width. More...
 
static void SDHC_CardDetectByData3 (SDHC_Type *base, bool enable)
 detect card insert status. More...
 
void SDHC_SetTransferConfig (SDHC_Type *base, const sdhc_transfer_config_t *config)
 Sets the card transfer-related configuration. More...
 
static uint32_t SDHC_GetCommandResponse (SDHC_Type *base, uint32_t index)
 Gets the command response. More...
 
static void SDHC_WriteData (SDHC_Type *base, uint32_t data)
 Fills the the data port. More...
 
static uint32_t SDHC_ReadData (SDHC_Type *base)
 Retrieves the data from the data port. More...
 
static void SDHC_EnableWakeupEvent (SDHC_Type *base, uint32_t mask, bool enable)
 Enables or disables a wakeup event in low-power mode. More...
 
static void SDHC_EnableCardDetectTest (SDHC_Type *base, bool enable)
 Enables or disables the card detection level for testing. More...
 
static void SDHC_SetCardDetectTestLevel (SDHC_Type *base, bool high)
 Sets the card detection test level. More...
 
void SDHC_EnableSdioControl (SDHC_Type *base, uint32_t mask, bool enable)
 Enables or disables the SDIO card control. More...
 
static void SDHC_SetContinueRequest (SDHC_Type *base)
 Restarts a transaction which has stopped at the block GAP for the SDIO card. More...
 
void SDHC_SetMmcBootConfig (SDHC_Type *base, const sdhc_boot_config_t *config)
 Configures the MMC boot feature. More...
 
static void SDHC_SetForceEvent (SDHC_Type *base, uint32_t mask)
 Forces generating events according to the given mask. More...
 

Transactional

status_t SDHC_TransferBlocking (SDHC_Type *base, uint32_t *admaTable, uint32_t admaTableWords, sdhc_transfer_t *transfer)
 Transfers the command/data using a blocking method. More...
 
void SDHC_TransferCreateHandle (SDHC_Type *base, sdhc_handle_t *handle, const sdhc_transfer_callback_t *callback, void *userData)
 Creates the SDHC handle. More...
 
status_t SDHC_TransferNonBlocking (SDHC_Type *base, sdhc_handle_t *handle, uint32_t *admaTable, uint32_t admaTableWords, sdhc_transfer_t *transfer)
 Transfers the command/data using an interrupt and an asynchronous method. More...
 
void SDHC_TransferHandleIRQ (SDHC_Type *base, sdhc_handle_t *handle)
 IRQ handler for the SDHC. More...
 

Data Structure Documentation

struct sdhc_adma2_descriptor_t

Data Fields

uint32_t attribute
 The control and status field.
 
const uint32_t * address
 The address field.
 
struct sdhc_capability_t

Defines a structure to save the capability information of SDHC.

Data Fields

uint32_t specVersion
 Specification version.
 
uint32_t vendorVersion
 Vendor version.
 
uint32_t maxBlockLength
 Maximum block length united as byte.
 
uint32_t maxBlockCount
 Maximum block count can be set one time.
 
uint32_t flags
 Capability flags to indicate the support information(_sdhc_capability_flag)
 
struct sdhc_transfer_config_t

Define structure to configure the transfer-related command index/argument/flags and data block size/data block numbers. This structure needs to be filled each time a command is sent to the card.

Data Fields

size_t dataBlockSize
 Data block size.
 
uint32_t dataBlockCount
 Data block count.
 
uint32_t commandArgument
 Command argument.
 
uint32_t commandIndex
 Command index.
 
uint32_t flags
 Transfer flags(_sdhc_transfer_flag)
 
struct sdhc_boot_config_t

Data Fields

uint32_t ackTimeoutCount
 Timeout value for the boot ACK. More...
 
sdhc_boot_mode_t bootMode
 Boot mode selection. More...
 
uint32_t blockCount
 Stop at block gap value of automatic mode. More...
 
bool enableBootAck
 Enable or disable boot ACK.
 
bool enableBoot
 Enable or disable fast boot.
 
bool enableAutoStopAtBlockGap
 Enable or disable auto stop at block gap function in boot period.
 

Field Documentation

uint32_t sdhc_boot_config_t::ackTimeoutCount

The available range is 0 ~ 15.

sdhc_boot_mode_t sdhc_boot_config_t::bootMode
uint32_t sdhc_boot_config_t::blockCount

Available range is 0 ~ 65535.

struct sdhc_config_t

Data Fields

bool cardDetectDat3
 Enable DAT3 as card detection pin.
 
sdhc_endian_mode_t endianMode
 Endian mode.
 
sdhc_dma_mode_t dmaMode
 DMA mode.
 
uint32_t readWatermarkLevel
 Watermark level for DMA read operation. More...
 
uint32_t writeWatermarkLevel
 Watermark level for DMA write operation. More...
 

Field Documentation

uint32_t sdhc_config_t::readWatermarkLevel

Available range is 1 ~ 128.

uint32_t sdhc_config_t::writeWatermarkLevel

Available range is 1 ~ 128.

struct sdhc_data_t

Defines a structure to contain data-related attribute. 'enableIgnoreError' is used for the case that upper card driver want to ignore the error event to read/write all the data not to stop read/write immediately when error event happen for example bus testing procedure for MMC card.

Data Fields

bool enableAutoCommand12
 Enable auto CMD12.
 
bool enableIgnoreError
 Enable to ignore error event to read/write all the data.
 
size_t blockSize
 Block size.
 
uint32_t blockCount
 Block count.
 
uint32_t * rxData
 Buffer to save data read.
 
const uint32_t * txData
 Data buffer to write.
 
struct sdhc_command_t

Define card command-related attribute.

Data Fields

uint32_t index
 Command index.
 
uint32_t argument
 Command argument.
 
sdhc_card_command_type_t type
 Command type.
 
sdhc_card_response_type_t responseType
 Command response type.
 
uint32_t response [4U]
 Response for this command.
 
uint32_t responseErrorFlags
 response error flag, the flag which need to check the command reponse
 
struct sdhc_transfer_t

Data Fields

sdhc_data_tdata
 Data to transfer.
 
sdhc_command_tcommand
 Command to send.
 
struct sdhc_transfer_callback_t

Data Fields

void(* CardInserted )(SDHC_Type *base, void *userData)
 Card inserted occurs when DAT3/CD pin is for card detect.
 
void(* CardRemoved )(SDHC_Type *base, void *userData)
 Card removed occurs.
 
void(* SdioInterrupt )(SDHC_Type *base, void *userData)
 SDIO card interrupt occurs.
 
void(* SdioBlockGap )(SDHC_Type *base, void *userData)
 SDIO card stopped at block gap occurs.
 
void(* TransferComplete )(SDHC_Type *base, sdhc_handle_t *handle, status_t status, void *userData)
 Transfer complete callback.
 
struct _sdhc_handle

SDHC handle typedef.

Defines the structure to save the SDHC state information and callback function. The detailed interrupt status when sending a command or transfering data can be obtained from the interruptFlags field by using the mask defined in sdhc_interrupt_flag_t.

Note
All the fields except interruptFlags and transferredWords must be allocated by the user.

Data Fields

sdhc_data_t *volatile data
 Data to transfer.
 
sdhc_command_t *volatile command
 Command to send.
 
volatile uint32_t interruptFlags
 Interrupt flags of last transaction.
 
volatile uint32_t transferredWords
 Words transferred by DATAPORT way.
 
sdhc_transfer_callback_t callback
 Callback function.
 
void * userData
 Parameter for transfer complete callback.
 
struct sdhc_host_t

Data Fields

SDHC_Type * base
 SDHC peripheral base address.
 
uint32_t sourceClock_Hz
 SDHC source clock frequency united in Hz.
 
sdhc_config_t config
 SDHC configuration.
 
sdhc_capability_t capability
 SDHC capability information.
 
sdhc_transfer_function_t transfer
 SDHC transfer function.
 

Macro Definition Documentation

#define FSL_SDHC_DRIVER_VERSION   (MAKE_VERSION(2U, 1U, 6U))

Typedef Documentation

typedef uint32_t sdhc_adma1_descriptor_t
typedef status_t(* sdhc_transfer_function_t)(SDHC_Type *base, sdhc_transfer_t *content)

Enumeration Type Documentation

Enumerator
kStatus_SDHC_BusyTransferring 

Transfer is on-going.

kStatus_SDHC_PrepareAdmaDescriptorFailed 

Set DMA descriptor failed.

kStatus_SDHC_SendCommandFailed 

Send command failed.

kStatus_SDHC_TransferDataFailed 

Transfer data failed.

kStatus_SDHC_DMADataBufferAddrNotAlign 

data buffer addr not align in DMA mode

Enumerator
kSDHC_SupportAdmaFlag 

Support ADMA.

kSDHC_SupportHighSpeedFlag 

Support high-speed.

kSDHC_SupportDmaFlag 

Support DMA.

kSDHC_SupportSuspendResumeFlag 

Support suspend/resume.

kSDHC_SupportV330Flag 

Support voltage 3.3V.

kSDHC_Support4BitFlag 

Support 4 bit mode.

kSDHC_Support8BitFlag 

Support 8 bit mode.

Enumerator
kSDHC_WakeupEventOnCardInt 

Wakeup on card interrupt.

kSDHC_WakeupEventOnCardInsert 

Wakeup on card insertion.

kSDHC_WakeupEventOnCardRemove 

Wakeup on card removal.

kSDHC_WakeupEventsAll 

All wakeup events.

Enumerator
kSDHC_ResetAll 

Reset all except card detection.

kSDHC_ResetCommand 

Reset command line.

kSDHC_ResetData 

Reset data line.

kSDHC_ResetsAll 

All reset types.

Enumerator
kSDHC_EnableDmaFlag 

Enable DMA.

kSDHC_CommandTypeSuspendFlag 

Suspend command.

kSDHC_CommandTypeResumeFlag 

Resume command.

kSDHC_CommandTypeAbortFlag 

Abort command.

kSDHC_EnableBlockCountFlag 

Enable block count.

kSDHC_EnableAutoCommand12Flag 

Enable auto CMD12.

kSDHC_DataReadFlag 

Enable data read.

kSDHC_MultipleBlockFlag 

Multiple block data read/write.

kSDHC_ResponseLength136Flag 

136 bit response length

kSDHC_ResponseLength48Flag 

48 bit response length

kSDHC_ResponseLength48BusyFlag 

48 bit response length with busy status

kSDHC_EnableCrcCheckFlag 

Enable CRC check.

kSDHC_EnableIndexCheckFlag 

Enable index check.

kSDHC_DataPresentFlag 

Data present flag.

Enumerator
kSDHC_CommandInhibitFlag 

Command inhibit.

kSDHC_DataInhibitFlag 

Data inhibit.

kSDHC_DataLineActiveFlag 

Data line active.

kSDHC_SdClockStableFlag 

SD bus clock stable.

kSDHC_WriteTransferActiveFlag 

Write transfer active.

kSDHC_ReadTransferActiveFlag 

Read transfer active.

kSDHC_BufferWriteEnableFlag 

Buffer write enable.

kSDHC_BufferReadEnableFlag 

Buffer read enable.

kSDHC_CardInsertedFlag 

Card inserted.

kSDHC_CommandLineLevelFlag 

Command line signal level.

kSDHC_Data0LineLevelFlag 

Data0 line signal level.

kSDHC_Data1LineLevelFlag 

Data1 line signal level.

kSDHC_Data2LineLevelFlag 

Data2 line signal level.

kSDHC_Data3LineLevelFlag 

Data3 line signal level.

kSDHC_Data4LineLevelFlag 

Data4 line signal level.

kSDHC_Data5LineLevelFlag 

Data5 line signal level.

kSDHC_Data6LineLevelFlag 

Data6 line signal level.

kSDHC_Data7LineLevelFlag 

Data7 line signal level.

Enumerator
kSDHC_CommandCompleteFlag 

Command complete.

kSDHC_DataCompleteFlag 

Data complete.

kSDHC_BlockGapEventFlag 

Block gap event.

kSDHC_DmaCompleteFlag 

DMA interrupt.

kSDHC_BufferWriteReadyFlag 

Buffer write ready.

kSDHC_BufferReadReadyFlag 

Buffer read ready.

kSDHC_CardInsertionFlag 

Card inserted.

kSDHC_CardRemovalFlag 

Card removed.

kSDHC_CardInterruptFlag 

Card interrupt.

kSDHC_CommandTimeoutFlag 

Command timeout error.

kSDHC_CommandCrcErrorFlag 

Command CRC error.

kSDHC_CommandEndBitErrorFlag 

Command end bit error.

kSDHC_CommandIndexErrorFlag 

Command index error.

kSDHC_DataTimeoutFlag 

Data timeout error.

kSDHC_DataCrcErrorFlag 

Data CRC error.

kSDHC_DataEndBitErrorFlag 

Data end bit error.

kSDHC_AutoCommand12ErrorFlag 

Auto CMD12 error.

kSDHC_DmaErrorFlag 

DMA error.

kSDHC_CommandErrorFlag 

Command error.

kSDHC_DataErrorFlag 

Data error.

kSDHC_ErrorFlag 

All error.

kSDHC_DataFlag 

Data interrupts.

kSDHC_CommandFlag 

Command interrupts.

kSDHC_CardDetectFlag 

Card detection interrupts.

kSDHC_AllInterruptFlags 

All flags mask.

Enumerator
kSDHC_AutoCommand12NotExecutedFlag 

Not executed error.

kSDHC_AutoCommand12TimeoutFlag 

Timeout error.

kSDHC_AutoCommand12EndBitErrorFlag 

End bit error.

kSDHC_AutoCommand12CrcErrorFlag 

CRC error.

kSDHC_AutoCommand12IndexErrorFlag 

Index error.

kSDHC_AutoCommand12NotIssuedFlag 

Not issued error.

Enumerator
kSDHC_AdmaLenghMismatchFlag 

Length mismatch error.

kSDHC_AdmaDescriptorErrorFlag 

Descriptor error.

This state is the detail state when ADMA error has occurred.

Enumerator
kSDHC_AdmaErrorStateStopDma 

Stop DMA.

kSDHC_AdmaErrorStateFetchDescriptor 

Fetch descriptor.

kSDHC_AdmaErrorStateChangeAddress 

Change address.

kSDHC_AdmaErrorStateTransferData 

Transfer data.

Enumerator
kSDHC_ForceEventAutoCommand12NotExecuted 

Auto CMD12 not executed error.

kSDHC_ForceEventAutoCommand12Timeout 

Auto CMD12 timeout error.

kSDHC_ForceEventAutoCommand12CrcError 

Auto CMD12 CRC error.

kSDHC_ForceEventEndBitError 

Auto CMD12 end bit error.

kSDHC_ForceEventAutoCommand12IndexError 

Auto CMD12 index error.

kSDHC_ForceEventAutoCommand12NotIssued 

Auto CMD12 not issued error.

kSDHC_ForceEventCommandTimeout 

Command timeout error.

kSDHC_ForceEventCommandCrcError 

Command CRC error.

kSDHC_ForceEventCommandEndBitError 

Command end bit error.

kSDHC_ForceEventCommandIndexError 

Command index error.

kSDHC_ForceEventDataTimeout 

Data timeout error.

kSDHC_ForceEventDataCrcError 

Data CRC error.

kSDHC_ForceEventDataEndBitError 

Data end bit error.

kSDHC_ForceEventAutoCommand12Error 

Auto CMD12 error.

kSDHC_ForceEventCardInt 

Card interrupt.

kSDHC_ForceEventDmaError 

Dma error.

kSDHC_ForceEventsAll 

All force event flags mask.

Enumerator
kSDHC_DataBusWidth1Bit 

1-bit mode

kSDHC_DataBusWidth4Bit 

4-bit mode

kSDHC_DataBusWidth8Bit 

8-bit mode

Enumerator
kSDHC_EndianModeBig 

Big endian mode.

kSDHC_EndianModeHalfWordBig 

Half word big endian mode.

kSDHC_EndianModeLittle 

Little endian mode.

Enumerator
kSDHC_DmaModeNo 

No DMA.

kSDHC_DmaModeAdma1 

ADMA1 is selected.

kSDHC_DmaModeAdma2 

ADMA2 is selected.

Enumerator
kSDHC_StopAtBlockGapFlag 

Stop at block gap.

kSDHC_ReadWaitControlFlag 

Read wait control.

kSDHC_InterruptAtBlockGapFlag 

Interrupt at block gap.

kSDHC_ExactBlockNumberReadFlag 

Exact block number read.

Enumerator
kSDHC_BootModeNormal 

Normal boot.

kSDHC_BootModeAlternative 

Alternative boot.

Enumerator
kCARD_CommandTypeNormal 

Normal command.

kCARD_CommandTypeSuspend 

Suspend command.

kCARD_CommandTypeResume 

Resume command.

kCARD_CommandTypeAbort 

Abort command.

Define the command response type from card to host controller.

Enumerator
kCARD_ResponseTypeNone 

Response type: none.

kCARD_ResponseTypeR1 

Response type: R1.

kCARD_ResponseTypeR1b 

Response type: R1b.

kCARD_ResponseTypeR2 

Response type: R2.

kCARD_ResponseTypeR3 

Response type: R3.

kCARD_ResponseTypeR4 

Response type: R4.

kCARD_ResponseTypeR5 

Response type: R5.

kCARD_ResponseTypeR5b 

Response type: R5b.

kCARD_ResponseTypeR6 

Response type: R6.

kCARD_ResponseTypeR7 

Response type: R7.

Enumerator
kSDHC_Adma1DescriptorValidFlag 

Valid flag.

kSDHC_Adma1DescriptorEndFlag 

End flag.

kSDHC_Adma1DescriptorInterrupFlag 

Interrupt flag.

kSDHC_Adma1DescriptorActivity1Flag 

Activity 1 flag.

kSDHC_Adma1DescriptorActivity2Flag 

Activity 2 flag.

kSDHC_Adma1DescriptorTypeNop 

No operation.

kSDHC_Adma1DescriptorTypeTransfer 

Transfer data.

kSDHC_Adma1DescriptorTypeLink 

Link descriptor.

kSDHC_Adma1DescriptorTypeSetLength 

Set data length.

Enumerator
kSDHC_Adma2DescriptorValidFlag 

Valid flag.

kSDHC_Adma2DescriptorEndFlag 

End flag.

kSDHC_Adma2DescriptorInterruptFlag 

Interrupt flag.

kSDHC_Adma2DescriptorActivity1Flag 

Activity 1 mask.

kSDHC_Adma2DescriptorActivity2Flag 

Activity 2 mask.

kSDHC_Adma2DescriptorTypeNop 

No operation.

kSDHC_Adma2DescriptorTypeReserved 

Reserved.

kSDHC_Adma2DescriptorTypeTransfer 

Transfer type.

kSDHC_Adma2DescriptorTypeLink 

Link type.

Function Documentation

void SDHC_Init ( SDHC_Type *  base,
const sdhc_config_t config 
)

Configures the SDHC according to the user configuration.

Example:

config.cardDetectDat3 = false;
config.readWatermarkLevel = 128U;
config.writeWatermarkLevel = 128U;
SDHC_Init(SDHC, &config);
Parameters
baseSDHC peripheral base address.
configSDHC configuration information.
Return values
kStatus_SuccessOperate successfully.
void SDHC_Deinit ( SDHC_Type *  base)
Parameters
baseSDHC peripheral base address.
bool SDHC_Reset ( SDHC_Type *  base,
uint32_t  mask,
uint32_t  timeout 
)
Parameters
baseSDHC peripheral base address.
maskThe reset type mask(_sdhc_reset).
timeoutTimeout for reset.
Return values
trueReset successfully.
falseReset failed.
status_t SDHC_SetAdmaTableConfig ( SDHC_Type *  base,
sdhc_dma_mode_t  dmaMode,
uint32_t *  table,
uint32_t  tableWords,
const uint32_t *  data,
uint32_t  dataBytes 
)
Parameters
baseSDHC peripheral base address.
dmaModeDMA mode.
tableADMA table address.
tableWordsADMA table buffer length united as Words.
dataData buffer address.
dataBytesData length united as bytes.
Return values
kStatus_OutOfRangeADMA descriptor table length isn't enough to describe data.
kStatus_SuccessOperate successfully.
static void SDHC_EnableInterruptStatus ( SDHC_Type *  base,
uint32_t  mask 
)
inlinestatic
Parameters
baseSDHC peripheral base address.
maskInterrupt status flags mask(_sdhc_interrupt_status_flag).
static void SDHC_DisableInterruptStatus ( SDHC_Type *  base,
uint32_t  mask 
)
inlinestatic
Parameters
baseSDHC peripheral base address.
maskThe interrupt status flags mask(_sdhc_interrupt_status_flag).
static void SDHC_EnableInterruptSignal ( SDHC_Type *  base,
uint32_t  mask 
)
inlinestatic
Parameters
baseSDHC peripheral base address.
maskThe interrupt status flags mask(_sdhc_interrupt_status_flag).
static void SDHC_DisableInterruptSignal ( SDHC_Type *  base,
uint32_t  mask 
)
inlinestatic
Parameters
baseSDHC peripheral base address.
maskThe interrupt status flags mask(_sdhc_interrupt_status_flag).
static uint32_t SDHC_GetInterruptStatusFlags ( SDHC_Type *  base)
inlinestatic
Parameters
baseSDHC peripheral base address.
Returns
Current interrupt status flags mask(_sdhc_interrupt_status_flag).
static void SDHC_ClearInterruptStatusFlags ( SDHC_Type *  base,
uint32_t  mask 
)
inlinestatic
Parameters
baseSDHC peripheral base address.
maskThe interrupt status flags mask(_sdhc_interrupt_status_flag).
static uint32_t SDHC_GetAutoCommand12ErrorStatusFlags ( SDHC_Type *  base)
inlinestatic
Parameters
baseSDHC peripheral base address.
Returns
Auto command 12 error status flags mask(_sdhc_auto_command12_error_status_flag).
static uint32_t SDHC_GetAdmaErrorStatusFlags ( SDHC_Type *  base)
inlinestatic
Parameters
baseSDHC peripheral base address.
Returns
ADMA error status flags mask(_sdhc_adma_error_status_flag).
static uint32_t SDHC_GetPresentStatusFlags ( SDHC_Type *  base)
inlinestatic

This function gets the present SDHC's status except for an interrupt status and an error status.

Parameters
baseSDHC peripheral base address.
Returns
Present SDHC's status flags mask(_sdhc_present_status_flag).
void SDHC_GetCapability ( SDHC_Type *  base,
sdhc_capability_t capability 
)
Parameters
baseSDHC peripheral base address.
capabilityStructure to save capability information.
static void SDHC_EnableSdClock ( SDHC_Type *  base,
bool  enable 
)
inlinestatic
Parameters
baseSDHC peripheral base address.
enableTrue to enable, false to disable.
uint32_t SDHC_SetSdClock ( SDHC_Type *  base,
uint32_t  srcClock_Hz,
uint32_t  busClock_Hz 
)
Parameters
baseSDHC peripheral base address.
srcClock_HzSDHC source clock frequency united in Hz.
busClock_HzSD bus clock frequency united in Hz.
Returns
The nearest frequency of busClock_Hz configured to SD bus.
bool SDHC_SetCardActive ( SDHC_Type *  base,
uint32_t  timeout 
)

This function must be called each time the card is inserted to ensure that the card can receive the command correctly.

Parameters
baseSDHC peripheral base address.
timeoutTimeout to initialize card.
Return values
trueSet card active successfully.
falseSet card active failed.
static void SDHC_SetDataBusWidth ( SDHC_Type *  base,
sdhc_data_bus_width_t  width 
)
inlinestatic
Parameters
baseSDHC peripheral base address.
widthData transfer width.
static void SDHC_CardDetectByData3 ( SDHC_Type *  base,
bool  enable 
)
inlinestatic
Parameters
baseSDHC peripheral base address.
enable/disableflag
void SDHC_SetTransferConfig ( SDHC_Type *  base,
const sdhc_transfer_config_t config 
)

This function fills the card transfer-related command argument/transfer flag/data size. The command and data are sent by SDHC after calling this function.

Example:

sdhc_transfer_config_t transferConfig;
transferConfig.dataBlockSize = 512U;
transferConfig.dataBlockCount = 2U;
transferConfig.commandArgument = 0x01AAU;
transferConfig.commandIndex = 8U;
SDHC_SetTransferConfig(SDHC, &transferConfig);
Parameters
baseSDHC peripheral base address.
configCommand configuration structure.
static uint32_t SDHC_GetCommandResponse ( SDHC_Type *  base,
uint32_t  index 
)
inlinestatic
Parameters
baseSDHC peripheral base address.
indexThe index of response register, range from 0 to 3.
Returns
Response register transfer.
static void SDHC_WriteData ( SDHC_Type *  base,
uint32_t  data 
)
inlinestatic

This function is used to implement the data transfer by Data Port instead of DMA.

Parameters
baseSDHC peripheral base address.
dataThe data about to be sent.
static uint32_t SDHC_ReadData ( SDHC_Type *  base)
inlinestatic

This function is used to implement the data transfer by Data Port instead of DMA.

Parameters
baseSDHC peripheral base address.
Returns
The data has been read.
static void SDHC_EnableWakeupEvent ( SDHC_Type *  base,
uint32_t  mask,
bool  enable 
)
inlinestatic
Parameters
baseSDHC peripheral base address.
maskWakeup events mask(_sdhc_wakeup_event).
enableTrue to enable, false to disable.
static void SDHC_EnableCardDetectTest ( SDHC_Type *  base,
bool  enable 
)
inlinestatic
Parameters
baseSDHC peripheral base address.
enableTrue to enable, false to disable.
static void SDHC_SetCardDetectTestLevel ( SDHC_Type *  base,
bool  high 
)
inlinestatic

This function sets the card detection test level to indicate whether the card is inserted into the SDHC when DAT[3]/ CD pin is selected as a card detection pin. This function can also assert the pin logic when DAT[3]/CD pin is selected as the card detection pin.

Parameters
baseSDHC peripheral base address.
highTrue to set the card detect level to high.
void SDHC_EnableSdioControl ( SDHC_Type *  base,
uint32_t  mask,
bool  enable 
)
Parameters
baseSDHC peripheral base address.
maskSDIO card control flags mask(_sdhc_sdio_control_flag).
enableTrue to enable, false to disable.
static void SDHC_SetContinueRequest ( SDHC_Type *  base)
inlinestatic
Parameters
baseSDHC peripheral base address.
void SDHC_SetMmcBootConfig ( SDHC_Type *  base,
const sdhc_boot_config_t config 
)

Example:

config.ackTimeoutCount = 4;
config.blockCount = 5;
config.enableBootAck = true;
config.enableBoot = true;
SDHC_SetMmcBootConfig(SDHC, &config);
Parameters
baseSDHC peripheral base address.
configThe MMC boot configuration information.
static void SDHC_SetForceEvent ( SDHC_Type *  base,
uint32_t  mask 
)
inlinestatic
Parameters
baseSDHC peripheral base address.
maskThe force events mask(_sdhc_force_event).
status_t SDHC_TransferBlocking ( SDHC_Type *  base,
uint32_t *  admaTable,
uint32_t  admaTableWords,
sdhc_transfer_t transfer 
)

This function waits until the command response/data is received or the SDHC encounters an error by polling the status flag. This function support non word align data addr transfer support, if data buffer addr is not align in DMA mode, the API will continue finish the transfer by polling IO directly The application must not call this API in multiple threads at the same time. Because of that this API doesn't support the re-entry mechanism.

Note
There is no need to call the API 'SDHC_TransferCreateHandle' when calling this API.
Parameters
baseSDHC peripheral base address.
admaTableADMA table address, can't be null if transfer way is ADMA1/ADMA2.
admaTableWordsADMA table length united as words, can't be 0 if transfer way is ADMA1/ADMA2.
transferTransfer content.
Return values
kStatus_InvalidArgumentArgument is invalid.
kStatus_SDHC_PrepareAdmaDescriptorFailedPrepare ADMA descriptor failed.
kStatus_SDHC_SendCommandFailedSend command failed.
kStatus_SDHC_TransferDataFailedTransfer data failed.
kStatus_SuccessOperate successfully.
void SDHC_TransferCreateHandle ( SDHC_Type *  base,
sdhc_handle_t *  handle,
const sdhc_transfer_callback_t callback,
void *  userData 
)
Parameters
baseSDHC peripheral base address.
handleSDHC handle pointer.
callbackStructure pointer to contain all callback functions.
userDataCallback function parameter.
status_t SDHC_TransferNonBlocking ( SDHC_Type *  base,
sdhc_handle_t *  handle,
uint32_t *  admaTable,
uint32_t  admaTableWords,
sdhc_transfer_t transfer 
)

This function sends a command and data and returns immediately. It doesn't wait the transfer complete or encounter an error. This function support non word align data addr transfer support, if data buffer addr is not align in DMA mode, the API will continue finish the transfer by polling IO directly The application must not call this API in multiple threads at the same time. Because of that this API doesn't support the re-entry mechanism.

Note
Call the API 'SDHC_TransferCreateHandle' when calling this API.
Parameters
baseSDHC peripheral base address.
handleSDHC handle.
admaTableADMA table address, can't be null if transfer way is ADMA1/ADMA2.
admaTableWordsADMA table length united as words, can't be 0 if transfer way is ADMA1/ADMA2.
transferTransfer content.
Return values
kStatus_InvalidArgumentArgument is invalid.
kStatus_SDHC_BusyTransferringBusy transferring.
kStatus_SDHC_PrepareAdmaDescriptorFailedPrepare ADMA descriptor failed.
kStatus_SuccessOperate successfully.
void SDHC_TransferHandleIRQ ( SDHC_Type *  base,
sdhc_handle_t *  handle 
)

This function deals with the IRQs on the given host controller.

Parameters
baseSDHC peripheral base address.
handleSDHC handle.