![]() |
MCUXpresso SDK API Reference Manual
Rev 2.11.0
NXP Semiconductors
|
This section describes the programming interface of the CAAM Non-blocking RNG driver.
Functions | |
| status_t | CAAM_RNG_GetRandomDataNonBlocking (CAAM_Type *base, caam_handle_t *handle, caam_rng_state_handle_t stateHandle, caam_desc_rng_t descriptor, void *data, size_t dataSize, caam_rng_random_type_t dataType, caam_rng_generic256_t additionalEntropy) |
| Request random data. More... | |
| status_t CAAM_RNG_GetRandomDataNonBlocking | ( | CAAM_Type * | base, |
| caam_handle_t * | handle, | ||
| caam_rng_state_handle_t | stateHandle, | ||
| caam_desc_rng_t | descriptor, | ||
| void * | data, | ||
| size_t | dataSize, | ||
| caam_rng_random_type_t | dataType, | ||
| caam_rng_generic256_t | additionalEntropy | ||
| ) |
This function schedules the request for random data from CAAM RNG. Memory at memory pointers will be accessed by CAAM shortly after this function returns, according to actual CAAM schedule.
| base | CAAM peripheral base address | |
| handle | RNG handle used for this request | |
| stateHandle | RNG state handle used to generate random data | |
| [out] | descriptor | memory for CAAM commands |
| [out] | data | Pointer address used to store random data |
| dataSize | Size of the buffer pointed by the data parameter, in bytes. | |
| dataType | Type of random data to be generated. | |
| additionalEntropy | NULL or Pointer to optional 256-bit additional entropy. |