![]() |
MCUXpresso SDK API Reference Manual
Rev 2.11.0
NXP Semiconductors
|
This section describes the programming interface of the CAAM Non-blocking AES driver.
Functions | |
| status_t | CAAM_AES_EncryptEcbNonBlocking (CAAM_Type *base, caam_handle_t *handle, caam_desc_aes_ecb_t descriptor, const uint8_t *plaintext, uint8_t *ciphertext, size_t size, const uint8_t *key, size_t keySize) |
| Encrypts AES using the ECB block mode. More... | |
| status_t | CAAM_AES_DecryptEcbNonBlocking (CAAM_Type *base, caam_handle_t *handle, caam_desc_aes_ecb_t descriptor, const uint8_t *ciphertext, uint8_t *plaintext, size_t size, const uint8_t *key, size_t keySize) |
| Decrypts AES using ECB block mode. More... | |
| status_t | CAAM_AES_EncryptCbcNonBlocking (CAAM_Type *base, caam_handle_t *handle, caam_desc_aes_cbc_t descriptor, const uint8_t *plaintext, uint8_t *ciphertext, size_t size, const uint8_t *iv, const uint8_t *key, size_t keySize) |
| Encrypts AES using CBC block mode. More... | |
| status_t | CAAM_AES_DecryptCbcNonBlocking (CAAM_Type *base, caam_handle_t *handle, caam_desc_aes_cbc_t descriptor, const uint8_t *ciphertext, uint8_t *plaintext, size_t size, const uint8_t *iv, const uint8_t *key, size_t keySize) |
| Decrypts AES using CBC block mode. More... | |
| status_t | CAAM_AES_CryptCtrNonBlocking (CAAM_Type *base, caam_handle_t *handle, caam_desc_aes_ctr_t descriptor, const uint8_t *input, uint8_t *output, size_t size, uint8_t *counter, const uint8_t *key, size_t keySize, uint8_t *counterlast, size_t *szLeft) |
| Encrypts or decrypts AES using CTR block mode. More... | |
| status_t | CAAM_AES_EncryptTagCcmNonBlocking (CAAM_Type *base, caam_handle_t *handle, caam_desc_aes_ccm_t descriptor, const uint8_t *plaintext, uint8_t *ciphertext, size_t size, const uint8_t *iv, size_t ivSize, const uint8_t *aad, size_t aadSize, const uint8_t *key, size_t keySize, uint8_t *tag, size_t tagSize) |
| Encrypts AES and tags using CCM block mode. More... | |
| status_t | CAAM_AES_DecryptTagCcmNonBlocking (CAAM_Type *base, caam_handle_t *handle, caam_desc_aes_ccm_t descriptor, const uint8_t *ciphertext, uint8_t *plaintext, size_t size, const uint8_t *iv, size_t ivSize, const uint8_t *aad, size_t aadSize, const uint8_t *key, size_t keySize, const uint8_t *tag, size_t tagSize) |
| Decrypts AES and authenticates using CCM block mode. More... | |
| status_t | CAAM_AES_EncryptTagGcmNonBlocking (CAAM_Type *base, caam_handle_t *handle, caam_desc_aes_gcm_t descriptor, const uint8_t *plaintext, uint8_t *ciphertext, size_t size, const uint8_t *iv, size_t ivSize, const uint8_t *aad, size_t aadSize, const uint8_t *key, size_t keySize, uint8_t *tag, size_t tagSize) |
| Encrypts AES and tags using GCM block mode. More... | |
| status_t | CAAM_AES_DecryptTagGcmNonBlocking (CAAM_Type *base, caam_handle_t *handle, caam_desc_aes_gcm_t descriptor, const uint8_t *ciphertext, uint8_t *plaintext, size_t size, const uint8_t *iv, size_t ivSize, const uint8_t *aad, size_t aadSize, const uint8_t *key, size_t keySize, const uint8_t *tag, size_t tagSize) |
| Decrypts AES and authenticates using GCM block mode. More... | |
| status_t CAAM_AES_EncryptEcbNonBlocking | ( | CAAM_Type * | base, |
| caam_handle_t * | handle, | ||
| caam_desc_aes_ecb_t | descriptor, | ||
| const uint8_t * | plaintext, | ||
| uint8_t * | ciphertext, | ||
| size_t | size, | ||
| const uint8_t * | key, | ||
| size_t | keySize | ||
| ) |
Puts AES ECB encrypt descriptor to CAAM input job ring.
| base | CAAM peripheral base address | |
| handle | Handle used for this request. Specifies jobRing. | |
| plaintext | Input plain text to encrypt | |
| [out] | descriptor | Memory for the CAAM descriptor. |
| [out] | ciphertext | Output cipher text |
| size | Size of input and output data in bytes. Must be multiple of 16 bytes. | |
| key | Input key to use for encryption | |
| keySize | Size of the input key, in bytes. Must be 16, 24, or 32. |
| status_t CAAM_AES_DecryptEcbNonBlocking | ( | CAAM_Type * | base, |
| caam_handle_t * | handle, | ||
| caam_desc_aes_ecb_t | descriptor, | ||
| const uint8_t * | ciphertext, | ||
| uint8_t * | plaintext, | ||
| size_t | size, | ||
| const uint8_t * | key, | ||
| size_t | keySize | ||
| ) |
Puts AES ECB decrypt descriptor to CAAM input job ring.
| base | CAAM peripheral base address | |
| handle | Handle used for this request. Specifies jobRing. | |
| [out] | descriptor | Memory for the CAAM descriptor. |
| ciphertext | Input cipher text to decrypt | |
| [out] | plaintext | Output plain text |
| size | Size of input and output data in bytes. Must be multiple of 16 bytes. | |
| key | Input key. | |
| keySize | Size of the input key, in bytes. Must be 16, 24, or 32. |
| status_t CAAM_AES_EncryptCbcNonBlocking | ( | CAAM_Type * | base, |
| caam_handle_t * | handle, | ||
| caam_desc_aes_cbc_t | descriptor, | ||
| const uint8_t * | plaintext, | ||
| uint8_t * | ciphertext, | ||
| size_t | size, | ||
| const uint8_t * | iv, | ||
| const uint8_t * | key, | ||
| size_t | keySize | ||
| ) |
Puts AES CBC encrypt descriptor to CAAM input job ring.
| base | CAAM peripheral base address | |
| handle | Handle used for this request. Specifies jobRing. | |
| [out] | descriptor | Memory for the CAAM descriptor. |
| plaintext | Input plain text to encrypt | |
| [out] | ciphertext | Output cipher text |
| size | Size of input and output data in bytes. Must be multiple of 16 bytes. | |
| iv | Input initial vector to combine with the first input block. | |
| key | Input key to use for encryption | |
| keySize | Size of the input key, in bytes. Must be 16, 24, or 32. |
| status_t CAAM_AES_DecryptCbcNonBlocking | ( | CAAM_Type * | base, |
| caam_handle_t * | handle, | ||
| caam_desc_aes_cbc_t | descriptor, | ||
| const uint8_t * | ciphertext, | ||
| uint8_t * | plaintext, | ||
| size_t | size, | ||
| const uint8_t * | iv, | ||
| const uint8_t * | key, | ||
| size_t | keySize | ||
| ) |
Puts AES CBC decrypt descriptor to CAAM input job ring.
| base | CAAM peripheral base address | |
| handle | Handle used for this request. Specifies jobRing. | |
| [out] | descriptor | Memory for the CAAM descriptor. |
| ciphertext | Input cipher text to decrypt | |
| [out] | plaintext | Output plain text |
| size | Size of input and output data in bytes. Must be multiple of 16 bytes. | |
| iv | Input initial vector to combine with the first input block. | |
| key | Input key to use for decryption | |
| keySize | Size of the input key, in bytes. Must be 16, 24, or 32. |
| status_t CAAM_AES_CryptCtrNonBlocking | ( | CAAM_Type * | base, |
| caam_handle_t * | handle, | ||
| caam_desc_aes_ctr_t | descriptor, | ||
| const uint8_t * | input, | ||
| uint8_t * | output, | ||
| size_t | size, | ||
| uint8_t * | counter, | ||
| const uint8_t * | key, | ||
| size_t | keySize, | ||
| uint8_t * | counterlast, | ||
| size_t * | szLeft | ||
| ) |
Encrypts or decrypts AES using CTR block mode. AES CTR mode uses only forward AES cipher and same algorithm for encryption and decryption. The only difference between encryption and decryption is that, for encryption, the input argument is plain text and the output argument is cipher text. For decryption, the input argument is cipher text and the output argument is plain text.
Puts AES CTR crypt descriptor to CAAM input job ring.
| base | CAAM peripheral base address | |
| handle | Handle used for this request. Specifies jobRing. | |
| [out] | descriptor | Memory for the CAAM descriptor. |
| input | Input data for CTR block mode | |
| [out] | output | Output data for CTR block mode |
| size | Size of input and output data in bytes | |
| [in,out] | counter | Input counter (updates on return) |
| key | Input key to use for forward AES cipher | |
| keySize | Size of the input key, in bytes. Must be 16, 24, or 32. | |
| [out] | counterlast | Output cipher of last counter, for chained CTR calls. NULL can be passed if chained calls are not used. |
| [out] | szLeft | Output number of bytes in left unused in counterlast block. NULL can be passed if chained calls are not used. |
| status_t CAAM_AES_EncryptTagCcmNonBlocking | ( | CAAM_Type * | base, |
| caam_handle_t * | handle, | ||
| caam_desc_aes_ccm_t | descriptor, | ||
| const uint8_t * | plaintext, | ||
| uint8_t * | ciphertext, | ||
| size_t | size, | ||
| const uint8_t * | iv, | ||
| size_t | ivSize, | ||
| const uint8_t * | aad, | ||
| size_t | aadSize, | ||
| const uint8_t * | key, | ||
| size_t | keySize, | ||
| uint8_t * | tag, | ||
| size_t | tagSize | ||
| ) |
Puts AES CCM encrypt and tag descriptor to CAAM input job ring.
| base | CAAM peripheral base address | |
| handle | Handle used for this request. Specifies jobRing. | |
| [out] | descriptor | Memory for the CAAM descriptor. |
| plaintext | Input plain text to encrypt | |
| [out] | ciphertext | Output cipher text. |
| size | Size of input and output data in bytes. Zero means authentication only. | |
| iv | Nonce | |
| ivSize | Length of the Nonce in bytes. Must be 7, 8, 9, 10, 11, 12, or 13. | |
| aad | Input additional authentication data. Can be NULL if aadSize is zero. | |
| aadSize | Input size in bytes of AAD. Zero means data mode only (authentication skipped). | |
| key | Input key to use for encryption | |
| keySize | Size of the input key, in bytes. Must be 16, 24, or 32. | |
| [out] | tag | Generated output tag. Set to NULL to skip tag processing. |
| tagSize | Input size of the tag to generate, in bytes. Must be 4, 6, 8, 10, 12, 14, or 16. |
| status_t CAAM_AES_DecryptTagCcmNonBlocking | ( | CAAM_Type * | base, |
| caam_handle_t * | handle, | ||
| caam_desc_aes_ccm_t | descriptor, | ||
| const uint8_t * | ciphertext, | ||
| uint8_t * | plaintext, | ||
| size_t | size, | ||
| const uint8_t * | iv, | ||
| size_t | ivSize, | ||
| const uint8_t * | aad, | ||
| size_t | aadSize, | ||
| const uint8_t * | key, | ||
| size_t | keySize, | ||
| const uint8_t * | tag, | ||
| size_t | tagSize | ||
| ) |
Puts AES CCM decrypt and check tag descriptor to CAAM input job ring.
| base | CAAM peripheral base address | |
| handle | Handle used for this request. Specifies jobRing. | |
| [out] | descriptor | Memory for the CAAM descriptor. |
| ciphertext | Input cipher text to decrypt | |
| [out] | plaintext | Output plain text. |
| size | Size of input and output data in bytes. Zero means authentication data only. | |
| iv | Nonce | |
| ivSize | Length of the Nonce in bytes. Must be 7, 8, 9, 10, 11, 12, or 13. | |
| aad | Input additional authentication data. Can be NULL if aadSize is zero. | |
| aadSize | Input size in bytes of AAD. Zero means data mode only (authentication data skipped). | |
| key | Input key to use for decryption | |
| keySize | Size of the input key, in bytes. Must be 16, 24, or 32. | |
| tag | Received tag. Set to NULL to skip tag processing. | |
| tagSize | Input size of the received tag to compare with the computed tag, in bytes. Must be 4, 6, 8, 10, 12, 14, or 16. |
| status_t CAAM_AES_EncryptTagGcmNonBlocking | ( | CAAM_Type * | base, |
| caam_handle_t * | handle, | ||
| caam_desc_aes_gcm_t | descriptor, | ||
| const uint8_t * | plaintext, | ||
| uint8_t * | ciphertext, | ||
| size_t | size, | ||
| const uint8_t * | iv, | ||
| size_t | ivSize, | ||
| const uint8_t * | aad, | ||
| size_t | aadSize, | ||
| const uint8_t * | key, | ||
| size_t | keySize, | ||
| uint8_t * | tag, | ||
| size_t | tagSize | ||
| ) |
Encrypts AES and optionally tags using GCM block mode. If plaintext is NULL, only the GHASH is calculated and output in the 'tag' field. Puts AES GCM encrypt and tag descriptor to CAAM input job ring.
| base | CAAM peripheral base address | |
| handle | Handle used for this request. Specifies jobRing. | |
| [out] | descriptor | Memory for the CAAM descriptor. |
| plaintext | Input plain text to encrypt | |
| [out] | ciphertext | Output cipher text. |
| size | Size of input and output data in bytes | |
| iv | Input initial vector | |
| ivSize | Size of the IV | |
| aad | Input additional authentication data | |
| aadSize | Input size in bytes of AAD | |
| key | Input key to use for encryption | |
| keySize | Size of the input key, in bytes. Must be 16, 24, or 32. | |
| [out] | tag | Output hash tag. Set to NULL to skip tag processing. |
| tagSize | Input size of the tag to generate, in bytes. Must be 4,8,12,13,14,15 or 16. |
| status_t CAAM_AES_DecryptTagGcmNonBlocking | ( | CAAM_Type * | base, |
| caam_handle_t * | handle, | ||
| caam_desc_aes_gcm_t | descriptor, | ||
| const uint8_t * | ciphertext, | ||
| uint8_t * | plaintext, | ||
| size_t | size, | ||
| const uint8_t * | iv, | ||
| size_t | ivSize, | ||
| const uint8_t * | aad, | ||
| size_t | aadSize, | ||
| const uint8_t * | key, | ||
| size_t | keySize, | ||
| const uint8_t * | tag, | ||
| size_t | tagSize | ||
| ) |
Decrypts AES and optionally authenticates using GCM block mode. If ciphertext is NULL, only the GHASH is calculated and compared with the received GHASH in 'tag' field. Puts AES GCM decrypt and check tag descriptor to CAAM input job ring.
| base | CAAM peripheral base address | |
| handle | Handle used for this request. Specifies jobRing. | |
| [out] | descriptor | Memory for the CAAM descriptor. |
| ciphertext | Input cipher text to decrypt | |
| [out] | plaintext | Output plain text. |
| size | Size of input and output data in bytes | |
| iv | Input initial vector | |
| ivSize | Size of the IV | |
| aad | Input additional authentication data | |
| aadSize | Input size in bytes of AAD | |
| key | Input key to use for encryption | |
| keySize | Size of the input key, in bytes. Must be 16, 24, or 32. | |
| tag | Input hash tag to compare. Set to NULL to skip tag processing. | |
| tagSize | Input size of the tag, in bytes. Must be 4, 8, 12, 13, 14, 15, or 16. |