![]() |
MCUXpresso SDK API Reference Manual
Rev 2.11.0
NXP Semiconductors
|
Data Structures | |
| struct | ftfx_prefetch_speculation_status_t |
| FTFx prefetch speculation status. More... | |
| struct | ftfx_cache_config_t |
| FTFx cache driver state information. More... | |
Enumerations | |
| enum | _ftfx_cache_ram_func_constants { kFTFx_CACHE_RamFuncMaxSizeInWords = 16U } |
| Constants for execute-in-RAM flash function. More... | |
Functions | |
| status_t | FTFx_CACHE_Init (ftfx_cache_config_t *config) |
| Initializes the global FTFx cache structure members. More... | |
| status_t | FTFx_CACHE_ClearCachePrefetchSpeculation (ftfx_cache_config_t *config, bool isPreProcess) |
| Process the cache/prefetch/speculation to the flash. More... | |
| status_t | FTFx_CACHE_PflashSetPrefetchSpeculation (ftfx_prefetch_speculation_status_t *speculationStatus) |
| Sets the PFlash prefetch speculation to the intended speculation status. More... | |
| status_t | FTFx_CACHE_PflashGetPrefetchSpeculation (ftfx_prefetch_speculation_status_t *speculationStatus) |
| Gets the PFlash prefetch speculation status. More... | |
| struct ftfx_prefetch_speculation_status_t |
Data Fields | |
| bool | instructionOff |
| Instruction speculation. More... | |
| bool | dataOff |
| Data speculation. More... | |
| bool ftfx_prefetch_speculation_status_t::instructionOff |
| bool ftfx_prefetch_speculation_status_t::dataOff |
| struct ftfx_cache_config_t |
An instance of this structure is allocated by the user of the flash driver and passed into each of the driver APIs.
Data Fields | |
| uint8_t | flashMemoryIndex |
| 0 - primary flash; 1 - secondary flash | |
| function_bit_operation_ptr_t | bitOperFuncAddr |
| An buffer point to the flash execute-in-RAM function. More... | |
| function_bit_operation_ptr_t ftfx_cache_config_t::bitOperFuncAddr |
| status_t FTFx_CACHE_Init | ( | ftfx_cache_config_t * | config | ) |
This function checks and initializes the Flash module for the other FTFx cache APIs.
| config | Pointer to the storage for the driver runtime state. |
| kStatus_FTFx_Success | API was executed successfully. |
| kStatus_FTFx_InvalidArgument | An invalid argument is provided. |
| kStatus_FTFx_ExecuteInRamFunctionNotReady | Execute-in-RAM function is not available. |
| status_t FTFx_CACHE_ClearCachePrefetchSpeculation | ( | ftfx_cache_config_t * | config, |
| bool | isPreProcess | ||
| ) |
| config | A pointer to the storage for the driver runtime state. |
| isPreProcess | The possible option used to control flash cache/prefetch/speculation |
| kStatus_FTFx_Success | API was executed successfully. |
| kStatus_FTFx_InvalidArgument | Invalid argument is provided. |
| kStatus_FTFx_ExecuteInRamFunctionNotReady | Execute-in-RAM function is not available. |
| status_t FTFx_CACHE_PflashSetPrefetchSpeculation | ( | ftfx_prefetch_speculation_status_t * | speculationStatus | ) |
| speculationStatus | The expected protect status to set to the PFlash protection register. Each bit is |
| kStatus_FTFx_Success | API was executed successfully. |
| kStatus_FTFx_InvalidSpeculationOption | An invalid speculation option argument is provided. |
| status_t FTFx_CACHE_PflashGetPrefetchSpeculation | ( | ftfx_prefetch_speculation_status_t * | speculationStatus | ) |
| speculationStatus | Speculation status returned by the PFlash IP. |
| kStatus_FTFx_Success | API was executed successfully. |