![]() |
MCUXpresso SDK API Reference Manual
Rev 2.11.0
NXP Semiconductors
|
Data Structures | |
| struct | uart_edma_handle_t |
| UART eDMA handle. More... | |
Typedefs | |
| typedef void(* | uart_edma_transfer_callback_t )(UART_Type *base, uart_edma_handle_t *handle, status_t status, void *userData) |
| UART transfer callback function. More... | |
Driver version | |
| #define | FSL_UART_EDMA_DRIVER_VERSION (MAKE_VERSION(2, 5, 2)) |
| UART EDMA driver version. More... | |
eDMA transactional | |
| void | UART_TransferCreateHandleEDMA (UART_Type *base, uart_edma_handle_t *handle, uart_edma_transfer_callback_t callback, void *userData, edma_handle_t *txEdmaHandle, edma_handle_t *rxEdmaHandle) |
| Initializes the UART handle which is used in transactional functions. More... | |
| status_t | UART_SendEDMA (UART_Type *base, uart_edma_handle_t *handle, uart_transfer_t *xfer) |
| Sends data using eDMA. More... | |
| status_t | UART_ReceiveEDMA (UART_Type *base, uart_edma_handle_t *handle, uart_transfer_t *xfer) |
| Receives data using eDMA. More... | |
| void | UART_TransferAbortSendEDMA (UART_Type *base, uart_edma_handle_t *handle) |
| Aborts the sent data using eDMA. More... | |
| void | UART_TransferAbortReceiveEDMA (UART_Type *base, uart_edma_handle_t *handle) |
| Aborts the receive data using eDMA. More... | |
| status_t | UART_TransferGetSendCountEDMA (UART_Type *base, uart_edma_handle_t *handle, uint32_t *count) |
| Gets the number of bytes that have been written to UART TX register. More... | |
| status_t | UART_TransferGetReceiveCountEDMA (UART_Type *base, uart_edma_handle_t *handle, uint32_t *count) |
| Gets the number of received bytes. More... | |
| void | UART_TransferEdmaHandleIRQ (UART_Type *base, void *uartEdmaHandle) |
| UART eDMA IRQ handle function. More... | |
| struct _uart_edma_handle |
Data Fields | |
| uart_edma_transfer_callback_t | callback |
| Callback function. More... | |
| void * | userData |
| UART callback function parameter. More... | |
| size_t | rxDataSizeAll |
| Size of the data to receive. More... | |
| size_t | txDataSizeAll |
| Size of the data to send out. More... | |
| edma_handle_t * | txEdmaHandle |
| The eDMA TX channel used. More... | |
| edma_handle_t * | rxEdmaHandle |
| The eDMA RX channel used. More... | |
| uint8_t | nbytes |
| eDMA minor byte transfer count initially configured. More... | |
| volatile uint8_t | txState |
| TX transfer state. More... | |
| volatile uint8_t | rxState |
| RX transfer state. | |
| uart_edma_transfer_callback_t uart_edma_handle_t::callback |
| void* uart_edma_handle_t::userData |
| size_t uart_edma_handle_t::rxDataSizeAll |
| size_t uart_edma_handle_t::txDataSizeAll |
| edma_handle_t* uart_edma_handle_t::txEdmaHandle |
| edma_handle_t* uart_edma_handle_t::rxEdmaHandle |
| uint8_t uart_edma_handle_t::nbytes |
| volatile uint8_t uart_edma_handle_t::txState |
| #define FSL_UART_EDMA_DRIVER_VERSION (MAKE_VERSION(2, 5, 2)) |
| typedef void(* uart_edma_transfer_callback_t)(UART_Type *base, uart_edma_handle_t *handle, status_t status, void *userData) |
| void UART_TransferCreateHandleEDMA | ( | UART_Type * | base, |
| uart_edma_handle_t * | handle, | ||
| uart_edma_transfer_callback_t | callback, | ||
| void * | userData, | ||
| edma_handle_t * | txEdmaHandle, | ||
| edma_handle_t * | rxEdmaHandle | ||
| ) |
| base | UART peripheral base address. |
| handle | Pointer to the uart_edma_handle_t structure. |
| callback | UART callback, NULL means no callback. |
| userData | User callback function data. |
| rxEdmaHandle | User-requested DMA handle for RX DMA transfer. |
| txEdmaHandle | User-requested DMA handle for TX DMA transfer. |
| status_t UART_SendEDMA | ( | UART_Type * | base, |
| uart_edma_handle_t * | handle, | ||
| uart_transfer_t * | xfer | ||
| ) |
This function sends data using eDMA. This is a non-blocking function, which returns right away. When all data is sent, the send callback function is called.
| base | UART peripheral base address. |
| handle | UART handle pointer. |
| xfer | UART eDMA transfer structure. See uart_transfer_t. |
| kStatus_Success | if succeeded; otherwise failed. |
| kStatus_UART_TxBusy | Previous transfer ongoing. |
| kStatus_InvalidArgument | Invalid argument. |
| status_t UART_ReceiveEDMA | ( | UART_Type * | base, |
| uart_edma_handle_t * | handle, | ||
| uart_transfer_t * | xfer | ||
| ) |
This function receives data using eDMA. This is a non-blocking function, which returns right away. When all data is received, the receive callback function is called.
| base | UART peripheral base address. |
| handle | Pointer to the uart_edma_handle_t structure. |
| xfer | UART eDMA transfer structure. See uart_transfer_t. |
| kStatus_Success | if succeeded; otherwise failed. |
| kStatus_UART_RxBusy | Previous transfer ongoing. |
| kStatus_InvalidArgument | Invalid argument. |
| void UART_TransferAbortSendEDMA | ( | UART_Type * | base, |
| uart_edma_handle_t * | handle | ||
| ) |
This function aborts sent data using eDMA.
| base | UART peripheral base address. |
| handle | Pointer to the uart_edma_handle_t structure. |
| void UART_TransferAbortReceiveEDMA | ( | UART_Type * | base, |
| uart_edma_handle_t * | handle | ||
| ) |
This function aborts receive data using eDMA.
| base | UART peripheral base address. |
| handle | Pointer to the uart_edma_handle_t structure. |
| status_t UART_TransferGetSendCountEDMA | ( | UART_Type * | base, |
| uart_edma_handle_t * | handle, | ||
| uint32_t * | count | ||
| ) |
This function gets the number of bytes that have been written to UART TX register by DMA.
| base | UART peripheral base address. |
| handle | UART handle pointer. |
| count | Send bytes count. |
| kStatus_NoTransferInProgress | No send in progress. |
| kStatus_InvalidArgument | Parameter is invalid. |
| kStatus_Success | Get successfully through the parameter count; |
| status_t UART_TransferGetReceiveCountEDMA | ( | UART_Type * | base, |
| uart_edma_handle_t * | handle, | ||
| uint32_t * | count | ||
| ) |
This function gets the number of received bytes.
| base | UART peripheral base address. |
| handle | UART handle pointer. |
| count | Receive bytes count. |
| kStatus_NoTransferInProgress | No receive in progress. |
| kStatus_InvalidArgument | Parameter is invalid. |
| kStatus_Success | Get successfully through the parameter count; |
| void UART_TransferEdmaHandleIRQ | ( | UART_Type * | base, |
| void * | uartEdmaHandle | ||
| ) |
This function handles the UART transmit complete IRQ request and invoke user callback.
| base | UART peripheral base address. |
| uartEdmaHandle | UART handle pointer. |