MCUXpresso SDK API Reference Manual  Rev 2.11.0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
PORT: Port Control and Interrupts

Overview

The MCUXpresso SDK provides a driver for the Port Control and Interrupts (PORT) module of MCUXpresso SDK devices.

Data Structures

struct  port_digital_filter_config_t
 PORT digital filter feature configuration definition. More...
 
struct  port_pin_config_t
 PORT pin configuration structure. More...
 

Enumerations

enum  _port_pull {
  kPORT_PullDisable = 0U,
  kPORT_PullDown = 2U,
  kPORT_PullUp = 3U
}
 Internal resistor pull feature selection. More...
 
enum  _port_slew_rate {
  kPORT_FastSlewRate = 0U,
  kPORT_SlowSlewRate = 1U
}
 Slew rate selection. More...
 
enum  _port_open_drain_enable {
  kPORT_OpenDrainDisable = 0U,
  kPORT_OpenDrainEnable = 1U
}
 Open Drain feature enable/disable. More...
 
enum  _port_passive_filter_enable {
  kPORT_PassiveFilterDisable = 0U,
  kPORT_PassiveFilterEnable = 1U
}
 Passive filter feature enable/disable. More...
 
enum  _port_drive_strength {
  kPORT_LowDriveStrength = 0U,
  kPORT_HighDriveStrength = 1U
}
 Configures the drive strength. More...
 
enum  _port_lock_register {
  kPORT_UnlockRegister = 0U,
  kPORT_LockRegister = 1U
}
 Unlock/lock the pin control register field[15:0]. More...
 
enum  port_mux_t {
  kPORT_PinDisabledOrAnalog = 0U,
  kPORT_MuxAsGpio = 1U,
  kPORT_MuxAlt2 = 2U,
  kPORT_MuxAlt3 = 3U,
  kPORT_MuxAlt4 = 4U,
  kPORT_MuxAlt5 = 5U,
  kPORT_MuxAlt6 = 6U,
  kPORT_MuxAlt7 = 7U,
  kPORT_MuxAlt8 = 8U,
  kPORT_MuxAlt9 = 9U,
  kPORT_MuxAlt10 = 10U,
  kPORT_MuxAlt11 = 11U,
  kPORT_MuxAlt12 = 12U,
  kPORT_MuxAlt13 = 13U,
  kPORT_MuxAlt14 = 14U,
  kPORT_MuxAlt15 = 15U
}
 Pin mux selection. More...
 
enum  port_interrupt_t {
  kPORT_InterruptOrDMADisabled = 0x0U,
  kPORT_DMARisingEdge = 0x1U,
  kPORT_DMAFallingEdge = 0x2U,
  kPORT_DMAEitherEdge = 0x3U,
  kPORT_FlagRisingEdge = 0x05U,
  kPORT_FlagFallingEdge = 0x06U,
  kPORT_FlagEitherEdge = 0x07U,
  kPORT_InterruptLogicZero = 0x8U,
  kPORT_InterruptRisingEdge = 0x9U,
  kPORT_InterruptFallingEdge = 0xAU,
  kPORT_InterruptEitherEdge = 0xBU,
  kPORT_InterruptLogicOne = 0xCU,
  kPORT_ActiveHighTriggerOutputEnable = 0xDU,
  kPORT_ActiveLowTriggerOutputEnable = 0xEU
}
 Configures the interrupt generation condition. More...
 
enum  port_digital_filter_clock_source_t {
  kPORT_BusClock = 0U,
  kPORT_LpoClock = 1U
}
 Digital filter clock source selection. More...
 

Driver version

#define FSL_PORT_DRIVER_VERSION   (MAKE_VERSION(2, 2, 0))
 Version 2.1.1. More...
 

Configuration

static void PORT_SetPinConfig (PORT_Type *base, uint32_t pin, const port_pin_config_t *config)
 Sets the port PCR register. More...
 
static void PORT_SetMultiplePinsConfig (PORT_Type *base, uint32_t mask, const port_pin_config_t *config)
 Sets the port PCR register for multiple pins. More...
 
static void PORT_SetPinMux (PORT_Type *base, uint32_t pin, port_mux_t mux)
 Configures the pin muxing. More...
 
static void PORT_EnablePinsDigitalFilter (PORT_Type *base, uint32_t mask, bool enable)
 Enables the digital filter in one port, each bit of the 32-bit register represents one pin. More...
 
static void PORT_SetDigitalFilterConfig (PORT_Type *base, const port_digital_filter_config_t *config)
 Sets the digital filter in one port, each bit of the 32-bit register represents one pin. More...
 

Interrupt

static void PORT_SetPinInterruptConfig (PORT_Type *base, uint32_t pin, port_interrupt_t config)
 Configures the port pin interrupt/DMA request. More...
 
static void PORT_SetPinDriveStrength (PORT_Type *base, uint32_t pin, uint8_t strength)
 Configures the port pin drive strength. More...
 
static uint32_t PORT_GetPinsInterruptFlags (PORT_Type *base)
 Reads the whole port status flag. More...
 
static void PORT_ClearPinsInterruptFlags (PORT_Type *base, uint32_t mask)
 Clears the multiple pin interrupt status flag. More...
 

Data Structure Documentation

struct port_digital_filter_config_t

Data Fields

uint32_t digitalFilterWidth
 Set digital filter width.
 
port_digital_filter_clock_source_t clockSource
 Set digital filter clockSource.
 
struct port_pin_config_t

Data Fields

uint16_t pullSelect: 2
 No-pull/pull-down/pull-up select.
 
uint16_t slewRate: 1
 Fast/slow slew rate Configure.
 
uint16_t passiveFilterEnable: 1
 Passive filter enable/disable.
 
uint16_t openDrainEnable: 1
 Open drain enable/disable.
 
uint16_t driveStrength: 1
 Fast/slow drive strength configure.
 
uint16_t mux: 3
 Pin mux Configure.
 
uint16_t lockRegister: 1
 Lock/unlock the PCR field[15:0].
 

Macro Definition Documentation

#define FSL_PORT_DRIVER_VERSION   (MAKE_VERSION(2, 2, 0))

Enumeration Type Documentation

enum _port_pull
Enumerator
kPORT_PullDisable 

Internal pull-up/down resistor is disabled.

kPORT_PullDown 

Internal pull-down resistor is enabled.

kPORT_PullUp 

Internal pull-up resistor is enabled.

Enumerator
kPORT_FastSlewRate 

Fast slew rate is configured.

kPORT_SlowSlewRate 

Slow slew rate is configured.

Enumerator
kPORT_OpenDrainDisable 

Open drain output is disabled.

kPORT_OpenDrainEnable 

Open drain output is enabled.

Enumerator
kPORT_PassiveFilterDisable 

Passive input filter is disabled.

kPORT_PassiveFilterEnable 

Passive input filter is enabled.

Enumerator
kPORT_LowDriveStrength 

Low-drive strength is configured.

kPORT_HighDriveStrength 

High-drive strength is configured.

Enumerator
kPORT_UnlockRegister 

Pin Control Register fields [15:0] are not locked.

kPORT_LockRegister 

Pin Control Register fields [15:0] are locked.

enum port_mux_t
Enumerator
kPORT_PinDisabledOrAnalog 

Corresponding pin is disabled, but is used as an analog pin.

kPORT_MuxAsGpio 

Corresponding pin is configured as GPIO.

kPORT_MuxAlt2 

Chip-specific.

kPORT_MuxAlt3 

Chip-specific.

kPORT_MuxAlt4 

Chip-specific.

kPORT_MuxAlt5 

Chip-specific.

kPORT_MuxAlt6 

Chip-specific.

kPORT_MuxAlt7 

Chip-specific.

kPORT_MuxAlt8 

Chip-specific.

kPORT_MuxAlt9 

Chip-specific.

kPORT_MuxAlt10 

Chip-specific.

kPORT_MuxAlt11 

Chip-specific.

kPORT_MuxAlt12 

Chip-specific.

kPORT_MuxAlt13 

Chip-specific.

kPORT_MuxAlt14 

Chip-specific.

kPORT_MuxAlt15 

Chip-specific.

Enumerator
kPORT_InterruptOrDMADisabled 

Interrupt/DMA request is disabled.

kPORT_DMARisingEdge 

DMA request on rising edge.

kPORT_DMAFallingEdge 

DMA request on falling edge.

kPORT_DMAEitherEdge 

DMA request on either edge.

kPORT_FlagRisingEdge 

Flag sets on rising edge.

kPORT_FlagFallingEdge 

Flag sets on falling edge.

kPORT_FlagEitherEdge 

Flag sets on either edge.

kPORT_InterruptLogicZero 

Interrupt when logic zero.

kPORT_InterruptRisingEdge 

Interrupt on rising edge.

kPORT_InterruptFallingEdge 

Interrupt on falling edge.

kPORT_InterruptEitherEdge 

Interrupt on either edge.

kPORT_InterruptLogicOne 

Interrupt when logic one.

kPORT_ActiveHighTriggerOutputEnable 

Enable active high-trigger output.

kPORT_ActiveLowTriggerOutputEnable 

Enable active low-trigger output.

Enumerator
kPORT_BusClock 

Digital filters are clocked by the bus clock.

kPORT_LpoClock 

Digital filters are clocked by the 1 kHz LPO clock.

Function Documentation

static void PORT_SetPinConfig ( PORT_Type *  base,
uint32_t  pin,
const port_pin_config_t *  config 
)
inlinestatic

This is an example to define an input pin or output pin PCR configuration.

* // Define a digital input pin PCR configuration
* port_pin_config_t config = {
* kPORT_UnLockRegister,
* };
*
Parameters
basePORT peripheral base pointer.
pinPORT pin number.
configPORT PCR register configuration structure.
static void PORT_SetMultiplePinsConfig ( PORT_Type *  base,
uint32_t  mask,
const port_pin_config_t *  config 
)
inlinestatic

This is an example to define input pins or output pins PCR configuration.

* Define a digital input pin PCR configuration
* port_pin_config_t config = {
* kPORT_PullEnable,
* };
*
Parameters
basePORT peripheral base pointer.
maskPORT pin number macro.
configPORT PCR register configuration structure.
static void PORT_SetPinMux ( PORT_Type *  base,
uint32_t  pin,
port_mux_t  mux 
)
inlinestatic
Parameters
basePORT peripheral base pointer.
pinPORT pin number.
muxpin muxing slot selection.
Note
: This function is NOT recommended to use together with the PORT_SetPinsConfig, because the PORT_SetPinsConfig need to configure the pin mux anyway (Otherwise the pin mux is reset to zero : kPORT_PinDisabledOrAnalog). This function is recommended to use to reset the pin mux
static void PORT_EnablePinsDigitalFilter ( PORT_Type *  base,
uint32_t  mask,
bool  enable 
)
inlinestatic
Parameters
basePORT peripheral base pointer.
maskPORT pin number macro.
enablePORT digital filter configuration.
static void PORT_SetDigitalFilterConfig ( PORT_Type *  base,
const port_digital_filter_config_t *  config 
)
inlinestatic
Parameters
basePORT peripheral base pointer.
configPORT digital filter configuration structure.
static void PORT_SetPinInterruptConfig ( PORT_Type *  base,
uint32_t  pin,
port_interrupt_t  config 
)
inlinestatic
Parameters
basePORT peripheral base pointer.
pinPORT pin number.
configPORT pin interrupt configuration.
static void PORT_SetPinDriveStrength ( PORT_Type *  base,
uint32_t  pin,
uint8_t  strength 
)
inlinestatic
Parameters
basePORT peripheral base pointer.
pinPORT pin number.
strengthPORT pin drive strength
static uint32_t PORT_GetPinsInterruptFlags ( PORT_Type *  base)
inlinestatic

If a pin is configured to generate the DMA request, the corresponding flag is cleared automatically at the completion of the requested DMA transfer. Otherwise, the flag remains set until a logic one is written to that flag. If configured for a level sensitive interrupt that remains asserted, the flag is set again immediately.

Parameters
basePORT peripheral base pointer.
Returns
Current port interrupt status flags, for example, 0x00010001 means the pin 0 and 16 have the interrupt.
static void PORT_ClearPinsInterruptFlags ( PORT_Type *  base,
uint32_t  mask 
)
inlinestatic
Parameters
basePORT peripheral base pointer.
maskPORT pin number macro.