MCUXpresso SDK API Reference Manual  Rev 2.11.0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
SYSMPU: System Memory Protection Unit

Overview

The SYSMPU driver provides hardware access control for all memory references generated in the device. Use the SYSMPU driver to program the region descriptors that define memory spaces and their access rights. After initialization, the SYSMPU concurrently monitors the system bus transactions and evaluates their appropriateness.

Initialization and Deinitialization

To initialize the SYSMPU module, call the SYSMPU_Init() function and provide the user configuration data structure. This function sets the configuration of the SYSMPU module automatically and enables the SYSMPU module.
Note that the configuration start address, end address, the region valid value, and the debugger's access permission for the SYSMPU region 0 cannot be changed.

This is an example code to configure the SYSMPU driver.

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/sysmpu

Basic Control Operations

SYSMPU can be enabled/disabled for the entire memory protection region by calling the SYSMPU_Enable() function. To save the power for any unused special regions when the entire memory protection region is disabled, call the SYSMPU_RegionEnable().

After SYSMPU initialization, the SYSMPU_SetRegionLowMasterAccessRights() and SYSMPU_SetRegionHighMasterAccessRights() can be used to change the access rights for special master ports and for special region numbers. The SYSMPU_SetRegionConfig can be used to set the whole region with the start/end address with access rights.

The SYSMPU_GetHardwareInfo() API is provided to get the hardware information for the device. The SYSMPU_GetSlavePortErrorStatus() API is provided to get the error status of a special slave port. When an error happens in this port, the SYSMPU_GetDetailErrorAccessInfo() API is provided to get the detailed error information.

Data Structures

struct  sysmpu_hardware_info_t
 SYSMPU hardware basic information. More...
 
struct  sysmpu_access_err_info_t
 SYSMPU detail error access information. More...
 
struct  sysmpu_rwxrights_master_access_control_t
 SYSMPU read/write/execute rights control for bus master 0 ~ 3. More...
 
struct  sysmpu_rwrights_master_access_control_t
 SYSMPU read/write access control for bus master 4 ~ 7. More...
 
struct  sysmpu_region_config_t
 SYSMPU region configuration structure. More...
 
struct  sysmpu_config_t
 The configuration structure for the SYSMPU initialization. More...
 

Macros

#define SYSMPU_MASTER_RWATTRIBUTE_START_PORT   (4U)
 define the start master port with read and write attributes. More...
 
#define SYSMPU_REGION_RWXRIGHTS_MASTER_SHIFT(n)   ((n)*6U)
 SYSMPU the bit shift for masters with privilege rights: read write and execute. More...
 
#define SYSMPU_REGION_RWXRIGHTS_MASTER_MASK(n)   (0x1FUL << SYSMPU_REGION_RWXRIGHTS_MASTER_SHIFT(n))
 SYSMPU masters with read, write and execute rights bit mask. More...
 
#define SYSMPU_REGION_RWXRIGHTS_MASTER_WIDTH   5U
 SYSMPU masters with read, write and execute rights bit width. More...
 
#define SYSMPU_REGION_RWXRIGHTS_MASTER(n, x)   (((uint32_t)(((uint32_t)(x)) << SYSMPU_REGION_RWXRIGHTS_MASTER_SHIFT(n))) & SYSMPU_REGION_RWXRIGHTS_MASTER_MASK(n))
 SYSMPU masters with read, write and execute rights priority setting. More...
 
#define SYSMPU_REGION_RWXRIGHTS_MASTER_PE_SHIFT(n)   ((n)*6U + SYSMPU_REGION_RWXRIGHTS_MASTER_WIDTH)
 SYSMPU masters with read, write and execute rights process enable bit shift. More...
 
#define SYSMPU_REGION_RWXRIGHTS_MASTER_PE_MASK(n)   (0x1UL << SYSMPU_REGION_RWXRIGHTS_MASTER_PE_SHIFT(n))
 SYSMPU masters with read, write and execute rights process enable bit mask. More...
 
#define SYSMPU_REGION_RWXRIGHTS_MASTER_PE(n, x)
 SYSMPU masters with read, write and execute rights process enable setting. More...
 
#define SYSMPU_REGION_RWRIGHTS_MASTER_SHIFT(n)   (((n)-SYSMPU_MASTER_RWATTRIBUTE_START_PORT) * 2U + 24U)
 SYSMPU masters with normal read write permission bit shift. More...
 
#define SYSMPU_REGION_RWRIGHTS_MASTER_MASK(n)   (0x3UL << SYSMPU_REGION_RWRIGHTS_MASTER_SHIFT(n))
 SYSMPU masters with normal read write rights bit mask. More...
 
#define SYSMPU_REGION_RWRIGHTS_MASTER(n, x)   (((uint32_t)(((uint32_t)(x)) << SYSMPU_REGION_RWRIGHTS_MASTER_SHIFT(n))) & SYSMPU_REGION_RWRIGHTS_MASTER_MASK(n))
 SYSMPU masters with normal read write rights priority setting. More...
 

Enumerations

enum  sysmpu_region_total_num_t {
  kSYSMPU_8Regions = 0x0U,
  kSYSMPU_12Regions = 0x1U,
  kSYSMPU_16Regions = 0x2U
}
 Describes the number of SYSMPU regions. More...
 
enum  sysmpu_slave_t {
  kSYSMPU_Slave0 = 0U,
  kSYSMPU_Slave1 = 1U,
  kSYSMPU_Slave2 = 2U,
  kSYSMPU_Slave3 = 3U,
  kSYSMPU_Slave4 = 4U
}
 SYSMPU slave port number. More...
 
enum  sysmpu_err_access_control_t {
  kSYSMPU_NoRegionHit = 0U,
  kSYSMPU_NoneOverlappRegion = 1U,
  kSYSMPU_OverlappRegion = 2U
}
 SYSMPU error access control detail. More...
 
enum  sysmpu_err_access_type_t {
  kSYSMPU_ErrTypeRead = 0U,
  kSYSMPU_ErrTypeWrite = 1U
}
 SYSMPU error access type. More...
 
enum  sysmpu_err_attributes_t {
  kSYSMPU_InstructionAccessInUserMode = 0U,
  kSYSMPU_DataAccessInUserMode = 1U,
  kSYSMPU_InstructionAccessInSupervisorMode = 2U,
  kSYSMPU_DataAccessInSupervisorMode = 3U
}
 SYSMPU access error attributes. More...
 
enum  sysmpu_supervisor_access_rights_t {
  kSYSMPU_SupervisorReadWriteExecute = 0U,
  kSYSMPU_SupervisorReadExecute = 1U,
  kSYSMPU_SupervisorReadWrite = 2U,
  kSYSMPU_SupervisorEqualToUsermode = 3U
}
 SYSMPU access rights in supervisor mode for bus master 0 ~ 3. More...
 
enum  sysmpu_user_access_rights_t {
  kSYSMPU_UserNoAccessRights = 0U,
  kSYSMPU_UserExecute = 1U,
  kSYSMPU_UserWrite = 2U,
  kSYSMPU_UserWriteExecute = 3U,
  kSYSMPU_UserRead = 4U,
  kSYSMPU_UserReadExecute = 5U,
  kSYSMPU_UserReadWrite = 6U,
  kSYSMPU_UserReadWriteExecute = 7U
}
 SYSMPU access rights in user mode for bus master 0 ~ 3. More...
 

Driver version

#define FSL_SYSMPU_DRIVER_VERSION   (MAKE_VERSION(2, 2, 3))
 SYSMPU driver version 2.2.3. More...
 

Initialization and deinitialization

void SYSMPU_Init (SYSMPU_Type *base, const sysmpu_config_t *config)
 Initializes the SYSMPU with the user configuration structure. More...
 
void SYSMPU_Deinit (SYSMPU_Type *base)
 Deinitializes the SYSMPU regions. More...
 

Basic Control Operations

static void SYSMPU_Enable (SYSMPU_Type *base, bool enable)
 Enables/disables the SYSMPU globally. More...
 
static void SYSMPU_RegionEnable (SYSMPU_Type *base, uint32_t number, bool enable)
 Enables/disables the SYSMPU for a special region. More...
 
void SYSMPU_GetHardwareInfo (SYSMPU_Type *base, sysmpu_hardware_info_t *hardwareInform)
 Gets the SYSMPU basic hardware information. More...
 
void SYSMPU_SetRegionConfig (SYSMPU_Type *base, const sysmpu_region_config_t *regionConfig)
 Sets the SYSMPU region. More...
 
void SYSMPU_SetRegionAddr (SYSMPU_Type *base, uint32_t regionNum, uint32_t startAddr, uint32_t endAddr)
 Sets the region start and end address. More...
 
void SYSMPU_SetRegionRwxMasterAccessRights (SYSMPU_Type *base, uint32_t regionNum, uint32_t masterNum, const sysmpu_rwxrights_master_access_control_t *accessRights)
 Sets the SYSMPU region access rights for masters with read, write, and execute rights. More...
 
void SYSMPU_SetRegionRwMasterAccessRights (SYSMPU_Type *base, uint32_t regionNum, uint32_t masterNum, const sysmpu_rwrights_master_access_control_t *accessRights)
 Sets the SYSMPU region access rights for masters with read and write rights. More...
 
bool SYSMPU_GetSlavePortErrorStatus (SYSMPU_Type *base, sysmpu_slave_t slaveNum)
 Gets the numbers of slave ports where errors occur. More...
 
void SYSMPU_GetDetailErrorAccessInfo (SYSMPU_Type *base, sysmpu_slave_t slaveNum, sysmpu_access_err_info_t *errInform)
 Gets the SYSMPU detailed error access information. More...
 

Data Structure Documentation

struct sysmpu_hardware_info_t

Data Fields

uint8_t hardwareRevisionLevel
 Specifies the SYSMPU's hardware and definition reversion level. More...
 
uint8_t slavePortsNumbers
 Specifies the number of slave ports connected to SYSMPU. More...
 
sysmpu_region_total_num_t regionsNumbers
 Indicates the number of region descriptors implemented. More...
 

Field Documentation

uint8_t sysmpu_hardware_info_t::hardwareRevisionLevel
uint8_t sysmpu_hardware_info_t::slavePortsNumbers
sysmpu_region_total_num_t sysmpu_hardware_info_t::regionsNumbers
struct sysmpu_access_err_info_t

Data Fields

uint32_t master
 Access error master. More...
 
sysmpu_err_attributes_t attributes
 Access error attributes. More...
 
sysmpu_err_access_type_t accessType
 Access error type. More...
 
sysmpu_err_access_control_t accessControl
 Access error control. More...
 
uint32_t address
 Access error address. More...
 
uint8_t processorIdentification
 Access error processor identification. More...
 

Field Documentation

uint32_t sysmpu_access_err_info_t::master
sysmpu_err_attributes_t sysmpu_access_err_info_t::attributes
sysmpu_err_access_type_t sysmpu_access_err_info_t::accessType
sysmpu_err_access_control_t sysmpu_access_err_info_t::accessControl
uint32_t sysmpu_access_err_info_t::address
uint8_t sysmpu_access_err_info_t::processorIdentification
struct sysmpu_rwxrights_master_access_control_t

Data Fields

sysmpu_supervisor_access_rights_t superAccessRights
 Master access rights in supervisor mode. More...
 
sysmpu_user_access_rights_t userAccessRights
 Master access rights in user mode. More...
 
bool processIdentifierEnable
 Enables or disables process identifier. More...
 

Field Documentation

sysmpu_supervisor_access_rights_t sysmpu_rwxrights_master_access_control_t::superAccessRights
sysmpu_user_access_rights_t sysmpu_rwxrights_master_access_control_t::userAccessRights
bool sysmpu_rwxrights_master_access_control_t::processIdentifierEnable
struct sysmpu_rwrights_master_access_control_t

Data Fields

bool writeEnable
 Enables or disables write permission. More...
 
bool readEnable
 Enables or disables read permission. More...
 

Field Documentation

bool sysmpu_rwrights_master_access_control_t::writeEnable
bool sysmpu_rwrights_master_access_control_t::readEnable
struct sysmpu_region_config_t

This structure is used to configure the regionNum region. The accessRights1[0] ~ accessRights1[3] are used to configure the bus master 0 ~ 3 with the privilege rights setting. The accessRights2[0] ~ accessRights2[3] are used to configure the high master 4 ~ 7 with the normal read write permission. The master port assignment is the chip configuration. Normally, the core is the master 0, debugger is the master 1. Note that the SYSMPU assigns a priority scheme where the debugger is treated as the highest priority master followed by the core and then all the remaining masters. SYSMPU protection does not allow writes from the core to affect the "regionNum 0" start and end address nor the permissions associated with the debugger. It can only write the permission fields associated with the other masters. This protection guarantees that the debugger always has access to the entire address space and those rights can't be changed by the core or any other bus master. Prepare the region configuration when regionNum is 0.

Data Fields

uint32_t regionNum
 SYSMPU region number, range form 0 ~ FSL_FEATURE_SYSMPU_DESCRIPTOR_COUNT - 1. More...
 
uint32_t startAddress
 Memory region start address. More...
 
uint32_t endAddress
 Memory region end address. More...
 
sysmpu_rwxrights_master_access_control_t accessRights1 [4]
 Masters with read, write and execute rights setting. More...
 
sysmpu_rwrights_master_access_control_t accessRights2 [4]
 Masters with normal read write rights setting. More...
 
uint8_t processIdentifier
 Process identifier used when "processIdentifierEnable" set with true. More...
 
uint8_t processIdMask
 Process identifier mask. More...
 

Field Documentation

uint32_t sysmpu_region_config_t::regionNum
uint32_t sysmpu_region_config_t::startAddress

Note: bit0 ~ bit4 always be marked as 0 by SYSMPU. The actual start address is 0-modulo-32 byte address.

uint32_t sysmpu_region_config_t::endAddress

Note: bit0 ~ bit4 always be marked as 1 by SYSMPU. The actual end address is 31-modulo-32 byte address.

sysmpu_rwxrights_master_access_control_t sysmpu_region_config_t::accessRights1[4]
sysmpu_rwrights_master_access_control_t sysmpu_region_config_t::accessRights2[4]
uint8_t sysmpu_region_config_t::processIdentifier
uint8_t sysmpu_region_config_t::processIdMask

The setting bit will ignore the same bit in process identifier.

struct sysmpu_config_t

This structure is used when calling the SYSMPU_Init function.

Data Fields

sysmpu_region_config_t regionConfig
 Region access permission. More...
 
struct _sysmpu_config * next
 Pointer to the next structure. More...
 

Field Documentation

sysmpu_region_config_t sysmpu_config_t::regionConfig
struct _sysmpu_config* sysmpu_config_t::next

Macro Definition Documentation

#define FSL_SYSMPU_DRIVER_VERSION   (MAKE_VERSION(2, 2, 3))
#define SYSMPU_MASTER_RWATTRIBUTE_START_PORT   (4U)
#define SYSMPU_REGION_RWXRIGHTS_MASTER_SHIFT (   n)    ((n)*6U)
#define SYSMPU_REGION_RWXRIGHTS_MASTER_MASK (   n)    (0x1FUL << SYSMPU_REGION_RWXRIGHTS_MASTER_SHIFT(n))
#define SYSMPU_REGION_RWXRIGHTS_MASTER_WIDTH   5U
#define SYSMPU_REGION_RWXRIGHTS_MASTER (   n,
  x 
)    (((uint32_t)(((uint32_t)(x)) << SYSMPU_REGION_RWXRIGHTS_MASTER_SHIFT(n))) & SYSMPU_REGION_RWXRIGHTS_MASTER_MASK(n))
#define SYSMPU_REGION_RWXRIGHTS_MASTER_PE_SHIFT (   n)    ((n)*6U + SYSMPU_REGION_RWXRIGHTS_MASTER_WIDTH)
#define SYSMPU_REGION_RWXRIGHTS_MASTER_PE_MASK (   n)    (0x1UL << SYSMPU_REGION_RWXRIGHTS_MASTER_PE_SHIFT(n))
#define SYSMPU_REGION_RWXRIGHTS_MASTER_PE (   n,
  x 
)
Value:
(((uint32_t)(((uint32_t)(x)) << SYSMPU_REGION_RWXRIGHTS_MASTER_PE_SHIFT(n))) & \
#define SYSMPU_REGION_RWXRIGHTS_MASTER_PE_MASK(n)
SYSMPU masters with read, write and execute rights process enable bit mask.
Definition: fsl_sysmpu.h:49
#define SYSMPU_REGION_RWXRIGHTS_MASTER_PE_SHIFT(n)
SYSMPU masters with read, write and execute rights process enable bit shift.
Definition: fsl_sysmpu.h:46
#define SYSMPU_REGION_RWRIGHTS_MASTER_SHIFT (   n)    (((n)-SYSMPU_MASTER_RWATTRIBUTE_START_PORT) * 2U + 24U)
#define SYSMPU_REGION_RWRIGHTS_MASTER_MASK (   n)    (0x3UL << SYSMPU_REGION_RWRIGHTS_MASTER_SHIFT(n))
#define SYSMPU_REGION_RWRIGHTS_MASTER (   n,
  x 
)    (((uint32_t)(((uint32_t)(x)) << SYSMPU_REGION_RWRIGHTS_MASTER_SHIFT(n))) & SYSMPU_REGION_RWRIGHTS_MASTER_MASK(n))

Enumeration Type Documentation

Enumerator
kSYSMPU_8Regions 

SYSMPU supports 8 regions.

kSYSMPU_12Regions 

SYSMPU supports 12 regions.

kSYSMPU_16Regions 

SYSMPU supports 16 regions.

Enumerator
kSYSMPU_Slave0 

SYSMPU slave port 0.

kSYSMPU_Slave1 

SYSMPU slave port 1.

kSYSMPU_Slave2 

SYSMPU slave port 2.

kSYSMPU_Slave3 

SYSMPU slave port 3.

kSYSMPU_Slave4 

SYSMPU slave port 4.

Enumerator
kSYSMPU_NoRegionHit 

No region hit error.

kSYSMPU_NoneOverlappRegion 

Access single region error.

kSYSMPU_OverlappRegion 

Access overlapping region error.

Enumerator
kSYSMPU_ErrTypeRead 

SYSMPU error access type — read.

kSYSMPU_ErrTypeWrite 

SYSMPU error access type — write.

Enumerator
kSYSMPU_InstructionAccessInUserMode 

Access instruction error in user mode.

kSYSMPU_DataAccessInUserMode 

Access data error in user mode.

kSYSMPU_InstructionAccessInSupervisorMode 

Access instruction error in supervisor mode.

kSYSMPU_DataAccessInSupervisorMode 

Access data error in supervisor mode.

Enumerator
kSYSMPU_SupervisorReadWriteExecute 

Read write and execute operations are allowed in supervisor mode.

kSYSMPU_SupervisorReadExecute 

Read and execute operations are allowed in supervisor mode.

kSYSMPU_SupervisorReadWrite 

Read write operations are allowed in supervisor mode.

kSYSMPU_SupervisorEqualToUsermode 

Access permission equal to user mode.

Enumerator
kSYSMPU_UserNoAccessRights 

No access allowed in user mode.

kSYSMPU_UserExecute 

Execute operation is allowed in user mode.

kSYSMPU_UserWrite 

Write operation is allowed in user mode.

kSYSMPU_UserWriteExecute 

Write and execute operations are allowed in user mode.

kSYSMPU_UserRead 

Read is allowed in user mode.

kSYSMPU_UserReadExecute 

Read and execute operations are allowed in user mode.

kSYSMPU_UserReadWrite 

Read and write operations are allowed in user mode.

kSYSMPU_UserReadWriteExecute 

Read write and execute operations are allowed in user mode.

Function Documentation

void SYSMPU_Init ( SYSMPU_Type *  base,
const sysmpu_config_t *  config 
)

This function configures the SYSMPU module with the user-defined configuration.

Parameters
baseSYSMPU peripheral base address.
configThe pointer to the configuration structure.
void SYSMPU_Deinit ( SYSMPU_Type *  base)
Parameters
baseSYSMPU peripheral base address.
static void SYSMPU_Enable ( SYSMPU_Type *  base,
bool  enable 
)
inlinestatic

Call this API to enable or disable the SYSMPU module.

Parameters
baseSYSMPU peripheral base address.
enableTrue enable SYSMPU, false disable SYSMPU.
static void SYSMPU_RegionEnable ( SYSMPU_Type *  base,
uint32_t  number,
bool  enable 
)
inlinestatic

When SYSMPU is enabled, call this API to disable an unused region of an enabled SYSMPU. Call this API to minimize the power dissipation.

Parameters
baseSYSMPU peripheral base address.
numberSYSMPU region number.
enableTrue enable the special region SYSMPU, false disable the special region SYSMPU.
void SYSMPU_GetHardwareInfo ( SYSMPU_Type *  base,
sysmpu_hardware_info_t *  hardwareInform 
)
Parameters
baseSYSMPU peripheral base address.
hardwareInformThe pointer to the SYSMPU hardware information structure. See "sysmpu_hardware_info_t".
void SYSMPU_SetRegionConfig ( SYSMPU_Type *  base,
const sysmpu_region_config_t *  regionConfig 
)

Note: Due to the SYSMPU protection, the region number 0 does not allow writes from core to affect the start and end address nor the permissions associated with the debugger. It can only write the permission fields associated with the other masters.

Parameters
baseSYSMPU peripheral base address.
regionConfigThe pointer to the SYSMPU user configuration structure. See "sysmpu_region_config_t".
void SYSMPU_SetRegionAddr ( SYSMPU_Type *  base,
uint32_t  regionNum,
uint32_t  startAddr,
uint32_t  endAddr 
)

Memory region start address. Note: bit0 ~ bit4 is always marked as 0 by SYSMPU. The actual start address by SYSMPU is 0-modulo-32 byte address. Memory region end address. Note: bit0 ~ bit4 always be marked as 1 by SYSMPU. The end address used by the SYSMPU is 31-modulo-32 byte address. Note: Due to the SYSMPU protection, the startAddr and endAddr can't be changed by the core when regionNum is 0.

Parameters
baseSYSMPU peripheral base address.
regionNumSYSMPU region number. The range is from 0 to FSL_FEATURE_SYSMPU_DESCRIPTOR_COUNT - 1.
startAddrRegion start address.
endAddrRegion end address.
void SYSMPU_SetRegionRwxMasterAccessRights ( SYSMPU_Type *  base,
uint32_t  regionNum,
uint32_t  masterNum,
const sysmpu_rwxrights_master_access_control_t *  accessRights 
)

The SYSMPU access rights depend on two board classifications of bus masters. The privilege rights masters and the normal rights masters. The privilege rights masters have the read, write, and execute access rights. Except the normal read and write rights, the execute rights are also allowed for these masters. The privilege rights masters normally range from bus masters 0 - 3. However, the maximum master number is device-specific. See the "SYSMPU_PRIVILEGED_RIGHTS_MASTER_MAX_INDEX". The normal rights masters access rights control see "SYSMPU_SetRegionRwMasterAccessRights()".

Parameters
baseSYSMPU peripheral base address.
regionNumSYSMPU region number. Should range from 0 to FSL_FEATURE_SYSMPU_DESCRIPTOR_COUNT - 1.
masterNumSYSMPU bus master number. Should range from 0 to SYSMPU_PRIVILEGED_RIGHTS_MASTER_MAX_INDEX.
accessRightsThe pointer to the SYSMPU access rights configuration. See "sysmpu_rwxrights_master_access_control_t".
void SYSMPU_SetRegionRwMasterAccessRights ( SYSMPU_Type *  base,
uint32_t  regionNum,
uint32_t  masterNum,
const sysmpu_rwrights_master_access_control_t *  accessRights 
)

The SYSMPU access rights depend on two board classifications of bus masters. The privilege rights masters and the normal rights masters. The normal rights masters only have the read and write access permissions. The privilege rights access control see "SYSMPU_SetRegionRwxMasterAccessRights".

Parameters
baseSYSMPU peripheral base address.
regionNumSYSMPU region number. The range is from 0 to FSL_FEATURE_SYSMPU_DESCRIPTOR_COUNT - 1.
masterNumSYSMPU bus master number. Should range from SYSMPU_MASTER_RWATTRIBUTE_START_PORT to ~ FSL_FEATURE_SYSMPU_MASTER_COUNT - 1.
accessRightsThe pointer to the SYSMPU access rights configuration. See "sysmpu_rwrights_master_access_control_t".
bool SYSMPU_GetSlavePortErrorStatus ( SYSMPU_Type *  base,
sysmpu_slave_t  slaveNum 
)
Parameters
baseSYSMPU peripheral base address.
slaveNumSYSMPU slave port number.
Returns
The slave ports error status. true - error happens in this slave port. false - error didn't happen in this slave port.
void SYSMPU_GetDetailErrorAccessInfo ( SYSMPU_Type *  base,
sysmpu_slave_t  slaveNum,
sysmpu_access_err_info_t *  errInform 
)
Parameters
baseSYSMPU peripheral base address.
slaveNumSYSMPU slave port number.
errInformThe pointer to the SYSMPU access error information. See "sysmpu_access_err_info_t".