MCUXpresso SDK API Reference Manual  Rev 2.11.0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
PORT Driver

Overview

This driver configures the PORT, including function mux, filter, pull up or down, and so on.

Macros

#define FSL_PORT_FILTER_SELECT_BITMASK   (0x3U)
 The IOFLT Filter selection bit mask . More...
 

Enumerations

enum  port_module_t {
  kPORT_NMI = SIM_SOPT_NMIE_MASK,
  kPORT_RESET = SIM_SOPT_RSTPE_MASK,
  kPORT_SWDE = SIM_SOPT_SWDE_MASK,
  kPORT_I2C0 = SIM_PINSEL_I2C0PS_MASK,
  kPORT_SPI0 = SIM_PINSEL_SPI0PS_MASK,
  kPORT_UART0 = SIM_PINSEL_UART0PS_MASK,
  kPORT_FTM0CH0 = SIM_PINSEL_FTM0PS0_MASK,
  kPORT_FTM0CH1 = SIM_PINSEL_FTM0PS1_MASK,
  kPORT_FTM2CH2 = SIM_PINSEL_FTM2PS2_MASK,
  kPORT_FTM2CH3 = SIM_PINSEL_FTM2PS3_MASK,
  kPORT_FTM0CLK = SIM_PINSEL_FTM0CLKPS_MASK,
  kPORT_FTM2CLK = SIM_PINSEL_FTM2CLKPS_MASK,
  kPORT_PWTCLK = (int)SIM_PINSEL_PWTCLKPS_MASK
}
 Module or peripheral for port pin selection. More...
 
enum  port_type_t {
  kPORT_PTA = 0U,
  kPORT_PTB = 1U,
  kPORT_PTC = 2U
}
 Port type. More...
 
enum  port_pin_index_t {
  kPORT_PinIdx0 = 0U,
  kPORT_PinIdx1 = 1U,
  kPORT_PinIdx2 = 2U,
  kPORT_PinIdx3 = 3U,
  kPORT_PinIdx4 = 4U,
  kPORT_PinIdx5 = 5U,
  kPORT_PinIdx6 = 6U,
  kPORT_PinIdx7 = 7U
}
 Pin number, Notice this index enum has been deprecated and it will be removed in the next release. More...
 
enum  port_pin_select_t {
  kPORT_NMI_OTHERS = 0U,
  kPORT_NMI_NMIE = 1U,
  kPORT_RST_OTHERS = 0U,
  kPORT_RST_RSTPE = 1U,
  kPORT_SWDE_OTHERS = 0U,
  kPORT_SWDE_SWDE = 1U,
  kPORT_I2C0_SCLPTA3_SDAPTA2 = 0U,
  kPORT_I2C0_SCLPTB7_SDAPTB6 = 1U,
  kPORT_SPI0_SCKPTB2_MOSIPTB3_MISOPTB4_PCSPTB5 = 0U,
  kPORT_SPI0_SCKPTA6_MOSIPTA7_MISOPTB1_PCSPTB0,
  kPORT_UART0_RXPTB0_TXPTB1 = 0U,
  kPORT_UART0_RXPTA2_TXPTA3 = 1U,
  kPORT_FTM0_CH0_PTA0 = 0U,
  kPORT_FTM0_CH0_PTB2 = 1U,
  kPORT_FTM0_CH1_PTA1 = 0U,
  kPORT_FTM0_CH1_PTB3 = 1U,
  kPORT_FTM2_CH2_PTC2 = 0U,
  kPORT_FTM2_CH2_PTC4 = 1U,
  kPORT_FTM2_CH3_PTC3 = 0U,
  kPORT_FTM2_CH3_PTC5 = 1U,
  kPORT_FTM0CLK_TCLK1 = 0U,
  kPORT_FTM0CLK_TCLK2 = 1U,
  kPORT_FTM2CLK_TCLK1 = 0U,
  kPORT_FTM2CLK_TCLK2 = 1U,
  kPORT_PWTCLK_TCLK1 = 0U,
  kPORT_PWTCLK_TCLK2 = 1U
}
 Pin selection. More...
 
enum  port_filter_pin_t {
  kPORT_FilterPTA = PORT_IOFLT_FLTA_SHIFT,
  kPORT_FilterPTB = PORT_IOFLT_FLTB_SHIFT,
  kPORT_FilterPTC = PORT_IOFLT_FLTC_SHIFT,
  kPORT_FilterIIC = PORT_IOFLT_FLTIIC_SHIFT,
  kPORT_FilterFTM0 = PORT_IOFLT_FLTFTM0_SHIFT,
  kPORT_FilterPWT = PORT_IOFLT_FLTPWT_SHIFT,
  kPORT_FilterRST = PORT_IOFLT_FLTRST_SHIFT,
  kPORT_FilterKBI0 = PORT_IOFLT_FLTKBI0_SHIFT,
  kPORT_FilterKBI1 = PORT_IOFLT_FLTKBI1_SHIFT,
  kPORT_FilterNMI = PORT_IOFLT_FLTNMI_SHIFT
}
 The PORT pins for input glitch filter configure. More...
 
enum  port_filter_select_t {
  kPORT_BUSCLK_OR_NOFILTER,
  kPORT_FILTERDIV1 = 1U,
  kPORT_FILTERDIV2 = 2U,
  kPORT_FILTERDIV3_OR_BUSCLK = 3U
}
 The Filter selection for input pins. More...
 
enum  port_highdrive_pin_t {
  kPORT_HighDrive_PTB5 = PORT_HDRVE_PTB5_MASK,
  kPORT_HighDrive_PTC1 = PORT_HDRVE_PTC1_MASK,
  kPORT_HighDrive_PTC5 = PORT_HDRVE_PTC5_MASK
}
 Port pin for high driver enable/disable control. More...
 

Driver version

#define FSL_PORT_DRIVER_VERSION   (MAKE_VERSION(2, 0, 2))
 Version 2.0.2. More...
 

Configuration

void PORT_SetPinSelect (port_module_t module, port_pin_select_t pin)
 Selects pin for modules. More...
 
static void PORT_SetFilterSelect (PORT_Type *base, port_filter_pin_t port, port_filter_select_t filter)
 Selects the glitch filter for input pins. More...
 
static void PORT_SetFilterDIV1WidthThreshold (PORT_Type *base, uint8_t threshold)
 Sets the width threshold for glitch filter division set 1. More...
 
static void PORT_SetFilterDIV2WidthThreshold (PORT_Type *base, uint8_t threshold)
 Sets the width threshold for glitch filter division set 2. More...
 
static void PORT_SetFilterDIV3WidthThreshold (PORT_Type *base, uint8_t threshold)
 Sets the width threshold for glitch filter division set 3. More...
 
static void PORT_SetPinPullUpEnable (PORT_Type *base, port_type_t port, uint8_t num, bool enable)
 Enables or disables the port pull up. More...
 
static void PORT_SetHighDriveEnable (PORT_Type *base, port_highdrive_pin_t pin, bool enable)
 Set High drive for port pins. More...
 

Macro Definition Documentation

#define FSL_PORT_DRIVER_VERSION   (MAKE_VERSION(2, 0, 2))
#define FSL_PORT_FILTER_SELECT_BITMASK   (0x3U)

Enumeration Type Documentation

Enumerator
kPORT_NMI 

NMI port pin select.

kPORT_RESET 

RESET pin select.

kPORT_SWDE 

Single wire debug port pin.

kPORT_I2C0 

I2C0 Port pin select.

kPORT_SPI0 

SPI0 port pin select.

kPORT_UART0 

UART0 port pin select.

kPORT_FTM0CH0 

FTM0_CH0 port pin select.

kPORT_FTM0CH1 

FTM0_CH1 port pin select.

kPORT_FTM2CH2 

FTM2_CH2 port pin select.

kPORT_FTM2CH3 

FTM2_CH3 port pin select.

kPORT_FTM0CLK 

FTM0 clock pin select.

kPORT_FTM2CLK 

FTM2 clock pin select.

kPORT_PWTCLK 

PWT clock pin select.

Enumerator
kPORT_PTA 

PORT PTA.

kPORT_PTB 

PORT PTB.

kPORT_PTC 

PORT PTC.

Enumerator
kPORT_PinIdx0 

PORT PIN index 0.

kPORT_PinIdx1 

PORT PIN index 1.

kPORT_PinIdx2 

PORT PIN index 2.

kPORT_PinIdx3 

PORT PIN index 3.

kPORT_PinIdx4 

PORT PIN index 4.

kPORT_PinIdx5 

PORT PIN index 5.

kPORT_PinIdx6 

PORT PIN index 6.

kPORT_PinIdx7 

PORT PIN index 7.

Enumerator
kPORT_NMI_OTHERS 

PTB4/FTM2_CH4 etc function as PTB4/FTM2_CH4 etc.

kPORT_NMI_NMIE 

PTB4/FTM2_CH4 etc function as NMI.

kPORT_RST_OTHERS 

PTA5/IRQ etc function as PTA5/IRQ etc.

kPORT_RST_RSTPE 

PTA5/IRQ etc function as REST.

kPORT_SWDE_OTHERS 

PTA4/ACMP0 etc function as PTA4/ACMP0 etc.

kPORT_SWDE_SWDE 

PTA4/ACMP0 etc function as SWD.

kPORT_I2C0_SCLPTA3_SDAPTA2 

I2C0_SCL and I2C0_SDA are mapped on PTA3 and PTA2, respectively.

kPORT_I2C0_SCLPTB7_SDAPTB6 

I2C0_SCL and I2C0_SDA are mapped on PTB7 and PTB6, respectively.

kPORT_SPI0_SCKPTB2_MOSIPTB3_MISOPTB4_PCSPTB5 

SPI0_SCK/MOSI/MISO/PCS0 are mapped on PTB2/PTB3/PTB4/PTB5.

kPORT_SPI0_SCKPTA6_MOSIPTA7_MISOPTB1_PCSPTB0 

SPI0_SCK/MOSI/MISO/PCS0 are mapped on PTA6/PTA7/PTB1/PTB0.

kPORT_UART0_RXPTB0_TXPTB1 

UART0_RX and UART0_TX are mapped on PTB0 and PTB1.

kPORT_UART0_RXPTA2_TXPTA3 

UART0_RX and UART0_TX are mapped on PTA2 and PTA3.

kPORT_FTM0_CH0_PTA0 

FTM0_CH0 channels are mapped on PTA0.

kPORT_FTM0_CH0_PTB2 

FTM0_CH0 channels are mapped on PTB2.

kPORT_FTM0_CH1_PTA1 

FTM0_CH1 channels are mapped on PTA1.

kPORT_FTM0_CH1_PTB3 

FTM0_CH1 channels are mapped on PTB3.

kPORT_FTM2_CH2_PTC2 

FTM2_CH2 channels are mapped on PTC2.

kPORT_FTM2_CH2_PTC4 

FTM2_CH2 channels are mapped on PTD2.

kPORT_FTM2_CH3_PTC3 

FTM2_CH3 channels are mapped on PTC3.

kPORT_FTM2_CH3_PTC5 

FTM2_CH3 channels are mapped on PTC5.

kPORT_FTM0CLK_TCLK1 

FTM0 CLK using the TCLK1 pin.

kPORT_FTM0CLK_TCLK2 

FTM0 CLK using the TCLK2 pin.

kPORT_FTM2CLK_TCLK1 

FTM2 CLK using the TCLK1 pin.

kPORT_FTM2CLK_TCLK2 

FTM2 CLK using the TCLK2 pin.

kPORT_PWTCLK_TCLK1 

PWT CLK using the TCLK1 pin.

kPORT_PWTCLK_TCLK2 

PWT CLK using the TCLK2 pin.

Enumerator
kPORT_FilterPTA 

Filter for input from PTA.

kPORT_FilterPTB 

Filter for input from PTB.

kPORT_FilterPTC 

Filter for input from PTC.

kPORT_FilterIIC 

Filter for input from I2C.

kPORT_FilterFTM0 

Filter for input from FTM0.

kPORT_FilterPWT 

Filter for input from PWT.

kPORT_FilterRST 

Filter for input from RESET/IRQ.

kPORT_FilterKBI0 

Filter for input from KBI0.

kPORT_FilterKBI1 

Filter for input from KBI1.

kPORT_FilterNMI 

Filter for input from NMI.

Enumerator
kPORT_BUSCLK_OR_NOFILTER 

Filter section BUSCLK for PTA~PTC, No filter for REST/KBI0/KBI1/NMI/PWT/FTM0/I2C.

kPORT_FILTERDIV1 

Filter Division Set 1.

kPORT_FILTERDIV2 

Filter Division Set 2.

kPORT_FILTERDIV3_OR_BUSCLK 

Filter Division Set 3.

Enumerator
kPORT_HighDrive_PTB5 

PTB5.

kPORT_HighDrive_PTC1 

PTC1.

kPORT_HighDrive_PTC5 

PTC5.

Function Documentation

void PORT_SetPinSelect ( port_module_t  module,
port_pin_select_t  pin 
)

This API is used to select the port pin for the module with multiple port pin selection. For example the FTM Channel 0 can be mapped to ether PTA0 or PTB2. Select FTM channel 0 map to PTA0 port pin as:

Note
: This API doesn't support to select specified ALT for a given port pin. The ALT feature is automatically selected by hardware according to the ALT priority: Low --—> high: Alt1, Alt2, … when peripheral modules has been enabled.

If you want to select a specified ALT for a given port pin, please add two more steps after calling PORT_SetPinSelect:

  1. Enable module or the port control in the module for the ALT you want to select. For I2C ALT feature:all port enable is controlled by the module enable, so set IICEN in I2CX_C1 to enable the port pins for I2C feature. For KBI ALT feature:each port pin is controlled independently by each bit in KBIx_PE. set related bit in this register to enable the KBI feature in the port pin.
  2. Make sure there is no module enabled with higher priority than the ALT module feature you want to select.
Parameters
moduleModules for pin selection. For NMI/RST module are write-once attribute after reset.
pinPort pin selection for modules.
static void PORT_SetFilterSelect ( PORT_Type *  base,
port_filter_pin_t  port,
port_filter_select_t  filter 
)
inlinestatic
Parameters
basePORT peripheral base pointer.
portPORT pin, see "port_filter_pin_t".
filterFilter select, see "port_filter_select_t".
static void PORT_SetFilterDIV1WidthThreshold ( PORT_Type *  base,
uint8_t  threshold 
)
inlinestatic

`

Parameters
basePORT peripheral base pointer.
thresholdPORT glitch filter width threshold, take refer to reference manual for detail information. 0 - LPOCLK 1 - LPOCLK/2 2 - LPOCLK/4 3 - LPOCLK/8 4 - LPOCLK/16 5 - LPOCLK/32 6 - LPOCLK/64 7 - LPOCLK/128
static void PORT_SetFilterDIV2WidthThreshold ( PORT_Type *  base,
uint8_t  threshold 
)
inlinestatic

`

Parameters
basePORT peripheral base pointer.
thresholdPORT glitch filter width threshold, take refer to reference manual for detail information. 0 - BUSCLK/32 1 - BUSCLK/64 2 - BUSCLK/128 3 - BUSCLK/256 4 - BUSCLK/512 5 - BUSCLK/1024 6 - BUSCLK/2048 7 - BUSCLK/4096
static void PORT_SetFilterDIV3WidthThreshold ( PORT_Type *  base,
uint8_t  threshold 
)
inlinestatic

`

Parameters
basePORT peripheral base pointer.
thresholdPORT glitch filter width threshold, take refer to reference manual for detail information. 0 - BUSCLK/2 1 - BUSCLK/4 2 - BUSCLK/8 3 - BUSCLK/16
static void PORT_SetPinPullUpEnable ( PORT_Type *  base,
port_type_t  port,
uint8_t  num,
bool  enable 
)
inlinestatic
Parameters
basePORT peripheral base pointer.
portPORT type, such as PTA/PTB/PTC etc, see "port_type_t".
numPORT pin number, such as 0, 1, 2.... For PTC, there are only six pins from 0 ~ 5, the PTC6, PTC7 are not exists in this device. so when set PTC please don't set the 6 and 7, take refer to the reference manual.
enableEnable or disable the pull up feature switch.
static void PORT_SetHighDriveEnable ( PORT_Type *  base,
port_highdrive_pin_t  pin,
bool  enable 
)
inlinestatic
Parameters
basePORT peripheral base pointer.
pinPORT pin support high drive.
enableEnable or disable the high driver feature switch.