![]() |
MCUXpresso SDK API Reference Manual
Rev 2.11.0
NXP Semiconductors
|
Data Structures | |
| struct | asrc_channel_pair_config_t |
| asrc channel pair configuation More... | |
| struct | asrc_transfer_t |
| SAI transfer structure. More... | |
| struct | asrc_in_handle_t |
| asrc in handler More... | |
| struct | asrc_out_handle_t |
| output handler More... | |
| struct | asrc_handle_t |
| ASRC handle structure. More... | |
Macros | |
| #define | ASRC_XFER_QUEUE_SIZE (4U) |
| ASRC transfer queue size, user can refine it according to use case. More... | |
| #define | FSL_ASRC_CHANNEL_PAIR_COUNT (4U) |
| ASRC channel pair count. | |
| #define | FSL_ASRC_CHANNEL_PAIR_FIFO_DEPTH (64U) |
| ASRC FIFO depth. | |
| #define | ASRC_ASRCTR_AT_MASK(index) ((uint32_t)1U << (ASRC_ASRCTR_ATSA_SHIFT + (uint32_t)(index))) |
| ASRC register access macro. | |
Typedefs | |
| typedef void(* | asrc_transfer_callback_t )(ASRC_Type *base, asrc_handle_t *handle, status_t status, void *userData) |
| ASRC transfer callback prototype. | |
Driver version | |
| #define | FSL_ASRC_DRIVER_VERSION (MAKE_VERSION(2, 1, 2)) |
| Version 2.1.2. | |
Initialization and deinitialization | |
| uint32_t | ASRC_GetInstance (ASRC_Type *base) |
| Get instance number of the ASRC peripheral. More... | |
| void | ASRC_Init (ASRC_Type *base, uint32_t asrcPeripheralClock_Hz) |
| brief Initializes the asrc peripheral. More... | |
| void | ASRC_Deinit (ASRC_Type *base) |
| De-initializes the ASRC peripheral. More... | |
| void | ASRC_SoftwareReset (ASRC_Type *base) |
| Do software reset . More... | |
| status_t | ASRC_SetChannelPairConfig (ASRC_Type *base, asrc_channel_pair_t channelPair, asrc_channel_pair_config_t *config, uint32_t inputSampleRate, uint32_t outputSampleRate) |
| ASRC configure channel pair. More... | |
| uint32_t | ASRC_GetOutSamplesSize (ASRC_Type *base, asrc_channel_pair_t channelPair, uint32_t inSampleRate, uint32_t outSampleRate, uint32_t inSamplesize) |
| Get output sample buffer size. More... | |
| uint32_t | ASRC_MapSamplesWidth (ASRC_Type *base, asrc_channel_pair_t channelPair, uint32_t *inWidth, uint32_t *outWidth) |
| Map register sample width to real sample width. More... | |
| uint32_t | ASRC_GetRemainFifoSamples (ASRC_Type *base, asrc_channel_pair_t channelPair, uint32_t *buffer, uint32_t outSampleWidth, uint32_t remainSamples) |
| Get left samples in fifo. More... | |
| static void | ASRC_ModuleEnable (ASRC_Type *base, bool enable) |
| ASRC module enable. More... | |
| static void | ASRC_ChannelPairEnable (ASRC_Type *base, asrc_channel_pair_t channelPair, bool enable) |
| ASRC enable channel pair. More... | |
Interrupts | |
| static void | ASRC_EnableInterrupt (ASRC_Type *base, uint32_t mask) |
| ASRC interrupt enable This function enable the ASRC interrupt with the provided mask. More... | |
| static void | ASRC_DisableInterrupt (ASRC_Type *base, uint32_t mask) |
| ASRC interrupt disable This function disable the ASRC interrupt with the provided mask. More... | |
Status | |
| static uint32_t | ASRC_GetStatus (ASRC_Type *base) |
| Gets the ASRC status flag state. More... | |
| static bool | ASRC_GetChannelPairInitialStatus (ASRC_Type *base, asrc_channel_pair_t channel) |
| Gets the ASRC channel pair initialization state. More... | |
| static uint32_t | ASRC_GetChannelPairFifoStatus (ASRC_Type *base, asrc_channel_pair_t channelPair) |
| Gets the ASRC channel A fifo a status flag state. More... | |
Bus Operations | |
| static void | ASRC_ChannelPairWriteData (ASRC_Type *base, asrc_channel_pair_t channelPair, uint32_t data) |
| Writes data into ASRC channel pair FIFO. More... | |
| static uint32_t | ASRC_ChannelPairReadData (ASRC_Type *base, asrc_channel_pair_t channelPair) |
| Read data from ASRC channel pair FIFO. More... | |
| static uint32_t | ASRC_GetInputDataRegisterAddress (ASRC_Type *base, asrc_channel_pair_t channelPair) |
| Get input data fifo address. More... | |
| static uint32_t | ASRC_GetOutputDataRegisterAddress (ASRC_Type *base, asrc_channel_pair_t channelPair) |
| Get output data fifo address. More... | |
| status_t | ASRC_SetIdealRatioConfig (ASRC_Type *base, asrc_channel_pair_t channelPair, uint32_t inputSampleRate, uint32_t outputSampleRate) |
| ASRC configure ideal ratio. More... | |
Transactional | |
| status_t | ASRC_TransferSetChannelPairConfig (ASRC_Type *base, asrc_handle_t *handle, asrc_channel_pair_config_t *config, uint32_t inputSampleRate, uint32_t outputSampleRate) |
| ASRC configure channel pair. More... | |
| void | ASRC_TransferCreateHandle (ASRC_Type *base, asrc_handle_t *handle, asrc_channel_pair_t channelPair, asrc_transfer_callback_t inCallback, asrc_transfer_callback_t outCallback, void *userData) |
| Initializes the ASRC handle. More... | |
| status_t | ASRC_TransferNonBlocking (ASRC_Type *base, asrc_handle_t *handle, asrc_transfer_t *xfer) |
| Performs an interrupt non-blocking convert on asrc. More... | |
| status_t | ASRC_TransferBlocking (ASRC_Type *base, asrc_channel_pair_t channelPair, asrc_transfer_t *xfer) |
| Performs an blocking convert on asrc. More... | |
| status_t | ASRC_TransferGetConvertedCount (ASRC_Type *base, asrc_handle_t *handle, size_t *count) |
| Get converted byte count. More... | |
| void | ASRC_TransferAbortConvert (ASRC_Type *base, asrc_handle_t *handle) |
| Aborts the current convert. More... | |
| void | ASRC_TransferTerminateConvert (ASRC_Type *base, asrc_handle_t *handle) |
| Terminate all ASRC convert. More... | |
| void | ASRC_TransferHandleIRQ (ASRC_Type *base, asrc_handle_t *handle) |
| ASRC convert interrupt handler. More... | |
| struct asrc_channel_pair_config_t |
Data Fields | |
| asrc_audio_channel_t | audioDataChannels |
| audio data channel numbers | |
| asrc_clock_source_t | inClockSource |
| input clock source, reference the clock source definition in SOC header file | |
| uint32_t | inSourceClock_Hz |
| input source clock frequency | |
| asrc_clock_source_t | outClockSource |
| output clock source, reference the clock source definition in SOC header file | |
| uint32_t | outSourceClock_Hz |
| output source clock frequency | |
| asrc_ratio_t | sampleRateRatio |
| sample rate ratio type | |
| asrc_data_width_t | inDataWidth |
| input data width | |
| asrc_data_align_t | inDataAlign |
| input data alignment | |
| asrc_data_width_t | outDataWidth |
| output data width | |
| asrc_data_align_t | outDataAlign |
| output data alignment | |
| asrc_sign_extension_t | outSignExtension |
| output extension | |
| uint8_t | outFifoThreshold |
| output fifo threshold | |
| uint8_t | inFifoThreshold |
| input fifo threshold | |
| bool | bufStallWhenFifoEmptyFull |
| stall Pair A conversion in case of Buffer near empty full condition | |
| struct asrc_transfer_t |
Data Fields | |
| void * | inData |
| Data address to convert. More... | |
| size_t | inDataSize |
| input data size. More... | |
| void * | outData |
| Data address to store converted data. | |
| size_t | outDataSize |
| output data size. More... | |
| void* asrc_transfer_t::inData |
| size_t asrc_transfer_t::inDataSize |
| size_t asrc_transfer_t::outDataSize |
| struct asrc_in_handle_t |
Data Fields | |
| asrc_transfer_callback_t | callback |
| Callback function called at convert complete. | |
| uint32_t | sampleWidth |
| data width | |
| uint32_t | sampleMask |
| data mask | |
| uint32_t | fifoThreshold |
| fifo threshold | |
| uint8_t * | asrcQueue [ASRC_XFER_QUEUE_SIZE] |
| Transfer queue storing queued transfer. | |
| size_t | transferSamples [ASRC_XFER_QUEUE_SIZE] |
| Data bytes need to convert. | |
| volatile uint8_t | queueUser |
| Index for user to queue transfer. | |
| volatile uint8_t | queueDriver |
| Index for driver to get the transfer data and size. | |
| struct asrc_out_handle_t |
Data Fields | |
| asrc_transfer_callback_t | callback |
| Callback function called at convert complete. | |
| uint32_t | sampleWidth |
| data width | |
| uint32_t | fifoThreshold |
| fifo threshold | |
| uint8_t * | asrcQueue [ASRC_XFER_QUEUE_SIZE] |
| Transfer queue storing queued transfer. | |
| size_t | transferSamples [ASRC_XFER_QUEUE_SIZE] |
| Data bytes need to convert. | |
| volatile uint8_t | queueUser |
| Index for user to queue transfer. | |
| volatile uint8_t | queueDriver |
| Index for driver to get the transfer data and size. | |
| struct _asrc_handle |
asrc handler
Data Fields | |
| ASRC_Type * | base |
| base address | |
| uint32_t | state |
| Transfer status. | |
| void * | userData |
| Callback parameter passed to callback function. | |
| asrc_audio_channel_t | audioDataChannels |
| audio channel number | |
| asrc_channel_pair_t | channelPair |
| channel pair mask | |
| asrc_in_handle_t | in |
| asrc input handler | |
| asrc_out_handle_t | out |
| asrc output handler | |
| #define ASRC_XFER_QUEUE_SIZE (4U) |
| anonymous enum |
| enum asrc_channel_pair_t |
| anonymous enum |
| anonymous enum |
| anonymous enum |
| anonymous enum |
| enum asrc_ratio_t |
| enum asrc_audio_channel_t |
| enum asrc_data_width_t |
| enum asrc_data_align_t |
| uint32_t ASRC_GetInstance | ( | ASRC_Type * | base | ) |
| base | ASRC base pointer. |
| void ASRC_Init | ( | ASRC_Type * | base, |
| uint32_t | asrcPeripheralClock_Hz | ||
| ) |
This API gates the asrc clock. The asrc module can't operate unless ASRC_Init is called to enable the clock.
param base asrc base pointer. param asrcPeripheralClock_Hz peripheral clock of ASRC.
| void ASRC_Deinit | ( | ASRC_Type * | base | ) |
This API gates the ASRC clock and disable ASRC module. The ASRC module can't operate unless ASRC_Init
| base | ASRC base pointer. |
| void ASRC_SoftwareReset | ( | ASRC_Type * | base | ) |
This software reset bit is self-clear bit, it will generate a software reset signal inside ASRC. After 9 cycles of the ASRC processing clock, this reset process will stop and this bit will cleared automatically.
| base | ASRC base pointer |
| status_t ASRC_SetChannelPairConfig | ( | ASRC_Type * | base, |
| asrc_channel_pair_t | channelPair, | ||
| asrc_channel_pair_config_t * | config, | ||
| uint32_t | inputSampleRate, | ||
| uint32_t | outputSampleRate | ||
| ) |
| base | ASRC base pointer. |
| channelPair | index of channel pair, reference _asrc_channel_pair. |
| config | ASRC channel pair configuration pointer. |
| inputSampleRate | input audio data sample rate. |
| outputSampleRate | output audio data sample rate. |
| uint32_t ASRC_GetOutSamplesSize | ( | ASRC_Type * | base, |
| asrc_channel_pair_t | channelPair, | ||
| uint32_t | inSampleRate, | ||
| uint32_t | outSampleRate, | ||
| uint32_t | inSamplesize | ||
| ) |
| base | asrc base pointer. |
| channelPair | ASRC channel pair number. |
| inSampleRate | input sample rate. |
| outSampleRate | output sample rate. |
| inSamplesize | input sampleS size. |
| output | buffer size in byte. |
| uint32_t ASRC_MapSamplesWidth | ( | ASRC_Type * | base, |
| asrc_channel_pair_t | channelPair, | ||
| uint32_t * | inWidth, | ||
| uint32_t * | outWidth | ||
| ) |
| base | asrc base pointer. |
| channelPair | asrc channel pair index. |
| inWidth | ASRC channel pair number. |
| outWidth | input sample rate. |
| input | sample mask value. |
| uint32_t ASRC_GetRemainFifoSamples | ( | ASRC_Type * | base, |
| asrc_channel_pair_t | channelPair, | ||
| uint32_t * | buffer, | ||
| uint32_t | outSampleWidth, | ||
| uint32_t | remainSamples | ||
| ) |
| base | asrc base pointer. |
| channelPair | ASRC channel pair number. |
| buffer | input sample numbers. |
| outSampleWidth | output sample width. |
| remainSamples | output sample rate. |
| remain | samples number. |
|
inlinestatic |
| base | ASRC base pointer. |
| enable | true is enable, false is disable |
|
inlinestatic |
| base | ASRC base pointer. |
| channelPair | channel pair mask value, reference _asrc_channel_pair_mask. |
| enable | true is enable, false is disable. |
|
inlinestatic |
| base | ASRC peripheral base address. |
| mask | The interrupts to enable. Logical OR of _asrc_interrupt_mask. |
|
inlinestatic |
| base | ASRC peripheral base address. |
| mask | The interrupts to disable. Logical OR of _asrc_interrupt_mask. |
|
inlinestatic |
| base | ASRC base pointer |
|
inlinestatic |
| base | ASRC base pointer |
| channel | ASRC channel pair. |
|
inlinestatic |
| base | ASRC base pointer |
| channelPair | ASRC channel pair. |
|
inlinestatic |
Note: ASRC fifo width is 24bit.
| base | ASRC base pointer. |
| channelPair | ASRC channel pair. |
| data | Data needs to be written. |
|
inlinestatic |
Note: ASRC fifo width is 24bit.
| base | ASRC base pointer. |
| channelPair | ASRC channel pair. |
| value | read from fifo. |
|
inlinestatic |
Note: ASRC fifo width is 24bit.
| base | ASRC base pointer. |
| channelPair | ASRC channel pair. |
|
inlinestatic |
Note: ASRC fifo width is 24bit.
| base | ASRC base pointer. |
| channelPair | ASRC channel pair. |
| status_t ASRC_SetIdealRatioConfig | ( | ASRC_Type * | base, |
| asrc_channel_pair_t | channelPair, | ||
| uint32_t | inputSampleRate, | ||
| uint32_t | outputSampleRate | ||
| ) |
The ideal ratio should be used when input clock source is not avalible.
| base | ASRC base pointer. |
| channelPair | ASRC channel pair. |
| inputSampleRate | input audio data sample rate. |
| outputSampleRate | output audio data sample rate. |
| status_t ASRC_TransferSetChannelPairConfig | ( | ASRC_Type * | base, |
| asrc_handle_t * | handle, | ||
| asrc_channel_pair_config_t * | config, | ||
| uint32_t | inputSampleRate, | ||
| uint32_t | outputSampleRate | ||
| ) |
| base | ASRC base pointer. |
| handle | ASRC transactional handle pointer. |
| config | ASRC channel pair configuration pointer. |
| inputSampleRate | input audio data sample rate. |
| outputSampleRate | output audio data sample rate. |
| void ASRC_TransferCreateHandle | ( | ASRC_Type * | base, |
| asrc_handle_t * | handle, | ||
| asrc_channel_pair_t | channelPair, | ||
| asrc_transfer_callback_t | inCallback, | ||
| asrc_transfer_callback_t | outCallback, | ||
| void * | userData | ||
| ) |
This function initializes the handle for the ASRC transactional APIs. Call this function once to get the handle initialized.
| base | ASRC base pointer |
| handle | ASRC handle pointer. |
| channelPair | ASRC channel pair. |
| inCallback | Pointer to the user callback function. |
| outCallback | Pointer to the user callback function. |
| userData | User parameter passed to the callback function |
| status_t ASRC_TransferNonBlocking | ( | ASRC_Type * | base, |
| asrc_handle_t * | handle, | ||
| asrc_transfer_t * | xfer | ||
| ) |
| base | asrc base pointer. |
| handle | Pointer to the asrc_handle_t structure which stores the transfer state. |
| xfer | Pointer to the ASRC_transfer_t structure. |
| kStatus_Success | Successfully started the data receive. |
| kStatus_ASRCBusy | Previous receive still not finished. |
| status_t ASRC_TransferBlocking | ( | ASRC_Type * | base, |
| asrc_channel_pair_t | channelPair, | ||
| asrc_transfer_t * | xfer | ||
| ) |
| base | asrc base pointer. |
| channelPair | channel pair index. |
| xfer | Pointer to the ASRC_transfer_t structure. |
| kStatus_Success | Successfully started the data receive. |
| status_t ASRC_TransferGetConvertedCount | ( | ASRC_Type * | base, |
| asrc_handle_t * | handle, | ||
| size_t * | count | ||
| ) |
| base | ASRC base pointer. |
| handle | Pointer to the asrc_handle_t structure which stores the transfer state. |
| count | Bytes count sent. |
| kStatus_Success | Succeed get the transfer count. |
| kStatus_ASRCIdle | There is not a non-blocking transaction currently in progress. |
| void ASRC_TransferAbortConvert | ( | ASRC_Type * | base, |
| asrc_handle_t * | handle | ||
| ) |
| base | ASRC base pointer. |
| handle | Pointer to the asrc_handle_t structure which stores the transfer state. |
| void ASRC_TransferTerminateConvert | ( | ASRC_Type * | base, |
| asrc_handle_t * | handle | ||
| ) |
This function will clear all transfer slots buffered in the asrc queue. If users only want to abort the current transfer slot, please call ASRC_TransferAbortConvert.
| base | ASRC base pointer. |
| handle | ASRC eDMA handle pointer. |
| void ASRC_TransferHandleIRQ | ( | ASRC_Type * | base, |
| asrc_handle_t * | handle | ||
| ) |
| base | ASRC base pointer. |
| handle | Pointer to the asrc_handle_t structure. |