![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Enumerations | |
enum | messaging_status_t { kMSG_Success = kStatus_Success, kMSG_Error = MAKE_STATUS(kStatusGroup_MSG, 1) } |
The msg status. More... | |
Functions | |
void * | MSG_Alloc (uint32_t length) |
Allocates a message node with the length. More... | |
void | MSG_Free (void *buffer) |
frees a buffer allocated by MSG_Alloc. More... | |
messaging_status_t | MSG_QueueAddTail (messaging_t *msgQueue, void *msg) |
Links a message to the tail of the message queue. More... | |
messaging_status_t | MSG_QueueAddHead (messaging_t *msgQueue, void *msg) |
Links a message to the head of the message queue. More... | |
messaging_status_t | MSG_QueueAddPrev (void *msg, void *newMsg) |
Links a message to the previous of the given message. More... | |
messaging_status_t | MSG_QueueRemove (void *msg) |
Unlinks a message from its message queue. More... | |
void * | MSG_QueueRemoveHead (messaging_t *msgQueue) |
Unlinks the head from the message queue. More... | |
void * | MSG_QueueGetHead (messaging_t *msgQueue) |
Gets the head of the message queue. More... | |
void * | MSG_QueueGetNext (void *msg) |
Gets the next node of a given message. More... | |
void * | MSG_QueueGetPrev (void *msg) |
Gets the previous node of a given message. More... | |
enum messaging_status_t |
void* MSG_Alloc | ( | uint32_t | length | ) |
This function allocates a message node with the length.
length | The length of the message. |
The | allocated memory buffer address. |
void MSG_Free | ( | void * | buffer | ) |
This function frees a buffer allocated by MSG_Alloc.
buffer | The buffer address. |
messaging_status_t MSG_QueueAddTail | ( | messaging_t * | msgQueue, |
void * | msg | ||
) |
The function links a message to the tail of the message queue. The memory space of the message must be allocated by calling the function MSG_Alloc. And the memory space of the message must be freed by calling the function MSG_Free.
msgQueue | The message queue pointer. |
msg | The pointer of the message allocated by the MSG_Alloc. |
kMSG_Success | The message is added. |
kMSG_Error | The message addition failed. |
messaging_status_t MSG_QueueAddHead | ( | messaging_t * | msgQueue, |
void * | msg | ||
) |
The function links a message to the head of the message queue. The memory space of the message must be allocated by calling the function MSG_Alloc. And the memory space of the message must be freed by calling the function MSG_Free.
msgQueue | The message queue pointer. |
msg | The pointer of the message allocated by the MSG_Alloc. |
kMSG_Success | The message is added. |
kMSG_Error | The message addition failed. |
messaging_status_t MSG_QueueAddPrev | ( | void * | msg, |
void * | newMsg | ||
) |
The function links a message to the previous of the given message. The memory space of the message must be allocated by calling the function MSG_Alloc. And the memory space of the message must be freed by calling the function MSG_Free.
msg | The given message pointer. |
newMsg | A new message pointer needs to be added. |
kMSG_Success | The message is added. |
kMSG_Error | The message addition failed. |
messaging_status_t MSG_QueueRemove | ( | void * | msg | ) |
The function unlinks a message from its message queue. The memory space of the message must be allocated by calling the function MSG_Alloc. And the memory space of the message must be freed by calling the function MSG_Free.
msg | The message pointer. |
kMSG_Success | The message is removed. |
kMSG_Error | The message removal failed. |
void* MSG_QueueRemoveHead | ( | messaging_t * | msgQueue | ) |
The function unlinks the head from the message queue.
msgQueue | The message queue pointer. |
NULL | if the message queue is empty, or the pointer of removed message if removal was successful. |
void* MSG_QueueGetHead | ( | messaging_t * | msgQueue | ) |
The function gets the head of the message queue.
msgQueue | The message queue pointer. |
The | pointer of the message if the head is not NULL, or NULL. |
void* MSG_QueueGetNext | ( | void * | msg | ) |
The function gets the next node of a given message. The memory space of the message must be allocated by calling the function MSG_Alloc. And the memory space of the message must be freed by calling the function MSG_Free.
msg | The message pointer. |
The | pointer of the message if the next pointer is not NULL, or NULL. |
void* MSG_QueueGetPrev | ( | void * | msg | ) |
The function gets the previous node of a given message. The memory space of the message must be allocated by calling the function MSG_Alloc. And the memory space of the message must be freed by calling the function MSG_Free.
msg | The message pointer. |
The | pointer of the message if the previous pointer is not NULL, or NULL. |