The MCUXpresso SDK provides the peripheral driver for the Cryptographic Acceleration and Assurance Module (CAAM) module. CAAM is a multi-functional accelerator that supports the cryptographic functions common in many security protocols. This includes AES128, AES256, DES, 3DES, SHA1, SHA224, SHA256, RSA-4096, and a random number generator with a true entropic seed. CAAM includes a DMA engine that is descriptor-based to reduce processor-accelerator interaction.
The driver comprises two sets of API functions.
In the first set, blocking APIs are provided for the selected subset of operations supported by CAAM hardware. The CAAM operations are complete, and results are made availabe for further usage, when a function returns. When called, these functions do not return until a CAAM operation is complete. These functions use main CPU for simple polling loops to determine operation complete or error status.
The CAAM job descriptor is placed on the system stack during the blocking API calls. The driver uses global variable to manage the input and output job rings. The driver uses critical section (implemented as global interrupt enable/disable) for a short time, whenever it needs to access these global variables. Therefore, the driver functions are designed to be re-entrant and as a consequence, one CPU thread can call one blocking API, such as AES Encrypt, while other CPU thread can call another blocking API, such as SHA-256 Update. The blocking functions provide typical interface to upper layer or application software.
In the second set, non-blocking variants of the first set APIs are provided. Internally, the blocking APIs are implemented as a non-blocking operation start, followed by a blocking wait (CPU polling CAAM output job ring). for an operation completion. The non-blocking functions allow upper layer to inject an application specific operation after the CAAM job start and CAAM job complete events. The RTOS event wait and RTOS event set can be an example of such an operation.
CAAM Driver Initialization and Configuration
The CAAM Job Ring interface is a software job programming interface. CAAM implements 2 Job Ring interfaces. The CAAM driver uses caam_job_ring_interface_t data type as the Job Ring interface. Job Ring interface 0 is mandatory to be configured for the CAAM driver, Job Ring interface 1 is optional.
Initialize CAAM after Power On Reset or reset cycle See the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/caam.
The CAAM Driver is initialized by calling the CAAM_Init() function. It enables the CAAM module clock, it configures the Job Ring interface(s) and instantiates the CAAM RNG module in normal (non-deterministic) mode. Then, it calls CAAM_RNG_GenerateSecureKey() to load the JDKEK, TDKEK, and TDSK registers and finally configures the CAAM SCFGR register.
Comments about API usage in RTOS
CAAM operations provided by this driver are re-entrant by protecting global variables (Job Ring interface) in critical section (global interrupt enable/disable by EnableGlobalIRQ() and DisableGlobalIRQ() MCUXpresso SDK APIs). If required, different RTOS threads can call CAAM driver APIs simultaneously, given that EnableGlobalIRQ() and DisableGlobalIRQ() can a create critical section.
Comments about API usage in interrupt handler
All APIs can be used from interrupt handler although execution time should be considered (interrupt latency of equal and lower priority interrupts increases).
Comments about DCACHE
Usually the output data are not cached, because CAAM driver cleans them before scheduling job and invalidate after that, but in some cases the computing can take longer time and data could be written to memory by CAAM after invalidate happen, so it's recommended to invalidate CAAM output data again, right before their usage.
CAAM Driver Examples
Simple examples
Encrypt plaintext by DES engine Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/caam Encrypt plaintext by AES engine Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/caam Compute keyed hash by AES engine (CMAC) Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/caam Compute hash by MDHA engine (SHA-256) Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/caam Compute modular integer exponentiation Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/caam Compute elliptic curve point addition Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/caam
|
|
typedef uint32_t | caam_desc_aes_ecb_t [64] |
| | Memory buffer to hold CAAM descriptor for AESA ECB job.
|
| |
|
typedef uint32_t | caam_desc_aes_cbc_t [64] |
| | Memory buffer to hold CAAM descriptor for AESA CBC job.
|
| |
|
typedef uint32_t | caam_desc_aes_ctr_t [64] |
| | Memory buffer to hold CAAM descriptor for AESA CTR job.
|
| |
|
typedef uint32_t | caam_desc_aes_ccm_t [64] |
| | Memory buffer to hold CAAM descriptor for AESA CCM job.
|
| |
|
typedef uint32_t | caam_desc_aes_gcm_t [64] |
| | Memory buffer to hold CAAM descriptor for AESA GCM job.
|
| |
|
typedef uint32_t | caam_desc_hash_t [64] |
| | Memory buffer to hold CAAM descriptor for MDHA job or AESA CMAC job.
|
| |
|
typedef uint32_t | caam_desc_rng_t [64] |
| | Memory buffer to hold CAAM descriptor for RNG jobs.
|
| |
|
typedef uint32_t | caam_desc_cipher_des_t [64] |
| | Memory buffer to hold CAAM descriptor for DESA jobs.
|
| |
|
typedef uint32_t | caam_desc_pkha_t [64] |
| | Memory buffer to hold CAAM descriptor for PKHA jobs.
|
| |
|
typedef uint32_t | caam_desc_pkha_ecc_t [64] |
| | Memory buffer to hold CAAM descriptor for PKHA ECC jobs.
|
| |
|
| enum | {
kStatus_CAAM_Again = MAKE_STATUS(kStatusGroup_CAAM, 0),
kStatus_CAAM_DataOverflow = MAKE_STATUS(kStatusGroup_CAAM, 1)
} |
| | CAAM status return codes. More...
|
| |
| enum | caam_job_ring_t {
kCAAM_JobRing0 = 0u,
kCAAM_JobRing1 = 1u,
kCAAM_JobRing2 = 2u,
kCAAM_JobRing3 = 3u
} |
| | CAAM job ring selection. More...
|
| |
| enum | caam_wait_mode_t {
kCAAM_Blocking = 0u,
kCAAM_Nonblocking = 1u
} |
| | CAAM driver wait mechanism. More...
|
| |
| enum | caam_rng_sample_mode_t {
kCAAM_RNG_SampleModeVonNeumann = 0U,
kCAAM_RNG_SampleModeRaw = 1U,
kCAAM_RNG_SampleModeVonNeumannRaw
} |
| | CAAM RNG sample mode. More...
|
| |
| enum | caam_rng_ring_osc_div_t {
kCAAM_RNG_RingOscDiv0 = 0U,
kCAAM_RNG_RingOscDiv2 = 1U,
kCAAM_RNG_RingOscDiv4 = 2U,
kCAAM_RNG_RingOscDiv8 = 3U
} |
| | CAAM RNG ring oscillator divide. More...
|
| |
| enum | caam_priblob_t {
kCAAM_PrivSecureBootBlobs = 0U,
kCAAM_PrivProvisioningBlobsType1 = 1U,
kCAAM_PrivProvisioningBlobsType2 = 2U,
kCAAM_NormalOperationBlobs = 3U
} |
| | CAAM Private Blob. More...
|
| |
| enum | caam_ext_key_xfr_source_t {
kCAAM_ExtKeyXfr_KeyRegisterClass1 = 1U,
kCAAM_ExtKeyXfr_KeyRegisterClass2 = 2U,
kCAAM_ExtKeyXfr_PkhaRamE = 3U
} |
| | CAAM External Key Transfer command SRC (The source from which the key will be obtained) More...
|
| |
| struct caam_job_callback_t |
Data Fields |
|
void(* | JobCompleted )(void *userData) |
| | CAAM Job complete callback.
|
| |
The user callback functions is invoked only if jobRing interrupt has been enabled by the user. By default the jobRing interrupt is disabled (default job complete test is polling CAAM output ring).
| bool caam_config_t::scfgrLockTrngProgramMode |
| bool caam_config_t::scfgrEnableRandomDataBuffer |
| bool caam_config_t::scfgrRandomRngStateHandle0 |
| bool caam_config_t::scfgrRandomDpaResistance |
Version 2.1.5.
Current version: 2.1.4
Change log:
- Version 2.0.0
- Version 2.0.1
- Version 2.0.2
- Add Data and Instruction Synchronization Barrier in caam_input_ring_set_jobs_added() to make sure that the descriptor will be loaded into CAAM correctly.
- Version 2.0.3
- Use MACRO instead of numbers in descriptor.
- Correct descriptor size mask.
- Version 2.1.0
- Add return codes check and handling.
- Version 2.1.1
- Version 2.1.2
- Add data offset feature to provide support for mirrored (high-speed) memory.
- Version 2.1.3
- Version 2.1.4
- Version 2.1.5
- Support EXTENDED data size for all AES, HASH and RNG operations.
- Support multiple De-Initialization/Initialization of CAAM driver within one POR event.
| Enumerator |
|---|
| kStatus_CAAM_Again |
Non-blocking function shall be called again.
|
| kStatus_CAAM_DataOverflow |
Input data too big.
|
| Enumerator |
|---|
| kCAAM_JobRing0 |
CAAM Job ring 0.
|
| kCAAM_JobRing1 |
CAAM Job ring 1.
|
| kCAAM_JobRing2 |
CAAM Job ring 2.
|
| kCAAM_JobRing3 |
CAAM Job ring 3.
|
| Enumerator |
|---|
| kCAAM_Blocking |
CAAM_Wait blocking mode.
|
| kCAAM_Nonblocking |
CAAM Wait non-blocking mode.
|
Used by caam_config_t.
| Enumerator |
|---|
| kCAAM_RNG_SampleModeVonNeumann |
Use von Neumann data in both Entropy shifter and Statistical Checker.
|
| kCAAM_RNG_SampleModeRaw |
Use raw data into both Entropy shifter and Statistical Checker.
|
| kCAAM_RNG_SampleModeVonNeumannRaw |
Use von Neumann data in Entropy shifter.
Use raw data into Statistical Checker.
|
Used by caam_config_t.
| Enumerator |
|---|
| kCAAM_RNG_RingOscDiv0 |
Ring oscillator with no divide.
|
| kCAAM_RNG_RingOscDiv2 |
Ring oscillator divided-by-2.
|
| kCAAM_RNG_RingOscDiv4 |
Ring oscillator divided-by-4.
|
| kCAAM_RNG_RingOscDiv8 |
Ring oscillator divided-by-8.
|
Used by caam_config_t.
| Enumerator |
|---|
| kCAAM_PrivSecureBootBlobs |
Private secure boot software blobs.
|
| kCAAM_PrivProvisioningBlobsType1 |
Private Provisioning Type 1 blobs.
|
| kCAAM_PrivProvisioningBlobsType2 |
Private Provisioning Type 2 blobs.
|
| kCAAM_NormalOperationBlobs |
Normal operation blobs.
|
| Enumerator |
|---|
| kCAAM_ExtKeyXfr_KeyRegisterClass1 |
The Class 1 Key Register is the source.
|
| kCAAM_ExtKeyXfr_KeyRegisterClass2 |
The Class 2 Key Register is the source.
|
| kCAAM_ExtKeyXfr_PkhaRamE |
The PKHA E RAM is the source.
|
This function initializes the CAAM driver, including CAAM's internal RNG.
- Parameters
-
| base | CAAM peripheral base address |
| config | Pointer to configuration structure. |
- Returns
- kStatus_Success the CAAM Init has completed with zero termination status word
-
kStatus_Fail the CAAM Init has completed with non-zero termination status word
| status_t CAAM_Deinit |
( |
CAAM_Type * |
base | ) |
|
This function deinitializes the CAAM driver.
- Parameters
-
| base | CAAM peripheral base address |
- Returns
- kStatus_Success the CAAM Deinit has completed with zero termination status word
-
kStatus_Fail the CAAM Deinit has completed with non-zero termination status word
This function initializes the CAAM configuration structure to a default value. The default values are as follows. caamConfig->rngSampleMode = kCAAM_RNG_SampleModeVonNeumann; caamConfig->rngRingOscDiv = kCAAM_RNG_RingOscDiv4;
- Parameters
-
| [out] | config | Pointer to configuration structure. |
This function polls CAAM output ring for a specific job.
The CAAM job ring is specified by the jobRing field in the caam_handle_t structure. The job to be waited is specified by it's descriptor address.
This function has two modes, determined by the mode argument. In blocking mode, the function polls the specified jobRing until the descriptor is available in the CAAM output job ring. In non-blocking mode, it polls the output ring once and returns status immediately.
The function can be called from multiple threads or interrupt service routines, as internally it uses global critical section (global interrupt disable enable) to protect it's operation against concurrent accesses. The global interrupt is disabled only when the descriptor is found in the output ring, for a very short time, to remove the descriptor from the output ring safely.
- Parameters
-
| base | CAAM peripheral base address |
| handle | Data structure with CAAM jobRing used for this request |
| descriptor | |
| mode | Blocking and non-blocking mode. Zero is blocking. Non-zero is non-blocking. |
- Returns
- kStatus_Success the CAAM job has completed with zero job termination status word
-
kStatus_Fail the CAAM job has completed with non-zero job termination status word
-
kStatus_Again In non-blocking mode, the job is not ready in the CAAM Output Ring
This function loads the given key source to an CAAM external destination via a private interface, such as Inline Encryption Engine IEE Private Key bus.
The CAAM job ring is specified by the jobRing field in the caam_handle_t structure.
This function is blocking.
- Parameters
-
| base | CAAM peripheral base address |
| handle | Data structure with CAAM jobRing used for this request. |
| keySource | The source from which the key will be obtained. |
| keySize | Size of the key in bytes. |
- Returns
- kStatus_Success the CAAM job has completed with zero job termination status word
-
kStatus_Fail the CAAM job has completed with non-zero job termination status word