![]() |
MCUXpresso SDK API Reference Manual
Rev 2.11.1
NXP Semiconductors
|
Data Structures | |
| struct | lpspi_master_edma_handle_t |
| LPSPI master eDMA transfer handle structure used for transactional API. More... | |
| struct | lpspi_slave_edma_handle_t |
| LPSPI slave eDMA transfer handle structure used for transactional API. More... | |
Typedefs | |
| typedef void(* | lpspi_master_edma_transfer_callback_t )(LPSPI_Type *base, lpspi_master_edma_handle_t *handle, status_t status, void *userData) |
| Completion callback function pointer type. More... | |
| typedef void(* | lpspi_slave_edma_transfer_callback_t )(LPSPI_Type *base, lpspi_slave_edma_handle_t *handle, status_t status, void *userData) |
| Completion callback function pointer type. More... | |
Functions | |
| void | LPSPI_MasterTransferCreateHandleEDMA (LPSPI_Type *base, lpspi_master_edma_handle_t *handle, lpspi_master_edma_transfer_callback_t callback, void *userData, edma_handle_t *edmaRxRegToRxDataHandle, edma_handle_t *edmaTxDataToTxRegHandle) |
| Initializes the LPSPI master eDMA handle. More... | |
| status_t | LPSPI_MasterTransferEDMA (LPSPI_Type *base, lpspi_master_edma_handle_t *handle, lpspi_transfer_t *transfer) |
| LPSPI master transfer data using eDMA. More... | |
| void | LPSPI_MasterTransferAbortEDMA (LPSPI_Type *base, lpspi_master_edma_handle_t *handle) |
| LPSPI master aborts a transfer which is using eDMA. More... | |
| status_t | LPSPI_MasterTransferGetCountEDMA (LPSPI_Type *base, lpspi_master_edma_handle_t *handle, size_t *count) |
| Gets the master eDMA transfer remaining bytes. More... | |
| void | LPSPI_SlaveTransferCreateHandleEDMA (LPSPI_Type *base, lpspi_slave_edma_handle_t *handle, lpspi_slave_edma_transfer_callback_t callback, void *userData, edma_handle_t *edmaRxRegToRxDataHandle, edma_handle_t *edmaTxDataToTxRegHandle) |
| Initializes the LPSPI slave eDMA handle. More... | |
| status_t | LPSPI_SlaveTransferEDMA (LPSPI_Type *base, lpspi_slave_edma_handle_t *handle, lpspi_transfer_t *transfer) |
| LPSPI slave transfers data using eDMA. More... | |
| void | LPSPI_SlaveTransferAbortEDMA (LPSPI_Type *base, lpspi_slave_edma_handle_t *handle) |
| LPSPI slave aborts a transfer which is using eDMA. More... | |
| status_t | LPSPI_SlaveTransferGetCountEDMA (LPSPI_Type *base, lpspi_slave_edma_handle_t *handle, size_t *count) |
| Gets the slave eDMA transfer remaining bytes. More... | |
Driver version | |
| #define | FSL_LPSPI_EDMA_DRIVER_VERSION (MAKE_VERSION(2, 1, 0)) |
| LPSPI EDMA driver version. More... | |
| struct _lpspi_master_edma_handle |
Forward declaration of the _lpspi_master_edma_handle typedefs.
Data Fields | |
| volatile bool | isPcsContinuous |
| Is PCS continuous in transfer. More... | |
| volatile bool | isByteSwap |
| A flag that whether should byte swap. More... | |
| volatile uint8_t | fifoSize |
| FIFO dataSize. More... | |
| volatile uint8_t | rxWatermark |
| Rx watermark. More... | |
| volatile uint8_t | bytesEachWrite |
| Bytes for each write TDR. More... | |
| volatile uint8_t | bytesEachRead |
| Bytes for each read RDR. More... | |
| volatile uint8_t | bytesLastRead |
| Bytes for last read RDR. More... | |
| volatile bool | isThereExtraRxBytes |
| Is there extra RX byte. More... | |
| uint8_t *volatile | txData |
| Send buffer. More... | |
| uint8_t *volatile | rxData |
| Receive buffer. More... | |
| volatile size_t | txRemainingByteCount |
| Number of bytes remaining to send. More... | |
| volatile size_t | rxRemainingByteCount |
| Number of bytes remaining to receive. More... | |
| volatile uint32_t | writeRegRemainingTimes |
| Write TDR register remaining times. More... | |
| volatile uint32_t | readRegRemainingTimes |
| Read RDR register remaining times. More... | |
| uint32_t | totalByteCount |
| Number of transfer bytes. | |
| uint32_t | txBuffIfNull |
| Used if there is not txData for DMA purpose. More... | |
| uint32_t | rxBuffIfNull |
| Used if there is not rxData for DMA purpose. More... | |
| uint32_t | transmitCommand |
| Used to write TCR for DMA purpose. More... | |
| volatile uint8_t | state |
| LPSPI transfer state , _lpspi_transfer_state. More... | |
| uint8_t | nbytes |
| eDMA minor byte transfer count initially configured. More... | |
| lpspi_master_edma_transfer_callback_t | callback |
| Completion callback. More... | |
| void * | userData |
| Callback user data. More... | |
| edma_handle_t * | edmaRxRegToRxDataHandle |
| edma_handle_t handle point used for RxReg to RxData buff | |
| edma_handle_t * | edmaTxDataToTxRegHandle |
| edma_handle_t handle point used for TxData to TxReg buff | |
| edma_tcd_t | lpspiSoftwareTCD [3] |
| SoftwareTCD, internal used. | |
| volatile bool lpspi_master_edma_handle_t::isPcsContinuous |
| volatile bool lpspi_master_edma_handle_t::isByteSwap |
| volatile uint8_t lpspi_master_edma_handle_t::fifoSize |
| volatile uint8_t lpspi_master_edma_handle_t::rxWatermark |
| volatile uint8_t lpspi_master_edma_handle_t::bytesEachWrite |
| volatile uint8_t lpspi_master_edma_handle_t::bytesEachRead |
| volatile uint8_t lpspi_master_edma_handle_t::bytesLastRead |
| volatile bool lpspi_master_edma_handle_t::isThereExtraRxBytes |
| uint8_t* volatile lpspi_master_edma_handle_t::txData |
| uint8_t* volatile lpspi_master_edma_handle_t::rxData |
| volatile size_t lpspi_master_edma_handle_t::txRemainingByteCount |
| volatile size_t lpspi_master_edma_handle_t::rxRemainingByteCount |
| volatile uint32_t lpspi_master_edma_handle_t::writeRegRemainingTimes |
| volatile uint32_t lpspi_master_edma_handle_t::readRegRemainingTimes |
| uint32_t lpspi_master_edma_handle_t::txBuffIfNull |
| uint32_t lpspi_master_edma_handle_t::rxBuffIfNull |
| uint32_t lpspi_master_edma_handle_t::transmitCommand |
| volatile uint8_t lpspi_master_edma_handle_t::state |
| uint8_t lpspi_master_edma_handle_t::nbytes |
| lpspi_master_edma_transfer_callback_t lpspi_master_edma_handle_t::callback |
| void* lpspi_master_edma_handle_t::userData |
| struct _lpspi_slave_edma_handle |
Forward declaration of the _lpspi_slave_edma_handle typedefs.
Data Fields | |
| volatile bool | isByteSwap |
| A flag that whether should byte swap. More... | |
| volatile uint8_t | fifoSize |
| FIFO dataSize. More... | |
| volatile uint8_t | rxWatermark |
| Rx watermark. More... | |
| volatile uint8_t | bytesEachWrite |
| Bytes for each write TDR. More... | |
| volatile uint8_t | bytesEachRead |
| Bytes for each read RDR. More... | |
| volatile uint8_t | bytesLastRead |
| Bytes for last read RDR. More... | |
| volatile bool | isThereExtraRxBytes |
| Is there extra RX byte. More... | |
| uint8_t | nbytes |
| eDMA minor byte transfer count initially configured. More... | |
| uint8_t *volatile | txData |
| Send buffer. More... | |
| uint8_t *volatile | rxData |
| Receive buffer. More... | |
| volatile size_t | txRemainingByteCount |
| Number of bytes remaining to send. More... | |
| volatile size_t | rxRemainingByteCount |
| Number of bytes remaining to receive. More... | |
| volatile uint32_t | writeRegRemainingTimes |
| Write TDR register remaining times. More... | |
| volatile uint32_t | readRegRemainingTimes |
| Read RDR register remaining times. More... | |
| uint32_t | totalByteCount |
| Number of transfer bytes. | |
| uint32_t | txBuffIfNull |
| Used if there is not txData for DMA purpose. More... | |
| uint32_t | rxBuffIfNull |
| Used if there is not rxData for DMA purpose. More... | |
| volatile uint8_t | state |
| LPSPI transfer state. More... | |
| uint32_t | errorCount |
| Error count for slave transfer. More... | |
| lpspi_slave_edma_transfer_callback_t | callback |
| Completion callback. More... | |
| void * | userData |
| Callback user data. More... | |
| edma_handle_t * | edmaRxRegToRxDataHandle |
| edma_handle_t handle point used for RxReg to RxData buff | |
| edma_handle_t * | edmaTxDataToTxRegHandle |
| edma_handle_t handle point used for TxData to TxReg | |
| edma_tcd_t | lpspiSoftwareTCD [2] |
| SoftwareTCD, internal used. | |
| volatile bool lpspi_slave_edma_handle_t::isByteSwap |
| volatile uint8_t lpspi_slave_edma_handle_t::fifoSize |
| volatile uint8_t lpspi_slave_edma_handle_t::rxWatermark |
| volatile uint8_t lpspi_slave_edma_handle_t::bytesEachWrite |
| volatile uint8_t lpspi_slave_edma_handle_t::bytesEachRead |
| volatile uint8_t lpspi_slave_edma_handle_t::bytesLastRead |
| volatile bool lpspi_slave_edma_handle_t::isThereExtraRxBytes |
| uint8_t lpspi_slave_edma_handle_t::nbytes |
| uint8_t* volatile lpspi_slave_edma_handle_t::txData |
| uint8_t* volatile lpspi_slave_edma_handle_t::rxData |
| volatile size_t lpspi_slave_edma_handle_t::txRemainingByteCount |
| volatile size_t lpspi_slave_edma_handle_t::rxRemainingByteCount |
| volatile uint32_t lpspi_slave_edma_handle_t::writeRegRemainingTimes |
| volatile uint32_t lpspi_slave_edma_handle_t::readRegRemainingTimes |
| uint32_t lpspi_slave_edma_handle_t::txBuffIfNull |
| uint32_t lpspi_slave_edma_handle_t::rxBuffIfNull |
| volatile uint8_t lpspi_slave_edma_handle_t::state |
| uint32_t lpspi_slave_edma_handle_t::errorCount |
| lpspi_slave_edma_transfer_callback_t lpspi_slave_edma_handle_t::callback |
| void* lpspi_slave_edma_handle_t::userData |
| #define FSL_LPSPI_EDMA_DRIVER_VERSION (MAKE_VERSION(2, 1, 0)) |
| typedef void(* lpspi_master_edma_transfer_callback_t)(LPSPI_Type *base, lpspi_master_edma_handle_t *handle, status_t status, void *userData) |
| base | LPSPI peripheral base address. |
| handle | Pointer to the handle for the LPSPI master. |
| status | Success or error code describing whether the transfer completed. |
| userData | Arbitrary pointer-dataSized value passed from the application. |
| typedef void(* lpspi_slave_edma_transfer_callback_t)(LPSPI_Type *base, lpspi_slave_edma_handle_t *handle, status_t status, void *userData) |
| base | LPSPI peripheral base address. |
| handle | Pointer to the handle for the LPSPI slave. |
| status | Success or error code describing whether the transfer completed. |
| userData | Arbitrary pointer-dataSized value passed from the application. |
| void LPSPI_MasterTransferCreateHandleEDMA | ( | LPSPI_Type * | base, |
| lpspi_master_edma_handle_t * | handle, | ||
| lpspi_master_edma_transfer_callback_t | callback, | ||
| void * | userData, | ||
| edma_handle_t * | edmaRxRegToRxDataHandle, | ||
| edma_handle_t * | edmaTxDataToTxRegHandle | ||
| ) |
This function initializes the LPSPI eDMA handle which can be used for other LPSPI transactional APIs. Usually, for a specified LPSPI instance, call this API once to get the initialized handle.
Note that the LPSPI eDMA has a separated (Rx and Rx as two sources) or shared (Rx and Tx are the same source) DMA request source. (1) For a separated DMA request source, enable and set the Rx DMAMUX source for edmaRxRegToRxDataHandle and Tx DMAMUX source for edmaIntermediaryToTxRegHandle. (2) For a shared DMA request source, enable and set the Rx/Rx DMAMUX source for edmaRxRegToRxDataHandle.
| base | LPSPI peripheral base address. |
| handle | LPSPI handle pointer to lpspi_master_edma_handle_t. |
| callback | LPSPI callback. |
| userData | callback function parameter. |
| edmaRxRegToRxDataHandle | edmaRxRegToRxDataHandle pointer to edma_handle_t. |
| edmaTxDataToTxRegHandle | edmaTxDataToTxRegHandle pointer to edma_handle_t. |
| status_t LPSPI_MasterTransferEDMA | ( | LPSPI_Type * | base, |
| lpspi_master_edma_handle_t * | handle, | ||
| lpspi_transfer_t * | transfer | ||
| ) |
This function transfers data using eDMA. This is a non-blocking function, which returns right away. When all data is transferred, the callback function is called.
Note: The transfer data size should be an integer multiple of bytesPerFrame if bytesPerFrame is less than or equal to 4. For bytesPerFrame greater than 4: The transfer data size should be equal to bytesPerFrame if the bytesPerFrame is not an integer multiple of 4. Otherwise, the transfer data size can be an integer multiple of bytesPerFrame.
| base | LPSPI peripheral base address. |
| handle | pointer to lpspi_master_edma_handle_t structure which stores the transfer state. |
| transfer | pointer to lpspi_transfer_t structure. |
| void LPSPI_MasterTransferAbortEDMA | ( | LPSPI_Type * | base, |
| lpspi_master_edma_handle_t * | handle | ||
| ) |
This function aborts a transfer which is using eDMA.
| base | LPSPI peripheral base address. |
| handle | pointer to lpspi_master_edma_handle_t structure which stores the transfer state. |
| status_t LPSPI_MasterTransferGetCountEDMA | ( | LPSPI_Type * | base, |
| lpspi_master_edma_handle_t * | handle, | ||
| size_t * | count | ||
| ) |
This function gets the master eDMA transfer remaining bytes.
| base | LPSPI peripheral base address. |
| handle | pointer to lpspi_master_edma_handle_t structure which stores the transfer state. |
| count | Number of bytes transferred so far by the EDMA transaction. |
| void LPSPI_SlaveTransferCreateHandleEDMA | ( | LPSPI_Type * | base, |
| lpspi_slave_edma_handle_t * | handle, | ||
| lpspi_slave_edma_transfer_callback_t | callback, | ||
| void * | userData, | ||
| edma_handle_t * | edmaRxRegToRxDataHandle, | ||
| edma_handle_t * | edmaTxDataToTxRegHandle | ||
| ) |
This function initializes the LPSPI eDMA handle which can be used for other LPSPI transactional APIs. Usually, for a specified LPSPI instance, call this API once to get the initialized handle.
Note that LPSPI eDMA has a separated (Rx and Tx as two sources) or shared (Rx and Tx as the same source) DMA request source.
(1) For a separated DMA request source, enable and set the Rx DMAMUX source for edmaRxRegToRxDataHandle and Tx DMAMUX source for edmaTxDataToTxRegHandle. (2) For a shared DMA request source, enable and set the Rx/Rx DMAMUX source for edmaRxRegToRxDataHandle .
| base | LPSPI peripheral base address. |
| handle | LPSPI handle pointer to lpspi_slave_edma_handle_t. |
| callback | LPSPI callback. |
| userData | callback function parameter. |
| edmaRxRegToRxDataHandle | edmaRxRegToRxDataHandle pointer to edma_handle_t. |
| edmaTxDataToTxRegHandle | edmaTxDataToTxRegHandle pointer to edma_handle_t. |
| status_t LPSPI_SlaveTransferEDMA | ( | LPSPI_Type * | base, |
| lpspi_slave_edma_handle_t * | handle, | ||
| lpspi_transfer_t * | transfer | ||
| ) |
This function transfers data using eDMA. This is a non-blocking function, which return right away. When all data is transferred, the callback function is called.
Note: The transfer data size should be an integer multiple of bytesPerFrame if bytesPerFrame is less than or equal to 4. For bytesPerFrame greater than 4: The transfer data size should be equal to bytesPerFrame if the bytesPerFrame is not an integer multiple of 4. Otherwise, the transfer data size can be an integer multiple of bytesPerFrame.
| base | LPSPI peripheral base address. |
| handle | pointer to lpspi_slave_edma_handle_t structure which stores the transfer state. |
| transfer | pointer to lpspi_transfer_t structure. |
| void LPSPI_SlaveTransferAbortEDMA | ( | LPSPI_Type * | base, |
| lpspi_slave_edma_handle_t * | handle | ||
| ) |
This function aborts a transfer which is using eDMA.
| base | LPSPI peripheral base address. |
| handle | pointer to lpspi_slave_edma_handle_t structure which stores the transfer state. |
| status_t LPSPI_SlaveTransferGetCountEDMA | ( | LPSPI_Type * | base, |
| lpspi_slave_edma_handle_t * | handle, | ||
| size_t * | count | ||
| ) |
This function gets the slave eDMA transfer remaining bytes.
| base | LPSPI peripheral base address. |
| handle | pointer to lpspi_slave_edma_handle_t structure which stores the transfer state. |
| count | Number of bytes transferred so far by the eDMA transaction. |