MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
NBOOT Driver

Overview

Data Structures

struct  nboot_secure_counter_t
 Data structure holding secure counter value used by nboot library. More...
 
struct  nboot_context_t
 NBOOT context type. More...
 
struct  nboot_rot_auth_parms_t
 NBOOT type for the root of trust parameters. More...
 
struct  nboot_sb3_load_manifest_parms_t
 manifest loading parameters More...
 
struct  nboot_img_auth_ecdsa_parms_t
 Data structure holding input arguments to POR secure boot (authentication) algorithm. More...
 
struct  nboot_img_authenticate_cmac_parms_t
 Data structure holding input arguments for CMAC authentication. More...
 

Macros

#define NXPCLHASH_WA_SIZE_MAX   (128U+64U)
 Define the max workarea size required for this component.
 
#define NXPCLCSS_HASH_RTF_OUTPUT_SIZE_HAL   ((size_t) 32U)
 Size of RTF appendix to hash output buffer, in bytes.
 
#define kNBOOT_RootKeyUsage_DebugCA_ImageCA_FwCA_ImageKey_FwKey   (0x0U)
 NBOOT type for the root key usage. More...
 
#define kNBOOT_RootKey_Enabled   (0xAAU)
 NBOOT type for the root key revocation. More...
 
#define kNBOOT_RootKey_Ecdsa_P256   (0x0000FE01U)
 NBOOT type specifying the elliptic curve to be used. More...
 
#define nboot_lc_nxpBlank   (0xFFFF0000U)
 Enumeration for SoC Lifecycle. More...
 

Typedefs

typedef uint32_t nboot_status_t
 Type for nboot status codes.
 
typedef uint64_t nboot_status_protected_t
 Type for nboot protected status codes.
 

Enumerations

enum  {
  kStatus_NBOOT_Success = 0x5A5A5A5AU,
  kStatus_NBOOT_Fail = 0x5A5AA5A5U,
  kStatus_NBOOT_InvalidArgument = 0x5A5AA5F0U,
  kStatus_NBOOT_RequestTimeout = 0x5A5AA5E1U,
  kStatus_NBOOT_KeyNotLoaded = 0x5A5AA5E2U,
  kStatus_NBOOT_AuthFail = 0x5A5AA5E4U,
  kStatus_NBOOT_OperationNotAvaialable = 0x5A5AA5E5U,
  kStatus_NBOOT_KeyNotAvailable = 0x5A5AA5E6U,
  kStatus_NBOOT_IvCounterOverflow = 0x5A5AA5E7U,
  kStatus_NBOOT_SelftestFail = 0x5A5AA5E8U,
  kStatus_NBOOT_InvalidDataFormat = 0x5A5AA5E9U,
  kStatus_NBOOT_IskCertUserDataTooBig = 0x5A5AA5EAU,
  kStatus_NBOOT_IskCertSignatureOffsetTooSmall = 0x5A5AA5EBU,
  kStatus_NBOOT_MemcpyFail =0x5A5A845AU
}
 nboot status codes. More...
 
enum  nboot_bool_t {
  kNBOOT_TRUE = 0x3C5AC33CU,
  kNBOOT_TRUE256 = 0x3C5AC35AU,
  kNBOOT_TRUE384 = 0x3C5AC3A5U,
  kNBOOT_FALSE = 0x5AA55AA5U
}
 Boolean type for the NBOOT functions. More...
 

Functions

status_t NBOOT_GenerateRandom (uint8_t *output, size_t outputByteLen)
 This API function is used to generate random number with specified length. More...
 
nboot_status_t NBOOT_ContextInit (nboot_context_t *context)
 The function is used for initializing of the nboot context data structure. More...
 
nboot_status_t NBOOT_ContextDeinit (nboot_context_t *context)
 The function is used to deinitialize nboot context data structure. More...
 
nboot_status_protected_t NBOOT_Sb3LoadManifest (nboot_context_t *context, uint32_t *manifest, nboot_sb3_load_manifest_parms_t *parms)
 Verify NBOOT SB3.1 manifest (header message) More...
 
nboot_status_protected_t NBOOT_Sb3LoadBlock (nboot_context_t *context, uint32_t *block)
 Verify NBOOT SB3.1 block. More...
 
nboot_status_protected_t NBOOT_ImgAuthenticateEcdsa (nboot_context_t *context, uint8_t imageStartAddress[], nboot_bool_t *isSignatureVerified, nboot_img_auth_ecdsa_parms_t *parms)
 This function authenticates image with asymmetric cryptography. More...
 
nboot_status_protected_t NBOOT_ImgAuthenticateCmac (nboot_context_t *context, uint8_t imageStartAddress[], nboot_bool_t *isSignatureVerified, nboot_img_authenticate_cmac_parms_t *parms)
 This function calculates the CMAC over the given image and compares it to the expected value. More...
 

Data Structure Documentation

struct nboot_secure_counter_t
struct nboot_context_t

This type defines the NBOOT context

Data Fields

uint32_t totalBlocks
 holds number of SB3 blocks. More...
 
uint32_t processData
 flag, initialized by nboot_sb3_load_header(). More...
 
uint32_t timeout
 timeout value for css operation. More...
 
uint32_t keyinfo [NBOOT_KEYINFO_WORDLEN]
 data for NBOOT key management. More...
 
uint32_t context [NBOOT_CONTEXT_WORDLEN]
 work area for NBOOT lib. More...
 
uint32_t uuid [4]
 holds UUID value from NMPA
 
uint32_t prngReadyFlag
 flag, used by nboot_rng_generate_lq_random() to determine whether CSS is ready to generate rnd number
 
uint32_t oemShareValidFlag
 flag, used during TP to determine whether valid oemShare was set by nboot_tp_isp_gen_oem_master_share()
 
uint32_t oemShare [4]
 buffer to store OEM_SHARE computed by nxpCLTrustProv_nboot_isp_gen_oem_master_share()
 
nboot_secure_counter_t secureCounter
 Secure counter used by nboot.
 

Field Documentation

uint32_t nboot_context_t::totalBlocks

Initialized by nboot_sb3_load_header().

uint32_t nboot_context_t::processData

SB3 related flag set by NBOOT in case the nboot_sb3_load_block() provides plain data to output buffer (for processing by ROM SB3 loader

uint32_t nboot_context_t::timeout

In case it is 0, infinite wait is performed

uint32_t nboot_context_t::keyinfo[NBOOT_KEYINFO_WORDLEN]
uint32_t nboot_context_t::context[NBOOT_CONTEXT_WORDLEN]
struct nboot_rot_auth_parms_t

This type defines the NBOOT root of trust parameters

Data Fields

nboot_root_key_revocation_t soc_rootKeyRevocation [NBOOT_ROOT_CERT_COUNT]
 Provided by caller based on NVM information in CFPA: ROTKH_REVOKE.
 
uint32_t soc_imageKeyRevocation
 Provided by caller based on NVM information in CFPA: IMAGE_KEY_REVOKE.
 
uint32_t soc_rkh [12]
 Provided by caller based on NVM information in CMPA: ROTKH (hash of hashes) More...
 
uint32_t soc_numberOfRootKeys
 unsigned int, between minimum = 1 and maximum = 4;
 
nboot_root_key_usage_t soc_rootKeyUsage [NBOOT_ROOT_CERT_COUNT]
 CMPA.
 
nboot_root_key_type_and_length_t soc_rootKeyTypeAndLength
 static selection between ECDSA P-256 or ECDSA P-384 based root keys
 

Field Documentation

uint32_t nboot_rot_auth_parms_t::soc_rkh[12]

In case of kNBOOT_RootKey_Ecdsa_P384, sock_rkh[0..11] are used In case of kNBOOT_RootKey_Ecdsa_P256, sock_rkh[0..7] are used

struct nboot_sb3_load_manifest_parms_t

This type defines the NBOOT SB3.1 manifest loading parameters

Data Fields

nboot_rot_auth_parms_t soc_RoTNVM
 trusted information originated from CFPA and NMPA
 
uint32_t soc_trustedFirmwareVersion
 Provided by caller based on NVM information in CFPA: Secure_FW_Version.
 
struct nboot_img_auth_ecdsa_parms_t

Shall be read from SoC trusted NVM or SoC fuses.

Data Fields

nboot_rot_auth_parms_t soc_RoTNVM
 trusted information originated from CFPA and NMPA
 
uint32_t soc_trustedFirmwareVersion
 Provided by caller based on NVM information in CFPA: Secure_FW_Version.
 
struct nboot_img_authenticate_cmac_parms_t

Data Fields

uint32_t expectedMAC [4]
 expected MAC result
 

Macro Definition Documentation

#define kNBOOT_RootKeyUsage_DebugCA_ImageCA_FwCA_ImageKey_FwKey   (0x0U)

This type defines the NBOOT root key usage; any other value means the root key is not valid (treat as if revoked).

#define kNBOOT_RootKey_Enabled   (0xAAU)

This type defines the NBOOT root key revocation; any other value means the root key is revoked.

#define kNBOOT_RootKey_Ecdsa_P256   (0x0000FE01U)

This type defines the elliptic curve type and length

#define nboot_lc_nxpBlank   (0xFFFF0000U)

Enumeration Type Documentation

anonymous enum
Enumerator
kStatus_NBOOT_Success 

Operation completed successfully.

kStatus_NBOOT_Fail 

Operation failed.

kStatus_NBOOT_InvalidArgument 

Invalid argument passed to the function.

kStatus_NBOOT_RequestTimeout 

Operation timed out.

kStatus_NBOOT_KeyNotLoaded 

The requested key is not loaded.

kStatus_NBOOT_AuthFail 

Authentication failed.

kStatus_NBOOT_OperationNotAvaialable 

Operation not available on this HW.

kStatus_NBOOT_KeyNotAvailable 

Key is not avaialble.

kStatus_NBOOT_IvCounterOverflow 

Overflow of IV counter (PRINCE/IPED).

kStatus_NBOOT_SelftestFail 

FIPS self-test failure.

kStatus_NBOOT_InvalidDataFormat 

Invalid data format for example antipole.

kStatus_NBOOT_IskCertUserDataTooBig 

Size of User data in ISK certificate is greater than 96 bytes.

kStatus_NBOOT_IskCertSignatureOffsetTooSmall 

Signature offset in ISK certificate is smaller than expected.

kStatus_NBOOT_MemcpyFail 

Unexpected error detected during nboot_memcpy()

This type defines boolean values used by NBOOT functions that are not easily disturbed by Fault Attacks

Enumerator
kNBOOT_TRUE 

Value for TRUE.

kNBOOT_TRUE256 

Value for TRUE when P256 was used to sign the image.

kNBOOT_TRUE384 

Value for TRUE when P384 was used to sign the image.

kNBOOT_FALSE 

Value for FALSE.

Function Documentation

status_t NBOOT_GenerateRandom ( uint8_t *  output,
size_t  outputByteLen 
)
Parameters
outputPointer to random number buffer
outputByteLenlength of generated random number in bytes. Length has to be in range <1, 2^16>
Return values
kStatus_NBOOT_InvalidArgumentInvalid input parameters (Input pointers points to NULL or length is invalid)
kStatus_NBOOT_SuccessOperation successfully finished
kStatus_NBOOT_FailError occured during operation
nboot_status_t NBOOT_ContextInit ( nboot_context_t *  context)
   It should be called prior to any other calls of nboot API.
Parameters
nbootCtxPointer to nboot_context_t structure.
Return values
kStatus_NBOOT_SuccessOperation successfully finished
kStatus_NBOOT_FailError occured during operation
nboot_status_t NBOOT_ContextDeinit ( nboot_context_t *  context)

Its contents are overwritten with random data so that any sensitive data does not remain in memory.

Parameters
contextPointer to nboot_context_t structure.
Return values
kStatus_NBOOT_SuccessOperation successfully finished
kStatus_NBOOT_FailError occured during operation
nboot_status_protected_t NBOOT_Sb3LoadManifest ( nboot_context_t *  context,
uint32_t *  manifest,
nboot_sb3_load_manifest_parms_t *  parms 
)

This function verifies the NBOOT SB3.1 manifest (header message), initializes the context and loads keys into the CSS key store so that they can be used by nboot_sb3_load_block function. The NBOOT context has to be initialized by the function nboot_context_init before calling this function. Please note that this API is intended to be used only by users who needs to split FW update process (loading of SB3.1 file) to partial steps to customize whole operation. For regular SB3.1 processing, please use API described in chapter ˇ°SBloader APIsˇ±.

Parameters
nbootCtxPointer to nboot_context_t structure.
manifestPointer to the input manifest buffer
paramsadditional input parameters. Please refer to nboot_sb3_load_manifest_parms_t definition for details.
Return values
kStatus_NBOOT_SuccessOperation successfully finished
kStatus_NBOOT_FailError occured during operation
nboot_status_protected_t NBOOT_Sb3LoadBlock ( nboot_context_t *  context,
uint32_t *  block 
)

This function verifies and decrypts an NBOOT SB3.1 block. Decryption is performed in-place. The NBOOT context has to be initialized by the function nboot_context_init before calling this function. Please note that this API is intended to be used only by users who needs to split FW update process (loading of SB3.1 file) to partial steps to customize whole operation. For regular SB3.1 processing, please use API described in chapter ˇ°SBloader APIsˇ±.

Parameters
contextPointer to nboot_context_t structure.
blockPointer to the input SB3.1 data block
Return values
kStatus_NBOOT_Successsuccessfully finished
kStatus_NBOOT_Failoccured during operation
nboot_status_protected_t NBOOT_ImgAuthenticateEcdsa ( nboot_context_t *  context,
uint8_t  imageStartAddress[],
nboot_bool_t *  isSignatureVerified,
nboot_img_auth_ecdsa_parms_t *  parms 
)
   The NBOOT context has to be initialized by the function nboot_context_init
   before calling this function.
Parameters
contextPointer to nboot_context_t structure.
imageStartAddressPointer to start of the image in memory.
isSignatureVerifiedPointer to memory holding function call result. After the function returns, the value will be set to kNBOOT_TRUE when the image is authentic. Any other value means the authentication does not pass.
parmsPointer to a data structure in trusted memory, holding input parameters for the algorithm. The data structure shall be correctly filled before the function call.
Return values
kStatus_NBOOT_SuccessOperation successfully finished
kStatus_NBOOT_FailReturned in all other cases. Doesn't always mean invalid image, it could also mean transient error caused by short time environmental conditions.
nboot_status_protected_t NBOOT_ImgAuthenticateCmac ( nboot_context_t *  context,
uint8_t  imageStartAddress[],
nboot_bool_t *  isSignatureVerified,
nboot_img_authenticate_cmac_parms_t *  parms 
)

To be more resistant against SPA, it is recommended that imageStartAddress is word aligned. The NBOOT context has to be initialized by the nboot_context_init() before calling this function.

Parameters
contextPointer to nboot_context_t structure.
imageStartAddressPointer to start of the image in memory.
isSignatureVerifiedPointer to memory holding function call result. After the function returns, the value will be set to
parmsPointer to a data structure in trusted memory, holding the reference MAC. The data structure shall be correctly filled before the function call.
Return values
kStatus_NBOOT_Success
kStatus_NBOOT_Fail