MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
Power Driver

Overview

Power driver provides APIs to control peripherals power and control the system power mode.

Macros

#define WAKEUP_SYS   (1UL << 0) /*!< [SLEEP, DEEP SLEEP ] */ /* WWDT0_IRQ and BOD_IRQ*/
 Low Power Modes Wake up sources.
 
#define WAKEUP_SDMA0   (1UL << 1)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_GPIO_GLOBALINT0   (1UL << 2)
 [SLEEP, DEEP SLEEP, POWER DOWN ]
 
#define WAKEUP_GPIO_GLOBALINT1   (1UL << 3)
 [SLEEP, DEEP SLEEP, POWER DOWN ]
 
#define WAKEUP_GPIO_INT0_0   (1UL << 4)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_GPIO_INT0_1   (1UL << 5)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_GPIO_INT0_2   (1UL << 6)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_GPIO_INT0_3   (1UL << 7)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_UTICK   (1UL << 8)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_MRT   (1UL << 9)
 [SLEEP, ]
 
#define WAKEUP_CTIMER0   (1UL << 10)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_CTIMER1   (1UL << 11)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_SCT   (1UL << 12)
 [SLEEP, ]
 
#define WAKEUP_CTIMER3   (1UL << 13)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_FLEXCOMM0   (1UL << 14)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_FLEXCOMM1   (1UL << 15)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_FLEXCOMM2   (1UL << 16)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_FLEXCOMM3   (1UL << 17)
 [SLEEP, DEEP SLEEP, POWER DOWN ]
 
#define WAKEUP_FLEXCOMM4   (1UL << 18)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_FLEXCOMM5   (1UL << 19)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_FLEXCOMM6   (1UL << 20)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_FLEXCOMM7   (1UL << 21)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_ADC0   (1UL << 22)
 [SLEEP, ]
 
#define WAKEUP_ADC1   (1UL << 23)
 [SLEEP, ]
 
#define WAKEUP_ACMP   (1UL << 24)
 [SLEEP, DEEP SLEEP, POWER DOWN ]
 
#define WAKEUP_DMIC   (1UL << 25)
 [SLEEP, ]
 
#define WAKEUP_HWVAD   (1UL << 26)
 [SLEEP, DEEP SLEEP, ]
 
#define WAKEUP_USB0_NEEDCLK   (1UL << 27)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_USB0   (1UL << 28)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_RTC_ALARM_WAKEUP   (1UL << 29)
 [SLEEP, DEEP SLEEP, POWER DOWN, DEEP POWER DOWN]
 
#define WAKEUP_EZH_ARCH_B   (1UL << 30)
 [SLEEP, ]
 
#define WAKEUP_WAKEUP_MAILBOX   (1UL << 31)
 [SLEEP, DEEP SLEEP, ]
 
#define WAKEUP_GPIO_INT0_4   (1UL << 0)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_GPIO_INT0_5   (1UL << 1)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_GPIO_INT0_6   (1UL << 2)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_GPIO_INT0_7   (1UL << 3)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_CTIMER2   (1UL << 4)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_CTIMER4   (1UL << 5)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_OS_EVENT_TIMER   (1UL << 6)
 [SLEEP, DEEP SLEEP, POWER DOWN, DEEP POWER DOWN]
 
#define WAKEUP_FLEXSPI   (1UL << 7)
 [SLEEP, ]
 
#define WAKEUP_CAN0_0   (1UL << 11)
 [SLEEP, ]
 
#define WAKEUP_CAN0_1   (1UL << 12)
 [SLEEP, ]
 
#define WAKEUP_SPIFILTER   (1UL << 13)
 [SLEEP, ]
 
#define WAKEUP_SEC_HYPERVISOR_CALL   (1UL << 17)
 [SLEEP, ]
 
#define WAKEUP_SEC_GPIO_INT0_0   (1UL << 18)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_SEC_GPIO_INT0_1   (1UL << 19)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_SEC_VIO   (1UL << 21)
 [SLEEP, ]
 
#define WAKEUP_CSS_IRQ0   (1UL << 22)
 [SLEEP, ]
 
#define WAKEUP_PKC   (1UL << 23)
 [SLEEP, ]
 
#define WAKEUP_PUF   (1UL << 24)
 [SLEEP, ]
 
#define WAKEUP_PQ   (1UL << 25)
 [SLEEP, ]
 
#define WAKEUP_SDMA1   (1UL << 26)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_LSPI_HS   (1UL << 27)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_CODE_WDG   (1UL << 28)
 [SLEEP, ]
 
#define WAKEUP_I3C   (1UL << 30)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_NEUTRON   (1UL << 0)
 [SLEEP, ]
 
#define WAKEUP_CSS_IRQ1   (1UL << 1)
 [SLEEP, ]
 
#define WAKEUP_DAC0   (1UL << 10)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_DAC1   (1UL << 11)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_DAC2   (1UL << 12)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_HS_COMP0   (1UL << 13)
 [SLEEP, ]
 
#define WAKEUP_HS_COMP1   (1UL << 14)
 [SLEEP, ]
 
#define WAKEUP_HS_COMP2   (1UL << 15)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM0_CAPTURE   (1UL << 16)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM0_FAULT   (1UL << 17)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM0_RELOAD_ERROR   (1UL << 18)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM0_COMPARE0   (1UL << 19)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM0_RELOAD0   (1UL << 20)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM0_COMPARE1   (1UL << 21)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM0_RELOAD1   (1UL << 22)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM0_COMPARE2   (1UL << 23)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM0_RELOAD2   (1UL << 24)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM0_COMPARE3   (1UL << 25)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM0_RELOAD3   (1UL << 26)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM1_CAPTURE   (1UL << 27)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM1_FAULT   (1UL << 28)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM1_RELOAD_ERROR   (1UL << 29)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM1_COMPARE0   (1UL << 30)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM1_RELOAD0   (1UL << 31)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM1_COMPARE1   (1UL << 0)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM1_RELOAD1   (1UL << 1)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM1_COMPARE2   (1UL << 2)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM1_RELOAD2   (1UL << 3)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM1_COMPARE3   (1UL << 4)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM1_RELOAD3   (1UL << 5)
 [SLEEP, ]
 
#define WAKEUP_ENC0_COMPARE   (1UL << 6)
 [SLEEP, ]
 
#define WAKEUP_ENC0_HOME   (1UL << 7)
 [SLEEP, ]
 
#define WAKEUP_ENC0_WDG   (1UL << 8)
 [SLEEP, ]
 
#define WAKEUP_ENC0_IDX   (1UL << 9)
 [SLEEP, ]
 
#define WAKEUP_ENC1_COMPARE   (1UL << 10)
 [SLEEP, ]
 
#define WAKEUP_ENC1_HOME   (1UL << 11)
 [SLEEP, ]
 
#define WAKEUP_ENC1_WDG   (1UL << 12)
 [SLEEP, ]
 
#define WAKEUP_ENC1_IDX   (1UL << 13)
 [SLEEP, ]
 
#define WAKEUP_ITRC   (1UL << 14)
 [SLEEP, DEEP SLEEP, POWER DOWN ]
 
#define WAKEUP_CF_DSP24L_IRQ0   (1UL << 15)
 [SLEEP, ]
 
#define WAKEUP_CF_DSP24L_IRQ1   (1UL << 16)
 [SLEEP, ]
 
#define WAKEUP_FTM0   (1UL << 17)
 [SLEEP, ]
 
#define LOWPOWER_HWWAKE_FORCED   (1UL << 0)
 Sleep Postpone (DEEP-SLEEP) More...
 
#define LOWPOWER_HWWAKE_PERIPHERALS   (1UL << 1)
 Wake for Flexcomms. More...
 
#define LOWPOWER_HWWAKE_DMIC   (1UL << 2)
 Wake for DMIC. More...
 
#define LOWPOWER_HWWAKE_SDMA0   (1UL << 3)
 Wake for DMA0. More...
 
#define LOWPOWER_HWWAKE_SDMA1   (1UL << 5)
 Wake for DMA1. More...
 
#define LOWPOWER_HWWAKE_DAC   (1UL << 6)
 Wake for DAC0, DAC1, DAC2. More...
 
#define LOWPOWER_HWWAKE_ENABLE_FRO192M   (1UL << 31)
 Need to be set if FRO192M is disable - via PDCTRL0 - in Deep Sleep mode and any of \ LOWPOWER_HWWAKE_PERIPHERALS, LOWPOWER_HWWAKE_SDMA0, LOWPOWER_HWWAKE_SDMA1 or LOWPOWER_HWWAKE_DAC is \ set.
 
#define LOWPOWER_CPURETCTRL_ENA_DISABLE   0
 CPU State retention (POWER-DOWN) More...
 
#define LOWPOWER_CPURETCTRL_ENA_ENABLE   1
 In POWER DOWN mode, CPU Retention is enabled.
 
#define LOWPOWER_WAKEUPIOSRC_PIO0_INDEX   0
 Wake up I/O sources (DEEP POWER-DOWN) More...
 
#define LOWPOWER_WAKEUPIOSRC_PIO1_INDEX   2
 Pin P0(28)
 
#define LOWPOWER_WAKEUPIOSRC_PIO2_INDEX   4
 Pin P1(18)
 
#define LOWPOWER_WAKEUPIOSRC_PIO3_INDEX   6
 Pin P1(30)
 
#define LOWPOWER_WAKEUPIOSRC_PIO4_INDEX   8
 Pin P0(26)
 
#define LOWPOWER_WAKEUPIOSRC_DISABLE   0
 Wake up is disable.
 
#define LOWPOWER_WAKEUPIOSRC_RISING   1
 Wake up on rising edge.
 
#define LOWPOWER_WAKEUPIOSRC_FALLING   2
 Wake up on falling edge.
 
#define LOWPOWER_WAKEUPIOSRC_RISING_FALLING   3
 Wake up on both rising or falling edges.
 
#define LOWPOWER_WAKEUPIOSRC_PIO0MODE_INDEX   10
 Pin P1( 1)
 
#define LOWPOWER_WAKEUPIOSRC_PIO1MODE_INDEX   12
 Pin P0(28)
 
#define LOWPOWER_WAKEUPIOSRC_PIO2MODE_INDEX   14
 Pin P1(18)
 
#define LOWPOWER_WAKEUPIOSRC_PIO3MODE_INDEX   16
 Pin P1(30)
 
#define LOWPOWER_WAKEUPIOSRC_PIO4MODE_INDEX   18
 Pin P0(26)
 
#define LOWPOWER_WAKEUPIOSRC_IO_MODE_PLAIN   0
 Wake up Pad is plain input.
 
#define LOWPOWER_WAKEUPIOSRC_IO_MODE_PULLDOWN   1
 Wake up Pad is pull-down.
 
#define LOWPOWER_WAKEUPIOSRC_IO_MODE_PULLUP   2
 Wake up Pad is pull-up.
 
#define LOWPOWER_WAKEUPIOSRC_IO_MODE_REPEATER   3
 Wake up Pad is in repeater.
 
#define LOWPOWER_WAKEUPIO_PIO0_DISABLEPULLUPDOWN_INDEX   20
 Wake-up I/O 0 pull-up/down disable/enable control index.
 
#define LOWPOWER_WAKEUPIO_PIO1_DISABLEPULLUPDOWN_INDEX   21
 Wake-up I/O 1 pull-up/down disable/enable control index.
 
#define LOWPOWER_WAKEUPIO_PIO2_DISABLEPULLUPDOWN_INDEX   22
 Wake-up I/O 2 pull-up/down disable/enable control index.
 
#define LOWPOWER_WAKEUPIO_PIO3_DISABLEPULLUPDOWN_INDEX   23
 Wake-up I/O 3 pull-up/down disable/enable control index.
 
#define LOWPOWER_WAKEUPIO_PIO4_DISABLEPULLUPDOWN_INDEX   24
 Wake-up I/O 4 pull-up/down disable/enable control index.
 
#define LOWPOWER_WAKEUPIO_PIO0_DISABLEPULLUPDOWN_MASK   (1UL << LOWPOWER_WAKEUPIO_PIO0_DISABLEPULLUPDOWN_INDEX)
 Wake-up I/O 0 pull-up/down disable/enable mask.
 
#define LOWPOWER_WAKEUPIO_PIO1_DISABLEPULLUPDOWN_MASK   (1UL << LOWPOWER_WAKEUPIO_PIO1_DISABLEPULLUPDOWN_INDEX)
 Wake-up I/O 1 pull-up/down disable/enable mask.
 
#define LOWPOWER_WAKEUPIO_PIO2_DISABLEPULLUPDOWN_MASK   (1UL << LOWPOWER_WAKEUPIO_PIO2_DISABLEPULLUPDOWN_INDEX)
 Wake-up I/O 2 pull-up/down disable/enable mask.
 
#define LOWPOWER_WAKEUPIO_PIO3_DISABLEPULLUPDOWN_MASK   (1UL << LOWPOWER_WAKEUPIO_PIO3_DISABLEPULLUPDOWN_INDEX)
 Wake-up I/O 3 pull-up/down disable/enable mask.
 
#define LOWPOWER_WAKEUPIO_PIO4_DISABLEPULLUPDOWN_MASK   (1UL << LOWPOWER_WAKEUPIO_PIO4_DISABLEPULLUPDOWN_INDEX)
 Wake-up I/O 4 pull-up/down disable/enable mask.
 
#define LOWPOWER_WAKEUPIO_PIO0_PULLUPDOWN_INDEX   25
 Wake-up I/O 0 pull-up/down configuration index.
 
#define LOWPOWER_WAKEUPIO_PIO1_PULLUPDOWN_INDEX   26
 Wake-up I/O 1 pull-up/down configuration index.
 
#define LOWPOWER_WAKEUPIO_PIO2_PULLUPDOWN_INDEX   27
 Wake-up I/O 2 pull-up/down configuration index.
 
#define LOWPOWER_WAKEUPIO_PIO3_PULLUPDOWN_INDEX   28
 Wake-up I/O 3 pull-up/down configuration index.
 
#define LOWPOWER_WAKEUPIO_PIO4_PULLUPDOWN_INDEX   29
 Wake-up I/O 4 pull-up/down configuration index.
 
#define LOWPOWER_WAKEUPIO_PIO0_PULLUPDOWN_MASK   (1UL << LOWPOWER_WAKEUPIO_PIO0_PULLUPDOWN_INDEX)
 Wake-up I/O 0 pull-up/down mask.
 
#define LOWPOWER_WAKEUPIO_PIO1_PULLUPDOWN_MASK   (1UL << LOWPOWER_WAKEUPIO_PIO1_PULLUPDOWN_INDEX)
 Wake-up I/O 1 pull-up/down mask.
 
#define LOWPOWER_WAKEUPIO_PIO2_PULLUPDOWN_MASK   (1UL << LOWPOWER_WAKEUPIO_PIO2_PULLUPDOWN_INDEX)
 Wake-up I/O 2 pull-up/down mask.
 
#define LOWPOWER_WAKEUPIO_PIO3_PULLUPDOWN_MASK   (1UL << LOWPOWER_WAKEUPIO_PIO3_PULLUPDOWN_INDEX)
 Wake-up I/O 3 pull-up/down mask.
 
#define LOWPOWER_WAKEUPIO_PIO4_PULLUPDOWN_MASK   (1UL << LOWPOWER_WAKEUPIO_PIO4_PULLUPDOWN_INDEX)
 Wake-up I/O 4 pull-up/down mask.
 
#define LOWPOWER_WAKEUPIO_PULLDOWN   0
 Select pull-down.
 
#define LOWPOWER_WAKEUPIO_PULLUP   1
 Select pull-up.
 
#define LOWPOWER_WAKEUPIO_CFG_SRC_IOCON   0
 Wake-up pins configuration (in/out, pull up/down plain input ...) is coming from IOCON (valid for \ DEEP-SLEEP and POWER-DOWN)
 
#define LOWPOWER_WAKEUPIO_CFG_SRC_PMC   1
 Wake-up pins configuration (in/out, pull up/down plain input ...) is coming from PMC and set up via \ the second parameter (wakeup_io_ctrl) of POWER_SetWakeUpPins API (valid for DEEP-SLEEP and POWER-DOWN)
 

Enumerations

enum  power_mode_cfg_t
 Low Power Modes configuration.
 
enum  power_reset_cause_t {
  kRESET_CAUSE_POR = 0UL,
  kRESET_CAUSE_PADRESET = 1UL,
  kRESET_CAUSE_BODRESET = 2UL,
  kRESET_CAUSE_ARMSYSTEMRESET = 3UL,
  kRESET_CAUSE_WDTRESET = 4UL,
  kRESET_CAUSE_SWRRESET = 5UL,
  kRESET_CAUSE_CDOGRESET = 6UL,
  kRESET_CAUSE_DPDRESET_WAKEUPIO = 7UL,
  kRESET_CAUSE_DPDRESET_RTC = 8UL,
  kRESET_CAUSE_DPDRESET_OSTIMER = 9UL,
  kRESET_CAUSE_DPDRESET_WAKEUPIO_RTC,
  kRESET_CAUSE_DPDRESET_WAKEUPIO_OSTIMER,
  kRESET_CAUSE_DPDRESET_RTC_OSTIMER,
  kRESET_CAUSE_DPDRESET_WAKEUPIO_RTC_OSTIMER = 13UL,
  kRESET_CAUSE_NOT_RELEVANT,
  kRESET_CAUSE_NOT_DETERMINISTIC = 15UL
}
 Device Reset Causes. More...
 
enum  power_boot_mode_t {
  kBOOT_MODE_POWER_UP,
  kBOOT_MODE_LP_DEEP_SLEEP = 1UL,
  kBOOT_MODE_LP_POWER_DOWN = 2UL,
  kBOOT_MODE_LP_DEEP_POWER_DOWN = 4UL
}
 Device Boot Modes. More...
 
enum  power_wakeup_pin_t {
  kWAKEUP_PIN_NONE = 0UL,
  kWAKEUP_PIN_0 = (1UL << 0),
  kWAKEUP_PIN_1 = (1UL << 1),
  kWAKEUP_PIN_2 = (1UL << 2),
  kWAKEUP_PIN_3 = (1UL << 3),
  kWAKEUP_PIN_4 = (1UL << 4),
  kWAKEUP_PIN_MULTIPLE = 0x1FUL
}
 Device wake up pins events. More...
 
enum  pd_bit_t
 analog components power modes control during low power modes
 
enum  power_sram_bit_t {
  kPOWER_SRAM_RAM_X0 = (1UL << 0),
  kPOWER_SRAM_RAM_00 = (1UL << 1),
  kPOWER_SRAM_RAM_01 = (1UL << 2),
  kPOWER_SRAM_RAM_02 = (1UL << 3),
  kPOWER_SRAM_RAM_03 = (1UL << 4),
  kPOWER_SRAM_RAM_10 = (1UL << 5),
  kPOWER_SRAM_RAM_20 = (1UL << 6),
  kPOWER_SRAM_RAM_30 = (1UL << 7),
  kPOWER_SRAM_RAM_40 = (1UL << 8),
  kPOWER_SRAM_RAM_41 = (1UL << 9),
  kPOWER_SRAM_RAM_42 = (1UL << 10),
  kPOWER_SRAM_RAM_43 = (1UL << 11),
  kPOWER_SRAM_FLASHCACHE = (1UL << 12),
  kPOWER_SRAM_FLEXSPICACHE = (1UL << 13),
  kPOWER_SRAM_FLEXSPIH2PREG = (1UL << 14),
  kPOWER_SRAM_DSLP_MASK = 0x7FFFUL,
  kPOWER_SRAM_PDWN_MASK = 0xFFFUL,
  kPOWER_SRAM_DPWD_MASK = 0xF3FUL
}
 SRAM instances bit masks. More...
 
enum  power_sram_index_t {
  kPOWER_SRAM_IDX_RAM_X0 = 0UL,
  kPOWER_SRAM_IDX_RAM_00 = 1UL,
  kPOWER_SRAM_IDX_RAM_01 = 2UL,
  kPOWER_SRAM_IDX_RAM_02 = 3UL,
  kPOWER_SRAM_IDX_RAM_03 = 4UL,
  kPOWER_SRAM_IDX_RAM_10 = 5UL,
  kPOWER_SRAM_IDX_RAM_20 = 6UL,
  kPOWER_SRAM_IDX_RAM_30 = 7UL,
  kPOWER_SRAM_IDX_RAM_40 = 8UL,
  kPOWER_SRAM_IDX_RAM_41 = 9UL,
  kPOWER_SRAM_IDX_RAM_42 = 10UL,
  kPOWER_SRAM_IDX_RAM_43 = 11UL,
  kPOWER_SRAM_IDX_FLASHCACHE = 12UL,
  kPOWER_SRAM_IDX_FLEXSPICACHE = 13UL,
  kPOWER_SRAM_IDX_FLEXSPIH2PREG = 14UL
}
 SRAM instances indexes. More...
 
enum  power_sram_pwr_mode_t {
  kPOWER_SRAMPwrActive = 0U,
  kPOWER_SRAMPwrLightSleep = 1U,
  kPOWER_SRAMPwrDeepSleep = 2U,
  kPOWER_SRAMPwrShutDown = 3U
}
 
enum  power_bod_vddmain_level_t {
  kPOWER_BodVddmainLevel1000mv = 0,
  kPOWER_BodVddmainLevel1100mv = 1,
  kPOWER_BodVddmainLevel1200mv = 2,
  kPOWER_BodVddmainLevel1300mv = 3,
  kPOWER_BodVddmainLevel1400mv = 4,
  kPOWER_BodVddmainLevel1500mv = 5,
  kPOWER_BodVddmainLevel1600mv = 6,
  kPOWER_BodVddmainLevel1650mv = 7,
  kPOWER_BodVddmainLevel1700mv = 8,
  kPOWER_BodVddmainLevel1750mv = 9,
  kPOWER_BodVddmainLevel1800mv = 10,
  kPOWER_BodVddmainLevel1900mv = 11,
  kPOWER_BodVddmainLevel2000mv = 12,
  kPOWER_BodVddmainLevel2100mv = 13,
  kPOWER_BodVddmainLevel2200mv = 14,
  kPOWER_BodVddmainLevel2300mv = 15,
  kPOWER_BodVddmainLevel2400mv = 16,
  kPOWER_BodVddmainLevel2500mv = 17,
  kPOWER_BodVddmainLevel2600mv = 18,
  kPOWER_BodVddmainLevel2700mv = 19,
  kPOWER_BodVddmainLevel2800mv = 20,
  kPOWER_BodVddmainLevel2900mv = 21,
  kPOWER_BodVddmainLevel3000mv = 22,
  kPOWER_BodVddmainLevel3100mv = 23,
  kPOWER_BodVddmainLevel3200mv = 24,
  kPOWER_BodVddmainLevel3300mv = 25
}
 
enum  power_bod_core_level_t {
  kPOWER_BodCoreLevel600mv = 0,
  kPOWER_BodCoreLevel650mv = 1,
  kPOWER_BodCoreLevel700mv = 2,
  kPOWER_BodCoreLevel750mv = 3,
  kPOWER_BodCoreLevel800mv = 4,
  kPOWER_BodCoreLevel850mv = 5,
  kPOWER_BodCoreLevel900mv = 6,
  kPOWER_BodCoreLevel950mv = 7
}
 
enum  power_bod_hyst_t {
  kPOWER_BodHystLevel25mv = 0U,
  kPOWER_BodHystLevel50mv = 1U,
  kPOWER_BodHystLevel75mv = 2U,
  kPOWER_BodHystLevel100mv = 3U
}
 
enum  power_core_pwr_source_t {
  kPOWER_CoreSrcDCDC = 0U,
  kPOWER_CoreSrcLDOCoreHP = 1U,
  kPOWER_CoreSrcLDOCoreLP = 2U,
  kPOWER_CoreSrcExternal = 3U
}
 
enum  power_core_pwr_state_t {
  kPOWER_CorePwrDisable = 0U,
  kPOWER_CorePwrEnable = 1U
}
 
enum  power_status_t {
  kPOWER_Status_Success = 0U,
  kPOWER_Status_Fail = 1U
}
 

Functions

static void POWER_EnablePD (pd_bit_t en)
 API to enable PDRUNCFG bit in the Syscon. More...
 
static void POWER_DisablePD (pd_bit_t en)
 API to disable PDRUNCFG bit in the Syscon. More...
 
power_status_t POWER_PowerInit (void)
 SoC Power Management Controller initialization. More...
 
power_status_t POWER_SetCorePowerSource (power_core_pwr_source_t pwr_source)
 Selects the core logic supply source. More...
 
power_core_pwr_source_t POWER_GetCorePowerSource (void)
 Returns the current core logic supply source. More...
 
power_status_t POWER_CorePowerSourceControl (power_core_pwr_source_t pwr_source, power_core_pwr_state_t pwr_state)
 Allows to control the state (enabled or disabled) of the core logic internal regulators (DCDC, LDO_CORE) More...
 
power_status_t POWER_SRAMPowerModeControl (power_sram_bit_t sram_inst, power_sram_pwr_mode_t pwr_mode)
 Allows to configure SRAM instances (low) power modes when the part is in ACTIVE mode. More...
 
power_sram_pwr_mode_t POWER_GetSRAMPowerMode (power_sram_index_t sram_index)
 
void POWER_EnterSleep (void)
 Configures and enters in SLEEP low power mode. More...
 
void POWER_EnterDeepSleep (uint32_t exclude_from_pd[2], uint32_t sram_retention_ctrl, uint32_t wakeup_interrupts[4], uint32_t hardware_wake_ctrl)
 Configures and enters in DEEP-SLEEP low power mode. More...
 
void POWER_EnterPowerDown (uint32_t exclude_from_pd[1], uint32_t sram_retention_ctrl, uint32_t wakeup_interrupts[4], uint32_t cpu_retention_addr)
 Configures and enters in POWERDOWN low power mode. More...
 
void POWER_EnterDeepPowerDown (uint32_t exclude_from_pd[1], uint32_t sram_retention_ctrl, uint32_t wakeup_interrupts[2], uint32_t wakeup_io_ctrl)
 Configures and enters in DEEPPOWERDOWN low power mode. More...
 
void POWER_SetWakeUpPins (uint32_t wakeup_io_cfg_src, uint32_t wakeup_io_ctrl)
 Configures the 5 wake-up pins to wake up the part in DEEP-SLEEP and POWER-DOWN low power modes. More...
 
void POWER_GetWakeUpCause (power_reset_cause_t *reset_cause, power_boot_mode_t *boot_mode, power_wakeup_pin_t *wakeup_pin_cause)
 Return some key information related to the device reset causes / wake-up sources, for all power modes. More...
 
void POWER_SetVoltageForFreq (uint32_t system_freq_hz)
 Configures the device internal power control settings. More...
 

Driver version

#define FSL_POWER_DRIVER_VERSION   (MAKE_VERSION(1, 0, 0))
 power driver version 1.0.0. More...
 

Macro Definition Documentation

#define FSL_POWER_DRIVER_VERSION   (MAKE_VERSION(1, 0, 0))
#define LOWPOWER_HWWAKE_FORCED   (1UL << 0)

Force peripheral clocking to stay on during deep-sleep mode.

#define LOWPOWER_HWWAKE_PERIPHERALS   (1UL << 1)

Any Flexcomm FIFO reaching the level specified by its own TXLVL will cause \ peripheral clocking to wake up temporarily while the related status is asserted

#define LOWPOWER_HWWAKE_DMIC   (1UL << 2)

DMIC being busy will cause peripheral clocking to remain running until DMIC \ completes. Used in conjonction with LOWPOWER_HWWAKE_PERIPHERALS

#define LOWPOWER_HWWAKE_SDMA0   (1UL << 3)

DMA0 being busy will cause peripheral clocking to remain running until DMA \ completes. Used in conjonction with LOWPOWER_HWWAKE_PERIPHERALS or LOWPOWER_HWWAKE_DAC

#define LOWPOWER_HWWAKE_SDMA1   (1UL << 5)

DMA0 being busy will cause peripheral clocking to remain running until DMA \ completes. Used in conjonction with LOWPOWER_HWWAKE_PERIPHERALS or LOWPOWER_HWWAKE_DAC

#define LOWPOWER_HWWAKE_DAC   (1UL << 6)

Any DAC0/1/2 FIFO reaching the level specified by the configuration \ will generate an asynchronous SDMA0 request, and SDMA0 will wake up the bus \ clock temporarily to transfer data to DAC0/1/2.

#define LOWPOWER_CPURETCTRL_ENA_DISABLE   0

In POWER DOWN mode, CPU Retention is disabled

#define LOWPOWER_WAKEUPIOSRC_PIO0_INDEX   0

Pin P1( 1)

Enumeration Type Documentation

Enumerator
kRESET_CAUSE_POR 

Power On Reset.

kRESET_CAUSE_PADRESET 

Hardware Pin Reset.

kRESET_CAUSE_BODRESET 

Brown-out Detector reset (either BODVBAT or BODCORE)

kRESET_CAUSE_ARMSYSTEMRESET 

ARM System Reset.

kRESET_CAUSE_WDTRESET 

Watchdog Timer Reset.

kRESET_CAUSE_SWRRESET 

Software Reset.

kRESET_CAUSE_CDOGRESET 

Code Watchdog Reset.

kRESET_CAUSE_DPDRESET_WAKEUPIO 

Any of the 5 wake-up pins.

kRESET_CAUSE_DPDRESET_RTC 

Real Time Clock (RTC)

kRESET_CAUSE_DPDRESET_OSTIMER 

OS Event Timer (OSTIMER)

kRESET_CAUSE_DPDRESET_WAKEUPIO_RTC 

Any of the 5 wake-up pins and RTC (the 2 events occured within 1 nano-second of each other)

kRESET_CAUSE_DPDRESET_WAKEUPIO_OSTIMER 

Any of the 5 wake-up pins and OSTIMER (the 2 events occured within 1 nano-second of each other)

kRESET_CAUSE_DPDRESET_RTC_OSTIMER 

Real Time Clock or OS Event Timer (the 2 events occured within 1 nano-second of each other)

kRESET_CAUSE_DPDRESET_WAKEUPIO_RTC_OSTIMER 

Any of the 5 wake-up pins or RTC or OS Event Timer (the 3 events occured within 1 nano-second of each other)

kRESET_CAUSE_NOT_RELEVANT 

No reset cause (for example, this code is used when waking up from DEEP-SLEEP low power mode)

kRESET_CAUSE_NOT_DETERMINISTIC 

Unknown Reset Cause.

Should be treated like "Hardware Pin Reset" from an application point of view.

Enumerator
kBOOT_MODE_POWER_UP 

All non Low Power Mode wake up (Power On Reset, Pin Reset, BoD Reset, ARM System Reset ...

)

kBOOT_MODE_LP_DEEP_SLEEP 

Wake up from DEEP-SLEEP Low Power mode.

kBOOT_MODE_LP_POWER_DOWN 

Wake up from POWER-DOWN Low Power mode.

kBOOT_MODE_LP_DEEP_POWER_DOWN 

Wake up from DEEP-POWER-DOWN Low Power mode.

Enumerator
kWAKEUP_PIN_NONE 

No wake up pin event.

kWAKEUP_PIN_0 

Wake up pin 0 event.

kWAKEUP_PIN_1 

Wake up pin 1 event.

kWAKEUP_PIN_2 

Wake up pin 2 event.

kWAKEUP_PIN_3 

Wake up pin 3 event.

kWAKEUP_PIN_4 

Wake up pin 4 event.

kWAKEUP_PIN_MULTIPLE 

More than 1 wake up pins events occured (within 1 nano-second of each other)

Enumerator
kPOWER_SRAM_RAM_X0 

RAM_X0.

kPOWER_SRAM_RAM_00 

RAM_00.

kPOWER_SRAM_RAM_01 

RAM_01.

kPOWER_SRAM_RAM_02 

RAM_02.

kPOWER_SRAM_RAM_03 

RAM_03.

kPOWER_SRAM_RAM_10 

RAM_10.

kPOWER_SRAM_RAM_20 

RAM_20.

kPOWER_SRAM_RAM_30 

RAM_30.

kPOWER_SRAM_RAM_40 

RAM_40.

kPOWER_SRAM_RAM_41 

RAM_41.

kPOWER_SRAM_RAM_42 

RAM_42.

kPOWER_SRAM_RAM_43 

RAM_43.

kPOWER_SRAM_FLASHCACHE 

Reserved.

Flash Cache SRAM instance

kPOWER_SRAM_FLEXSPICACHE 

Reserved.

FlexSPI Cache SRAM instance

kPOWER_SRAM_FLEXSPIH2PREG 

Reserved.

FlexSPI Dual Port Register Files instances

kPOWER_SRAM_DSLP_MASK 

Reserved.

DEEP-SLEEP SRAM instances

kPOWER_SRAM_PDWN_MASK 

Reserved.

POWER-DOWN SRAM instances

kPOWER_SRAM_DPWD_MASK 

Reserved.

DEEP-POWER-DOWN SRAM instances (RAM_20 & RAM_30 excluded).

Enumerator
kPOWER_SRAM_IDX_RAM_X0 

RAM_X0.

kPOWER_SRAM_IDX_RAM_00 

RAM_00.

kPOWER_SRAM_IDX_RAM_01 

RAM_01.

kPOWER_SRAM_IDX_RAM_02 

RAM_02.

kPOWER_SRAM_IDX_RAM_03 

RAM_03.

kPOWER_SRAM_IDX_RAM_10 

RAM_10.

kPOWER_SRAM_IDX_RAM_20 

RAM_20.

kPOWER_SRAM_IDX_RAM_30 

RAM_30.

kPOWER_SRAM_IDX_RAM_40 

RAM_40.

kPOWER_SRAM_IDX_RAM_41 

RAM_41.

kPOWER_SRAM_IDX_RAM_42 

RAM_42.

kPOWER_SRAM_IDX_RAM_43 

RAM_43.

kPOWER_SRAM_IDX_FLASHCACHE 

Reserved.

Flash Cache SRAM instance

kPOWER_SRAM_IDX_FLEXSPICACHE 

Reserved.

FlexSPI Cache SRAM instance

kPOWER_SRAM_IDX_FLEXSPIH2PREG 

Reserved.

FlexSPI Dual Port Register Files instances

Enumerator
kPOWER_SRAMPwrActive 

Active.

kPOWER_SRAMPwrLightSleep 

RESERVED, DO NOT USE (Light Sleep)

kPOWER_SRAMPwrDeepSleep 

Deep Sleep : SRAM content retained.

kPOWER_SRAMPwrShutDown 

Shutdown: SRAM content lost.

Enumerator
kPOWER_BodVddmainLevel1000mv 

VDDMAIN Brown out detector level 1V.

kPOWER_BodVddmainLevel1100mv 

VDDMAIN Brown out detector level 1.1V.

kPOWER_BodVddmainLevel1200mv 

VDDMAIN Brown out detector level 1.2V.

kPOWER_BodVddmainLevel1300mv 

VDDMAIN Brown out detector level 1.3V.

kPOWER_BodVddmainLevel1400mv 

VDDMAIN Brown out detector level 1.4V.

kPOWER_BodVddmainLevel1500mv 

VDDMAIN Brown out detector level 1.5V.

kPOWER_BodVddmainLevel1600mv 

VDDMAIN Brown out detector level 1.6V.

kPOWER_BodVddmainLevel1650mv 

VDDMAIN Brown out detector level 1.65V.

kPOWER_BodVddmainLevel1700mv 

VDDMAIN Brown out detector level 1.7V.

kPOWER_BodVddmainLevel1750mv 

VDDMAIN Brown out detector level 1.75V.

kPOWER_BodVddmainLevel1800mv 

VDDMAIN Brown out detector level 1.8V.

kPOWER_BodVddmainLevel1900mv 

VDDMAIN Brown out detector level 1.9V.

kPOWER_BodVddmainLevel2000mv 

VDDMAIN Brown out detector level 2V.

kPOWER_BodVddmainLevel2100mv 

VDDMAIN Brown out detector level 2.1V.

kPOWER_BodVddmainLevel2200mv 

VDDMAIN Brown out detector level 2.2V.

kPOWER_BodVddmainLevel2300mv 

VDDMAIN Brown out detector level 2.3V.

kPOWER_BodVddmainLevel2400mv 

VDDMAIN Brown out detector level 2.4V.

kPOWER_BodVddmainLevel2500mv 

VDDMAIN Brown out detector level 2.5V.

kPOWER_BodVddmainLevel2600mv 

VDDMAIN Brown out detector level 2.6V.

kPOWER_BodVddmainLevel2700mv 

VDDMAIN Brown out detector level 2.7V.

kPOWER_BodVddmainLevel2800mv 

VDDMAIN Brown out detector level 2.80 V.

kPOWER_BodVddmainLevel2900mv 

VDDMAIN Brown out detector level 2.9V.

kPOWER_BodVddmainLevel3000mv 

VDDMAIN Brown out detector level 3.0V.

kPOWER_BodVddmainLevel3100mv 

VDDMAIN Brown out detector level 3.1V.

kPOWER_BodVddmainLevel3200mv 

VDDMAIN Brown out detector level 3.2V.

kPOWER_BodVddmainLevel3300mv 

VDDMAIN Brown out detector level 3.3V.

Enumerator
kPOWER_BodCoreLevel600mv 

core Brown out detector level 600mV

kPOWER_BodCoreLevel650mv 

core Brown out detector level 650mV

kPOWER_BodCoreLevel700mv 

core Brown out detector level 700mV

kPOWER_BodCoreLevel750mv 

core Brown out detector level 750mV

kPOWER_BodCoreLevel800mv 

core Brown out detector level 800mV

kPOWER_BodCoreLevel850mv 

core Brown out detector level 850mV

kPOWER_BodCoreLevel900mv 

core Brown out detector level 900mV

kPOWER_BodCoreLevel950mv 

core Brown out detector level 950mV

Enumerator
kPOWER_BodHystLevel25mv 

BOD Hysteresis control level 25mv.

kPOWER_BodHystLevel50mv 

BOD Hysteresis control level 50mv.

kPOWER_BodHystLevel75mv 

BOD Hysteresis control level 75mv.

kPOWER_BodHystLevel100mv 

BOD Hysteresis control level 100mv.

Enumerator
kPOWER_CoreSrcDCDC 

DCDC.

kPOWER_CoreSrcLDOCoreHP 

LDO Core High Power Mode.

kPOWER_CoreSrcLDOCoreLP 

LDO Core Low Power Mode (DO NOT USE : Reserved for test purposes)

kPOWER_CoreSrcExternal 

External (DO NOT USE : Reserved for test purposes)

Enumerator
kPOWER_CorePwrDisable 

Disable.

kPOWER_CorePwrEnable 

Enable.

Enumerator
kPOWER_Status_Success 

OK.

kPOWER_Status_Fail 

Generic error code.

Function Documentation

static void POWER_EnablePD ( pd_bit_t  en)
inlinestatic

Note that enabling the bit powers down the peripheral

Parameters
enperipheral for which to enable the PDRUNCFG bit
Returns
none
static void POWER_DisablePD ( pd_bit_t  en)
inlinestatic

Note that disabling the bit powers up the peripheral

Parameters
enperipheral for which to disable the PDRUNCFG bit
Returns
none
power_status_t POWER_PowerInit ( void  )
Returns
power_status_t
power_status_t POWER_SetCorePowerSource ( power_core_pwr_source_t  pwr_source)
Parameters
pwr_source: Defines which regulator will be used to power the part core logic (internally)
Returns
power_status_t
power_core_pwr_source_t POWER_GetCorePowerSource ( void  )
Returns
power_core_pwr_source_t
power_status_t POWER_CorePowerSourceControl ( power_core_pwr_source_t  pwr_source,
power_core_pwr_state_t  pwr_state 
)
Parameters
pwr_source: Defines which regulator will be enabled or disabled
pwr_state: Defines the state of the internal regulator indicated by pwr_source
Returns
power_status_t
power_status_t POWER_SRAMPowerModeControl ( power_sram_bit_t  sram_inst,
power_sram_pwr_mode_t  pwr_mode 
)
Parameters
sram_inst: Defines the SRAM instance(s) to be configured.
pwr_mode: Defines the SRAM low power mode to be applied to all SRAM instances given by sram_inst
Returns
power_status_t
power_sram_pwr_mode_t POWER_GetSRAMPowerMode ( power_sram_index_t  sram_index)
Parameters
p_sram_index:
Returns
power_sram_pwr_mode_t
void POWER_EnterSleep ( void  )
Returns
Nothing
void POWER_EnterDeepSleep ( uint32_t  exclude_from_pd[2],
uint32_t  sram_retention_ctrl,
uint32_t  wakeup_interrupts[4],
uint32_t  hardware_wake_ctrl 
)
Parameters
exclude_from_pd,:defines which analog peripherals shall NOT be powered down (it is a 2 x 32-bit vectors, aligned with "pd_bit_t" definition)
sram_retention_ctrl:defineswhich SRAM instances will be put in "retention" mode during deep-sleep (aligned with "power_sram_bit_t" definition)
wakeup_interrupts,:defines which peripheral interrupts can be a wake-up source during deep-sleep (it is a 4 x 32-bit vectors, aligned with "WAKEUP_" #defines)
hardware_wake_ctrl,:configure DMA services during deep-sleep without waking up entire device (see "LOWPOWER_HWWAKE_*" #defines).
Returns
Nothing
     !!! IMPORTANT NOTES :
      1 - CPU & System CLock frequency is switched to FRO12MHz and is NOT restored back by the API.
void POWER_EnterPowerDown ( uint32_t  exclude_from_pd[1],
uint32_t  sram_retention_ctrl,
uint32_t  wakeup_interrupts[4],
uint32_t  cpu_retention_addr 
)
Parameters
exclude_from_pd,:defines which analog peripherals shall NOT be powered down (it is a 1 x 32-bit vector, aligned with "pd_bit_t" definition)
sram_retention_ctrl:defineswhich SRAM instances will be put in "retention" mode during power-down (aligned with "power_sram_bit_t" definition)
wakeup_interrupts,:defines which peripheral interrupts can be a wake-up source during power-down (it is a 2 x 32-bit vectors, aligned with "WAKEUP_" #defines)
cpu_retention_addr,:Must be:
  • Word aligned (address ending by 0x0, 0x4, 0x8 and 0xC).
  • Between 0x2000_0000 and 0x2000_09FC (inside RAM_00) or
  • Between 0x2000_1000 and 0x2000_19FC (inside RAM_01) or
  • Between 0x2000_2000 and 0x2000_29FC (inside RAM_02) or
  • Between 0x2000_3000 and 0x2000_39FC (inside RAM_03)
  • The CPU state will be stored in SRAM from "cpu_retention_addr" to "cpu_retention_addr + 1540". Therefore, any data present in this area before calling the function will be lost.
Returns
Nothing
     !!! IMPORTANT NOTES :
      1 - CPU0 & System Clock frequency is switched to FRO12MHz and is NOT restored back by the API.
      2 - It is the responsability of the user to make sure that SRAM instance containing the application
          software stack and variables WILL BE preserved during low power (via parameter "sram_retention_ctrl")
void POWER_EnterDeepPowerDown ( uint32_t  exclude_from_pd[1],
uint32_t  sram_retention_ctrl,
uint32_t  wakeup_interrupts[2],
uint32_t  wakeup_io_ctrl 
)
Parameters
exclude_from_pd,:defines which analog peripherals shall NOT be powered down (it is a 1 x 32-bit vector, aligned with "pd_bit_t" definition)
sram_retention_ctrl,:defines which SRAM instances will be put in "retention" mode during deep power-down (aligned with "power_sram_bit_t" definition)
wakeup_interrupts,:defines which peripheral interrupts can be a wake-up source during deep power-down (it is a 2 x 32-bit vectors, aligned with "WAKEUP_" #defines)
wakeup_io_ctrl,:configure the 5 wake-up pins that can wake-up the part from deep power-down mode (see "LOWPOWER_WAKEUPIOSRC_*" #defines)
Returns
Nothing
     !!! IMPORTANT NOTES :
      1 - CPU0 & System Clock frequency is switched to FRO12MHz and is NOT restored back by the API.
      2 - The HARD FAULT handler should execute from SRAM. (The Hard fault handler should initiate a full chip
reset)
void POWER_SetWakeUpPins ( uint32_t  wakeup_io_cfg_src,
uint32_t  wakeup_io_ctrl 
)
Parameters
wakeup_io_cfg_src: for all wake-up pins : indicates if the config is from IOCON (0) or from PMC (1).
wakeup_io_ctrl,:the 5 wake-up pins configurations (see "LOWPOWER_WAKEUPIOSRC_*" #defines)
Returns
Nothing
     !!! IMPORTANT NOTES :
      1 - To be called just before POWER_EnterDeepSleep() or POWER_EnterPowerDown().
void POWER_GetWakeUpCause ( power_reset_cause_t *  reset_cause,
power_boot_mode_t *  boot_mode,
power_wakeup_pin_t *  wakeup_pin_cause 
)
Parameters
reset_cause: the device reset cause, according to the definition of power_reset_cause_t type.
boot_mode: the device boot mode, according to the definition of power_boot_mode_t type.
wakeup_pin_cause,:the wake-up pin sources, according to the definition of power_wakeup_pin_t type.
Returns
Nothing
void POWER_SetVoltageForFreq ( uint32_t  system_freq_hz)
Parameters
system_freq_hz,:operating frequency required (in Hertz).
Returns
Nothing
     prepare on-chip power regulators (DC-DC Converter / Core and Always-on
     Low Drop-Out regulators)  to deliver the amount of power needed for the
     requested performance level, as defined by the CPU operating frequency.