MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
SCTimer: SCTimer/PWM (SCT)

Overview

The MCUXpresso SDK provides a driver for the SCTimer Module (SCT) of MCUXpresso SDK devices.

Function groups

The SCTimer driver supports the generation of PWM signals. The driver also supports enabling events in various states of the SCTimer and the actions that will be triggered when an event occurs.

Initialization and deinitialization

The function SCTIMER_Init() initializes the SCTimer with specified configurations. The function SCTIMER_GetDefaultConfig() gets the default configurations.

The function SCTIMER_Deinit() halts the SCTimer counter and turns off the module clock.

PWM Operations

The function SCTIMER_SetupPwm() sets up SCTimer channels for PWM output. The function can set up the PWM signal properties duty cycle and level-mode (active low or high) to use. However, the same PWM period and PWM mode (edge or center-aligned) is applied to all channels requesting the PWM output. The signal duty cycle is provided as a percentage of the PWM period. Its value should be between 1 and 100.

The function SCTIMER_UpdatePwmDutycycle() updates the PWM signal duty cycle of a particular SCTimer channel.

Status

Provides functions to get and clear the SCTimer status.

Interrupt

Provides functions to enable/disable SCTimer interrupts and get current enabled interrupts.

SCTimer State machine and operations

The SCTimer has 10 states and each state can have a set of events enabled that can trigger a user specified action when the event occurs.

SCTimer event operations

The user can create an event and enable it in the current state using the functions SCTIMER_CreateAndScheduleEvent() and SCTIMER_ScheduleEvent(). SCTIMER_CreateAndScheduleEvent() creates a new event based on the users preference and enables it in the current state. SCTIMER_ScheduleEvent() enables an event created earlier in the current state.

SCTimer state operations

The user can get the current state number by calling SCTIMER_GetCurrentState(), he can use this state number to set state transitions when a particular event is triggered.

Once the user has created and enabled events for the current state he can go to the next state by calling the function SCTIMER_IncreaseState(). The user can then start creating events to be enabled in this new state.

SCTimer action operations

There are a set of functions that decide what action should be taken when an event is triggered. SCTIMER_SetupCaptureAction() sets up which counter to capture and which capture register to read on event trigger. SCTIMER_SetupNextStateAction() sets up which state the SCTimer state machine should transition to on event trigger. SCTIMER_SetupOutputSetAction() sets up which pin to set on event trigger. SCTIMER_SetupOutputClearAction() sets up which pin to clear on event trigger. SCTIMER_SetupOutputToggleAction() sets up which pin to toggle on event trigger. SCTIMER_SetupCounterLimitAction() sets up which counter will be limited on event trigger. SCTIMER_SetupCounterStopAction() sets up which counter will be stopped on event trigger. SCTIMER_SetupCounterStartAction() sets up which counter will be started on event trigger. SCTIMER_SetupCounterHaltAction() sets up which counter will be halted on event trigger. SCTIMER_SetupDmaTriggerAction() sets up which DMA request will be activated on event trigger.

16-bit counter mode

The SCTimer is configurable to run as two 16-bit counters via the enableCounterUnify flag that is available in the configuration structure passed in to the SCTIMER_Init() function.

When operating in 16-bit mode, it is important the user specify the appropriate counter to use when working with the functions: SCTIMER_StartTimer(), SCTIMER_StopTimer(), SCTIMER_CreateAndScheduleEvent(), SCTIMER_SetupCaptureAction(), SCTIMER_SetupCounterLimitAction(), SCTIMER_SetupCounterStopAction(), SCTIMER_SetupCounterStartAction(), and SCTIMER_SetupCounterHaltAction().

Typical use case

PWM output

Output a PWM signal on 2 SCTimer channels with different duty cycles. Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/sctimer

Files

file  fsl_sctimer.h
 

Data Structures

struct  sctimer_pwm_signal_param_t
 Options to configure a SCTimer PWM signal. More...
 
struct  sctimer_config_t
 SCTimer configuration structure. More...
 

Typedefs

typedef void(* sctimer_event_callback_t )(void)
 SCTimer callback typedef. More...
 

Enumerations

enum  sctimer_pwm_mode_t {
  kSCTIMER_EdgeAlignedPwm = 0U,
  kSCTIMER_CenterAlignedPwm
}
 SCTimer PWM operation modes. More...
 
enum  sctimer_counter_t {
  kSCTIMER_Counter_L = (1U << 0),
  kSCTIMER_Counter_H = (1U << 1),
  kSCTIMER_Counter_U = (1U << 2)
}
 SCTimer counters type. More...
 
enum  sctimer_input_t {
  kSCTIMER_Input_0 = 0U,
  kSCTIMER_Input_1,
  kSCTIMER_Input_2,
  kSCTIMER_Input_3,
  kSCTIMER_Input_4,
  kSCTIMER_Input_5,
  kSCTIMER_Input_6,
  kSCTIMER_Input_7
}
 List of SCTimer input pins. More...
 
enum  sctimer_out_t {
  kSCTIMER_Out_0 = 0U,
  kSCTIMER_Out_1,
  kSCTIMER_Out_2,
  kSCTIMER_Out_3,
  kSCTIMER_Out_4,
  kSCTIMER_Out_5,
  kSCTIMER_Out_6,
  kSCTIMER_Out_7,
  kSCTIMER_Out_8,
  kSCTIMER_Out_9
}
 List of SCTimer output pins. More...
 
enum  sctimer_pwm_level_select_t {
  kSCTIMER_LowTrue = 0U,
  kSCTIMER_HighTrue
}
 SCTimer PWM output pulse mode: high-true, low-true or no output. More...
 
enum  sctimer_clock_mode_t {
  kSCTIMER_System_ClockMode = 0U,
  kSCTIMER_Sampled_ClockMode,
  kSCTIMER_Input_ClockMode,
  kSCTIMER_Asynchronous_ClockMode
}
 SCTimer clock mode options. More...
 
enum  sctimer_clock_select_t {
  kSCTIMER_Clock_On_Rise_Input_0 = 0U,
  kSCTIMER_Clock_On_Fall_Input_0,
  kSCTIMER_Clock_On_Rise_Input_1,
  kSCTIMER_Clock_On_Fall_Input_1,
  kSCTIMER_Clock_On_Rise_Input_2,
  kSCTIMER_Clock_On_Fall_Input_2,
  kSCTIMER_Clock_On_Rise_Input_3,
  kSCTIMER_Clock_On_Fall_Input_3,
  kSCTIMER_Clock_On_Rise_Input_4,
  kSCTIMER_Clock_On_Fall_Input_4,
  kSCTIMER_Clock_On_Rise_Input_5,
  kSCTIMER_Clock_On_Fall_Input_5,
  kSCTIMER_Clock_On_Rise_Input_6,
  kSCTIMER_Clock_On_Fall_Input_6,
  kSCTIMER_Clock_On_Rise_Input_7,
  kSCTIMER_Clock_On_Fall_Input_7
}
 SCTimer clock select options. More...
 
enum  sctimer_conflict_resolution_t {
  kSCTIMER_ResolveNone = 0U,
  kSCTIMER_ResolveSet,
  kSCTIMER_ResolveClear,
  kSCTIMER_ResolveToggle
}
 SCTimer output conflict resolution options. More...
 
enum  sctimer_event_active_direction_t {
  kSCTIMER_ActiveIndependent = 0U,
  kSCTIMER_ActiveInCountUp,
  kSCTIMER_ActiveInCountDown
}
 List of SCTimer event generation active direction when the counters are operating in BIDIR mode. More...
 
enum  sctimer_event_t
 List of SCTimer event types.
 
enum  sctimer_interrupt_enable_t {
  kSCTIMER_Event0InterruptEnable = (1U << 0),
  kSCTIMER_Event1InterruptEnable = (1U << 1),
  kSCTIMER_Event2InterruptEnable = (1U << 2),
  kSCTIMER_Event3InterruptEnable = (1U << 3),
  kSCTIMER_Event4InterruptEnable = (1U << 4),
  kSCTIMER_Event5InterruptEnable = (1U << 5),
  kSCTIMER_Event6InterruptEnable = (1U << 6),
  kSCTIMER_Event7InterruptEnable = (1U << 7),
  kSCTIMER_Event8InterruptEnable = (1U << 8),
  kSCTIMER_Event9InterruptEnable = (1U << 9),
  kSCTIMER_Event10InterruptEnable = (1U << 10),
  kSCTIMER_Event11InterruptEnable = (1U << 11),
  kSCTIMER_Event12InterruptEnable = (1U << 12)
}
 List of SCTimer interrupts. More...
 
enum  sctimer_status_flags_t {
  kSCTIMER_Event0Flag = (1U << 0),
  kSCTIMER_Event1Flag = (1U << 1),
  kSCTIMER_Event2Flag = (1U << 2),
  kSCTIMER_Event3Flag = (1U << 3),
  kSCTIMER_Event4Flag = (1U << 4),
  kSCTIMER_Event5Flag = (1U << 5),
  kSCTIMER_Event6Flag = (1U << 6),
  kSCTIMER_Event7Flag = (1U << 7),
  kSCTIMER_Event8Flag = (1U << 8),
  kSCTIMER_Event9Flag = (1U << 9),
  kSCTIMER_Event10Flag = (1U << 10),
  kSCTIMER_Event11Flag = (1U << 11),
  kSCTIMER_Event12Flag = (1U << 12),
  kSCTIMER_BusErrorLFlag,
  kSCTIMER_BusErrorHFlag
}
 List of SCTimer flags. More...
 

Driver version

#define FSL_SCTIMER_DRIVER_VERSION   (MAKE_VERSION(2, 4, 0))
 Version.
 

Initialization and deinitialization

status_t SCTIMER_Init (SCT_Type *base, const sctimer_config_t *config)
 Ungates the SCTimer clock and configures the peripheral for basic operation. More...
 
void SCTIMER_Deinit (SCT_Type *base)
 Gates the SCTimer clock. More...
 
void SCTIMER_GetDefaultConfig (sctimer_config_t *config)
 Fills in the SCTimer configuration structure with the default settings. More...
 

PWM setup operations

status_t SCTIMER_SetupPwm (SCT_Type *base, const sctimer_pwm_signal_param_t *pwmParams, sctimer_pwm_mode_t mode, uint32_t pwmFreq_Hz, uint32_t srcClock_Hz, uint32_t *event)
 Configures the PWM signal parameters. More...
 
void SCTIMER_UpdatePwmDutycycle (SCT_Type *base, sctimer_out_t output, uint8_t dutyCyclePercent, uint32_t event)
 Updates the duty cycle of an active PWM signal. More...
 

Interrupt Interface

static void SCTIMER_EnableInterrupts (SCT_Type *base, uint32_t mask)
 Enables the selected SCTimer interrupts. More...
 
static void SCTIMER_DisableInterrupts (SCT_Type *base, uint32_t mask)
 Disables the selected SCTimer interrupts. More...
 
static uint32_t SCTIMER_GetEnabledInterrupts (SCT_Type *base)
 Gets the enabled SCTimer interrupts. More...
 

Status Interface

static uint32_t SCTIMER_GetStatusFlags (SCT_Type *base)
 Gets the SCTimer status flags. More...
 
static void SCTIMER_ClearStatusFlags (SCT_Type *base, uint32_t mask)
 Clears the SCTimer status flags. More...
 

Counter Start and Stop

static void SCTIMER_StartTimer (SCT_Type *base, uint32_t countertoStart)
 Starts the SCTimer counter. More...
 
static void SCTIMER_StopTimer (SCT_Type *base, uint32_t countertoStop)
 Halts the SCTimer counter. More...
 

Functions to create a new event and manage the state logic

status_t SCTIMER_CreateAndScheduleEvent (SCT_Type *base, sctimer_event_t howToMonitor, uint32_t matchValue, uint32_t whichIO, sctimer_counter_t whichCounter, uint32_t *event)
 Create an event that is triggered on a match or IO and schedule in current state. More...
 
void SCTIMER_ScheduleEvent (SCT_Type *base, uint32_t event)
 Enable an event in the current state. More...
 
status_t SCTIMER_IncreaseState (SCT_Type *base)
 Increase the state by 1. More...
 
uint32_t SCTIMER_GetCurrentState (SCT_Type *base)
 Provides the current state. More...
 
static void SCTIMER_SetCounterState (SCT_Type *base, sctimer_counter_t whichCounter, uint32_t state)
 Set the counter current state. More...
 
static uint16_t SCTIMER_GetCounterState (SCT_Type *base, sctimer_counter_t whichCounter)
 Get the counter current state value. More...
 

Actions to take in response to an event

status_t SCTIMER_SetupCaptureAction (SCT_Type *base, sctimer_counter_t whichCounter, uint32_t *captureRegister, uint32_t event)
 Setup capture of the counter value on trigger of a selected event. More...
 
void SCTIMER_SetCallback (SCT_Type *base, sctimer_event_callback_t callback, uint32_t event)
 Receive noticification when the event trigger an interrupt. More...
 
static void SCTIMER_SetupStateLdMethodAction (SCT_Type *base, uint32_t event, bool fgLoad)
 Change the load method of transition to the specified state. More...
 
static void SCTIMER_SetupNextStateActionwithLdMethod (SCT_Type *base, uint32_t nextState, uint32_t event, bool fgLoad)
 Transition to the specified state with Load method. More...
 
static void SCTIMER_SetupNextStateAction (SCT_Type *base, uint32_t nextState, uint32_t event)
 Transition to the specified state. More...
 
static void SCTIMER_SetupEventActiveDirection (SCT_Type *base, sctimer_event_active_direction_t activeDirection, uint32_t event)
 Setup event active direction when the counters are operating in BIDIR mode. More...
 
static void SCTIMER_SetupOutputSetAction (SCT_Type *base, uint32_t whichIO, uint32_t event)
 Set the Output. More...
 
static void SCTIMER_SetupOutputClearAction (SCT_Type *base, uint32_t whichIO, uint32_t event)
 Clear the Output. More...
 
void SCTIMER_SetupOutputToggleAction (SCT_Type *base, uint32_t whichIO, uint32_t event)
 Toggle the output level. More...
 
static void SCTIMER_SetupCounterLimitAction (SCT_Type *base, sctimer_counter_t whichCounter, uint32_t event)
 Limit the running counter. More...
 
static void SCTIMER_SetupCounterStopAction (SCT_Type *base, sctimer_counter_t whichCounter, uint32_t event)
 Stop the running counter. More...
 
static void SCTIMER_SetupCounterStartAction (SCT_Type *base, sctimer_counter_t whichCounter, uint32_t event)
 Re-start the stopped counter. More...
 
static void SCTIMER_SetupCounterHaltAction (SCT_Type *base, sctimer_counter_t whichCounter, uint32_t event)
 Halt the running counter. More...
 
static void SCTIMER_SetupDmaTriggerAction (SCT_Type *base, uint32_t dmaNumber, uint32_t event)
 Generate a DMA request. More...
 
static void SCTIMER_SetCOUNTValue (SCT_Type *base, sctimer_counter_t whichCounter, uint32_t value)
 Set the value of counter. More...
 
static uint32_t SCTIMER_GetCOUNTValue (SCT_Type *base, sctimer_counter_t whichCounter)
 Get the value of counter. More...
 
static void SCTIMER_SetEventInState (SCT_Type *base, uint32_t event, uint32_t state)
 Set the state mask bit field of EV_STATE register. More...
 
static void SCTIMER_ClearEventInState (SCT_Type *base, uint32_t event, uint32_t state)
 Clear the state mask bit field of EV_STATE register. More...
 
static bool SCTIMER_GetEventInState (SCT_Type *base, uint32_t event, uint32_t state)
 Get the state mask bit field of EV_STATE register. More...
 
void SCTIMER_EventHandleIRQ (SCT_Type *base)
 SCTimer interrupt handler. More...
 

Data Structure Documentation

struct sctimer_pwm_signal_param_t

Data Fields

sctimer_out_t output
 The output pin to use to generate the PWM signal.
 
sctimer_pwm_level_select_t level
 PWM output active level select. More...
 
uint8_t dutyCyclePercent
 PWM pulse width, value should be between 0 to 100 0 = always inactive signal (0% duty cycle) 100 = always active signal (100% duty cycle). More...
 

Field Documentation

sctimer_pwm_level_select_t sctimer_pwm_signal_param_t::level
uint8_t sctimer_pwm_signal_param_t::dutyCyclePercent
struct sctimer_config_t

This structure holds the configuration settings for the SCTimer peripheral. To initialize this structure to reasonable defaults, call the SCTMR_GetDefaultConfig() function and pass a pointer to the configuration structure instance.

The configuration structure can be made constant so as to reside in flash.

Data Fields

bool enableCounterUnify
 true: SCT operates as a unified 32-bit counter; false: SCT operates as two 16-bit counters. More...
 
sctimer_clock_mode_t clockMode
 SCT clock mode value.
 
sctimer_clock_select_t clockSelect
 SCT clock select value.
 
bool enableBidirection_l
 true: Up-down count mode for the L or unified counter false: Up count mode only for the L or unified counter
 
bool enableBidirection_h
 true: Up-down count mode for the H or unified counter false: Up count mode only for the H or unified counter. More...
 
uint8_t prescale_l
 Prescale value to produce the L or unified counter clock.
 
uint8_t prescale_h
 Prescale value to produce the H counter clock. More...
 
uint8_t outInitState
 Defines the initial output value.
 
uint8_t inputsync
 SCT INSYNC value, INSYNC field in the CONFIG register, from bit9 to bit 16. More...
 

Field Documentation

bool sctimer_config_t::enableCounterUnify

User can use the 16-bit low counter and the 16-bit high counters at the same time; for Hardware limit, user can not use unified 32-bit counter and any 16-bit low/high counter at the same time.

bool sctimer_config_t::enableBidirection_h

This field is used only if the enableCounterUnify is set to false

uint8_t sctimer_config_t::prescale_h

This field is used only if the enableCounterUnify is set to false

uint8_t sctimer_config_t::inputsync

it is used to define synchronization for input N: bit 9 = input 0 bit 10 = input 1 bit 11 = input 2 bit 12 = input 3 All other bits are reserved (bit13 ~bit 16). How User to set the the value for the member inputsync. IE: delay for input0, and input 1, bypasses for input 2 and input 3 MACRO definition in user level. #define INPUTSYNC0 (0U) #define INPUTSYNC1 (1U) #define INPUTSYNC2 (2U) #define INPUTSYNC3 (3U) User Code. sctimerInfo.inputsync = (1 << INPUTSYNC2) | (1 << INPUTSYNC3);

Typedef Documentation

typedef void(* sctimer_event_callback_t)(void)

Enumeration Type Documentation

Enumerator
kSCTIMER_EdgeAlignedPwm 

Edge-aligned PWM.

kSCTIMER_CenterAlignedPwm 

Center-aligned PWM.

Enumerator
kSCTIMER_Counter_L 

16-bit Low counter.

kSCTIMER_Counter_H 

16-bit High counter.

kSCTIMER_Counter_U 

32-bit Unified counter.

Enumerator
kSCTIMER_Input_0 

SCTIMER input 0.

kSCTIMER_Input_1 

SCTIMER input 1.

kSCTIMER_Input_2 

SCTIMER input 2.

kSCTIMER_Input_3 

SCTIMER input 3.

kSCTIMER_Input_4 

SCTIMER input 4.

kSCTIMER_Input_5 

SCTIMER input 5.

kSCTIMER_Input_6 

SCTIMER input 6.

kSCTIMER_Input_7 

SCTIMER input 7.

Enumerator
kSCTIMER_Out_0 

SCTIMER output 0.

kSCTIMER_Out_1 

SCTIMER output 1.

kSCTIMER_Out_2 

SCTIMER output 2.

kSCTIMER_Out_3 

SCTIMER output 3.

kSCTIMER_Out_4 

SCTIMER output 4.

kSCTIMER_Out_5 

SCTIMER output 5.

kSCTIMER_Out_6 

SCTIMER output 6.

kSCTIMER_Out_7 

SCTIMER output 7.

kSCTIMER_Out_8 

SCTIMER output 8.

kSCTIMER_Out_9 

SCTIMER output 9.

Enumerator
kSCTIMER_LowTrue 

Low true pulses.

kSCTIMER_HighTrue 

High true pulses.

Enumerator
kSCTIMER_System_ClockMode 

System Clock Mode.

kSCTIMER_Sampled_ClockMode 

Sampled System Clock Mode.

kSCTIMER_Input_ClockMode 

SCT Input Clock Mode.

kSCTIMER_Asynchronous_ClockMode 

Asynchronous Mode.

Enumerator
kSCTIMER_Clock_On_Rise_Input_0 

Rising edges on input 0.

kSCTIMER_Clock_On_Fall_Input_0 

Falling edges on input 0.

kSCTIMER_Clock_On_Rise_Input_1 

Rising edges on input 1.

kSCTIMER_Clock_On_Fall_Input_1 

Falling edges on input 1.

kSCTIMER_Clock_On_Rise_Input_2 

Rising edges on input 2.

kSCTIMER_Clock_On_Fall_Input_2 

Falling edges on input 2.

kSCTIMER_Clock_On_Rise_Input_3 

Rising edges on input 3.

kSCTIMER_Clock_On_Fall_Input_3 

Falling edges on input 3.

kSCTIMER_Clock_On_Rise_Input_4 

Rising edges on input 4.

kSCTIMER_Clock_On_Fall_Input_4 

Falling edges on input 4.

kSCTIMER_Clock_On_Rise_Input_5 

Rising edges on input 5.

kSCTIMER_Clock_On_Fall_Input_5 

Falling edges on input 5.

kSCTIMER_Clock_On_Rise_Input_6 

Rising edges on input 6.

kSCTIMER_Clock_On_Fall_Input_6 

Falling edges on input 6.

kSCTIMER_Clock_On_Rise_Input_7 

Rising edges on input 7.

kSCTIMER_Clock_On_Fall_Input_7 

Falling edges on input 7.

Specifies what action should be taken if multiple events dictate that a given output should be both set and cleared at the same time

Enumerator
kSCTIMER_ResolveNone 

No change.

kSCTIMER_ResolveSet 

Set output.

kSCTIMER_ResolveClear 

Clear output.

kSCTIMER_ResolveToggle 

Toggle output.

Enumerator
kSCTIMER_ActiveIndependent 

This event is triggered regardless of the count direction.

kSCTIMER_ActiveInCountUp 

This event is triggered only during up-counting when BIDIR = 1.

kSCTIMER_ActiveInCountDown 

This event is triggered only during down-counting when BIDIR = 1.

Enumerator
kSCTIMER_Event0InterruptEnable 

Event 0 interrupt.

kSCTIMER_Event1InterruptEnable 

Event 1 interrupt.

kSCTIMER_Event2InterruptEnable 

Event 2 interrupt.

kSCTIMER_Event3InterruptEnable 

Event 3 interrupt.

kSCTIMER_Event4InterruptEnable 

Event 4 interrupt.

kSCTIMER_Event5InterruptEnable 

Event 5 interrupt.

kSCTIMER_Event6InterruptEnable 

Event 6 interrupt.

kSCTIMER_Event7InterruptEnable 

Event 7 interrupt.

kSCTIMER_Event8InterruptEnable 

Event 8 interrupt.

kSCTIMER_Event9InterruptEnable 

Event 9 interrupt.

kSCTIMER_Event10InterruptEnable 

Event 10 interrupt.

kSCTIMER_Event11InterruptEnable 

Event 11 interrupt.

kSCTIMER_Event12InterruptEnable 

Event 12 interrupt.

Enumerator
kSCTIMER_Event0Flag 

Event 0 Flag.

kSCTIMER_Event1Flag 

Event 1 Flag.

kSCTIMER_Event2Flag 

Event 2 Flag.

kSCTIMER_Event3Flag 

Event 3 Flag.

kSCTIMER_Event4Flag 

Event 4 Flag.

kSCTIMER_Event5Flag 

Event 5 Flag.

kSCTIMER_Event6Flag 

Event 6 Flag.

kSCTIMER_Event7Flag 

Event 7 Flag.

kSCTIMER_Event8Flag 

Event 8 Flag.

kSCTIMER_Event9Flag 

Event 9 Flag.

kSCTIMER_Event10Flag 

Event 10 Flag.

kSCTIMER_Event11Flag 

Event 11 Flag.

kSCTIMER_Event12Flag 

Event 12 Flag.

kSCTIMER_BusErrorLFlag 

Bus error due to write when L counter was not halted.

kSCTIMER_BusErrorHFlag 

Bus error due to write when H counter was not halted.

Function Documentation

status_t SCTIMER_Init ( SCT_Type *  base,
const sctimer_config_t config 
)
Note
This API should be called at the beginning of the application using the SCTimer driver.
Parameters
baseSCTimer peripheral base address
configPointer to the user configuration structure.
Returns
kStatus_Success indicates success; Else indicates failure.
void SCTIMER_Deinit ( SCT_Type *  base)
Parameters
baseSCTimer peripheral base address
void SCTIMER_GetDefaultConfig ( sctimer_config_t config)

The default values are:

* config->enableCounterUnify = true;
* config->clockMode = kSCTIMER_System_ClockMode;
* config->clockSelect = kSCTIMER_Clock_On_Rise_Input_0;
* config->enableBidirection_l = false;
* config->enableBidirection_h = false;
* config->prescale_l = 0U;
* config->prescale_h = 0U;
* config->outInitState = 0U;
* config->inputsync = 0xFU;
*
Parameters
configPointer to the user configuration structure.
status_t SCTIMER_SetupPwm ( SCT_Type *  base,
const sctimer_pwm_signal_param_t pwmParams,
sctimer_pwm_mode_t  mode,
uint32_t  pwmFreq_Hz,
uint32_t  srcClock_Hz,
uint32_t *  event 
)

Call this function to configure the PWM signal period, mode, duty cycle, and edge. This function will create 2 events; one of the events will trigger on match with the pulse value and the other will trigger when the counter matches the PWM period. The PWM period event is also used as a limit event to reset the counter or change direction. Both events are enabled for the same state. The state number can be retrieved by calling the function SCTIMER_GetCurrentStateNumber(). The counter is set to operate as one 32-bit counter (unify bit is set to 1). The counter operates in bi-directional mode when generating a center-aligned PWM.

Note
When setting PWM output from multiple output pins, they all should use the same PWM mode i.e all PWM's should be either edge-aligned or center-aligned. When using this API, the PWM signal frequency of all the initialized channels must be the same. Otherwise all the initialized channels' PWM signal frequency is equal to the last call to the API's pwmFreq_Hz.
Parameters
baseSCTimer peripheral base address
pwmParamsPWM parameters to configure the output
modePWM operation mode, options available in enumeration sctimer_pwm_mode_t
pwmFreq_HzPWM signal frequency in Hz
srcClock_HzSCTimer counter clock in Hz
eventPointer to a variable where the PWM period event number is stored
Returns
kStatus_Success on success kStatus_Fail If we have hit the limit in terms of number of events created or if an incorrect PWM dutycylce is passed in.
void SCTIMER_UpdatePwmDutycycle ( SCT_Type *  base,
sctimer_out_t  output,
uint8_t  dutyCyclePercent,
uint32_t  event 
)

Before calling this function, the counter is set to operate as one 32-bit counter (unify bit is set to 1).

Parameters
baseSCTimer peripheral base address
outputThe output to configure
dutyCyclePercentNew PWM pulse width; the value should be between 1 to 100
eventEvent number associated with this PWM signal. This was returned to the user by the function SCTIMER_SetupPwm().
static void SCTIMER_EnableInterrupts ( SCT_Type *  base,
uint32_t  mask 
)
inlinestatic
Parameters
baseSCTimer peripheral base address
maskThe interrupts to enable. This is a logical OR of members of the enumeration sctimer_interrupt_enable_t
static void SCTIMER_DisableInterrupts ( SCT_Type *  base,
uint32_t  mask 
)
inlinestatic
Parameters
baseSCTimer peripheral base address
maskThe interrupts to enable. This is a logical OR of members of the enumeration sctimer_interrupt_enable_t
static uint32_t SCTIMER_GetEnabledInterrupts ( SCT_Type *  base)
inlinestatic
Parameters
baseSCTimer peripheral base address
Returns
The enabled interrupts. This is the logical OR of members of the enumeration sctimer_interrupt_enable_t
static uint32_t SCTIMER_GetStatusFlags ( SCT_Type *  base)
inlinestatic
Parameters
baseSCTimer peripheral base address
Returns
The status flags. This is the logical OR of members of the enumeration sctimer_status_flags_t
static void SCTIMER_ClearStatusFlags ( SCT_Type *  base,
uint32_t  mask 
)
inlinestatic
Parameters
baseSCTimer peripheral base address
maskThe status flags to clear. This is a logical OR of members of the enumeration sctimer_status_flags_t
static void SCTIMER_StartTimer ( SCT_Type *  base,
uint32_t  countertoStart 
)
inlinestatic
Note
In 16-bit mode, we can enable both Counter_L and Counter_H, In 32-bit mode, we only can select Counter_U.
Parameters
baseSCTimer peripheral base address
countertoStartThe SCTimer counters to enable. This is a logical OR of members of the enumeration sctimer_counter_t.
static void SCTIMER_StopTimer ( SCT_Type *  base,
uint32_t  countertoStop 
)
inlinestatic
Parameters
baseSCTimer peripheral base address
countertoStopThe SCTimer counters to stop. This is a logical OR of members of the enumeration sctimer_counter_t.
status_t SCTIMER_CreateAndScheduleEvent ( SCT_Type *  base,
sctimer_event_t  howToMonitor,
uint32_t  matchValue,
uint32_t  whichIO,
sctimer_counter_t  whichCounter,
uint32_t *  event 
)

This function will configure an event using the options provided by the user. If the event type uses the counter match, then the function will set the user provided match value into a match register and put this match register number into the event control register. The event is enabled for the current state and the event number is increased by one at the end. The function returns the event number; this event number can be used to configure actions to be done when this event is triggered.

Parameters
baseSCTimer peripheral base address
howToMonitorEvent type; options are available in the enumeration sctimer_interrupt_enable_t
matchValueThe match value that will be programmed to a match register
whichIOThe input or output that will be involved in event triggering. This field is ignored if the event type is "match only"
whichCounterSCTimer counter to use. In 16-bit mode, we can select Counter_L and Counter_H, In 32-bit mode, we can select Counter_U.
eventPointer to a variable where the new event number is stored
Returns
kStatus_Success on success kStatus_Error if we have hit the limit in terms of number of events created or if we have reached the limit in terms of number of match registers
void SCTIMER_ScheduleEvent ( SCT_Type *  base,
uint32_t  event 
)

This function will allow the event passed in to trigger in the current state. The event must be created earlier by either calling the function SCTIMER_SetupPwm() or function SCTIMER_CreateAndScheduleEvent() .

Parameters
baseSCTimer peripheral base address
eventEvent number to enable in the current state
status_t SCTIMER_IncreaseState ( SCT_Type *  base)

All future events created by calling the function SCTIMER_ScheduleEvent() will be enabled in this new state.

Parameters
baseSCTimer peripheral base address
Returns
kStatus_Success on success kStatus_Error if we have hit the limit in terms of states used
uint32_t SCTIMER_GetCurrentState ( SCT_Type *  base)

User can use this to set the next state by calling the function SCTIMER_SetupNextStateAction().

Parameters
baseSCTimer peripheral base address
Returns
The current state
static void SCTIMER_SetCounterState ( SCT_Type *  base,
sctimer_counter_t  whichCounter,
uint32_t  state 
)
inlinestatic

The function is to set the state variable bit field of STATE register. Writing to the STATE_L, STATE_H, or unified register is only allowed when the corresponding counter is halted (HALT bits are set to 1 in the CTRL register).

Parameters
baseSCTimer peripheral base address
whichCounterSCTimer counter to use. In 16-bit mode, we can select Counter_L and Counter_H, In 32-bit mode, we can select Counter_U.
stateThe counter current state number (only support range from 0~31).
static uint16_t SCTIMER_GetCounterState ( SCT_Type *  base,
sctimer_counter_t  whichCounter 
)
inlinestatic

The function is to get the state variable bit field of STATE register.

Parameters
baseSCTimer peripheral base address
whichCounterSCTimer counter to use. In 16-bit mode, we can select Counter_L and Counter_H, In 32-bit mode, we can select Counter_U.
Returns
The the counter current state value.
status_t SCTIMER_SetupCaptureAction ( SCT_Type *  base,
sctimer_counter_t  whichCounter,
uint32_t *  captureRegister,
uint32_t  event 
)
Parameters
baseSCTimer peripheral base address
whichCounterSCTimer counter to use. In 16-bit mode, we can select Counter_L and Counter_H, In 32-bit mode, we can select Counter_U.
captureRegisterPointer to a variable where the capture register number will be returned. User can read the captured value from this register when the specified event is triggered.
eventEvent number that will trigger the capture
Returns
kStatus_Success on success kStatus_Error if we have hit the limit in terms of number of match/capture registers available
void SCTIMER_SetCallback ( SCT_Type *  base,
sctimer_event_callback_t  callback,
uint32_t  event 
)

If the interrupt for the event is enabled by the user, then a callback can be registered which will be invoked when the event is triggered

Parameters
baseSCTimer peripheral base address
eventEvent number that will trigger the interrupt
callbackFunction to invoke when the event is triggered
static void SCTIMER_SetupStateLdMethodAction ( SCT_Type *  base,
uint32_t  event,
bool  fgLoad 
)
inlinestatic

Change the load method of transition, it will be triggered by the event number that is passed in by the user.

Parameters
baseSCTimer peripheral base address
eventEvent number that will change the method to trigger the state transition
fgLoadThe method to load highest-numbered event occurring for that state to the STATE register.
  • true: Load the STATEV value to STATE when the event occurs to be the next state.
  • false: Add the STATEV value to STATE when the event occurs to be the next state.
static void SCTIMER_SetupNextStateActionwithLdMethod ( SCT_Type *  base,
uint32_t  nextState,
uint32_t  event,
bool  fgLoad 
)
inlinestatic

This transition will be triggered by the event number that is passed in by the user, the method decide how to load the highest-numbered event occurring for that state to the STATE register.

Parameters
baseSCTimer peripheral base address
nextStateThe next state SCTimer will transition to
eventEvent number that will trigger the state transition
fgLoadThe method to load the highest-numbered event occurring for that state to the STATE register.
  • true: Load the STATEV value to STATE when the event occurs to be the next state.
  • false: Add the STATEV value to STATE when the event occurs to be the next state.
static void SCTIMER_SetupNextStateAction ( SCT_Type *  base,
uint32_t  nextState,
uint32_t  event 
)
inlinestatic
Deprecated:
Do not use this function. It has been superceded by SCTIMER_SetupNextStateActionwithLdMethod

This transition will be triggered by the event number that is passed in by the user.

Parameters
baseSCTimer peripheral base address
nextStateThe next state SCTimer will transition to
eventEvent number that will trigger the state transition
static void SCTIMER_SetupEventActiveDirection ( SCT_Type *  base,
sctimer_event_active_direction_t  activeDirection,
uint32_t  event 
)
inlinestatic
Parameters
baseSCTimer peripheral base address
activeDirectionEvent generation active direction, see sctimer_event_active_direction_t.
eventEvent number that need setup the active direction.
static void SCTIMER_SetupOutputSetAction ( SCT_Type *  base,
uint32_t  whichIO,
uint32_t  event 
)
inlinestatic

This output will be set when the event number that is passed in by the user is triggered.

Parameters
baseSCTimer peripheral base address
whichIOThe output to set
eventEvent number that will trigger the output change
static void SCTIMER_SetupOutputClearAction ( SCT_Type *  base,
uint32_t  whichIO,
uint32_t  event 
)
inlinestatic

This output will be cleared when the event number that is passed in by the user is triggered.

Parameters
baseSCTimer peripheral base address
whichIOThe output to clear
eventEvent number that will trigger the output change
void SCTIMER_SetupOutputToggleAction ( SCT_Type *  base,
uint32_t  whichIO,
uint32_t  event 
)

This change in the output level is triggered by the event number that is passed in by the user.

Parameters
baseSCTimer peripheral base address
whichIOThe output to toggle
eventEvent number that will trigger the output change
static void SCTIMER_SetupCounterLimitAction ( SCT_Type *  base,
sctimer_counter_t  whichCounter,
uint32_t  event 
)
inlinestatic

The counter is limited when the event number that is passed in by the user is triggered.

Parameters
baseSCTimer peripheral base address
whichCounterSCTimer counter to use. In 16-bit mode, we can select Counter_L and Counter_H, In 32-bit mode, we can select Counter_U.
eventEvent number that will trigger the counter to be limited
static void SCTIMER_SetupCounterStopAction ( SCT_Type *  base,
sctimer_counter_t  whichCounter,
uint32_t  event 
)
inlinestatic

The counter is stopped when the event number that is passed in by the user is triggered.

Parameters
baseSCTimer peripheral base address
whichCounterSCTimer counter to use. In 16-bit mode, we can select Counter_L and Counter_H, In 32-bit mode, we can select Counter_U.
eventEvent number that will trigger the counter to be stopped
static void SCTIMER_SetupCounterStartAction ( SCT_Type *  base,
sctimer_counter_t  whichCounter,
uint32_t  event 
)
inlinestatic

The counter will re-start when the event number that is passed in by the user is triggered.

Parameters
baseSCTimer peripheral base address
whichCounterSCTimer counter to use. In 16-bit mode, we can select Counter_L and Counter_H, In 32-bit mode, we can select Counter_U.
eventEvent number that will trigger the counter to re-start
static void SCTIMER_SetupCounterHaltAction ( SCT_Type *  base,
sctimer_counter_t  whichCounter,
uint32_t  event 
)
inlinestatic

The counter is disabled (halted) when the event number that is passed in by the user is triggered. When the counter is halted, all further events are disabled. The HALT condition can only be removed by calling the SCTIMER_StartTimer() function.

Parameters
baseSCTimer peripheral base address
whichCounterSCTimer counter to use. In 16-bit mode, we can select Counter_L and Counter_H, In 32-bit mode, we can select Counter_U.
eventEvent number that will trigger the counter to be halted
static void SCTIMER_SetupDmaTriggerAction ( SCT_Type *  base,
uint32_t  dmaNumber,
uint32_t  event 
)
inlinestatic

DMA request will be triggered by the event number that is passed in by the user.

Parameters
baseSCTimer peripheral base address
dmaNumberThe DMA request to generate
eventEvent number that will trigger the DMA request
static void SCTIMER_SetCOUNTValue ( SCT_Type *  base,
sctimer_counter_t  whichCounter,
uint32_t  value 
)
inlinestatic

The function is to set the value of Count register, Writing to the COUNT_L, COUNT_H, or unified register is only allowed when the corresponding counter is halted (HALT bits are set to 1 in the CTRL register).

Parameters
baseSCTimer peripheral base address
whichCounterSCTimer counter to use. In 16-bit mode, we can select Counter_L and Counter_H, In 32-bit mode, we can select Counter_U.
valuethe counter value update to the COUNT register.
static uint32_t SCTIMER_GetCOUNTValue ( SCT_Type *  base,
sctimer_counter_t  whichCounter 
)
inlinestatic

The function is to read the value of Count register, software can read the counter registers at any time..

Parameters
baseSCTimer peripheral base address
whichCounterSCTimer counter to use. In 16-bit mode, we can select Counter_L and Counter_H, In 32-bit mode, we can select Counter_U.
Returns
The value of counter selected.
static void SCTIMER_SetEventInState ( SCT_Type *  base,
uint32_t  event,
uint32_t  state 
)
inlinestatic
Parameters
baseSCTimer peripheral base address
eventThe EV_STATE register be set.
stateThe state value in which the event is enabled to occur.
static void SCTIMER_ClearEventInState ( SCT_Type *  base,
uint32_t  event,
uint32_t  state 
)
inlinestatic
Parameters
baseSCTimer peripheral base address
eventThe EV_STATE register be clear.
stateThe state value in which the event is disabled to occur.
static bool SCTIMER_GetEventInState ( SCT_Type *  base,
uint32_t  event,
uint32_t  state 
)
inlinestatic
Note
This function is to check whether the event is enabled in a specific state.
Parameters
baseSCTimer peripheral base address
eventThe EV_STATE register be read.
stateThe state value.
Returns
The the state mask bit field of EV_STATE register.
  • true: The event is enable in state.
  • false: The event is disable in state.
void SCTIMER_EventHandleIRQ ( SCT_Type *  base)
Parameters
baseSCTimer peripheral base address.