MCUXpresso SDK API Reference Manual  Rev 2.11.4
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
GenericList

Overview

Data Structures

struct  list_handle_t
 The list structure. More...
 
struct  list_element_handle_t
 The list element. More...
 

Macros

#define GENERIC_LIST_LIGHT   (1)
 Definition to determine whether use list light. More...
 
#define GENERIC_LIST_DUPLICATED_CHECKING   (0)
 Definition to determine whether enable list duplicated checking. More...
 

Enumerations

enum  list_status_t {
  kLIST_Ok = kStatus_Success,
  kLIST_DuplicateError = MAKE_STATUS(kStatusGroup_LIST, 1),
  kLIST_Full = MAKE_STATUS(kStatusGroup_LIST, 2),
  kLIST_Empty = MAKE_STATUS(kStatusGroup_LIST, 3),
  kLIST_OrphanElement = MAKE_STATUS(kStatusGroup_LIST, 4),
  kLIST_NotSupport = MAKE_STATUS(kStatusGroup_LIST, 5)
}
 The list status. More...
 

Functions

void LIST_Init (list_handle_t list, uint32_t max)
 Initialize the list. More...
 
list_handle_t LIST_GetList (list_element_handle_t element)
 Gets the list that contains the given element. More...
 
list_status_t LIST_AddHead (list_handle_t list, list_element_handle_t element)
 Links element to the head of the list. More...
 
list_status_t LIST_AddTail (list_handle_t list, list_element_handle_t element)
 Links element to the tail of the list. More...
 
list_element_handle_t LIST_RemoveHead (list_handle_t list)
 Unlinks element from the head of the list. More...
 
list_element_handle_t LIST_GetHead (list_handle_t list)
 Gets head element handle. More...
 
list_element_handle_t LIST_GetNext (list_element_handle_t element)
 Gets next element handle for given element handle. More...
 
list_element_handle_t LIST_GetPrev (list_element_handle_t element)
 Gets previous element handle for given element handle. More...
 
list_status_t LIST_RemoveElement (list_element_handle_t element)
 Unlinks an element from its list. More...
 
list_status_t LIST_AddPrevElement (list_element_handle_t element, list_element_handle_t newElement)
 Links an element in the previous position relative to a given member of a list. More...
 
uint32_t LIST_GetSize (list_handle_t list)
 Gets the current size of a list. More...
 
uint32_t LIST_GetAvailableSize (list_handle_t list)
 Gets the number of free places in the list. More...
 

Data Structure Documentation

struct list_label_t

Data Fields

struct list_element_tag * head
 list head
 
struct list_element_tag * tail
 list tail
 
uint16_t size
 list size
 
uint16_t max
 list max number of elements
 
struct list_element_t

Data Fields

struct list_element_tag * next
 next list element
 
struct list_label * list
 pointer to the list
 

Macro Definition Documentation

#define GENERIC_LIST_LIGHT   (1)
#define GENERIC_LIST_DUPLICATED_CHECKING   (0)

Enumeration Type Documentation

Enumerator
kLIST_Ok 

Success.

kLIST_DuplicateError 

Duplicate Error.

kLIST_Full 

FULL.

kLIST_Empty 

Empty.

kLIST_OrphanElement 

Orphan Element.

kLIST_NotSupport 

Not Support.

Function Documentation

void LIST_Init ( list_handle_t  list,
uint32_t  max 
)

This function initialize the list.

Parameters
list- List handle to initialize.
max- Maximum number of elements in list. 0 for unlimited.
list_handle_t LIST_GetList ( list_element_handle_t  element)
Parameters
element- Handle of the element.
Return values
NULLif element is orphan, Handle of the list the element is inserted into.
list_status_t LIST_AddHead ( list_handle_t  list,
list_element_handle_t  element 
)
Parameters
list- Handle of the list.
element- Handle of the element.
Return values
kLIST_Fullif list is full, kLIST_Ok if insertion was successful.
list_status_t LIST_AddTail ( list_handle_t  list,
list_element_handle_t  element 
)
Parameters
list- Handle of the list.
element- Handle of the element.
Return values
kLIST_Fullif list is full, kLIST_Ok if insertion was successful.
list_element_handle_t LIST_RemoveHead ( list_handle_t  list)
Parameters
list- Handle of the list.
Return values
NULLif list is empty, handle of removed element(pointer) if removal was successful.
list_element_handle_t LIST_GetHead ( list_handle_t  list)
Parameters
list- Handle of the list.
Return values
NULLif list is empty, handle of removed element(pointer) if removal was successful.
list_element_handle_t LIST_GetNext ( list_element_handle_t  element)
Parameters
element- Handle of the element.
Return values
NULLif list is empty, handle of removed element(pointer) if removal was successful.
list_element_handle_t LIST_GetPrev ( list_element_handle_t  element)
Parameters
element- Handle of the element.
Return values
NULLif list is empty, handle of removed element(pointer) if removal was successful.
list_status_t LIST_RemoveElement ( list_element_handle_t  element)
Parameters
element- Handle of the element.
Return values
kLIST_OrphanElementif element is not part of any list.
kLIST_Okif removal was successful.
list_status_t LIST_AddPrevElement ( list_element_handle_t  element,
list_element_handle_t  newElement 
)
Parameters
element- Handle of the element.
newElement- New element to insert before the given member.
Return values
kLIST_OrphanElementif element is not part of any list.
kLIST_Okif removal was successful.
uint32_t LIST_GetSize ( list_handle_t  list)
Parameters
list- Handle of the list.
Return values
Currentsize of the list.
uint32_t LIST_GetAvailableSize ( list_handle_t  list)
Parameters
list- Handle of the list.
Return values
Availablesize of the list.