![]() |
MCUXpresso SDK API Reference Manual
Rev 2.12.0
NXP Semiconductors
|
Data Structures | |
| struct | flexspi_dma_handle_t |
| FLEXSPI DMA transfer handle, users should not touch the content of the handle. More... | |
Typedefs | |
| typedef void(* | flexspi_dma_callback_t )(FLEXSPI_Type *base, flexspi_dma_handle_t *handle, status_t status, void *userData) |
| FLEXSPI dma transfer callback function for finish and error. | |
Enumerations | |
| enum | flexspi_dma_transfer_nsize_t { kFLEXPSI_DMAnSize1Bytes = 0x1U, kFLEXPSI_DMAnSize2Bytes = 0x2U, kFLEXPSI_DMAnSize4Bytes = 0x4U } |
| dma transfer configuration More... | |
Driver version | |
| #define | FSL_FLEXSPI_DMA_DRIVER_VERSION (MAKE_VERSION(2, 2, 1)) |
| FLEXSPI DMA driver version 2.2.1. More... | |
FLEXSPI dma Transactional | |
| void | FLEXSPI_TransferCreateHandleDMA (FLEXSPI_Type *base, flexspi_dma_handle_t *handle, flexspi_dma_callback_t callback, void *userData, dma_handle_t *txDmaHandle, dma_handle_t *rxDmaHandle) |
| Initializes the FLEXSPI handle for transfer which is used in transactional functions and set the callback. More... | |
| void | FLEXSPI_TransferUpdateSizeDMA (FLEXSPI_Type *base, flexspi_dma_handle_t *handle, flexspi_dma_transfer_nsize_t nsize) |
| Update FLEXSPI DMA transfer source data transfer size(SSIZE) and destination data transfer size(DSIZE). More... | |
| status_t | FLEXSPI_TransferDMA (FLEXSPI_Type *base, flexspi_dma_handle_t *handle, flexspi_transfer_t *xfer) |
| Transfers FLEXSPI data using an dma non-blocking method. More... | |
| void | FLEXSPI_TransferAbortDMA (FLEXSPI_Type *base, flexspi_dma_handle_t *handle) |
| Aborts the transfer data using dma. More... | |
| status_t | FLEXSPI_TransferGetTransferCountDMA (FLEXSPI_Type *base, flexspi_dma_handle_t *handle, size_t *count) |
| Gets the transferred counts of transfer. More... | |
| struct _flexspi_dma_handle |
Data Fields | |
| dma_handle_t * | txDmaHandle |
| dma handler for FLEXSPI Tx. More... | |
| dma_handle_t * | rxDmaHandle |
| dma handler for FLEXSPI Rx. More... | |
| size_t | transferSize |
| Bytes need to transfer. More... | |
| flexspi_dma_transfer_nsize_t | nsize |
| dma SSIZE/DSIZE in each transfer. More... | |
| uint8_t | nbytes |
| dma minor byte transfer count initially configured. More... | |
| uint8_t | count |
| The transfer data count in a DMA request. More... | |
| uint32_t | state |
| Internal state for FLEXSPI dma transfer. More... | |
| flexspi_dma_callback_t | completionCallback |
| A callback function called after the dma transfer is finished. More... | |
| void * | userData |
| User callback parameter. | |
| dma_handle_t* flexspi_dma_handle_t::txDmaHandle |
| dma_handle_t* flexspi_dma_handle_t::rxDmaHandle |
| size_t flexspi_dma_handle_t::transferSize |
| flexspi_dma_transfer_nsize_t flexspi_dma_handle_t::nsize |
| uint8_t flexspi_dma_handle_t::nbytes |
| uint8_t flexspi_dma_handle_t::count |
| uint32_t flexspi_dma_handle_t::state |
| flexspi_dma_callback_t flexspi_dma_handle_t::completionCallback |
| #define FSL_FLEXSPI_DMA_DRIVER_VERSION (MAKE_VERSION(2, 2, 1)) |
| void FLEXSPI_TransferCreateHandleDMA | ( | FLEXSPI_Type * | base, |
| flexspi_dma_handle_t * | handle, | ||
| flexspi_dma_callback_t | callback, | ||
| void * | userData, | ||
| dma_handle_t * | txDmaHandle, | ||
| dma_handle_t * | rxDmaHandle | ||
| ) |
| base | FLEXSPI peripheral base address |
| handle | Pointer to flexspi_dma_handle_t structure |
| callback | FLEXSPI callback, NULL means no callback. |
| userData | User callback function data. |
| txDmaHandle | User requested DMA handle for TX DMA transfer. |
| rxDmaHandle | User requested DMA handle for RX DMA transfer. |
| void FLEXSPI_TransferUpdateSizeDMA | ( | FLEXSPI_Type * | base, |
| flexspi_dma_handle_t * | handle, | ||
| flexspi_dma_transfer_nsize_t | nsize | ||
| ) |
| base | FLEXSPI peripheral base address |
| handle | Pointer to flexspi_dma_handle_t structure |
| nsize | FLEXSPI DMA transfer data transfer size(SSIZE/DSIZE), by default the size is kFLEXPSI_DMAnSize1Bytes(one byte). |
| status_t FLEXSPI_TransferDMA | ( | FLEXSPI_Type * | base, |
| flexspi_dma_handle_t * | handle, | ||
| flexspi_transfer_t * | xfer | ||
| ) |
This function writes/receives data to/from the FLEXSPI transmit/receive FIFO. This function is non-blocking.
| base | FLEXSPI peripheral base address. |
| handle | Pointer to flexspi_dma_handle_t structure |
| xfer | FLEXSPI transfer structure. |
| kStatus_FLEXSPI_Busy | FLEXSPI is busy transfer. |
| kStatus_InvalidArgument | The watermark configuration is invalid, the watermark should be power of 2 to do successfully DMA transfer. |
| kStatus_Success | FLEXSPI successfully start dma transfer. |
| void FLEXSPI_TransferAbortDMA | ( | FLEXSPI_Type * | base, |
| flexspi_dma_handle_t * | handle | ||
| ) |
This function aborts the transfer data using dma.
| base | FLEXSPI peripheral base address. |
| handle | Pointer to flexspi_dma_handle_t structure |
| status_t FLEXSPI_TransferGetTransferCountDMA | ( | FLEXSPI_Type * | base, |
| flexspi_dma_handle_t * | handle, | ||
| size_t * | count | ||
| ) |
| base | FLEXSPI peripheral base address. |
| handle | Pointer to flexspi_dma_handle_t structure. |
| count | Bytes transfer. |
| kStatus_Success | Succeed get the transfer count. |
| kStatus_NoTransferInProgress | There is not a non-blocking transaction currently in progress. |