![]() |
MCUXpresso SDK API Reference Manual
Rev 2.12.0
NXP Semiconductors
|
The MCUXpresso SDK provides a peripheral driver for the SMART DMA module of MCUXpresso SDK devices.
Data Structures | |
| struct | smartdma_flexio_mculcd_param_t |
| Parameter for FlexIO MCULCD except kSMARTDMA_FlexIO_DMA_ONELANE. More... | |
| struct | smartdma_flexio_onelane_mculcd_param_t |
| Parameter for kSMARTDMA_FlexIO_DMA_ONELANE. More... | |
| struct | smartdma_dsi_param_t |
| Parameter for MIPI DSI. More... | |
| struct | smartdma_rgb565_rgb888_param_t |
| Parameter for RGB565To888. More... | |
Macros | |
| #define | SMARTDMA_DISPLAY_MEM_ADDR 0x24100000 |
| The s_smartdmaDisplayFirmware firmware memory address. More... | |
| #define | SMARTDMA_DISPLAY_FIRMWARE_SIZE (s_smartdmaDisplayFirmwareSize) |
| Size of s_smartdmaDisplayFirmware. | |
| #define | s_smartdmaFlexioMcuLcdFirmware s_smartdmaDisplayFirmware |
| Compatibility redefinition. More... | |
Typedefs | |
| typedef void(* | smartdma_callback_t )(void *param) |
| Callback function prototype for the smartdma driver. More... | |
Enumerations | |
| enum | _smartdma_flexio_mculcd_api { , kSMARTDMA_FlexIO_DMA_Reverse, kSMARTDMA_RGB565To888, kSMARTDMA_FlexIO_DMA_RGB565To888, kSMARTDMA_FlexIO_DMA_ARGB2RGB, kSMARTDMA_FlexIO_DMA_ARGB2RGB_Endian_Swap, kSMARTDMA_FlexIO_DMA_ARGB2RGB_Endian_Swap_Reverse, kSMARTDMA_MIPI_RGB565_DMA, kSMARTDMA_MIPI_RGB888_DMA, kSMARTDMA_MIPI_XRGB2RGB_DMA, kSMARTDMA_MIPI_RGB565_R180_DMA, kSMARTDMA_MIPI_RGB888_R180_DMA, kSMARTDMA_FlexIO_DMA_ONELANE } |
| The API index when using s_smartdmaFlexioMcuLcdFirmware. More... | |
Functions | |
| void | SMARTDMA_Init (uint32_t apiMemAddr, const void *firmware, uint32_t firmwareSizeByte) |
| Initialize the SMARTDMA. More... | |
| void | SMARTDMA_InitWithoutFirmware (void) |
| Initialize the SMARTDMA. More... | |
| void | SMARTDMA_InstallFirmware (uint32_t apiMemAddr, const void *firmware, uint32_t firmwareSizeByte) |
| Install the firmware. More... | |
| void | SMARTDMA_InstallCallback (smartdma_callback_t callback, void *param) |
| Install the complete callback function. More... | |
| void | SMARTDMA_Boot (uint32_t apiIndex, void *pParam, uint8_t mask) |
| Boot the SMARTDMA to run program. More... | |
| void | SMARTDMA_Deinit (void) |
| Deinitialize the SMARTDMA. | |
| void | SMARTDMA_Reset (void) |
| Reset the SMARTDMA. | |
| void | SMARTDMA_HandleIRQ (void) |
| SMARTDMA IRQ. | |
Variables | |
| const uint8_t | s_smartdmaDisplayFirmware [] |
| The firmware used for display. More... | |
| const uint32_t | s_smartdmaDisplayFirmwareSize |
| Size of s_smartdmaDisplayFirmware. | |
Driver version | |
| #define | FSL_SMARTDMA_DRIVER_VERSION (MAKE_VERSION(2, 6, 3)) |
| SMARTDMA driver version. | |
| struct smartdma_flexio_mculcd_param_t |
| struct smartdma_flexio_onelane_mculcd_param_t |
| struct smartdma_dsi_param_t |
Data Fields | |
| const uint8_t * | p_buffer |
| Pointer to the buffer to send. More... | |
| uint32_t | buffersize |
| Buffer size in byte. More... | |
| uint32_t * | smartdma_stack |
| Stack used by SMARTDMA. More... | |
| uint32_t | disablePixelByteSwap |
| If set to 1, the pixels are filled to MIPI DSI FIFO directly. More... | |
| const uint8_t* smartdma_dsi_param_t::p_buffer |
| uint32_t smartdma_dsi_param_t::buffersize |
| uint32_t* smartdma_dsi_param_t::smartdma_stack |
| uint32_t smartdma_dsi_param_t::disablePixelByteSwap |
If set to 0, the pixel bytes are swapped then filled to MIPI DSI FIFO. For example, when set to 0 and frame buffer pixel format is RGB565: LSB MSB B0 B1 B2 B3 B4 G0 G1 G2 | G3 G4 G5 R0 R1 R2 R3 R4 Then the pixel filled to DSI FIFO is: LSB MSB G3 G4 G5 R0 R1 R2 R3 R4 | B0 B1 B2 B3 B4 G0 G1 G2
| struct smartdma_rgb565_rgb888_param_t |
| #define SMARTDMA_DISPLAY_MEM_ADDR 0x24100000 |
| #define s_smartdmaFlexioMcuLcdFirmware s_smartdmaDisplayFirmware |
| typedef void(* smartdma_callback_t)(void *param) |
| Enumerator | |
|---|---|
| kSMARTDMA_FlexIO_DMA_Reverse |
Send data to FlexIO with reverse order. |
| kSMARTDMA_RGB565To888 |
Convert RGB565 to RGB888 and save to output memory, use parameter smartdma_rgb565_rgb888_param_t. |
| kSMARTDMA_FlexIO_DMA_RGB565To888 |
Convert RGB565 to RGB888 and send to FlexIO, use parameter smartdma_flexio_mculcd_param_t. |
| kSMARTDMA_FlexIO_DMA_ARGB2RGB |
Convert ARGB to RGB and send to FlexIO, use parameter smartdma_flexio_mculcd_param_t. |
| kSMARTDMA_FlexIO_DMA_ARGB2RGB_Endian_Swap |
Convert ARGB to RGB, then swap endian, and send to FlexIO, use parameter smartdma_flexio_mculcd_param_t. |
| kSMARTDMA_FlexIO_DMA_ARGB2RGB_Endian_Swap_Reverse |
Convert ARGB to RGB, then swap endian and reverse, and send to FlexIO, use parameter smartdma_flexio_mculcd_param_t. |
| kSMARTDMA_MIPI_RGB565_DMA |
Send RGB565 data to MIPI DSI, use parameter smartdma_dsi_param_t. |
| kSMARTDMA_MIPI_RGB888_DMA |
Send RGB888 data to MIPI DSI, use parameter smartdma_dsi_param_t. |
| kSMARTDMA_MIPI_XRGB2RGB_DMA |
Send XRGB8888 data to MIPI DSI, use parameter smartdma_param_t. |
| kSMARTDMA_MIPI_RGB565_R180_DMA |
Send RGB565 data to MIPI DSI, Rotate 180, use parameter smartdma_dsi_param_t. |
| kSMARTDMA_MIPI_RGB888_R180_DMA |
Send RGB888 data to MIPI DSI, Rotate 180, use parameter smartdma_dsi_param_t. |
| kSMARTDMA_FlexIO_DMA_ONELANE |
FlexIO DMA for one SHIFTBUF, Write Data to SHIFTBUF[OFFSET]. |
| void SMARTDMA_Init | ( | uint32_t | apiMemAddr, |
| const void * | firmware, | ||
| uint32_t | firmwareSizeByte | ||
| ) |
| apiMemAddr | The address firmware will be copied to. |
| firmware | The firmware to use. |
| firmwareSizeByte | Size of firmware. |
| void SMARTDMA_InitWithoutFirmware | ( | void | ) |
This function is similar with SMARTDMA_Init, the difference is this function does not install the firmware, the firmware could be installed using SMARTDMA_InstallFirmware.
| void SMARTDMA_InstallFirmware | ( | uint32_t | apiMemAddr, |
| const void * | firmware, | ||
| uint32_t | firmwareSizeByte | ||
| ) |
| apiMemAddr | The address firmware will be copied to. |
| firmware | The firmware to use. |
| firmwareSizeByte | Size of firmware. |
| void SMARTDMA_InstallCallback | ( | smartdma_callback_t | callback, |
| void * | param | ||
| ) |
| callback | The callback called when smartdma program finished. |
| param | Parameter for the callback. |
| void SMARTDMA_Boot | ( | uint32_t | apiIndex, |
| void * | pParam, | ||
| uint8_t | mask | ||
| ) |
| apiIndex | Index of the API to call. |
| pParam | Pointer to the parameter. |
| mask | Value set to SMARTDMA_ARM2SMARTDMA[0:1]. |
| const uint8_t s_smartdmaDisplayFirmware[] |