ANACTRL function groups
More...
Function groups
The ANACTRL driver supports initialization/configuration/operation for optimization/customization purpose.
Initialization and deinitialization
This function group is to enable/disable the clock for the ANACTRL module.
Set oscillators
The function ANACTRL_SetFro192M sets the on-chip high-speed Free Running Oscillator. The function ANACTRL_GetDefaultFro192MConfig() gets the default configuration.
The function ANACTRL_SetXo32M sets the 32 MHz Crystal oscillator. The function ANACTRL_GetDefaultXo32MConfig() gets the default configuration.
Measure Frequency
This function measures the target frequency according to the reference frequency.
Interrupt
Provides functions to enable/disable/clear ANACTRL interrupts.
Status
Provides functions to get the ANACTRL status.
|
| enum | _anactrl_interrupt_flags {
kANACTRL_BodVbatFlag = ANACTRL_BOD_DCDC_INT_STATUS_BODVBAT_STATUS_MASK,
kANACTRL_BodVbatInterruptFlag = ANACTRL_BOD_DCDC_INT_STATUS_BODVBAT_INT_STATUS_MASK,
kANACTRL_BodVbatPowerFlag = ANACTRL_BOD_DCDC_INT_STATUS_BODVBAT_VAL_MASK,
kANACTRL_BodCoreFlag = ANACTRL_BOD_DCDC_INT_STATUS_BODCORE_STATUS_MASK,
kANACTRL_BodCoreInterruptFlag = ANACTRL_BOD_DCDC_INT_STATUS_BODCORE_INT_STATUS_MASK,
kANACTRL_BodCorePowerFlag = ANACTRL_BOD_DCDC_INT_STATUS_BODCORE_VAL_MASK,
kANACTRL_DcdcFlag = ANACTRL_BOD_DCDC_INT_STATUS_DCDC_STATUS_MASK,
kANACTRL_DcdcInterruptFlag = ANACTRL_BOD_DCDC_INT_STATUS_DCDC_INT_STATUS_MASK,
kANACTRL_DcdcPowerFlag = ANACTRL_BOD_DCDC_INT_STATUS_DCDC_VAL_MASK
} |
| | ANACTRL interrupt flags. More...
|
| |
| enum | _anactrl_interrupt {
kANACTRL_BodVbatInterruptEnable = ANACTRL_BOD_DCDC_INT_CTRL_BODVBAT_INT_ENABLE_MASK,
kANACTRL_BodCoreInterruptEnable = ANACTRL_BOD_DCDC_INT_CTRL_BODCORE_INT_ENABLE_MASK,
kANACTRL_DcdcInterruptEnable = ANACTRL_BOD_DCDC_INT_CTRL_DCDC_INT_ENABLE_MASK
} |
| | ANACTRL interrupt control. More...
|
| |
| enum | _anactrl_flags {
kANACTRL_FlashPowerDownFlag = ANACTRL_ANALOG_CTRL_STATUS_FLASH_PWRDWN_MASK,
kANACTRL_FlashInitErrorFlag = ANACTRL_ANALOG_CTRL_STATUS_FLASH_INIT_ERROR_MASK
} |
| | ANACTRL status flags. More...
|
| |
| enum | _anactrl_osc_flags {
kANACTRL_OutputClkValidFlag = ANACTRL_FRO192M_STATUS_CLK_VALID_MASK,
kANACTRL_CCOThresholdVoltageFlag = ANACTRL_FRO192M_STATUS_ATB_VCTRL_MASK,
kANACTRL_XO32MOutputReadyFlag = ANACTRL_XO32M_STATUS_XO_READY_MASK << 16U
} |
| | ANACTRL FRO192M and XO32M status flags. More...
|
| |
|
| void | ANACTRL_Init (ANACTRL_Type *base) |
| | Initializes the ANACTRL mode, the module's clock will be enabled by invoking this function. More...
|
| |
| void | ANACTRL_Deinit (ANACTRL_Type *base) |
| | De-initializes ANACTRL module, the module's clock will be disabled by invoking this function. More...
|
| |
| struct anactrl_fro192M_config_t |
This structure holds the configuration settings for the on-chip high-speed Free Running Oscillator. To initialize this structure to reasonable defaults, call the ANACTRL_GetDefaultFro192MConfig() function and pass a pointer to your config structure instance.
| bool anactrl_fro192M_config_t::enable12MHzClk |
| bool anactrl_fro192M_config_t::enable96MHzClk |
| struct anactrl_xo32M_config_t |
This structure holds the configuration settings for the 32 MHz crystal oscillator. To initialize this structure to reasonable defaults, call the ANACTRL_GetDefaultXo32MConfig() function and pass a pointer to your config structure instance.
| bool anactrl_xo32M_config_t::enableACBufferBypass |
| #define FSL_ANACTRL_DRIVER_VERSION (MAKE_VERSION(2, 3, 0)) /*!< Version 2.3.0. */` |
| Enumerator |
|---|
| kANACTRL_BodVbatFlag |
BOD VBAT Interrupt status before Interrupt Enable.
|
| kANACTRL_BodVbatInterruptFlag |
BOD VBAT Interrupt status after Interrupt Enable.
|
| kANACTRL_BodVbatPowerFlag |
Current value of BOD VBAT power status output.
|
| kANACTRL_BodCoreFlag |
BOD CORE Interrupt status before Interrupt Enable.
|
| kANACTRL_BodCoreInterruptFlag |
BOD CORE Interrupt status after Interrupt Enable.
|
| kANACTRL_BodCorePowerFlag |
Current value of BOD CORE power status output.
|
| kANACTRL_DcdcFlag |
DCDC Interrupt status before Interrupt Enable.
|
| kANACTRL_DcdcInterruptFlag |
DCDC Interrupt status after Interrupt Enable.
|
| kANACTRL_DcdcPowerFlag |
Current value of DCDC power status output.
|
| Enumerator |
|---|
| kANACTRL_BodVbatInterruptEnable |
BOD VBAT interrupt control.
|
| kANACTRL_BodCoreInterruptEnable |
BOD CORE interrupt control.
|
| kANACTRL_DcdcInterruptEnable |
DCDC interrupt control.
|
| Enumerator |
|---|
| kANACTRL_FlashPowerDownFlag |
Flash power-down status.
|
| kANACTRL_FlashInitErrorFlag |
Flash initialization error status.
|
| Enumerator |
|---|
| kANACTRL_OutputClkValidFlag |
Output clock valid signal.
|
| kANACTRL_CCOThresholdVoltageFlag |
CCO threshold voltage detector output (signal vcco_ok).
|
| kANACTRL_XO32MOutputReadyFlag |
Indicates XO out frequency statibilty.
|
| void ANACTRL_Init |
( |
ANACTRL_Type * |
base | ) |
|
- Parameters
-
| base | ANACTRL peripheral base address. |
| void ANACTRL_Deinit |
( |
ANACTRL_Type * |
base | ) |
|
- Parameters
-
| base | ANACTRL peripheral base address. |
- Parameters
-
| base | ANACTRL peripheral base address. |
| config | Pointer to FRO192M configuration structure. Refer to anactrl_fro192M_config_t structure. |
The default values are:
config->enable12MHzClk = true;
config->enable96MHzClk = false;
- Parameters
-
- Parameters
-
| base | ANACTRL peripheral base address. |
| config | Pointer to XO32M configuration structure. Refer to anactrl_xo32M_config_t structure. |
The default values are:
config->enableSysCLkOutput = false;
config->enableACBufferBypass = false;
- Parameters
-
| uint32_t ANACTRL_MeasureFrequency |
( |
ANACTRL_Type * |
base, |
|
|
uint8_t |
scale, |
|
|
uint32_t |
refClkFreq |
|
) |
| |
This function measures target frequency according to a accurate reference frequency.The formula is: Ftarget = (CAPVAL * Freference) / ((1<<SCALE)-1)
- Note
- Both tartget and reference clocks are selectable by programming the target clock select FREQMEAS_TARGET register in INPUTMUX and reference clock select FREQMEAS_REF register in INPUTMUX.
- Parameters
-
| base | ANACTRL peripheral base address. |
| scale | Define the power of 2 count that ref counter counts to during measurement, ranges from 2 to 31. |
| refClkFreq | frequency of the reference clock. |
- Returns
- frequency of the target clock.
| static void ANACTRL_EnableInterrupts |
( |
ANACTRL_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | ANACTRL peripheral base address. |
| mask | The interrupt mask. Refer to "_anactrl_interrupt" enumeration. |
| static void ANACTRL_DisableInterrupts |
( |
ANACTRL_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | ANACTRL peripheral base address. |
| mask | The interrupt mask. Refer to "_anactrl_interrupt" enumeration. |
| static void ANACTRL_ClearInterrupts |
( |
ANACTRL_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | ANACTRL peripheral base address. |
| mask | The interrupt mask. Refer to "_anactrl_interrupt" enumeration. |
| static uint32_t ANACTRL_GetStatusFlags |
( |
ANACTRL_Type * |
base | ) |
|
|
inlinestatic |
This function gets Analog control status flags. The flags are returned as the logical OR value of the enumerators _anactrl_flags. To check for a specific status, compare the return value with enumerators in the _anactrl_flags. For example, to check whether the flash is in power down mode:
- Parameters
-
| base | ANACTRL peripheral base address. |
- Returns
- ANACTRL status flags which are given in the enumerators in the _anactrl_flags.
| static uint32_t ANACTRL_GetOscStatusFlags |
( |
ANACTRL_Type * |
base | ) |
|
|
inlinestatic |
This function gets Anactrl oscillators status flags. The flags are returned as the logical OR value of the enumerators _anactrl_osc_flags. To check for a specific status, compare the return value with enumerators in the _anactrl_osc_flags. For example, to check whether the FRO192M clock output is valid:
- Parameters
-
| base | ANACTRL peripheral base address. |
- Returns
- ANACTRL oscillators status flags which are given in the enumerators in the _anactrl_osc_flags.
| static uint32_t ANACTRL_GetInterruptStatusFlags |
( |
ANACTRL_Type * |
base | ) |
|
|
inlinestatic |
This function gets Anactrl interrupt status flags. The flags are returned as the logical OR value of the enumerators _anactrl_interrupt_flags. To check for a specific status, compare the return value with enumerators in the _anactrl_interrupt_flags. For example, to check whether the VBAT voltage level is above the threshold:
- Parameters
-
| base | ANACTRL peripheral base address. |
- Returns
- ANACTRL oscillators status flags which are given in the enumerators in the _anactrl_osc_flags.
| static void ANACTRL_EnableVref1V |
( |
ANACTRL_Type * |
base, |
|
|
bool |
enable |
|
) |
| |
|
inlinestatic |
Enables/disabless 1V reference voltage buffer.
- Parameters
-
| base | ANACTRL peripheral base address. |
| enable | Used to enable or disable 1V reference voltage buffer. |