The MCUXpresso SDK provides a peripheral driver for the Direct Memory Access Multiplexer (DMAMUX) of MCUXpresso SDK devices.
Typical use case
DMAMUX Operation
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/dmamux 
      
        
          | #define FSL_DMAMUX_DRIVER_VERSION   (MAKE_VERSION(2, 0, 2)) | 
      
 
 
      
        
          | void DMAMUX_Init | ( | DMAMUX_Type * | base | ) |  | 
      
 
This function ungates the DMAMUX clock.
- Parameters
- 
  
    | base | DMAMUX peripheral base address. |  
 
 
 
      
        
          | void DMAMUX_Deinit | ( | DMAMUX_Type * | base | ) |  | 
      
 
This function gates the DMAMUX clock.
- Parameters
- 
  
    | base | DMAMUX peripheral base address. |  
 
 
 
  
  | 
        
          | static void DMAMUX_EnableChannel | ( | DMAMUX_Type * | base, |  
          |  |  | uint32_t | channel |  
          |  | ) |  |  |  | inlinestatic | 
 
This function enables the DMAMUX channel.
- Parameters
- 
  
    | base | DMAMUX peripheral base address. |  | channel | DMAMUX channel number. |  
 
 
 
  
  | 
        
          | static void DMAMUX_DisableChannel | ( | DMAMUX_Type * | base, |  
          |  |  | uint32_t | channel |  
          |  | ) |  |  |  | inlinestatic | 
 
This function disables the DMAMUX channel.
- Note
- The user must disable the DMAMUX channel before configuring it. 
- Parameters
- 
  
    | base | DMAMUX peripheral base address. |  | channel | DMAMUX channel number. |  
 
 
 
  
  | 
        
          | static void DMAMUX_SetSource | ( | DMAMUX_Type * | base, |  
          |  |  | uint32_t | channel, |  
          |  |  | uint32_t | source |  
          |  | ) |  |  |  | inlinestatic | 
 
- Parameters
- 
  
    | base | DMAMUX peripheral base address. |  | channel | DMAMUX channel number. |  | source | Channel source, which is used to trigger the DMA transfer. |  
 
 
 
  
  | 
        
          | static void DMAMUX_EnablePeriodTrigger | ( | DMAMUX_Type * | base, |  
          |  |  | uint32_t | channel |  
          |  | ) |  |  |  | inlinestatic | 
 
This function enables the DMAMUX period trigger feature.
- Parameters
- 
  
    | base | DMAMUX peripheral base address. |  | channel | DMAMUX channel number. |  
 
 
 
  
  | 
        
          | static void DMAMUX_DisablePeriodTrigger | ( | DMAMUX_Type * | base, |  
          |  |  | uint32_t | channel |  
          |  | ) |  |  |  | inlinestatic | 
 
This function disables the DMAMUX period trigger.
- Parameters
- 
  
    | base | DMAMUX peripheral base address. |  | channel | DMAMUX channel number. |  
 
 
 
  
  | 
        
          | static void DMAMUX_EnableAlwaysOn | ( | DMAMUX_Type * | base, |  
          |  |  | uint32_t | channel, |  
          |  |  | bool | enable |  
          |  | ) |  |  |  | inlinestatic | 
 
This function enables the DMAMUX channel always ON feature.
- Parameters
- 
  
    | base | DMAMUX peripheral base address. |  | channel | DMAMUX channel number. |  | enable | Switcher of the always ON feature. "true" means enabled, "false" means disabled. |