MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages

Overview

The MCUXpresso SDK provides a peripheral clock driver for the SYSCON module of MCUXpresso SDK devices.

Function description

Clock driver provides these functions:

SYSCON Clock frequency functions

SYSCON clock module provides clocks, such as MCLKCLK, ADCCLK, DMICCLK, MCGFLLCLK, FXCOMCLK,WDTOSC, RTCOSC, USBCLK and SYSPLL. The functions CLOCK_EnableClock() and CLOCK_DisableClock() enables and disables the various clocks. CLOCK_SetupFROClocking() initializes the FRO to 12MHz, 48 MHz or 96 MHz frequency. CLOCK_SetupPLLData(), CLOCK_SetupSystemPLLPrec(), and CLOCK_SetPLLFreq() functions are used to setup the PLL. The SYSCON clock driver provides functions to get the frequency of these clocks, such as CLOCK_GetFreq(), CLOCK_GetFro12MFreq(), CLOCK_GetExtClkFreq(), CLOCK_GetWdtOscFreq(), CLOCK_GetFroHfFreq(), CLOCK_GetPllOutFreq(), CLOCK_GetOsc32KFreq() , CLOCK_GetCoreSysClkFreq(), CLOCK_GetI2SMClkFreq(),CLOCK_GetFlexCommClkFreq and CLOCK_GetAsyncApbClkFreq.

SYSCON clock Selection Muxes

The SYSCON clock driver provides the function to configure the clock selected. The function CLOCK_AttachClk() is implemented for this. The function selects the clock source for a particular peripheral like MAINCLK, DMIC, FLEXCOMM, USB, ADC and PLL.

SYSCON clock dividers

The SYSCON clock module provides the function to setup the peripheral clock dividers. The function CLOCK_SetClkDiv() configures the CLKDIV registers for various periperals like USB, DMIC, I2S, SYSTICK, AHB, ADC and also for CLKOUT and TRACE functions.

SYSCON flash wait states

The SYSCON clock driver provides the function CLOCK_SetFLASHAccessCyclesForFreq() that configures FLASHCFG register with a selected FLASHTIM value.

Typical use case

POWER_DisablePD(kPDRUNCFG_PD_FRO_EN);
kFRO12M_to_MAIN_CLK);
CLOCK_SetFLASHAccessCyclesForFreq(48000000);
CLOCK_AttachClk(kFRO_HF_to_MAIN_CLK);

Files

file  fsl_clock.h
 

Data Structures

struct  pll_config_t
 PLL configuration structure. More...
 
struct  pll_setup_t
 PLL setup structure This structure can be used to pre-build a PLL setup configuration at run-time and quickly set the PLL to the configuration. More...
 
struct  usb_pll_setup_t
 PLL setup structure This structure can be used to pre-build a USB PLL setup configuration at run-time and quickly set the usb PLL to the configuration. More...
 

Macros

#define FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROL   0
 Configure whether driver controls clock. More...
 
#define CLOCK_USR_CFG_PLL_CONFIG_CACHE_COUNT   2U
 User-defined the size of cache for CLOCK_PllGetConfig() function. More...
 
#define CLOCK_FROHF_SETTING_API_ROM_ADDRESS   (0x03007933U)
 FROHF clock setting API address in ROM. More...
 
#define CLOCK_SetupFROClocking   (*((void (*)(uint32_t))(CLOCK_FROHF_SETTING_API_ROM_ADDRESS)))
 
#define ADC_CLOCKS
 Clock ip name array for ADC. More...
 
#define ROM_CLOCKS
 Clock ip name array for ROM. More...
 
#define SRAM_CLOCKS
 Clock ip name array for SRAM. More...
 
#define FLASH_CLOCKS
 Clock ip name array for FLASH. More...
 
#define FMC_CLOCKS
 Clock ip name array for FMC. More...
 
#define EEPROM_CLOCKS
 Clock ip name array for EEPROM. More...
 
#define SPIFI_CLOCKS
 Clock ip name array for SPIFI. More...
 
#define INPUTMUX_CLOCKS
 Clock ip name array for INPUTMUX. More...
 
#define IOCON_CLOCKS
 Clock ip name array for IOCON. More...
 
#define GPIO_CLOCKS
 Clock ip name array for GPIO. More...
 
#define PINT_CLOCKS
 Clock ip name array for PINT. More...
 
#define GINT_CLOCKS
 Clock ip name array for GINT. More...
 
#define DMA_CLOCKS
 Clock ip name array for DMA. More...
 
#define CRC_CLOCKS
 Clock ip name array for CRC. More...
 
#define WWDT_CLOCKS
 Clock ip name array for WWDT. More...
 
#define RTC_CLOCKS
 Clock ip name array for RTC. More...
 
#define ADC0_CLOCKS
 Clock ip name array for ADC0. More...
 
#define MRT_CLOCKS
 Clock ip name array for MRT. More...
 
#define RIT_CLOCKS
 Clock ip name array for RIT. More...
 
#define SCT_CLOCKS
 Clock ip name array for SCT0. More...
 
#define MCAN_CLOCKS
 Clock ip name array for MCAN. More...
 
#define UTICK_CLOCKS
 Clock ip name array for UTICK. More...
 
#define FLEXCOMM_CLOCKS
 Clock ip name array for FLEXCOMM. More...
 
#define LPUART_CLOCKS
 Clock ip name array for LPUART. More...
 
#define BI2C_CLOCKS
 Clock ip name array for BI2C. More...
 
#define LPSI_CLOCKS
 Clock ip name array for LSPI. More...
 
#define FLEXI2S_CLOCKS
 Clock ip name array for FLEXI2S. More...
 
#define DMIC_CLOCKS
 Clock ip name array for DMIC. More...
 
#define CTIMER_CLOCKS
 Clock ip name array for CT32B. More...
 
#define LCD_CLOCKS
 Clock ip name array for LCD. More...
 
#define SDIO_CLOCKS
 Clock ip name array for SDIO. More...
 
#define USBRAM_CLOCKS
 Clock ip name array for USBRAM. More...
 
#define EMC_CLOCKS
 Clock ip name array for EMC. More...
 
#define ETH_CLOCKS
 Clock ip name array for ETH. More...
 
#define AES_CLOCKS
 Clock ip name array for AES. More...
 
#define OTP_CLOCKS
 Clock ip name array for OTP. More...
 
#define RNG_CLOCKS
 Clock ip name array for RNG. More...
 
#define USBHMR0_CLOCKS
 Clock ip name array for USBHMR0. More...
 
#define USBHSL0_CLOCKS
 Clock ip name array for USBHSL0. More...
 
#define SHA0_CLOCKS
 Clock ip name array for SHA0. More...
 
#define SMARTCARD_CLOCKS
 Clock ip name array for SMARTCARD. More...
 
#define USBD_CLOCKS
 Clock ip name array for USBD. More...
 
#define USBH_CLOCKS
 Clock ip name array for USBH. More...
 
#define CLK_GATE_REG_OFFSET_SHIFT   8U
 Clock gate name used for CLOCK_EnableClock/CLOCK_DisableClock. More...
 
#define MUX_A(m, choice)   (((m) << 0) | ((choice + 1) << 8))
 Clock Mux Switches The encoding is as follows each connection identified is 64bits wide starting from LSB upwards. More...
 
#define PLL_CONFIGFLAG_USEINRATE   (1 << 0)
 PLL configuration structure flags for 'flags' field These flags control how the PLL configuration function sets up the PLL setup structure. More...
 
#define PLL_CONFIGFLAG_FORCENOFRACT
 Force non-fractional output mode, PLL output will not use the fractional, automatic bandwidth, or SS \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ hardware.
 
#define PLL_SETUPFLAG_POWERUP   (1 << 0)
 PLL setup structure flags for 'flags' field These flags control how the PLL setup function sets up the PLL. More...
 
#define PLL_SETUPFLAG_WAITLOCK   (1 << 1)
 Setup will wait for PLL lock, implies the PLL will be pwoered on.
 
#define PLL_SETUPFLAG_ADGVOLT   (1 << 2)
 Optimize system voltage for the new PLL rate.
 

Enumerations

enum  clock_ip_name_t
 Clock gate name used for CLOCK_EnableClock/CLOCK_DisableClock. More...
 
enum  clock_name_t {
  kCLOCK_CoreSysClk,
  kCLOCK_BusClk,
  kCLOCK_ClockOut,
  kCLOCK_FroHf,
  kCLOCK_SpiFi,
  kCLOCK_Adc,
  kCLOCK_Usb0,
  kCLOCK_Usb1,
  kCLOCK_UsbPll,
  kCLOCK_Mclk,
  kCLOCK_Sct,
  kCLOCK_SDio,
  kCLOCK_EMC,
  kCLOCK_LCD,
  kCLOCK_MCAN0,
  kCLOCK_MCAN1,
  kCLOCK_Fro12M,
  kCLOCK_ExtClk,
  kCLOCK_PllOut,
  kCLOCK_UsbClk,
  kClock_WdtOsc,
  kCLOCK_Frg,
  kCLOCK_Dmic,
  kCLOCK_AsyncApbClk,
  kCLOCK_FlexI2S,
  kCLOCK_Flexcomm0,
  kCLOCK_Flexcomm1,
  kCLOCK_Flexcomm2,
  kCLOCK_Flexcomm3,
  kCLOCK_Flexcomm4,
  kCLOCK_Flexcomm5,
  kCLOCK_Flexcomm6,
  kCLOCK_Flexcomm7,
  kCLOCK_Flexcomm8,
  kCLOCK_Flexcomm9,
  kCLOCK_Flexcomm10
}
 Clock name used to get clock frequency. More...
 
enum  async_clock_src_t {
  kCLOCK_AsyncMainClk = 0,
  kCLOCK_AsyncFro12Mhz
}
 
enum  pll_error_t {
  kStatus_PLL_Success = MAKE_STATUS(kStatusGroup_Generic, 0),
  kStatus_PLL_OutputTooLow = MAKE_STATUS(kStatusGroup_Generic, 1),
  kStatus_PLL_OutputTooHigh = MAKE_STATUS(kStatusGroup_Generic, 2),
  kStatus_PLL_InputTooLow = MAKE_STATUS(kStatusGroup_Generic, 3),
  kStatus_PLL_InputTooHigh = MAKE_STATUS(kStatusGroup_Generic, 4),
  kStatus_PLL_OutsideIntLimit = MAKE_STATUS(kStatusGroup_Generic, 5),
  kStatus_PLL_CCOTooLow = MAKE_STATUS(kStatusGroup_Generic, 6),
  kStatus_PLL_CCOTooHigh = MAKE_STATUS(kStatusGroup_Generic, 7)
}
 PLL status definitions. More...
 
enum  clock_usb_src_t {
  kCLOCK_UsbSrcFro = (uint32_t)kCLOCK_FroHf,
  kCLOCK_UsbSrcSystemPll = (uint32_t)kCLOCK_PllOut,
  kCLOCK_UsbSrcMainClock = (uint32_t)kCLOCK_CoreSysClk,
  kCLOCK_UsbSrcUsbPll = (uint32_t)kCLOCK_UsbPll,
  kCLOCK_UsbSrcNone = SYSCON_USB0CLKSEL_SEL(7)
}
 USB clock source definition. More...
 
enum  usb_pll_psel
 USB PDEL Divider. More...
 

Functions

void CLOCK_AttachClk (clock_attach_id_t connection)
 Configure the clock selection muxes. More...
 
void CLOCK_SetClkDiv (clock_div_name_t div_name, uint32_t divided_by_value, bool reset)
 Setup peripheral clock dividers. More...
 
uint32_t CLOCK_GetFreq (clock_name_t clockName)
 Return Frequency of selected clock. More...
 
uint32_t CLOCK_GetFro12MFreq (void)
 Return Frequency of FRO 12MHz. More...
 
uint32_t CLOCK_GetClockOutClkFreq (void)
 Return Frequency of ClockOut. More...
 
uint32_t CLOCK_GetSpifiClkFreq (void)
 Return Frequency of Spifi Clock. More...
 
uint32_t CLOCK_GetAdcClkFreq (void)
 Return Frequency of Adc Clock. More...
 
uint32_t CLOCK_GetUsb0ClkFreq (void)
 Return Frequency of Usb0 Clock. More...
 
uint32_t CLOCK_GetUsb1ClkFreq (void)
 Return Frequency of Usb1 Clock. More...
 
uint32_t CLOCK_GetMclkClkFreq (void)
 Return Frequency of MClk Clock. More...
 
uint32_t CLOCK_GetSctClkFreq (void)
 Return Frequency of SCTimer Clock. More...
 
uint32_t CLOCK_GetSdioClkFreq (void)
 Return Frequency of SDIO Clock. More...
 
uint32_t CLOCK_GetLcdClkFreq (void)
 Return Frequency of LCD Clock. More...
 
uint32_t CLOCK_GetLcdClkIn (void)
 Return Frequency of LCD CLKIN Clock. More...
 
uint32_t CLOCK_GetExtClkFreq (void)
 Return Frequency of External Clock. More...
 
uint32_t CLOCK_GetWdtOscFreq (void)
 Return Frequency of Watchdog Oscillator. More...
 
uint32_t CLOCK_GetFroHfFreq (void)
 Return Frequency of High-Freq output of FRO. More...
 
uint32_t CLOCK_GetFrgClkFreq (void)
 Return Frequency of frg. More...
 
uint32_t CLOCK_GetDmicClkFreq (void)
 Return Frequency of dmic. More...
 
uint32_t CLOCK_GetPllOutFreq (void)
 Return Frequency of PLL. More...
 
uint32_t CLOCK_GetUsbPllOutFreq (void)
 Return Frequency of USB PLL. More...
 
uint32_t CLOCK_GetAudioPllOutFreq (void)
 Return Frequency of AUDIO PLL. More...
 
uint32_t CLOCK_GetOsc32KFreq (void)
 Return Frequency of 32kHz osc. More...
 
uint32_t CLOCK_GetCoreSysClkFreq (void)
 Return Frequency of Core System. More...
 
uint32_t CLOCK_GetI2SMClkFreq (void)
 Return Frequency of I2S MCLK Clock. More...
 
uint32_t CLOCK_GetFlexCommClkFreq (uint32_t id)
 Return Frequency of Flexcomm functional Clock. More...
 
__STATIC_INLINE async_clock_src_t CLOCK_GetAsyncApbClkSrc (void)
 Return Asynchronous APB Clock source. More...
 
uint32_t CLOCK_GetAsyncApbClkFreq (void)
 Return Frequency of Asynchronous APB Clock. More...
 
uint32_t CLOCK_GetAudioPLLInClockRate (void)
 Return Audio PLL input clock rate. More...
 
uint32_t CLOCK_GetSystemPLLInClockRate (void)
 Return System PLL input clock rate. More...
 
uint32_t CLOCK_GetSystemPLLOutClockRate (bool recompute)
 Return System PLL output clock rate. More...
 
uint32_t CLOCK_GetAudioPLLOutClockRate (bool recompute)
 Return System AUDIO PLL output clock rate. More...
 
uint32_t CLOCK_GetUSbPLLOutClockRate (bool recompute)
 Return System USB PLL output clock rate. More...
 
__STATIC_INLINE void CLOCK_SetBypassPLL (bool bypass)
 Enables and disables PLL bypass mode. More...
 
__STATIC_INLINE bool CLOCK_IsSystemPLLLocked (void)
 Check if PLL is locked or not. More...
 
__STATIC_INLINE bool CLOCK_IsUsbPLLLocked (void)
 Check if USB PLL is locked or not. More...
 
__STATIC_INLINE bool CLOCK_IsAudioPLLLocked (void)
 Check if AUDIO PLL is locked or not. More...
 
__STATIC_INLINE void CLOCK_Enable_SysOsc (bool enable)
 Enables and disables SYS OSC. More...
 
void CLOCK_SetStoredPLLClockRate (uint32_t rate)
 Store the current PLL rate. More...
 
void CLOCK_SetStoredAudioPLLClockRate (uint32_t rate)
 Store the current AUDIO PLL rate. More...
 
uint32_t CLOCK_GetSystemPLLOutFromSetup (pll_setup_t *pSetup)
 Return System PLL output clock rate from setup structure. More...
 
uint32_t CLOCK_GetAudioPLLOutFromSetup (pll_setup_t *pSetup)
 Return System AUDIO PLL output clock rate from setup structure. More...
 
uint32_t CLOCK_GetAudioPLLOutFromFractSetup (pll_setup_t *pSetup)
 Return System AUDIO PLL output clock rate from audio fractioanl setup structure. More...
 
uint32_t CLOCK_GetUsbPLLOutFromSetup (const usb_pll_setup_t *pSetup)
 Return System USB PLL output clock rate from setup structure. More...
 
pll_error_t CLOCK_SetupPLLData (pll_config_t *pControl, pll_setup_t *pSetup)
 Set PLL output based on the passed PLL setup data. More...
 
pll_error_t CLOCK_SetupAudioPLLData (pll_config_t *pControl, pll_setup_t *pSetup)
 Set AUDIO PLL output based on the passed AUDIO PLL setup data. More...
 
pll_error_t CLOCK_SetupSystemPLLPrec (pll_setup_t *pSetup, uint32_t flagcfg)
 Set PLL output from PLL setup structure (precise frequency) More...
 
pll_error_t CLOCK_SetupAudioPLLPrec (pll_setup_t *pSetup, uint32_t flagcfg)
 Set AUDIO PLL output from AUDIOPLL setup structure (precise frequency) More...
 
pll_error_t CLOCK_SetupAudioPLLPrecFract (pll_setup_t *pSetup, uint32_t flagcfg)
 Set AUDIO PLL output from AUDIOPLL setup structure using the Audio Fractional divider register(precise frequency) More...
 
pll_error_t CLOCK_SetPLLFreq (const pll_setup_t *pSetup)
 Set PLL output from PLL setup structure (precise frequency) More...
 
pll_error_t CLOCK_SetAudioPLLFreq (const pll_setup_t *pSetup)
 Set Audio PLL output from Audio PLL setup structure (precise frequency) More...
 
pll_error_t CLOCK_SetUsbPLLFreq (const usb_pll_setup_t *pSetup)
 Set USB PLL output from USB PLL setup structure (precise frequency) More...
 
void CLOCK_SetupSystemPLLMult (uint32_t multiply_by, uint32_t input_freq)
 Set PLL output based on the multiplier and input frequency. More...
 
static void CLOCK_DisableUsbDevicefs0Clock (clock_ip_name_t clk)
 Disable USB clock. More...
 
bool CLOCK_EnableUsbfs0DeviceClock (clock_usb_src_t src, uint32_t freq)
 Enable USB Device FS clock. More...
 
bool CLOCK_EnableUsbfs0HostClock (clock_usb_src_t src, uint32_t freq)
 Enable USB HOST FS clock. More...
 
bool CLOCK_EnableUsbhs0DeviceClock (clock_usb_src_t src, uint32_t freq)
 Enable USB Device HS clock. More...
 
bool CLOCK_EnableUsbhs0HostClock (clock_usb_src_t src, uint32_t freq)
 Enable USB HOST HS clock. More...
 

Driver version

#define FSL_CLOCK_DRIVER_VERSION   (MAKE_VERSION(2, 0, 0))
 CLOCK driver version 2.0.0. More...
 

Data Structure Documentation

struct pll_config_t

This structure can be used to configure the settings for a PLL setup structure. Fill in the desired configuration for the PLL and call the PLL setup function to fill in a PLL setup structure.

Data Fields

uint32_t desiredRate
 Desired PLL rate in Hz.
 
uint32_t inputRate
 PLL input clock in Hz, only used if PLL_CONFIGFLAG_USEINRATE flag is set.
 
uint32_t flags
 PLL configuration flags, Or'ed value of PLL_CONFIGFLAG_* definitions.
 
struct pll_setup_t

It can be populated with the PLL setup function. If powering up or waiting for PLL lock, the PLL input clock source should be configured prior to PLL setup.

Data Fields

uint32_t pllctrl
 PLL control register SYSPLLCTRL.
 
uint32_t pllndec
 PLL NDEC register SYSPLLNDEC.
 
uint32_t pllpdec
 PLL PDEC register SYSPLLPDEC.
 
uint32_t pllmdec
 PLL MDEC registers SYSPLLPDEC.
 
uint32_t pllRate
 Acutal PLL rate.
 
uint32_t audpllfrac
 only aduio PLL has this function
 
uint32_t flags
 PLL setup flags, Or'ed value of PLL_SETUPFLAG_* definitions.
 
struct usb_pll_setup_t

It can be populated with the USB PLL setup function. If powering up or waiting for USB PLL lock, the PLL input clock source should be configured prior to USB PLL setup.

Data Fields

uint8_t msel
 USB PLL control register msel:1U-256U.
 
uint8_t psel
 USB PLL control register psel:only support inter 1U 2U 4U 8U.
 
uint8_t nsel
 USB PLL control register nsel:only suppoet inter 1U 2U 3U 4U.
 
bool direct
 USB PLL CCO output control.
 
bool bypass
 USB PLL inout clock bypass control.
 
bool fbsel
 USB PLL ineter mode and non-integer mode control.
 
uint32_t inputRate
 USB PLL input rate.
 

Macro Definition Documentation

#define FSL_CLOCK_DRIVER_VERSION   (MAKE_VERSION(2, 0, 0))
#define FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROL   0

When set to 0, peripheral drivers will enable clock in initialize function and disable clock in de-initialize function. When set to 1, peripheral driver will not control the clock, application could contol the clock out of the driver.

Note
All drivers share this feature switcher. If it is set to 1, application should handle clock enable and disable for all drivers.
#define CLOCK_USR_CFG_PLL_CONFIG_CACHE_COUNT   2U

Once define this MACRO to be non-zero value, CLOCK_PllGetConfig() function would cache the recent calulation and accelerate the execution to get the right settings.

#define CLOCK_FROHF_SETTING_API_ROM_ADDRESS   (0x03007933U)
#define CLOCK_SetupFROClocking   (*((void (*)(uint32_t))(CLOCK_FROHF_SETTING_API_ROM_ADDRESS)))

Initialize the Core clock to given frequency (12, 48 or 96 MHz), this API is implememnt in ROM code. Turns on FRO and uses default CCO, if freq is 12000000, then high speed output is off, else high speed output is enabled. Usage: CLOCK_SetupFROClocking(frequency), (frequency must be one of 12, 48 or 96 MHz) Note: Need to make sure ROM and OTP has power(PDRUNCFG0[17,29]= 0U) before calling this API since this API is implemented in ROM code and the FROHF TRIM value is stored in OTP

#define ADC_CLOCKS
Value:
{ \
kCLOCK_Adc0 \
}
#define ROM_CLOCKS
Value:
{ \
kCLOCK_Rom \
}
#define SRAM_CLOCKS
Value:
{ \
kCLOCK_Sram1, kCLOCK_Sram2, kCLOCK_Sram3 \
}
#define FLASH_CLOCKS
Value:
{ \
kCLOCK_Flash \
}
#define FMC_CLOCKS
Value:
{ \
kCLOCK_Fmc \
}
#define EEPROM_CLOCKS
Value:
{ \
kCLOCK_Eeprom \
}
#define SPIFI_CLOCKS
Value:
{ \
kCLOCK_Spifi \
}
#define INPUTMUX_CLOCKS
Value:
{ \
kCLOCK_InputMux \
}
#define IOCON_CLOCKS
Value:
{ \
kCLOCK_Iocon \
}
#define GPIO_CLOCKS
Value:
{ \
kCLOCK_Gpio0,kCLOCK_Gpio1, kCLOCK_Gpio2, kCLOCK_Gpio3, kCLOCK_Gpio4, kCLOCK_Gpio5 \
}
#define PINT_CLOCKS
Value:
{ \
kCLOCK_Pint \
}
#define GINT_CLOCKS
Value:
{ \
kCLOCK_Gint, kCLOCK_Gint \
}
#define DMA_CLOCKS
Value:
{ \
kCLOCK_Dma \
}
#define CRC_CLOCKS
Value:
{ \
kCLOCK_Crc \
}
#define WWDT_CLOCKS
Value:
{ \
kCLOCK_Wwdt \
}
#define RTC_CLOCKS
Value:
{ \
kCLOCK_Rtc \
}
#define ADC0_CLOCKS
Value:
{ \
kCLOCK_Adc0 \
}
#define MRT_CLOCKS
Value:
{ \
kCLOCK_Mrt \
}
#define RIT_CLOCKS
Value:
{ \
kCLOCK_Rit \
}
#define SCT_CLOCKS
Value:
{ \
kCLOCK_Sct0 \
}
#define MCAN_CLOCKS
Value:
{ \
kCLOCK_Mcan0, kCLOCK_Mcan1 \
}
#define UTICK_CLOCKS
Value:
{ \
kCLOCK_Utick \
}
#define FLEXCOMM_CLOCKS
Value:
{ \
kCLOCK_FlexComm0, kCLOCK_FlexComm1, kCLOCK_FlexComm2, kCLOCK_FlexComm3, \
kCLOCK_FlexComm4, kCLOCK_FlexComm5, kCLOCK_FlexComm6, kCLOCK_FlexComm7, \
kCLOCK_FlexComm8, kCLOCK_FlexComm9, kCLOCK_FlexComm10 \
}
#define LPUART_CLOCKS
Value:
{ \
kCLOCK_MinUart0, kCLOCK_MinUart1, kCLOCK_MinUart2, kCLOCK_MinUart3, kCLOCK_MinUart4, kCLOCK_MinUart5, \
kCLOCK_MinUart6, kCLOCK_MinUart7, kCLOCK_MinUart8,kCLOCK_MinUart9 \
}
#define BI2C_CLOCKS
Value:
{ \
kCLOCK_BI2c0, kCLOCK_BI2c1, kCLOCK_BI2c2, kCLOCK_BI2c3, kCLOCK_BI2c4, kCLOCK_BI2c5, kCLOCK_BI2c6, kCLOCK_BI2c7, \
kCLOCK_BI2c8, kCLOCK_BI2c9 \
}
#define LPSI_CLOCKS
Value:
{ \
kCLOCK_LSpi0, kCLOCK_LSpi1, kCLOCK_LSpi2, kCLOCK_LSpi3, kCLOCK_LSpi4, kCLOCK_LSpi5, kCLOCK_LSpi6, kCLOCK_LSpi7, \
kCLOCK_LSpi8, kCLOCK_LSpi9 \
}
#define FLEXI2S_CLOCKS
Value:
{ \
kCLOCK_FlexI2s0, kCLOCK_FlexI2s1, kCLOCK_FlexI2s2, kCLOCK_FlexI2s3, kCLOCK_FlexI2s4, kCLOCK_FlexI2s5, \
kCLOCK_FlexI2s6, kCLOCK_FlexI2s7, kCLOCK_FlexI2s8, kCLOCK_FlexI2s9 \
}
#define DMIC_CLOCKS
Value:
{ \
kCLOCK_DMic \
}
#define CTIMER_CLOCKS
Value:
{ \
kCLOCK_Ct32b0, kCLOCK_Ct32b1, kCLOCK_Ct32b2, kCLOCK_Ct32b3, kCLOCK_Ct32b4 \
}
#define LCD_CLOCKS
Value:
{ \
kCLOCK_Lcd \
}
#define SDIO_CLOCKS
Value:
{ \
kCLOCK_Sdio \
}
#define USBRAM_CLOCKS
Value:
{ \
kCLOCK_UsbRam1 \
}
#define EMC_CLOCKS
Value:
{ \
kCLOCK_Emc \
}
#define ETH_CLOCKS
Value:
{ \
kCLOCK_Eth \
}
#define AES_CLOCKS
Value:
{ \
kCLOCK_Aes \
}
#define OTP_CLOCKS
Value:
{ \
kCLOCK_Otp \
}
#define RNG_CLOCKS
Value:
{ \
kCLOCK_Rng \
}
#define USBHMR0_CLOCKS
Value:
{ \
kCLOCK_Usbhmr0 \
}
#define USBHSL0_CLOCKS
Value:
{ \
kCLOCK_Usbhsl0 \
}
#define SHA0_CLOCKS
Value:
{ \
kCLOCK_Sha0 \
}
#define SMARTCARD_CLOCKS
Value:
{ \
kCLOCK_SmartCard0, kCLOCK_SmartCard1 \
}
#define USBD_CLOCKS
Value:
{ \
kCLOCK_Usbd0, kCLOCK_Usbh1, kCLOCK_Usbd1 \
}
#define USBH_CLOCKS
Value:
{ \
kCLOCK_Usbh1 \
}
#define CLK_GATE_REG_OFFSET_SHIFT   8U
#define MUX_A (   m,
  choice 
)    (((m) << 0) | ((choice + 1) << 8))

[4 bits for choice, where 1 is A, 2 is B, 3 is C and 4 is D, 0 means end of descriptor] [8 bits mux ID]*

#define PLL_CONFIGFLAG_USEINRATE   (1 << 0)


When the PLL_CONFIGFLAG_USEINRATE flag is selected, the 'InputRate' field in the configuration structure must be assigned with the expected PLL frequency. If the PLL_CONFIGFLAG_USEINRATE is not used, 'InputRate' is ignored in the configuration function and the driver will determine the PLL rate from the currently selected PLL source. This flag might be used to configure the PLL input clock more accurately when using the WDT oscillator or a more dyanmic CLKIN source.

When the PLL_CONFIGFLAG_FORCENOFRACT flag is selected, the PLL hardware for the automatic bandwidth selection, Spread Spectrum (SS) support, and fractional M-divider are not used.
Flag to use InputRate in PLL configuration structure for setup

#define PLL_SETUPFLAG_POWERUP   (1 << 0)

Setup will power on the PLL after setup

Enumeration Type Documentation

Enumerator
kCLOCK_CoreSysClk 

Core/system clock (aka MAIN_CLK)

kCLOCK_BusClk 

Bus clock (AHB clock)

kCLOCK_ClockOut 

CLOCKOUT.

kCLOCK_FroHf 

FRO48/96.

kCLOCK_SpiFi 

SPIFI.

kCLOCK_Adc 

ADC.

kCLOCK_Usb0 

USB0.

kCLOCK_Usb1 

USB1.

kCLOCK_UsbPll 

USB1 PLL.

kCLOCK_Mclk 

MCLK.

kCLOCK_Sct 

SCT.

kCLOCK_SDio 

SDIO.

kCLOCK_EMC 

EMC.

kCLOCK_LCD 

LCD.

kCLOCK_MCAN0 

MCAN0.

kCLOCK_MCAN1 

MCAN1.

kCLOCK_Fro12M 

FRO12M.

kCLOCK_ExtClk 

External Clock.

kCLOCK_PllOut 

PLL Output.

kCLOCK_UsbClk 

USB input.

kClock_WdtOsc 

Watchdog Oscillator.

kCLOCK_Frg 

Frg Clock.

kCLOCK_Dmic 

Digital Mic clock.

kCLOCK_AsyncApbClk 

Async APB clock.

kCLOCK_FlexI2S 

FlexI2S clock.

kCLOCK_Flexcomm0 

Flexcomm0Clock.

kCLOCK_Flexcomm1 

Flexcomm1Clock.

kCLOCK_Flexcomm2 

Flexcomm2Clock.

kCLOCK_Flexcomm3 

Flexcomm3Clock.

kCLOCK_Flexcomm4 

Flexcomm4Clock.

kCLOCK_Flexcomm5 

Flexcomm5Clock.

kCLOCK_Flexcomm6 

Flexcomm6Clock.

kCLOCK_Flexcomm7 

Flexcomm7Clock.

kCLOCK_Flexcomm8 

Flexcomm8Clock.

kCLOCK_Flexcomm9 

Flexcomm9Clock.

kCLOCK_Flexcomm10 

Flexcomm10Clock.

Clock source selections for the asynchronous APB clock

Enumerator
kCLOCK_AsyncMainClk 

Main System clock.

kCLOCK_AsyncFro12Mhz 

12MHz FRO

Enumerator
kStatus_PLL_Success 

PLL operation was successful.

kStatus_PLL_OutputTooLow 

PLL output rate request was too low.

kStatus_PLL_OutputTooHigh 

PLL output rate request was too high.

kStatus_PLL_InputTooLow 

PLL input rate is too low.

kStatus_PLL_InputTooHigh 

PLL input rate is too high.

kStatus_PLL_OutsideIntLimit 

Requested output rate isn't possible.

kStatus_PLL_CCOTooLow 

Requested CCO rate isn't possible.

kStatus_PLL_CCOTooHigh 

Requested CCO rate isn't possible.

Enumerator
kCLOCK_UsbSrcFro 

Use FRO 96 or 48 MHz.

kCLOCK_UsbSrcSystemPll 

Use System PLL output.

kCLOCK_UsbSrcMainClock 

Use Main clock.

kCLOCK_UsbSrcUsbPll 

Use USB PLL clock.

kCLOCK_UsbSrcNone 

Use None, this may be selected in order to reduce power when no output is needed.

Function Documentation

void CLOCK_AttachClk ( clock_attach_id_t  connection)
Parameters
connection: Clock to be configured.
Returns
Nothing
void CLOCK_SetClkDiv ( clock_div_name_t  div_name,
uint32_t  divided_by_value,
bool  reset 
)
Parameters
div_name: Clock divider name
divided_by_value,:Value to be divided
reset: Whether to reset the divider counter.
Returns
Nothing
uint32_t CLOCK_GetFreq ( clock_name_t  clockName)
Returns
Frequency of selected clock
uint32_t CLOCK_GetFro12MFreq ( void  )
Returns
Frequency of FRO 12MHz
uint32_t CLOCK_GetClockOutClkFreq ( void  )
Returns
Frequency of ClockOut
uint32_t CLOCK_GetSpifiClkFreq ( void  )
Returns
Frequency of Spifi.
uint32_t CLOCK_GetAdcClkFreq ( void  )
Returns
Frequency of Adc Clock.
uint32_t CLOCK_GetUsb0ClkFreq ( void  )
Returns
Frequency of Usb0 Clock.
uint32_t CLOCK_GetUsb1ClkFreq ( void  )
Returns
Frequency of Usb1 Clock.
uint32_t CLOCK_GetMclkClkFreq ( void  )
Returns
Frequency of MClk Clock.
uint32_t CLOCK_GetSctClkFreq ( void  )
Returns
Frequency of SCTimer Clock.
uint32_t CLOCK_GetSdioClkFreq ( void  )
Returns
Frequency of SDIO Clock.
uint32_t CLOCK_GetLcdClkFreq ( void  )
Returns
Frequency of LCD Clock.
uint32_t CLOCK_GetLcdClkIn ( void  )
Returns
Frequency of LCD CLKIN Clock.
uint32_t CLOCK_GetExtClkFreq ( void  )
Returns
Frequency of External Clock. If no external clock is used returns 0.
uint32_t CLOCK_GetWdtOscFreq ( void  )
Returns
Frequency of Watchdog Oscillator
uint32_t CLOCK_GetFroHfFreq ( void  )
Returns
Frequency of High-Freq output of FRO
uint32_t CLOCK_GetFrgClkFreq ( void  )
Returns
Frequency of FRG
uint32_t CLOCK_GetDmicClkFreq ( void  )
Returns
Frequency of DMIC
uint32_t CLOCK_GetPllOutFreq ( void  )
Returns
Frequency of PLL
uint32_t CLOCK_GetUsbPllOutFreq ( void  )
Returns
Frequency of PLL
uint32_t CLOCK_GetAudioPllOutFreq ( void  )
Returns
Frequency of PLL
uint32_t CLOCK_GetOsc32KFreq ( void  )
Returns
Frequency of 32kHz osc
uint32_t CLOCK_GetCoreSysClkFreq ( void  )
Returns
Frequency of Core System
uint32_t CLOCK_GetI2SMClkFreq ( void  )
Returns
Frequency of I2S MCLK Clock
uint32_t CLOCK_GetFlexCommClkFreq ( uint32_t  id)
Returns
Frequency of Flexcomm functional Clock
__STATIC_INLINE async_clock_src_t CLOCK_GetAsyncApbClkSrc ( void  )
Returns
Asynchronous APB CLock source
uint32_t CLOCK_GetAsyncApbClkFreq ( void  )
Returns
Frequency of Asynchronous APB Clock Clock
uint32_t CLOCK_GetAudioPLLInClockRate ( void  )
Returns
Audio PLL input clock rate
uint32_t CLOCK_GetSystemPLLInClockRate ( void  )
Returns
System PLL input clock rate
uint32_t CLOCK_GetSystemPLLOutClockRate ( bool  recompute)
Parameters
recompute: Forces a PLL rate recomputation if true
Returns
System PLL output clock rate
Note
The PLL rate is cached in the driver in a variable as the rate computation function can take some time to perform. It is recommended to use 'false' with the 'recompute' parameter.
uint32_t CLOCK_GetAudioPLLOutClockRate ( bool  recompute)
Parameters
recompute: Forces a AUDIO PLL rate recomputation if true
Returns
System AUDIO PLL output clock rate
Note
The AUDIO PLL rate is cached in the driver in a variable as the rate computation function can take some time to perform. It is recommended to use 'false' with the 'recompute' parameter.
uint32_t CLOCK_GetUSbPLLOutClockRate ( bool  recompute)
Parameters
recompute: Forces a USB PLL rate recomputation if true
Returns
System USB PLL output clock rate
Note
The USB PLL rate is cached in the driver in a variable as the rate computation function can take some time to perform. It is recommended to use 'false' with the 'recompute' parameter.
__STATIC_INLINE void CLOCK_SetBypassPLL ( bool  bypass)

bypass : true to bypass PLL (PLL output = PLL input, false to disable bypass

Returns
System PLL output clock rate
__STATIC_INLINE bool CLOCK_IsSystemPLLLocked ( void  )
Returns
true if the PLL is locked, false if not locked
__STATIC_INLINE bool CLOCK_IsUsbPLLLocked ( void  )
Returns
true if the USB PLL is locked, false if not locked
__STATIC_INLINE bool CLOCK_IsAudioPLLLocked ( void  )
Returns
true if the AUDIO PLL is locked, false if not locked
__STATIC_INLINE void CLOCK_Enable_SysOsc ( bool  enable)

enable : true to enable SYS OSC, false to disable SYS OSC

void CLOCK_SetStoredPLLClockRate ( uint32_t  rate)
Parameters
rate,:Current rate of the PLL
Returns
Nothing
void CLOCK_SetStoredAudioPLLClockRate ( uint32_t  rate)
Parameters
rate,:Current rate of the PLL
Returns
Nothing
uint32_t CLOCK_GetSystemPLLOutFromSetup ( pll_setup_t *  pSetup)
Parameters
pSetup: Pointer to a PLL setup structure
Returns
System PLL output clock rate the setup structure will generate
uint32_t CLOCK_GetAudioPLLOutFromSetup ( pll_setup_t *  pSetup)
Parameters
pSetup: Pointer to a PLL setup structure
Returns
System PLL output clock rate the setup structure will generate
uint32_t CLOCK_GetAudioPLLOutFromFractSetup ( pll_setup_t *  pSetup)
Parameters
pSetup: Pointer to a PLL setup structure
Returns
System PLL output clock rate the setup structure will generate
uint32_t CLOCK_GetUsbPLLOutFromSetup ( const usb_pll_setup_t *  pSetup)
Parameters
pSetup: Pointer to a PLL setup structure
Returns
System PLL output clock rate the setup structure will generate
pll_error_t CLOCK_SetupPLLData ( pll_config_t *  pControl,
pll_setup_t *  pSetup 
)
Parameters
pControl: Pointer to populated PLL control structure to generate setup with
pSetup: Pointer to PLL setup structure to be filled
Returns
PLL_ERROR_SUCCESS on success, or PLL setup error code
Note
Actual frequency for setup may vary from the desired frequency based on the accuracy of input clocks, rounding, non-fractional PLL mode, etc.
pll_error_t CLOCK_SetupAudioPLLData ( pll_config_t *  pControl,
pll_setup_t *  pSetup 
)
Parameters
pControl: Pointer to populated PLL control structure to generate setup with
pSetup: Pointer to PLL setup structure to be filled
Returns
PLL_ERROR_SUCCESS on success, or PLL setup error code
Note
Actual frequency for setup may vary from the desired frequency based on the accuracy of input clocks, rounding, non-fractional PLL mode, etc.
pll_error_t CLOCK_SetupSystemPLLPrec ( pll_setup_t *  pSetup,
uint32_t  flagcfg 
)
Parameters
pSetup: Pointer to populated PLL setup structure
flagcfg: Flag configuration for PLL config structure
Returns
PLL_ERROR_SUCCESS on success, or PLL setup error code
Note
This function will power off the PLL, setup the PLL with the new setup data, and then optionally powerup the PLL, wait for PLL lock, and adjust system voltages to the new PLL rate. The function will not alter any source clocks (ie, main systen clock) that may use the PLL, so these should be setup prior to and after exiting the function.
pll_error_t CLOCK_SetupAudioPLLPrec ( pll_setup_t *  pSetup,
uint32_t  flagcfg 
)
Parameters
pSetup: Pointer to populated PLL setup structure
flagcfg: Flag configuration for PLL config structure
Returns
PLL_ERROR_SUCCESS on success, or PLL setup error code
Note
This function will power off the PLL, setup the PLL with the new setup data, and then optionally powerup the AUDIO PLL, wait for PLL lock, and adjust system voltages to the new AUDIOPLL rate. The function will not alter any source clocks (ie, main systen clock) that may use the AUDIO PLL, so these should be setup prior to and after exiting the function.
pll_error_t CLOCK_SetupAudioPLLPrecFract ( pll_setup_t *  pSetup,
uint32_t  flagcfg 
)
Parameters
pSetup: Pointer to populated PLL setup structure
flagcfg: Flag configuration for PLL config structure
Returns
PLL_ERROR_SUCCESS on success, or PLL setup error code
Note
This function will power off the PLL, setup the PLL with the new setup data, and then optionally powerup the AUDIO PLL, wait for PLL lock, and adjust system voltages to the new AUDIOPLL rate. The function will not alter any source clocks (ie, main systen clock) that may use the AUDIO PLL, so these should be setup prior to and after exiting the function.
pll_error_t CLOCK_SetPLLFreq ( const pll_setup_t *  pSetup)
Parameters
pSetup: Pointer to populated PLL setup structure
Returns
kStatus_PLL_Success on success, or PLL setup error code
Note
This function will power off the PLL, setup the PLL with the new setup data, and then optionally powerup the PLL, wait for PLL lock, and adjust system voltages to the new PLL rate. The function will not alter any source clocks (ie, main systen clock) that may use the PLL, so these should be setup prior to and after exiting the function.
pll_error_t CLOCK_SetAudioPLLFreq ( const pll_setup_t *  pSetup)
Parameters
pSetup: Pointer to populated PLL setup structure
Returns
kStatus_PLL_Success on success, or Audio PLL setup error code
Note
This function will power off the PLL, setup the Audio PLL with the new setup data, and then optionally powerup the PLL, wait for Audio PLL lock, and adjust system voltages to the new PLL rate. The function will not alter any source clocks (ie, main systen clock) that may use the Audio PLL, so these should be setup prior to and after exiting the function.
pll_error_t CLOCK_SetUsbPLLFreq ( const usb_pll_setup_t *  pSetup)
Parameters
pSetup: Pointer to populated USB PLL setup structure
Returns
kStatus_PLL_Success on success, or USB PLL setup error code
Note
This function will power off the USB PLL, setup the PLL with the new setup data, and then optionally powerup the USB PLL, wait for USB PLL lock, and adjust system voltages to the new USB PLL rate. The function will not alter any source clocks (ie, usb pll clock) that may use the USB PLL, so these should be setup prior to and after exiting the function.
void CLOCK_SetupSystemPLLMult ( uint32_t  multiply_by,
uint32_t  input_freq 
)
Parameters
multiply_by: multiplier
input_freq: Clock input frequency of the PLL
Returns
Nothing
Note
Unlike the Chip_Clock_SetupSystemPLLPrec() function, this function does not disable or enable PLL power, wait for PLL lock, or adjust system voltages. These must be done in the application. The function will not alter any source clocks (ie, main systen clock) that may use the PLL, so these should be setup prior to and after exiting the function.
static void CLOCK_DisableUsbDevicefs0Clock ( clock_ip_name_t  clk)
inlinestatic

Disable USB clock.

bool CLOCK_EnableUsbfs0DeviceClock ( clock_usb_src_t  src,
uint32_t  freq 
)
Parameters
src: clock source
freq,:clock frequency Enable USB Device Full Speed clock.
bool CLOCK_EnableUsbfs0HostClock ( clock_usb_src_t  src,
uint32_t  freq 
)
Parameters
src: clock source
freq,:clock frequency Enable USB HOST Full Speed clock.
bool CLOCK_EnableUsbhs0DeviceClock ( clock_usb_src_t  src,
uint32_t  freq 
)
Parameters
src: clock source
freq,:clock frequency Enable USB Device High Speed clock.
bool CLOCK_EnableUsbhs0HostClock ( clock_usb_src_t  src,
uint32_t  freq 
)
Parameters
src: clock source
freq,:clock frequency Enable USB HOST High Speed clock.