![]() |
MCUXpresso SDK API Reference Manual
Rev 2.12.0
NXP Semiconductors
|
The MCUXpresso SDK provides a peripheral driver for the Local Interconnect Network (LIN) module of MCUXpresso SDK devices.
For an example of Local Interconnect Network, see the driver example lin_master or lin_slave.
Data Structures | |
| struct | lin_user_config_t |
| LIN hardware configuration structure. More... | |
| struct | lin_state_t |
| Runtime state of the LIN driver. More... | |
| struct | lin_baudrate_values_t |
| Structure of baudrate properties. More... | |
| struct | lin_frame_struct |
| Informations of frame. More... | |
| struct | lin_protocol_user_config_t |
| Protocol configuration structure. More... | |
| struct | lin_product_id |
| Product id structure. More... | |
| struct | lin_serial_number |
| Serial number. More... | |
| struct | lin_protocol_state_t |
| Protocol state structure. More... | |
| struct | lin_node_attribute |
| Attributes of LIN node. More... | |
| struct | lin_master_data_t |
| LIN master data structure. More... | |
Variables | |
| uint8_t | lin_user_config_t::hardware_instance |
| interface instance number | |
| uint32_t | lin_user_config_t::baudRate |
| baudrate of LIN Hardware Interface to configure | |
| bool | lin_user_config_t::nodeFunction |
| Node function as Master or Slave. | |
| bool | lin_user_config_t::autobaudEnable |
| Enable Autobaud feature. | |
| lin_timer_get_time_interval_t | lin_user_config_t::timerGetTimeIntervalCallback |
| Callback function to get time interval in nano seconds. | |
| const uint8_t * | lin_state_t::txBuff |
| The buffer of data being sent. More... | |
| uint8_t * | lin_state_t::rxBuff |
| The buffer of received data. More... | |
| uint8_t | lin_state_t::cntByte |
| To count number of bytes already transmitted or received. More... | |
| volatile uint8_t | lin_state_t::txSize |
| The remaining number of bytes to be received. More... | |
| volatile uint8_t | lin_state_t::rxSize |
| The remaining number of bytes to be received. More... | |
| uint8_t | lin_state_t::checkSum |
| Checksum byte. More... | |
| volatile bool | lin_state_t::isTxBusy |
| True if the LIN interface is transmitting frame data. More... | |
| volatile bool | lin_state_t::isRxBusy |
| True if the LIN interface is receiving frame data. More... | |
| volatile bool | lin_state_t::isBusBusy |
| True if there are data, frame headers being transferred on bus. | |
| volatile bool | lin_state_t::isTxBlocking |
| True if transmit is blocking transaction. More... | |
| volatile bool | lin_state_t::isRxBlocking |
| True if receive is blocking transaction. More... | |
| lin_callback_t | lin_state_t::Callback |
| Callback function to invoke after receiving a byte or transmitting a byte. More... | |
| uint8_t | lin_state_t::currentId |
| Current ID. | |
| uint8_t | lin_state_t::currentPid |
| Current PID. | |
| volatile lin_event_id_t | lin_state_t::currentEventId |
| Current ID Event. | |
| volatile lin_node_state_t | lin_state_t::currentNodeState |
| Current Node state. | |
| volatile uint32_t | lin_state_t::timeoutCounter |
| Value of the timeout counter. | |
| volatile bool | lin_state_t::timeoutCounterFlag |
| Timeout counter flag. | |
| volatile bool | lin_state_t::baudrateEvalEnable |
| Baudrate Evaluation Process Enable. | |
| volatile uint8_t | lin_state_t::fallingEdgeInterruptCount |
| Falling Edge count of a sync byte. | |
| uint32_t | lin_state_t::linSourceClockFreq |
| Frequency of the source clock for LIN. | |
| volatile bool | lin_state_t::txCompleted |
| Used to wait for LIN interface ISR to complete transmission. More... | |
| volatile bool | lin_state_t::rxCompleted |
| Used to wait for LIN interface ISR to complete reception. | |
| lin_frame_type | lin_frame_struct::frm_type |
| Frame information (unconditional or event triggered..) | |
| uint8_t | lin_frame_struct::frm_len |
| Length of the frame. | |
| lin_frame_response | lin_frame_struct::frm_response |
| Action response when received PID. | |
| uint8_t | lin_frame_struct::frm_offset |
| Frame byte offset in frame buffer. | |
| uint8_t | lin_frame_struct::flag_offset |
| Flag byte offset in flag buffer. | |
| uint8_t | lin_frame_struct::flag_size |
| Flag size in flag buffer. | |
| uint32_t | lin_frame_struct::delay |
| Frame delay. | |
| const uint8_t * | lin_frame_struct::frame_data_ptr |
| List of Signal to which the frame is associated and its offset. | |
| lin_protocol_handle | lin_protocol_user_config_t::protocol_version |
| Protocol version. | |
| lin_protocol_handle | lin_protocol_user_config_t::language_version |
| Language version. | |
| uint8_t | lin_protocol_user_config_t::number_of_configurable_frames |
| Number of frame except diagnostic frames. | |
| uint8_t | lin_protocol_user_config_t::frame_start |
| Start index of frame list. | |
| const lin_frame_struct * | lin_protocol_user_config_t::frame_tbl_ptr |
| Frame list except diagnostic frames. | |
| const uint16_t * | lin_protocol_user_config_t::list_identifiers_ROM_ptr |
| Configuration in ROM. | |
| uint8_t * | lin_protocol_user_config_t::list_identifiers_RAM_ptr |
| Configuration in RAM. | |
| uint16_t | lin_protocol_user_config_t::max_idle_timeout_cnt |
| Max Idle timeout counter. | |
| uint16_t | lin_protocol_user_config_t::max_message_length |
| Max message length. | |
| uint16_t | lin_product_id::supplier_id |
| Supplier ID. | |
| uint16_t | lin_product_id::function_id |
| Function ID. | |
| uint8_t | lin_product_id::variant |
| Variant value. | |
| uint8_t | lin_serial_number::serial_0 |
| Serial 0. | |
| uint8_t | lin_serial_number::serial_1 |
| Serial 1. | |
| uint8_t | lin_serial_number::serial_2 |
| Serial 2. | |
| uint8_t | lin_serial_number::serial_3 |
| Serial 3. | |
| uint16_t | lin_protocol_state_t::baud_rate |
| Adjusted baud rate. | |
| uint8_t * | lin_protocol_state_t::response_buffer_ptr |
| Response buffer. | |
| uint8_t | lin_protocol_state_t::response_length |
| Response length. | |
| uint8_t | lin_protocol_state_t::successful_transfer |
| Sets when frame is transferred successfully. | |
| uint8_t | lin_protocol_state_t::error_in_response |
| Sets when frame received/transmitter by the node contains an error in the response field. | |
| uint8_t | lin_protocol_state_t::timeout_in_response |
| Timeout response. | |
| bool | lin_protocol_state_t::go_to_sleep_flg |
| Go to sleep flag. | |
| uint8_t | lin_protocol_state_t::current_id |
| Current PID. | |
| uint8_t | lin_protocol_state_t::num_of_processed_frame |
| Number of processed frames. | |
| uint8_t | lin_protocol_state_t::num_of_successfull_frame |
| Number of processed frames. | |
| uint8_t | lin_protocol_state_t::next_transmit_tick |
| Used to count the next transmit tick. | |
| bool | lin_protocol_state_t::save_config_flg |
| Set when save configuration request has been received. | |
| lin_diagnostic_mode | lin_protocol_state_t::diagnostic_mode |
| Diagnostic mode. | |
| uint16_t | lin_protocol_state_t::frame_timeout_cnt |
| Frame timeout counter. | |
| uint16_t | lin_protocol_state_t::idle_timeout_cnt |
| Idle timeout counter, node will go to sleep when count down to 0. | |
| bool | lin_protocol_state_t::transmit_error_resp_sig_flg |
| Flag indicates that the error response signal is going to be sent. | |
| bool | lin_protocol_state_t::event_trigger_collision_flg |
| Flag indicates collision on bus. | |
| uint8_t * | lin_node_attribute::configured_NAD_ptr |
| NAD value used in configuration command. | |
| uint8_t | lin_node_attribute::initial_NAD |
| Initial NAD. | |
| lin_product_id | lin_node_attribute::product_id |
| Product ID. | |
| lin_serial_number | lin_node_attribute::serial_number |
| Serial number. | |
| uint8_t * | lin_node_attribute::resp_err_frm_id_ptr |
| Pointer to the list of index of frames that carries response error signal. | |
| uint8_t | lin_node_attribute::num_frame_have_esignal |
| The count of frames that carry response error signal. | |
| uint8_t | lin_node_attribute::response_error_byte_offset |
| Byte offset of response error signal. | |
| uint8_t | lin_node_attribute::response_error_bit_offset |
| Bit offset of response error signal. | |
| uint8_t | lin_node_attribute::num_of_fault_state_signal |
| Number of Fault state signal. | |
| uint16_t | lin_node_attribute::P2_min |
| P2 min. | |
| uint16_t | lin_node_attribute::ST_min |
| ST min. | |
| uint16_t | lin_node_attribute::N_As_timeout |
| N_As_timeout. | |
| uint16_t | lin_node_attribute::N_Cr_timeout |
| N_Cr_timeout. | |
| uint8_t | lin_master_data_t::active_schedule_id |
| Active schedule table id. | |
| uint8_t | lin_master_data_t::previous_schedule_id |
| Previous schedule table id. | |
| uint8_t * | lin_master_data_t::schedule_start_entry_ptr |
| Start entry of each schedule table. | |
| uint8_t | lin_master_data_t::data_buffer [8] |
| Master data buffer. | |
Driver version | |
| enum | lin_frame_type { LIN_FRM_UNCD = 0x00U, LIN_FRM_EVNT = 0x01U, LIN_FRM_SPRDC = 0x10U, LIN_FRM_DIAG = 0x11U } |
| List of LIN frame types. More... | |
| enum | lin_frame_response { LIN_RES_NOTHING = 0x00U, LIN_RES_PUB = 0x01U, LIN_RES_SUB = 0x10U } |
| List of LIN frame response types. More... | |
| enum | lin_diagnostic_mode { DIAG_NONE = 0x00U, DIAG_INTERLEAVE_MODE = 0x01U, DIAG_ONLY_MODE = 0x02U } |
| Diagnostic mode. More... | |
| enum | lin_event_id_t { LIN_NO_EVENT = 0x00U, LIN_WAKEUP_SIGNAL = 0x01U, LIN_BAUDRATE_ADJUSTED = 0x02U, LIN_RECV_BREAK_FIELD_OK = 0x03U, LIN_SYNC_OK = 0x04U, LIN_SYNC_ERROR = 0x05U, LIN_PID_OK = 0x06U, LIN_PID_ERROR = 0x07U, LIN_FRAME_ERROR = 0x08U, LIN_READBACK_ERROR = 0x09U, LIN_CHECKSUM_ERROR = 0x0AU, LIN_TX_COMPLETED = 0x0BU, LIN_RX_COMPLETED = 0x0CU, LIN_NO_DATA_TIMEOUT = 0x0DU, LIN_BUS_ACTIVITY_TIMEOUT = 0x0EU, LIN_TIMEOUT_ERROR = 0x0FU, LIN_LAST_RESPONSE_SHORT_ERROR = 0x10U, LIN_NO_EVENT = 0x00U, LIN_WAKEUP_SIGNAL = 0x01U, LIN_BAUDRATE_ADJUSTED = 0x02U, LIN_RECV_BREAK_FIELD_OK = 0x03U, LIN_SYNC_OK = 0x04U, LIN_SYNC_ERROR = 0x05U, LIN_PID_OK = 0x06U, LIN_PID_ERROR = 0x07U, LIN_FRAME_ERROR = 0x08U, LIN_READBACK_ERROR = 0x09U, LIN_CHECKSUM_ERROR = 0x0AU, LIN_TX_COMPLETED = 0x0BU, LIN_RX_COMPLETED = 0x0CU, LIN_RX_OVERRUN = 0x0DU, LIN_LAST_RESPONSE_SHORT_ERROR = 0x0EU } |
| Defines types for an enumerating event related to an Identifier. More... | |
| enum | lin_status_t { LIN_IFC_NOT_SUPPORT = 0x00U, LIN_INITIALIZED = 0x01U, LIN_SUCCESS = 0x02U, LIN_ERROR = 0x03U, LIN_TX_BUSY = 0x04U, LIN_RX_BUSY = 0x05U, LIN_BUS_BUSY = 0x06U, LIN_NO_TRANSFER_IN_PROGRESS = 0x07U, LIN_TIMEOUT = 0x08U, LIN_LPUART_STAT_CLOCK_GATED_OFF = 0x09U, LIN_IFC_NOT_SUPPORT = 0x00U, LIN_INITIALIZED = 0x01U, LIN_SUCCESS = 0x02U, LIN_ERROR = 0x03U, LIN_TX_BUSY = 0x04U, LIN_RX_BUSY = 0x05U, LIN_BUS_BUSY = 0x06U, LIN_NO_TRANSFER_IN_PROGRESS = 0x07U, LIN_TIMEOUT = 0x08U, LIN_LPUART_STAT_CLOCK_GATED_OFF = 0x09U } |
| Defines Error codes of the LIN driver. More... | |
| enum | lin_node_state_t { LIN_NODE_STATE_UNINIT = 0x00U, LIN_NODE_STATE_SLEEP_MODE = 0x01U, LIN_NODE_STATE_IDLE = 0x02U, LIN_NODE_STATE_SEND_BREAK_FIELD = 0x03U, LIN_NODE_STATE_RECV_SYNC = 0x04U, LIN_NODE_STATE_SEND_PID = 0x05U, LIN_NODE_STATE_RECV_PID = 0x06U, LIN_NODE_STATE_RECV_DATA = 0x07U, LIN_NODE_STATE_RECV_DATA_COMPLETED = 0x08U, LIN_NODE_STATE_SEND_DATA = 0x09U, LIN_NODE_STATE_SEND_DATA_COMPLETED = 0x0AU, LIN_NODE_STATE_UNINIT = 0x00U, LIN_NODE_STATE_SLEEP_MODE = 0x01U, LIN_NODE_STATE_IDLE = 0x02U, LIN_NODE_STATE_SEND_BREAK_FIELD = 0x03U, LIN_NODE_STATE_RECV_SYNC = 0x04U, LIN_NODE_STATE_SEND_PID = 0x05U, LIN_NODE_STATE_RECV_PID = 0x06U, LIN_NODE_STATE_RECV_DATA = 0x07U, LIN_NODE_STATE_RECV_DATA_COMPLETED = 0x08U, LIN_NODE_STATE_SEND_DATA = 0x09U, LIN_NODE_STATE_SEND_DATA_COMPLETED = 0x0AU } |
| Define type for an enumerating LIN Node state. More... | |
| enum | lin_protocol_handle { LIN_PROTOCOL_21 = 0x00U, LIN_PROTOCOL_J2602 = 0x01U } |
| List of protocols. More... | |
| enum | lin_supported_baudrates_t |
| List of supported baudrates for autobaud feature. | |
| typedef void(* | lin_timer_get_time_interval_t )(uint32_t *nanoSeconds) |
| Callback function to get time interval in nano seconds. | |
| typedef void(* | lin_callback_t )(uint32_t instance, void *linState) |
| LIN Driver callback function type. | |
| LPUART_Type *const | g_linLpuartBase [FSL_FEATURE_SOC_LPUART_COUNT] |
| Table of base addresses for LPUART instances. More... | |
| const IRQn_Type | g_linLpuartRxTxIrqId [FSL_FEATURE_SOC_LPUART_COUNT] |
| Table to save LPUART IRQ enumeration numbers defined in the CMSIS header file. | |
| lin_baudrate_values_t | g_linConfigBaudrates [LIN_NUM_OF_SUPP_BAUDRATES] |
| Table to save LIN user config buadrate values. | |
| lin_state_t * | g_linStatePtr [FSL_FEATURE_SOC_LPUART_COUNT] |
| Pointers to LPUART bases for each instance. More... | |
| lin_user_config_t * | g_linUserconfigPtr [FSL_FEATURE_SOC_LPUART_COUNT] |
| Table to save LIN user config structure pointers. | |
| #define | FSL_LIN_DRIVER_VERSION (MAKE_VERSION(2, 2, 0)) |
| LIN driver version. | |
| #define | LIN_SLAVE 0U |
| #define | LIN_MASTER 1U |
| #define | MAKE_PARITY 0U |
| #define | CHECK_PARITY 1U |
| #define | LIN_TIME_OUT_UNIT_US 500U |
| #define | LIN_MAKE_UNCONDITIONAL_FRAME 0U |
| #define | LIN_UPDATE_UNCONDITIONAL_FRAME 1U |
| #define | LIN_NUM_OF_SUPP_BAUDRATES 5U |
LIN DRIVER | |
| uint32_t | LIN_CalcMaxHeaderTimeoutCnt (uint32_t baudRate) |
| Calculates maximal header time lenght. More... | |
| uint32_t | LIN_CalcMaxResTimeoutCnt (uint32_t baudRate, uint8_t size) |
| Calculates maximal header time length. More... | |
| lin_status_t | LIN_SetResponse (uint8_t instance, uint8_t *response_buff, uint8_t response_length, uint8_t max_frame_res_timeout) |
| Forwards a response to a lower level. More... | |
| lin_status_t | LIN_RxResponse (uint8_t instance, uint8_t *response_buff, uint8_t response_length, uint8_t max_frame_res_timeout) |
| Forwards a response to a higher level. More... | |
| lin_status_t | LIN_IgnoreResponse (uint8_t instance) |
| Put a node into idle state. More... | |
| void | LIN_GetSlaveDefaultConfig (lin_user_config_t *linUserConfig) |
| Initializes linUserConfig variable for a slave node. More... | |
| void | LIN_GetMasterDefaultConfig (lin_user_config_t *linUserConfig) |
| Initializes linUserConfig variable for a master node. More... | |
| void | LIN_CalculateBaudrate (uint32_t instance, uint32_t baudRate_Bps, uint32_t srcClock_Hz, uint32_t *osr, uint16_t *sbr) |
| Calculates baudrate registers values for given baudrate. More... | |
| void | LIN_SetBaudrate (uint32_t instance, uint32_t osr, uint16_t sbr) |
| Set baudrate registers values. More... | |
| lin_status_t | LIN_Init (uint32_t instance, lin_user_config_t *linUserConfig, lin_state_t *linCurrentState, uint32_t clockSource) |
| Initializes an instance LIN Hardware Interface for LIN Network. More... | |
| lin_status_t | LIN_Deinit (uint32_t instance) |
| Shuts down the LIN Hardware Interface by disabling interrupts and transmitter/receiver. More... | |
| lin_callback_t | LIN_InstallCallback (uint32_t instance, lin_callback_t function) |
| Installs callback function that is used for LIN_DRV_IRQHandler. More... | |
| lin_status_t | LIN_SendFrameDataBlocking (uint32_t instance, const uint8_t *txBuff, uint8_t txSize, uint32_t timeoutMSec) |
| Sends Frame data out through the LIN Hardware Interface using blocking method. More... | |
| lin_status_t | LIN_SendFrameData (uint32_t instance, const uint8_t *txBuff, uint8_t txSize) |
| Sends frame data out through the LIN Hardware Interface using non-blocking method. More... | |
| lin_status_t | LIN_GetTransmitStatus (uint32_t instance, uint8_t *bytesRemaining) |
| Get status of an on-going non-blocking transmission While sending frame data using non-blocking method, users can use this function to get status of that transmission. More... | |
| lin_status_t | LIN_ReceiveFrameDataBlocking (uint32_t instance, uint8_t *rxBuff, uint8_t rxSize, uint32_t timeoutMSec) |
| Receives frame data through the LIN Hardware Interface using blocking method. More... | |
| lin_status_t | LIN_ReceiveFrameData (uint32_t instance, uint8_t *rxBuff, uint8_t rxSize) |
| Receives frame data through the LIN Hardware Interface using non- blocking method. More... | |
| lin_status_t | LIN_AbortTransferData (uint32_t instance) |
| Aborts an on-going non-blocking transmission/reception. More... | |
| lin_status_t | LIN_GetReceiveStatus (uint32_t instance, uint8_t *bytesRemaining) |
| Get status of an on-going non-blocking reception While receiving frame data using non-blocking method, users can use this function to get status of that receiving. More... | |
| lin_status_t | LIN_GoToSleepMode (uint32_t instance) |
| Puts current LIN node to sleep mode This function changes current node state to LIN_NODE_STATE_SLEEP_MODE. More... | |
| lin_status_t | LIN_GotoIdleState (uint32_t instance) |
| Puts current LIN node to Idle state This function changes current node state to LIN_NODE_STATE_IDLE. More... | |
| lin_status_t | LIN_SendWakeupSignal (uint32_t instance) |
| Sends a wakeup signal through the LIN Hardware Interface. More... | |
| lin_node_state_t | LIN_GetCurrentNodeState (uint32_t instance) |
| Get the current LIN node state. More... | |
| void | LIN_TimeoutService (uint32_t instance) |
| Callback function for Timer Interrupt Handler Users may use (optional, not required) LIN_TimeoutService to check if timeout has occurred during non-blocking frame data transmission and reception. More... | |
| void | LIN_SetTimeoutCounter (uint32_t instance, uint32_t timeoutValue) |
| Set Value for Timeout Counter that is used in LIN_TimeoutService. More... | |
| lin_status_t | LIN_MasterSendHeader (uint32_t instance, uint8_t id) |
| Sends frame header out through the LIN Hardware Interface using a non-blocking method. More... | |
| lin_status_t | LIN_EnableIRQ (uint32_t instance) |
| Enables LIN hardware interrupts. More... | |
| lin_status_t | LIN_DisableIRQ (uint32_t instance) |
| Disables LIN hardware interrupts. More... | |
| void | LIN_IRQHandler (uint8_t instance) |
| Interrupt handler for LIN Hardware Interface. More... | |
| lin_status_t | LIN_AutoBaudCapture (uint32_t instance) |
| This function capture bits time to detect break char, calculate baudrate from sync bits and enable transceiver if autobaud successful. More... | |
| uint8_t | LIN_ProcessParity (uint8_t PID, uint8_t typeAction) |
| Makes or checks parity bits. More... | |
| uint8_t | LIN_MakeChecksumByte (const uint8_t *buffer, uint8_t sizeBuffer, uint8_t PID) |
| Makes the checksum byte for a frame. More... | |
LIN DRIVER | |
| lin_status_t | LIN_DRV_SetResponse (uint8_t instance, uint8_t *response_buff, uint8_t response_length, uint8_t max_frame_res_timeout) |
| Forwards a response to a lower level. More... | |
| lin_status_t | LIN_DRV_RxResponse (uint8_t instance, uint8_t *response_buff, uint8_t response_length, uint8_t max_frame_res_timeout) |
| Forwards a response to a higher level. More... | |
| lin_status_t | LIN_DRV_IgnoreResponse (uint8_t instance) |
| Put a node into idle state. More... | |
| void | LIN_DRV_CalculateBaudrate (uint32_t instance, uint32_t baudRate_Bps, uint32_t srcClock_Hz, uint32_t *osr, uint16_t *sbr) |
| Calculates baudrate registers values for given baudrate. More... | |
| void | LIN_DRV_SetBaudrate (uint32_t instance, uint32_t osr, uint16_t sbr) |
| Set baudrate registers values. More... | |
| lin_status_t | LIN_DRV_Init (uint32_t instance, lin_user_config_t *linUserConfig, lin_state_t *linCurrentState) |
| Initializes an instance LIN Hardware Interface for LIN Network. More... | |
| lin_status_t | LIN_DRV_Deinit (uint32_t instance) |
| Shuts down the LIN Hardware Interface by disabling interrupts and transmitter/receiver. More... | |
| lin_callback_t | LIN_DRV_InstallCallback (uint32_t instance, lin_callback_t function) |
| Installs callback function that is used for LIN_DRV_IRQHandler. More... | |
| lin_status_t | LIN_DRV_SendFrameDataBlocking (uint32_t instance, const uint8_t *txBuff, uint8_t txSize, uint32_t timeoutMSec) |
| Sends Frame data out through the LIN Hardware Interface using blocking method. More... | |
| lin_status_t | LIN_DRV_SendFrameData (uint32_t instance, const uint8_t *txBuff, uint8_t txSize) |
| Sends frame data out through the LIN Hardware Interface using non-blocking method. More... | |
| lin_status_t | LIN_DRV_GetTransmitStatus (uint32_t instance, uint8_t *bytesRemaining) |
| Get status of an on-going non-blocking transmission While sending frame data using non-blocking method, users can use this function to get status of that transmission. More... | |
| lin_status_t | LIN_DRV_ReceiveFrameDataBlocking (uint32_t instance, uint8_t *rxBuff, uint8_t rxSize, uint32_t timeoutMSec) |
| Receives frame data through the LIN Hardware Interface using blocking method. More... | |
| lin_status_t | LIN_DRV_ReceiveFrameData (uint32_t instance, uint8_t *rxBuff, uint8_t rxSize) |
| Receives frame data through the LIN Hardware Interface using non- blocking method. More... | |
| lin_status_t | LIN_DRV_AbortTransferData (uint32_t instance) |
| Aborts an on-going non-blocking transmission/reception. More... | |
| lin_status_t | LIN_DRV_GetReceiveStatus (uint32_t instance, uint8_t *bytesRemaining) |
| Get status of an on-going non-blocking reception While receiving frame data using non-blocking method, users can use this function to get status of that receiving. More... | |
| lin_status_t | LIN_DRV_GoToSleepMode (uint32_t instance) |
| Puts current LIN node to sleep mode This function changes current node state to LIN_NODE_STATE_SLEEP_MODE. More... | |
| lin_status_t | LIN_DRV_GotoIdleState (uint32_t instance) |
| Puts current LIN node to Idle state This function changes current node state to LIN_NODE_STATE_IDLE. More... | |
| lin_status_t | LIN_DRV_SendWakeupSignal (uint32_t instance) |
| Sends a wakeup signal through the LIN Hardware Interface. More... | |
| lin_node_state_t | LIN_DRV_GetCurrentNodeState (uint32_t instance) |
| Get the current LIN node state. More... | |
| void | LIN_DRV_TimeoutService (uint32_t instance) |
| Callback function for Timer Interrupt Handler Users may use (optional, not required) LIN_TimeoutService to check if timeout has occurred during non-blocking frame data transmission and reception. More... | |
| static void | LIN_DRV_SetTimeoutCounter (uint32_t instance, uint32_t timeoutValue) |
| Set Value for Timeout Counter that is used in LIN_TimeoutService. More... | |
| lin_status_t | LIN_DRV_MasterSendHeader (uint32_t instance, uint8_t id) |
| Sends frame header out through the LIN Hardware Interface using a non-blocking method. More... | |
| lin_status_t | LIN_DRV_EnableIRQ (uint32_t instance) |
| Enables LIN hardware interrupts. More... | |
| lin_status_t | LIN_DRV_DisableIRQ (uint32_t instance) |
| Disables LIN hardware interrupts. More... | |
| void | LIN_DRV_IRQHandler (uint8_t instance) |
| Interrupt handler for LIN Hardware Interface. More... | |
| static lin_status_t | LIN_DRV_AutoBaudCapture (uint32_t instance) |
| This function capture bits time to detect break char. More... | |
| static uint8_t | LIN_DRV_ProcessParity (uint8_t PID, uint8_t typeAction) |
| Makes or checks parity bits. More... | |
| static uint8_t | LIN_DRV_MakeChecksumByte (const uint8_t *buffer, uint8_t sizeBuffer, uint8_t PID) |
| Makes the checksum byte for a frame. More... | |
| struct lin_user_config_t |
Data Fields | |
| uint8_t | hardware_instance |
| interface instance number | |
| uint32_t | baudRate |
| baudrate of LIN Hardware Interface to configure | |
| bool | nodeFunction |
| Node function as Master or Slave. | |
| bool | autobaudEnable |
| Enable Autobaud feature. | |
| lin_timer_get_time_interval_t | timerGetTimeIntervalCallback |
| Callback function to get time interval in nano seconds. | |
| struct lin_state_t |
Note that the caller provides memory for the driver state structures during initialization because the driver does not statically allocate memory.
Data Fields | |
| const uint8_t * | txBuff |
| The buffer of data being sent. More... | |
| uint8_t * | rxBuff |
| The buffer of received data. More... | |
| uint8_t | cntByte |
| To count number of bytes already transmitted or received. More... | |
| volatile uint8_t | txSize |
| The remaining number of bytes to be received. More... | |
| volatile uint8_t | rxSize |
| The remaining number of bytes to be received. More... | |
| uint8_t | checkSum |
| Checksum byte. More... | |
| volatile bool | isTxBusy |
| True if the LIN interface is transmitting frame data. More... | |
| volatile bool | isRxBusy |
| True if the LIN interface is receiving frame data. More... | |
| volatile bool | isBusBusy |
| True if there are data, frame headers being transferred on bus. | |
| volatile bool | isTxBlocking |
| True if transmit is blocking transaction. More... | |
| volatile bool | isRxBlocking |
| True if receive is blocking transaction. More... | |
| lin_callback_t | Callback |
| Callback function to invoke after receiving a byte or transmitting a byte. More... | |
| uint8_t | currentId |
| Current ID. | |
| uint8_t | currentPid |
| Current PID. | |
| volatile lin_event_id_t | currentEventId |
| Current ID Event. | |
| volatile lin_node_state_t | currentNodeState |
| Current Node state. | |
| volatile uint32_t | timeoutCounter |
| Value of the timeout counter. | |
| volatile bool | timeoutCounterFlag |
| Timeout counter flag. | |
| volatile bool | baudrateEvalEnable |
| Baudrate Evaluation Process Enable. | |
| volatile uint8_t | fallingEdgeInterruptCount |
| Falling Edge count of a sync byte. | |
| uint32_t | linSourceClockFreq |
| Frequency of the source clock for LIN. | |
| volatile bool | txCompleted |
| Used to wait for LIN interface ISR to complete transmission. More... | |
| volatile bool | rxCompleted |
| Used to wait for LIN interface ISR to complete reception. | |
| struct lin_baudrate_values_t |
| struct lin_frame_struct |
Data Fields | |
| lin_frame_type | frm_type |
| Frame information (unconditional or event triggered..) | |
| uint8_t | frm_len |
| Length of the frame. | |
| lin_frame_response | frm_response |
| Action response when received PID. | |
| uint8_t | frm_offset |
| Frame byte offset in frame buffer. | |
| uint8_t | flag_offset |
| Flag byte offset in flag buffer. | |
| uint8_t | flag_size |
| Flag size in flag buffer. | |
| uint32_t | delay |
| Frame delay. | |
| const uint8_t * | frame_data_ptr |
| List of Signal to which the frame is associated and its offset. | |
| struct lin_protocol_user_config_t |
Data Fields | |
| lin_protocol_handle | protocol_version |
| Protocol version. | |
| lin_protocol_handle | language_version |
| Language version. | |
| uint8_t | number_of_configurable_frames |
| Number of frame except diagnostic frames. | |
| uint8_t | frame_start |
| Start index of frame list. | |
| const lin_frame_struct * | frame_tbl_ptr |
| Frame list except diagnostic frames. | |
| const uint16_t * | list_identifiers_ROM_ptr |
| Configuration in ROM. | |
| uint8_t * | list_identifiers_RAM_ptr |
| Configuration in RAM. | |
| uint16_t | max_idle_timeout_cnt |
| Max Idle timeout counter. | |
| uint16_t | max_message_length |
| Max message length. | |
| struct lin_product_id |
Data Fields | |
| uint16_t | supplier_id |
| Supplier ID. | |
| uint16_t | function_id |
| Function ID. | |
| uint8_t | variant |
| Variant value. | |
| struct lin_serial_number |
| struct lin_protocol_state_t |
Data Fields | |
| uint16_t | baud_rate |
| Adjusted baud rate. | |
| uint8_t * | response_buffer_ptr |
| Response buffer. | |
| uint8_t | response_length |
| Response length. | |
| uint8_t | successful_transfer |
| Sets when frame is transferred successfully. | |
| uint8_t | error_in_response |
| Sets when frame received/transmitter by the node contains an error in the response field. | |
| uint8_t | timeout_in_response |
| Timeout response. | |
| bool | go_to_sleep_flg |
| Go to sleep flag. | |
| uint8_t | current_id |
| Current PID. | |
| uint8_t | num_of_processed_frame |
| Number of processed frames. | |
| uint8_t | num_of_successfull_frame |
| Number of processed frames. | |
| uint8_t | next_transmit_tick |
| Used to count the next transmit tick. | |
| bool | save_config_flg |
| Set when save configuration request has been received. | |
| lin_diagnostic_mode | diagnostic_mode |
| Diagnostic mode. | |
| uint16_t | frame_timeout_cnt |
| Frame timeout counter. | |
| uint16_t | idle_timeout_cnt |
| Idle timeout counter, node will go to sleep when count down to 0. | |
| bool | transmit_error_resp_sig_flg |
| Flag indicates that the error response signal is going to be sent. | |
| bool | event_trigger_collision_flg |
| Flag indicates collision on bus. | |
| struct lin_node_attribute |
Data Fields | |
| uint8_t * | configured_NAD_ptr |
| NAD value used in configuration command. | |
| uint8_t | initial_NAD |
| Initial NAD. | |
| lin_product_id | product_id |
| Product ID. | |
| lin_serial_number | serial_number |
| Serial number. | |
| uint8_t * | resp_err_frm_id_ptr |
| Pointer to the list of index of frames that carries response error signal. | |
| uint8_t | num_frame_have_esignal |
| The count of frames that carry response error signal. | |
| uint8_t | response_error_byte_offset |
| Byte offset of response error signal. | |
| uint8_t | response_error_bit_offset |
| Bit offset of response error signal. | |
| uint8_t | num_of_fault_state_signal |
| Number of Fault state signal. | |
| uint16_t | P2_min |
| P2 min. | |
| uint16_t | ST_min |
| ST min. | |
| uint16_t | N_As_timeout |
| N_As_timeout. | |
| uint16_t | N_Cr_timeout |
| N_Cr_timeout. | |
| struct lin_master_data_t |
Data Fields | |
| uint8_t | active_schedule_id |
| Active schedule table id. | |
| uint8_t | previous_schedule_id |
| Previous schedule table id. | |
| uint8_t * | schedule_start_entry_ptr |
| Start entry of each schedule table. | |
| uint8_t | data_buffer [8] |
| Master data buffer. | |
| enum lin_frame_type |
| enum lin_frame_response |
| enum lin_diagnostic_mode |
| enum lin_event_id_t |
| enum lin_status_t |
| enum lin_node_state_t |
| enum lin_protocol_handle |
| enum lin_event_id_t |
| enum lin_status_t |
| enum lin_node_state_t |
| uint32_t LIN_CalcMaxHeaderTimeoutCnt | ( | uint32_t | baudRate | ) |
Theader_Maximum = 1.4 * THeader_Nominal, THeader_Nominal = 34 * TBit, ( 13 nominal bits of breack; 1 nominal bit of break delimiter; 10 bits for SYNC and 10 bits of PID) The function is not include time for conveying break and break delimiter TIME_OUT_UNIT is in micro second
| baudRate | baudrate |
| uint32_t LIN_CalcMaxResTimeoutCnt | ( | uint32_t | baudRate, |
| uint8_t | size | ||
| ) |
TResponse_Maximum = 1.4 * TResponse_Nominal, TResponse_Nominal = 10 * (NData+ 1) * TBit
| baudRate | Baudrate |
| size | Frame size |
| lin_status_t LIN_SetResponse | ( | uint8_t | instance, |
| uint8_t * | response_buff, | ||
| uint8_t | response_length, | ||
| uint8_t | max_frame_res_timeout | ||
| ) |
| instance | LPUART instance |
| response_buff | response message |
| response_length | length of response |
| max_frame_res_timeout | maximal timeout duration for message |
| lin_status_t LIN_RxResponse | ( | uint8_t | instance, |
| uint8_t * | response_buff, | ||
| uint8_t | response_length, | ||
| uint8_t | max_frame_res_timeout | ||
| ) |
| instance | LPUART instance |
| response_buff | response message |
| response_length | length of response |
| max_frame_res_timeout | maximal timeout duration for message |
| lin_status_t LIN_IgnoreResponse | ( | uint8_t | instance | ) |
| instance | LPUART instance |
| void LIN_GetSlaveDefaultConfig | ( | lin_user_config_t * | linUserConfig | ) |
| linUserConfig | Pointer to LIN user config structure |
| void LIN_GetMasterDefaultConfig | ( | lin_user_config_t * | linUserConfig | ) |
| linUserConfig | Pointer to LIN user config structure |
| void LIN_CalculateBaudrate | ( | uint32_t | instance, |
| uint32_t | baudRate_Bps, | ||
| uint32_t | srcClock_Hz, | ||
| uint32_t * | osr, | ||
| uint16_t * | sbr | ||
| ) |
| instance | LPUART instance |
| instance | baudRate_Bps LPUART baudrate |
| instance | srcClock_Hz LPUART clock frequency |
| instance | osr LPUART baudrate OSR value, return value |
| instance | sbr LPUART baudrate SBR value, return value |
| void LIN_SetBaudrate | ( | uint32_t | instance, |
| uint32_t | osr, | ||
| uint16_t | sbr | ||
| ) |
| instance | LPUART instance |
| instance | osr LPUART baudrate OSR value |
| instance | sbr LPUART baudrate SBR value |
| lin_status_t LIN_Init | ( | uint32_t | instance, |
| lin_user_config_t * | linUserConfig, | ||
| lin_state_t * | linCurrentState, | ||
| uint32_t | clockSource | ||
| ) |
The caller provides memory for the driver state structures during initialization. The user must select the LIN Hardware Interface clock source in the application to initialize the LIN Hardware Interface.
| instance | LPUART instance |
| linUserConfig | user configuration structure of type lin_user_config_t |
| linCurrentState | pointer to the LIN Hardware Interface driver state structure |
| lin_status_t LIN_Deinit | ( | uint32_t | instance | ) |
| instance | LPUART instance |
| lin_callback_t LIN_InstallCallback | ( | uint32_t | instance, |
| lin_callback_t | function | ||
| ) |
| instance | LPUART instance. |
| function | the LIN receive callback function. |
| lin_status_t LIN_SendFrameDataBlocking | ( | uint32_t | instance, |
| const uint8_t * | txBuff, | ||
| uint8_t | txSize, | ||
| uint32_t | timeoutMSec | ||
| ) |
This function will calculate the checksum byte and send it with the frame data. Blocking means that the function does not return until the transmission is complete.
| instance | LPUART instance |
| txBuff | source buffer containing 8-bit data chars to send |
| txSize | the number of bytes to send |
| timeoutMSec | timeout value in milli seconds |
| lin_status_t LIN_SendFrameData | ( | uint32_t | instance, |
| const uint8_t * | txBuff, | ||
| uint8_t | txSize | ||
| ) |
This enables an a-sync method for transmitting data. Non-blocking means that the function returns immediately. The application has to get the transmit status to know when the transmit is complete. This function will calculate the checksum byte and send it with the frame data.
| instance | LPUART instance |
| txBuff | source buffer containing 8-bit data chars to send |
| txSize | the number of bytes to send |
| lin_status_t LIN_GetTransmitStatus | ( | uint32_t | instance, |
| uint8_t * | bytesRemaining | ||
| ) |
The bytesRemaining shows number of bytes that still needed to transmit.
| instance | LPUART instance |
| bytesRemaining | Number of bytes still needed to transmit |
| lin_status_t LIN_ReceiveFrameDataBlocking | ( | uint32_t | instance, |
| uint8_t * | rxBuff, | ||
| uint8_t | rxSize, | ||
| uint32_t | timeoutMSec | ||
| ) |
This function will check the checksum byte. If the checksum is correct, it will receive the frame data. Blocking means that the function does not return until the reception is complete.
| instance | LPUART instance |
| rxBuff | buffer containing 8-bit received data |
| rxSize | the number of bytes to receive |
| timeoutMSec | timeout value in milli seconds |
| lin_status_t LIN_ReceiveFrameData | ( | uint32_t | instance, |
| uint8_t * | rxBuff, | ||
| uint8_t | rxSize | ||
| ) |
This function will check the checksum byte. If the checksum is correct, it will receive it with the frame data. Non-blocking means that the function returns immediately. The application has to get the receive status to know when the reception is complete.
| instance | LPUART instance |
| rxBuff | buffer containing 8-bit received data |
| rxSize | the number of bytes to receive |
| lin_status_t LIN_AbortTransferData | ( | uint32_t | instance | ) |
While performing a non-blocking transferring data, users can call this function to terminate immediately the transferring.
| instance | LPUART instance |
| lin_status_t LIN_GetReceiveStatus | ( | uint32_t | instance, |
| uint8_t * | bytesRemaining | ||
| ) |
This function return the current event ID, LIN_RX_BUSY while receiving and return LIN_SUCCESS, or timeout (LIN_TIMEOUT) when the reception is complete. The bytesRemaining shows number of bytes that still needed to receive.
| instance | LPUART instance |
| bytesRemaining | Number of bytes still needed to receive |
| lin_status_t LIN_GoToSleepMode | ( | uint32_t | instance | ) |
| instance | LPUART instance |
| lin_status_t LIN_GotoIdleState | ( | uint32_t | instance | ) |
| instance | LPUART instance |
| lin_status_t LIN_SendWakeupSignal | ( | uint32_t | instance | ) |
| instance | LPUART instance |
| lin_node_state_t LIN_GetCurrentNodeState | ( | uint32_t | instance | ) |
| instance | LPUART instance |
| void LIN_TimeoutService | ( | uint32_t | instance | ) |
User may initialize a timer (for example FTM) in Output Compare Mode with period of 500 micro seconds (recommended). In timer IRQ handler, call this function.
| instance | LPUART instance |
| void LIN_SetTimeoutCounter | ( | uint32_t | instance, |
| uint32_t | timeoutValue | ||
| ) |
| instance | LPUART instance |
| timeoutValue | Timeout Value to be set |
| lin_status_t LIN_MasterSendHeader | ( | uint32_t | instance, |
| uint8_t | id | ||
| ) |
This function sends LIN Break field, sync field then the ID with correct parity.
| instance | LPUART instance |
| id | Frame Identifier |
| lin_status_t LIN_EnableIRQ | ( | uint32_t | instance | ) |
| instance | LPUART instance |
| lin_status_t LIN_DisableIRQ | ( | uint32_t | instance | ) |
| instance | LPUART instance |
| void LIN_IRQHandler | ( | uint8_t | instance | ) |
| instance | LPUART instance |
| lin_status_t LIN_AutoBaudCapture | ( | uint32_t | instance | ) |
This function should only be used in Slave. The timer should be in mode input capture of both rising and falling edges. The timer input capture pin should be externally connected to RXD pin.
| instance | LPUART instance |
This function should only be used in Slave. The timer should be in mode input capture of both rising and falling edges. The timer input capture pin should be externally connected to RXD pin.
| instance | LPUART instance |
| uint8_t LIN_ProcessParity | ( | uint8_t | PID, |
| uint8_t | typeAction | ||
| ) |
If action is checking parity, the function returns ID value if parity bits are correct or 0xFF if parity bits are incorrect. If action is making parity bits, then from input value of ID, the function returns PID. This is not a public API as it is called by other API functions.
| PID | PID byte in case of checking parity bits or ID byte in case of making parity bits. |
| typeAction,: | 1 for Checking parity bits, 0 for making parity bits |
| uint8_t LIN_MakeChecksumByte | ( | const uint8_t * | buffer, |
| uint8_t | sizeBuffer, | ||
| uint8_t | PID | ||
| ) |
| buffer | Pointer to Tx buffer |
| sizeBuffer | Number of bytes that are contained in the buffer. |
| PID | Protected Identifier byte. |
| lin_status_t LIN_DRV_SetResponse | ( | uint8_t | instance, |
| uint8_t * | response_buff, | ||
| uint8_t | response_length, | ||
| uint8_t | max_frame_res_timeout | ||
| ) |
| instance | LPUART instance |
| response_buff | response message |
| response_length | length of response |
| max_frame_res_timeout | maximal timeout duration for message |
| lin_status_t LIN_DRV_RxResponse | ( | uint8_t | instance, |
| uint8_t * | response_buff, | ||
| uint8_t | response_length, | ||
| uint8_t | max_frame_res_timeout | ||
| ) |
| instance | LPUART instance |
| response_buff | response message |
| response_length | length of response |
| max_frame_res_timeout | maximal timeout duration for message |
| lin_status_t LIN_DRV_IgnoreResponse | ( | uint8_t | instance | ) |
| instance | LPUART instance |
| void LIN_DRV_CalculateBaudrate | ( | uint32_t | instance, |
| uint32_t | baudRate_Bps, | ||
| uint32_t | srcClock_Hz, | ||
| uint32_t * | osr, | ||
| uint16_t * | sbr | ||
| ) |
| instance | LPUART instance |
| instance | baudRate_Bps LPUART baudrate |
| instance | srcClock_Hz LPUART clock frequency |
| instance | osr LPUART baudrate OSR value, return value |
| instance | sbr LPUART baudrate SBR value, return value |
| void LIN_DRV_SetBaudrate | ( | uint32_t | instance, |
| uint32_t | osr, | ||
| uint16_t | sbr | ||
| ) |
| instance | LPUART instance |
| instance | osr LPUART baudrate OSR value |
| instance | sbr LPUART baudrate SBR value |
| lin_status_t LIN_DRV_Init | ( | uint32_t | instance, |
| lin_user_config_t * | linUserConfig, | ||
| lin_state_t * | linCurrentState | ||
| ) |
The caller provides memory for the driver state structures during initialization. The user must select the LIN Hardware Interface clock source in the application to initialize the LIN Hardware Interface.
| instance | LPUART instance |
| linUserConfig | user configuration structure of type lin_user_config_t |
| linCurrentState | pointer to the LIN Hardware Interface driver state structure |
| lin_status_t LIN_DRV_Deinit | ( | uint32_t | instance | ) |
| instance | LPUART instance |
| lin_callback_t LIN_DRV_InstallCallback | ( | uint32_t | instance, |
| lin_callback_t | function | ||
| ) |
| instance | LPUART instance. |
| function | the LIN receive callback function. |
| lin_status_t LIN_DRV_SendFrameDataBlocking | ( | uint32_t | instance, |
| const uint8_t * | txBuff, | ||
| uint8_t | txSize, | ||
| uint32_t | timeoutMSec | ||
| ) |
This function will calculate the checksum byte and send it with the frame data. Blocking means that the function does not return until the transmission is complete.
| instance | LIN instance |
| txBuff | source buffer containing 8-bit data chars to send |
| txSize | the number of bytes to send |
| timeoutMSec | timeout value in milli seconds |
| lin_status_t LIN_DRV_SendFrameData | ( | uint32_t | instance, |
| const uint8_t * | txBuff, | ||
| uint8_t | txSize | ||
| ) |
This enables an a-sync method for transmitting data. Non-blocking means that the function returns immediately. The application has to get the transmit status to know when the transmit is complete. This function will calculate the checksum byte and send it with the frame data.
| instance | LPUART instance |
| txBuff | source buffer containing 8-bit data chars to send |
| txSize | the number of bytes to send |
| lin_status_t LIN_DRV_GetTransmitStatus | ( | uint32_t | instance, |
| uint8_t * | bytesRemaining | ||
| ) |
The bytesRemaining shows number of bytes that still needed to transmit.
| instance | LIN instance |
| bytesRemaining | Number of bytes still needed to transmit |
| lin_status_t LIN_DRV_ReceiveFrameDataBlocking | ( | uint32_t | instance, |
| uint8_t * | rxBuff, | ||
| uint8_t | rxSize, | ||
| uint32_t | timeoutMSec | ||
| ) |
This function will check the checksum byte. If the checksum is correct, it will receive the frame data. Blocking means that the function does not return until the reception is complete.
| instance | LPUART instance |
| rxBuff | buffer containing 8-bit received data |
| rxSize | the number of bytes to receive |
| timeoutMSec | timeout value in milli seconds |
| lin_status_t LIN_DRV_ReceiveFrameData | ( | uint32_t | instance, |
| uint8_t * | rxBuff, | ||
| uint8_t | rxSize | ||
| ) |
This function will check the checksum byte. If the checksum is correct, it will receive it with the frame data. Non-blocking means that the function returns immediately. The application has to get the receive status to know when the reception is complete.
| instance | LPUART instance |
| rxBuff | buffer containing 8-bit received data |
| rxSize | the number of bytes to receive |
| lin_status_t LIN_DRV_AbortTransferData | ( | uint32_t | instance | ) |
While performing a non-blocking transferring data, users can call this function to terminate immediately the transferring.
| instance | LIN instance |
| lin_status_t LIN_DRV_GetReceiveStatus | ( | uint32_t | instance, |
| uint8_t * | bytesRemaining | ||
| ) |
This function return the current event ID, LIN_RX_BUSY while receiving and return LIN_SUCCESS, or timeout (LIN_TIMEOUT) when the reception is complete. The bytesRemaining shows number of bytes that still needed to receive.
| instance | LPUART instance |
| bytesRemaining | Number of bytes still needed to receive |
| lin_status_t LIN_DRV_GoToSleepMode | ( | uint32_t | instance | ) |
| instance | LPUART instance |
| lin_status_t LIN_DRV_GotoIdleState | ( | uint32_t | instance | ) |
| instance | LPUART instance |
| lin_status_t LIN_DRV_SendWakeupSignal | ( | uint32_t | instance | ) |
| instance | LPUART instance |
| lin_node_state_t LIN_DRV_GetCurrentNodeState | ( | uint32_t | instance | ) |
| instance | LPUART instance |
| void LIN_DRV_TimeoutService | ( | uint32_t | instance | ) |
User may initialize a timer (for example FTM) in Output Compare Mode with period of 500 micro seconds (recommended). In timer IRQ handler, call this function.
| instance | LPUART instance |
|
inlinestatic |
| instance | LPUART instance |
| timeoutValue | Timeout Value to be set |
| lin_status_t LIN_DRV_MasterSendHeader | ( | uint32_t | instance, |
| uint8_t | id | ||
| ) |
This function sends LIN Break field, sync field then the ID with correct parity.
| instance | LPUART instance |
| id | Frame Identifier |
| lin_status_t LIN_DRV_EnableIRQ | ( | uint32_t | instance | ) |
| instance | LPUART instance |
| lin_status_t LIN_DRV_DisableIRQ | ( | uint32_t | instance | ) |
| instance | LPUART instance |
| void LIN_DRV_IRQHandler | ( | uint8_t | instance | ) |
| instance | LPUART instance |
|
inlinestatic |
Adding this API is just for providing interface for LIN Stack.
| instance | LPUART instance |
|
inlinestatic |
This fucntion is the same with LIN_ProcessParity(). Adding this function is just to provide the interface for LIN Stack.
| PID | PID byte in case of checking parity bits or ID byte in case of making parity bits. |
| typeAction,: | 1 for Checking parity bits, 0 for making parity bits |
|
inlinestatic |
This function is the same with LIN_MakeChecksumByte(), And this API is just to provide interface for LIN Stack.
| buffer | Pointer to Tx buffer |
| sizeBuffer | Number of bytes that are contained in the buffer. |
| PID | Protected Identifier byte. |
| const uint8_t * lin_state_t::txBuff |
| uint8_t * lin_state_t::rxBuff |
| uint8_t lin_state_t::cntByte |
| volatile uint8_t lin_state_t::txSize |
| volatile uint8_t lin_state_t::rxSize |
| uint8_t lin_state_t::checkSum |
| volatile bool lin_state_t::isTxBusy |
| volatile bool lin_state_t::isRxBusy |
| volatile bool lin_state_t::isTxBlocking |
| volatile bool lin_state_t::isRxBlocking |
| lin_callback_t lin_state_t::Callback |
| volatile bool lin_state_t::txCompleted |
| LPUART_Type* const g_linLpuartBase[FSL_FEATURE_SOC_LPUART_COUNT] |
| lin_state_t* g_linStatePtr[FSL_FEATURE_SOC_LPUART_COUNT] |
Table to save LPUART state structure pointers
| LPUART_Type* const g_linLpuartBase[FSL_FEATURE_SOC_LPUART_COUNT] |