![]() |
MCUXpresso SDK API Reference Manual
Rev 2.12.0
NXP Semiconductors
|
Data Structures | |
| struct | lpspi_flash_driver_interface_t |
| Interface for the external flash driver via SPI NOR/EEPROM. More... | |
Macros | |
| #define | kROM_StatusGroup_LPSPI 4 |
| ROM Group number for LPSPI status codes. More... | |
Enumerations | |
| enum | { kStatus_ROM_LPSPI_Busy = MAKE_STATUS(kROM_StatusGroup_LPSPI, 0), kStatus_ROM_LPSPI_Error = MAKE_STATUS(kROM_StatusGroup_LPSPI, 1), kStatus_ROM_LPSPI_Idle = MAKE_STATUS(kROM_StatusGroup_LPSPI, 2), kStatus_ROM_LPSPI_OutOfRange = MAKE_STATUS(kROM_StatusGroup_LPSPI, 3) } |
| Status for the LPSPI driver. More... | |
| enum | { EepormCmd_GeneralRead = false, EepormCmd_FastRead = true } |
| The type of Read eeprom command. More... | |
| enum | eraseOptions_t { kSize_ErasePage = 0x1, kSize_Erase4K = 0x2 } |
| The length, given in bytes to be erased. More... | |
Functions | |
| status_t | SPI_EepromInit (uint32_t baudRate) |
| Initialize SPI NOR/EEPROM. More... | |
| status_t | SPI_EepromRead (uint8_t *dest, uint32_t length, uint32_t address, bool requestFastRead) |
| Read data via SPI NOR/EEPROM. More... | |
| status_t | SPI_EepromWrite (uint8_t *data, uint32_t length, uint32_t address) |
| Write data via SPI NOR/EEPROM. More... | |
| status_t | SPI_EepromErase (uint32_t address, eraseOptions_t option) |
| Erase data via SPI NOR/EEPROM. More... | |
| void | SPI_EepromFinalize (void) |
| De-initialize LPSPI. | |
| struct lpspi_flash_driver_interface_t |
| #define kROM_StatusGroup_LPSPI 4 |
| anonymous enum |
| anonymous enum |
| enum eraseOptions_t |
| status_t SPI_EepromInit | ( | uint32_t | baudRate | ) |
| baudRate | Config baudrate for SPI. |
| kStatus_Fail | EEPROM initialization failed. |
| kStatus_InvalidArgument | Invalid input parameter. |
| kStatus_ROM_LPSPI_Busy | LPSPI transfer is busy. |
| kStatus_Success | The eeprom is initialized successfully. |
| status_t SPI_EepromRead | ( | uint8_t * | dest, |
| uint32_t | length, | ||
| uint32_t | address, | ||
| bool | requestFastRead | ||
| ) |
| dest | A pointer to the buffer of data that is to be read from eeprom. |
| length | The length, given in bytes to be read. |
| address | The start address of the desired eeprom memory to be read. |
| requestFastRead | The type of Read eeprom command. FALSE: Use the general Read command to read eeprom TRUE: Use Fast Read command to read data from eeprom. |
| kStatus_Fail | Failed to read data from eeprom. |
| kStatus_Success | Read data from eeprom successfully. |
| kStatus_InvalidArgument | Invalid input parameter. |
| kStatus_ROM_LPSPI_Busy | LPSPI transfer is busy. |
| status_t SPI_EepromWrite | ( | uint8_t * | data, |
| uint32_t | length, | ||
| uint32_t | address | ||
| ) |
| data | A pointer to the source buffer of data that is to be programmed into the eeprom. |
| length | The length, given in bytes to be programmed. |
| address | The start address of the desired eeprom memory to be programed. |
| kStatus_Fail | Failed to write data to eeprom. |
| kStatus_Success | Successfully write data to eeprom. |
| kStatus_InvalidArgument | Invalid input parameter. |
| kStatus_ROM_LPSPI_Busy | LPSPI transfer is busy. |
| status_t SPI_EepromErase | ( | uint32_t | address, |
| eraseOptions_t | option | ||
| ) |
| address | The start address of the desired eeprom memory to be erased. |
| option | The length, given in bytes to be erased. |
| kStatus_Fail | Failed to erase data frome the eeprom. |
| kStatus_Success | Erase data from eeprom successfully. |
| kStatus_InvalidArgument | Invalid input parameter. |
| kStatus_ROM_LPSPI_Busy | LPSPI transfer is busy. |