| Enumerator |
|---|
| kSerialManager_UsbVirtualControllerKhci0 |
KHCI 0U.
|
| kSerialManager_UsbVirtualControllerKhci1 |
KHCI 1U, Currently, there are no platforms which have two KHCI IPs, this is reserved to be used in the future.
|
| kSerialManager_UsbVirtualControllerEhci0 |
EHCI 0U.
|
| kSerialManager_UsbVirtualControllerEhci1 |
EHCI 1U, Currently, there are no platforms which have two EHCI IPs, this is reserved to be used in the future.
|
| kSerialManager_UsbVirtualControllerLpcIp3511Fs0 |
LPC USB IP3511 FS controller 0.
|
| kSerialManager_UsbVirtualControllerLpcIp3511Fs1 |
LPC USB IP3511 FS controller 1, there are no platforms which have two IP3511 IPs, this is reserved to be used in the future.
|
| kSerialManager_UsbVirtualControllerLpcIp3511Hs0 |
LPC USB IP3511 HS controller 0.
|
| kSerialManager_UsbVirtualControllerLpcIp3511Hs1 |
LPC USB IP3511 HS controller 1, there are no platforms which have two IP3511 IPs, this is reserved to be used in the future.
|
| kSerialManager_UsbVirtualControllerOhci0 |
OHCI 0U.
|
| kSerialManager_UsbVirtualControllerOhci1 |
OHCI 1U, Currently, there are no platforms which have two OHCI IPs, this is reserved to be used in the future.
|
| kSerialManager_UsbVirtualControllerIp3516Hs0 |
IP3516HS 0U.
|
| kSerialManager_UsbVirtualControllerIp3516Hs1 |
IP3516HS 1U, Currently, there are no platforms which have two IP3516HS IPs, this is reserved to be used in the future.
|