![]() |
MCUXpresso SDK API Reference Manual
Rev 2.12.0
NXP Semiconductors
|
This section includes Power Mode macros, System Constraints macros, and Wakeup source macros. More...
This document consists of sections titled with Framework Overview, Data Structures, Enumerations, Functions, etc., each with an overview list and detailed documentation. It is recommended to read the Framework Overview first for it includes a comprehensive description of the framework. Other sections give detailed information for APIs, enums, macros, etc., for your further reference.
Macros | |
| #define | AT_ALWAYS_ON_DATA(var) var |
Framework OverviewThe power manager framework manages the transition of both active-to-sleep and sleep-to-active states of the MCU. More... | |
System basic resource constraints definitions. | |
| #define | PM_RESC_CORE_CLK_ON PM_ENCODE_RESC(PM_RESOURCE_FULL_ON, 13U) |
| Set the constraint that CORE clock should be ON. | |
| #define | PM_RESC_BUS_SYS_CLK_ON PM_ENCODE_RESC(PM_RESOURCE_FULL_ON, 12U) |
| Set the constraint that BUS and SYSTEM clock should be ON. | |
| #define | PM_RESC_CTCM0_ACTIVE PM_ENCODE_RESC(PM_RESOURCE_FULL_ON, 0U) |
| Set the constraint that CTCM0 should in Active mode. | |
| #define | PM_RESC_CTCM0_DEEPSLEEP PM_ENCODE_RESC(PM_RESOURCE_PARTABLE_ON1, 0U) |
| Set the constraint that CTCM0 should in DEEPSLEEP mode. | |
| #define | PM_RESC_CTCM1_ACTIVE PM_ENCODE_RESC(PM_RESOURCE_FULL_ON, 1U) |
| Set the constraint that CTCM1 should in Active mode. | |
| #define | PM_RESC_CTCM1_DEEPSLEEP PM_ENCODE_RESC(PM_RESOURCE_PARTABLE_ON1, 1U) |
| Set the constraint that CTCM1 should in DEEPSLEEP mode. | |
| #define | PM_RESC_STCM0_ACTIVE PM_ENCODE_RESC(PM_RESOURCE_FULL_ON, 2U) |
| Set the constraint that STCM0 should in Active mode. | |
| #define | PM_RESC_STCM0_DEEPSLEEP PM_ENCODE_RESC(PM_RESOURCE_PARTABLE_ON1, 2U) |
| Set the constraint that STCM0 should in DEEPSLEEP mode. | |
| #define | PM_RESC_STCM1_ACTIVE PM_ENCODE_RESC(PM_RESOURCE_FULL_ON, 3U) |
| Set the constraint that STCM1 should in Active mode. | |
| #define | PM_RESC_STCM1_DEEPSLEEP PM_ENCODE_RESC(PM_RESOURCE_PARTABLE_ON1, 3U) |
| Set the constraint that STCM1 should in DEEPSLEEP mode. | |
| #define | PM_RESC_STCM2_ACTIVE PM_ENCODE_RESC(PM_RESOURCE_FULL_ON, 4U) |
| Set the constraint that STCM2 should in Active mode. | |
| #define | PM_RESC_STCM2_DEEPSLEEP PM_ENCODE_RESC(PM_RESOURCE_PARTABLE_ON1, 4U) |
| Set the constraint that STCM2 should in DEEPSLEEP mode. | |
| #define | PM_RESC_STCM3_ACTIVE PM_ENCODE_RESC(PM_RESOURCE_FULL_ON, 5U) |
| Set the constraint that STCM3 should in Active mode. | |
| #define | PM_RESC_STCM3_DEEPSLEEP PM_ENCODE_RESC(PM_RESOURCE_PARTABLE_ON1, 5U) |
| Set the constraint that STCM3 should in DEEPSLEEP mode. | |
| #define | PM_RESC_STCM4_ACTIVE PM_ENCODE_RESC(PM_RESOURCE_FULL_ON, 6U) |
| Set the constraint that STCM4 should in Active mode. | |
| #define | PM_RESC_STCM4_DEEPSLEEP PM_ENCODE_RESC(PM_RESOURCE_PARTABLE_ON1, 6U) |
| Set the constraint that STCM4 should in DEEPSLEEP mode. | |
| #define | PM_RESC_FRO_192M_ON PM_ENCODE_RESC(PM_RESOURCE_FULL_ON, 7U) |
| Set the constraint that FRO_192M should be ON. | |
| #define | PM_RESC_FRO_6M_ON PM_ENCODE_RESC(PM_RESOURCE_FULL_ON, 8U) |
| Set the constraint that FRO_6M should be ON. | |
| #define | PM_RESC_MAIN_PD_PERI_OPERATIONAL PM_ENCODE_RESC(PM_RESOURCE_FULL_ON, 11U) |
| Set the constraint that peripherals in CORE_MAIN power domain still be operational. | |
| #define | PM_RESC_MAIN_PD_PERI_STATE_RETENTION PM_ENCODE_RESC(PM_RESOURCE_FULL_ON, 10U) |
| Set the constraint that peripherals in CORE_MAIN power domain are state retention, that means CORE_MAIN power domain can not be powered off. | |
| #define | PM_RESC_WAKE_PD_PERI_ACTIVE PM_ENCODE_RESC(PM_RESOURCE_FULL_ON, 9U) |
| Set the constraint that peripherals in CORE_WAKE power domain are active. | |
| #define | PM_RESC_WAKE_PD_PERI_OPERATIONAL PM_ENCODE_RESC(PM_RESOURCE_PARTABLE_ON2, 9U) |
| Set the constraint that peripherals in CORE_WAKE power domain are operational. | |
| #define | PM_RESC_WAKE_PD_PERI_STATE_RETENTION PM_ENCODE_RESC(PM_RESOURCE_PARTABLE_ON1, 9U) |
| Set the constraint that peripherals in CORE_WAKE power domain are state retention, that means CORE_WAKE power domain can not be powered off. | |
System Wakeup source definitions. | |
| #define | PM_WSID_PTA0_RISING_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 0UL, PORTA_IRQn, 1UL) |
| Enable PTA0 as a wakeup pin, detect on rising edge. | |
| #define | PM_WSID_PTA0_Falling_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 0UL, PORTA_IRQn, 2UL) |
| Enable PTA0 as a wakeup pin, detect on falling edge. | |
| #define | PM_WSID_PTA0_ANY_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 0UL, PORTA_IRQn, 3UL) |
| Enable PTA0 as a wakeup pin, detect on any edge. | |
| #define | PM_WSID_PTA2_RISING_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 1UL, PORTA_IRQn, 1UL) |
| Enable PTA2 as a wakeup pin, detect on rising edge. | |
| #define | PM_WSID_PTA2_FALLING_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 1UL, PORTA_IRQn, 2UL) |
| Enable PTA2 as a wakeup pin, detect on falling edge. | |
| #define | PM_WSID_PTA2_ANY_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 1UL, PORTA_IRQn, 3UL) |
| Enable PTA2 as a wakeup pin, detect on any edge. | |
| #define | PM_WSID_PTA4_RISING_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 2UL, PORTA_IRQn, 1UL) |
| Enable PTA4 as a wakeup pin, detect on rising edge. | |
| #define | PM_WSID_PTA4_FALLING_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 2UL, PORTA_IRQn, 2UL) |
| Enable PTA4 as a wakeup pin, detect on falling edge. | |
| #define | PM_WSID_PTA4_ANY_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 2UL, PORTA_IRQn, 3UL) |
| Enable PTA4 as a wakeup pin, detect on any edge. | |
| #define | PM_WSID_PTA17_RISING_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 3UL, PORTA_IRQn, 1UL) |
| Enable PTA17 as a wakeup pin, detect on rising edge. | |
| #define | PM_WSID_PTA17_FALLING_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 3UL, PORTA_IRQn, 2UL) |
| Enable PTA17 as a wakeup pin, detect on falling edge. | |
| #define | PM_WSID_PTA17_ANY_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 3UL, PORTA_IRQn, 3UL) |
| Enable PTA17 as a wakeup pin, detect on any edge. | |
| #define | PM_WSID_PTA19_RISING_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 4UL, PORTA_IRQn, 1UL) |
| Enable PTA19 as a wakeup pin, detect on rising edge. | |
| #define | PM_WSID_PTA19_FALLING_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 4UL, PORTA_IRQn, 2UL) |
| Enable PTA19 as a wakeup pin, detect on falling edge. | |
| #define | PM_WSID_PTA19_ANY_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 4UL, PORTA_IRQn, 3UL) |
| Enable PTA19 as a wakeup pin, detect on any edge. | |
| #define | PM_WSID_PTA21_RISING_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 5UL, PORTA_IRQn, 1UL) |
| Enable PTA21 as a wakeup pin, detect on rising edge. | |
| #define | PM_WSID_PTA21_FALLING_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 5UL, PORTA_IRQn, 2UL) |
| Enable PTA21 as a wakeup pin, detect on falling edge. | |
| #define | PM_WSID_PTA21_ANY_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 5UL, PORTA_IRQn, 3UL) |
| Enable PTA21 as a wakeup pin, detect on any edge. | |
| #define | PM_WSID_PTA22_RISING_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 6UL, PORTA_IRQn, 1UL) |
| Enable PTA22 as a wakeup pin, detect on rising edge. | |
| #define | PM_WSID_PTA22_FALLING_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 6UL, PORTA_IRQn, 2UL) |
| Enable PTA22 as a wakeup pin, detect on falling edge. | |
| #define | PM_WSID_PTA22_ANY_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 6UL, PORTA_IRQn, 3UL) |
| Enable PTA22 as a wakeup pin, detect on any edge. | |
| #define | PM_WSID_PTC0_RISING_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 7UL, PORTC_IRQn, 1UL) |
| Enable PTC0 as a wakeup pin, detect on rising edge. | |
| #define | PM_WSID_PTC0_FALLING_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 7UL, PORTC_IRQn, 2UL) |
| Enable PTC0 as a wakeup pin, detect on falling edge. | |
| #define | PM_WSID_PTC0_ANY_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 7UL, PORTC_IRQn, 3UL) |
| Enable PTC0 as a wakeup pin, detect on any edge. | |
| #define | PM_WSID_PTC1_RISING_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 8UL, PORTC_IRQn, 1UL) |
| Enable PTC1 as a wakeup pin, detect on rising edge. | |
| #define | PM_WSID_PTC1_FALLING_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 8UL, PORTC_IRQn, 2UL) |
| Enable PTC1 as a wakeup pin, detect on falling edge. | |
| #define | PM_WSID_PTC1_ANY_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 8UL, PORTC_IRQn, 3UL) |
| Enable PTC1 as a wakeup pin, detect on any edge. | |
| #define | PM_WSID_PTC2_RISING_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 9UL, PORTC_IRQn, 1UL) |
| Enable PTC2 as a wakeup pin, detect on rising edge. | |
| #define | PM_WSID_PTC2_FALLING_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 9UL, PORTC_IRQn, 2UL) |
| Enable PTC2 as a wakeup pin, detect on falling edge. | |
| #define | PM_WSID_PTC2_ANY_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 9UL, PORTC_IRQn, 3UL) |
| Enable PTC2 as a wakeup pin, detect on any edge. | |
| #define | PM_WSID_PTC4_RISING_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 10UL, PORTC_IRQn, 1UL) |
| Enable PTC4 as a wakeup pin, detect on rising edge. | |
| #define | PM_WSID_PTC4_FALLING_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 10UL, PORTC_IRQn, 2UL) |
| Enable PTC4 as a wakeup pin, detect on falling edge. | |
| #define | PM_WSID_PTC4_ANY_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 10UL, PORTC_IRQn, 3UL) |
| Enable PTC4 as a wakeup pin, detect on any edge. | |
| #define | PM_WSID_PTC6_RISING_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 11UL, PORTC_IRQn, 1UL) |
| Enable PTC6 as a wakeup pin, detect on rising edge. | |
| #define | PM_WSID_PTC6_FALLING_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 11UL, PORTC_IRQn, 2UL) |
| Enable PTC6 as a wakeup pin, detect on falling edge. | |
| #define | PM_WSID_PTC6_ANY_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 11UL, PORTC_IRQn, 3UL) |
| Enable PTC6 as a wakeup pin, detect on any edge. | |
| #define | PM_WSID_PTC7_RISING_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 12UL, PORTC_IRQn, 1UL) |
| Enable PTC7 as a wakeup pin, detect on rising edge. | |
| #define | PM_WSID_PTC7_FALLING_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 12UL, PORTC_IRQn, 2UL) |
| Enable PTC7 as a wakeup pin, detect on falling edge. | |
| #define | PM_WSID_PTC7_ANY_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 12UL, PORTC_IRQns, 3UL) |
| Enable PTC7 as a wakeup pin, detect on any edge. | |
| #define | PM_WSID_PTB0_RISING_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 13UL, PORTB_IRQn, 1UL) |
| Enable PTB0 as a wakeup pin, detect on rising edge. | |
| #define | PM_WSID_PTB0_FALLING_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 13UL, PORTB_IRQn, 2UL) |
| Enable PTB0 as a wakeup pin, detect on falling edge. | |
| #define | PM_WSID_PTB0_ANY_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 13UL, PORTB_IRQn, 3UL) |
| Enable PTB0 as a wakeup pin, detect on any edge. | |
| #define | PM_WSID_PTB3_RISING_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 14UL, PORTB_IRQn, 1UL) |
| Enable PTB3 as a wakeup pin, detect on rising edge. | |
| #define | PM_WSID_PTB3_FALLING_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 14UL, PORTB_IRQn, 2UL) |
| Enable PTB3 as a wakeup pin, detect on falling edge. | |
| #define | PM_WSID_PTB3_ANY_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 14UL, PORTB_IRQn, 3UL) |
| Enable PTB3 as a wakeup pin, detect on any edge. | |
| #define | PM_WSID_PTB4_RISING_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 15UL, PORTB_IRQn, 1UL) |
| Enable PTB4 as a wakeup pin, detect on rising edge. | |
| #define | PM_WSID_PTB4_FALLING_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 15UL, PORTB_IRQn, 2UL) |
| Enable PTB4 as a wakeup pin, detect on falling edge. | |
| #define | PM_WSID_PTB4_ANY_EDGE PM_ENCODE_WAKEUP_SOURCE_ID(0UL, 15UL, PORTB_IRQn, 3UL) |
| Enable PTB4 as a wakeup pin, detect on any edge. | |
| #define | PM_WSID_LPTMR0 PM_ENCODE_WAKEUP_SOURCE_ID(1UL, 0UL, LPTMR0_IRQn, 0UL) |
| Enable LPTMR0 as a wakeup source. | |
| #define | PM_WSID_LPTMR1 PM_ENCODE_WAKEUP_SOURCE_ID(1UL, 0UL, LPTMR1_IRQn, 0UL) |
| Enable LPTMR1 as a wakeup source. | |
| #define | PM_WSID_GPIOD_LOW PM_ENCODE_WAKEUP_SOURCE_ID(1UL, 1UL, GPIOD_INT0_IRQn, 0UL) |
| Enable GPIOD Low pins as wakeup source. | |
| #define | PM_WSID_GPIOD_HIGH PM_ENCODE_WAKEUP_SOURCE_ID(1UL, 2UL, GPIOD_INT1_IRQn, 0UL) |
| Enable GPIOD High pins as wakeup source. | |
| #define | PM_WSID_WFSPSD PM_ENCODE_WAKEUP_SOURCE_ID(1UL, 4UL, VBAT_IRQn, 0UL) |
| Enable VBAT module as wakeup source. | |
| #define | PM_WSID_RTC_ALARM PM_ENCODE_WAKEUP_SOURCE_ID(1UL, 6UL, RTC_Alarm_IRQn, 0UL) |
| Enable RTC Alarm as wakeup source. | |
| #define | PM_WSID_RTC_SECOND PM_ENCODE_WAKEUP_SOURCE_ID(1UL, 7UL, RTC_Second_IRQn, 0UL) |
| Enable RTC Second as wakeup source. | |
| #define AT_ALWAYS_ON_DATA | ( | var | ) | var |
It provides the upper layer software the ability to set and release constraints of the hardware basic resources(such as clock, power, ram, etc.) and the ability to register callback functions to be invoked before entering/after exiting the sleep mode. In addition, the upper layer software can register the wakeup source service function to be executed if related wakeup source occurs.
+-----------------------------------------------------------------+
| Application Software |
+-----------------------------------------------------------------+
+-----------------------------------------------------------------+
| Stacks and Components |
+-----------------------------------------------------------------+
+-----------------------------------------------------------------+
| Power Manager Framework |
+-----------------------------------------------------------------+
+---------------+ +---------------+ +-----------------------+
| Power Drivers | | Clock Drivers | | Wakeup Source Drivers |
+---------------+ +---------------+ +-----------------------+
As shown above, the power manager framework safely manages the transitions to and from power saving states by using MCUXpresso SDK drivers, and the upper layer software only need to use the APIs of power manager framework. Different MCUs have the same top-level APIs, concepts and conventions.
The power manager framework consists of four modules: policy module, sequencer module, wakeup source manager module, and notification module.
To make the power manager framework adapts to different MCU families, the power manager framework adopts a layer-designed idea, extracting common parts as the pm_core level, and separating device-related parts as the pm_device level. In details, the pm_core level contains policy module, wakeup source manager module, and notification module. The pm_device level contains sequencer module.