![]() |
MCUXpresso SDK API Reference Manual
Rev 2.12.1
NXP Semiconductors
|
Data Structures | |
| struct | IMU_Hdr_t |
| IMU message header structure. More... | |
| struct | IMU_Msg_t |
| IMU message structure. More... | |
| struct | IMU_Msg_Wrapper_long_t |
| IMU message wrapper 1. More... | |
| struct | IMU_Msg_Wrapper_short_t |
| IMU message wrapper 2. More... | |
| struct | rpmsg_std_hdr |
| Common header for all rpmsg messages. More... | |
| struct | rpmsg_std_msg |
| Common message structure. More... | |
| struct | hal_rpmsg_state_t |
| rpmsg state structure. More... | |
| struct | hal_rpmsg_ept_buf_t |
| rpmsg ept buf structure. More... | |
| struct | IMU_WLAN_TXQ_CTRL_st |
| IMU WLAN Tx buffer control structure. More... | |
| struct | RPMSG_TXQ_CTRL_st |
| RPMSG Tx buffer control structure. More... | |
| struct | hal_imu_handle_t |
| imu handle structure. More... | |
Macros | |
| #define | IRQ_IMU_CPU13 WL_MCI_WAKEUP0_IRQn |
| IRQ index should come from board level definition. More... | |
| #define | IMU_PAYLOAD_SIZE 8 |
| IMU message payload size. More... | |
| #define | IS_WLAN_TXBQ_EMPTY(q) ((q)->writeIndex == (q)->readIndex) |
| Checks whether a tx buffer queue is empty. | |
| #define | IS_WLAN_TXBQ_FULL(q) ((((q)->writeIndex & (1U<<31)) != ((q)->readIndex & (1U<<31))) && (((q)->writeIndex & IMU_TXQ_ENTRY_MASK) == ((q)->readIndex & IMU_TXQ_ENTRY_MASK))) |
| Checks whether a tx buffer queue is full. | |
| #define | INCR_WLAN_TXBQ_WR_INDEX(q, n) |
| Increments write pointer. | |
| #define | INCR_WLAN_TXBQ_RD_INDEX(q, n) |
| Increments read pointer. | |
| #define | IS_RPMSG_TXBQ_EMPTY(q) ((q)->writeIndex == (q)->readIndex) |
| Checks whether a tx buffer queue is empty. | |
| #define | IS_RPMSG_TXBQ_FULL(q) ((((q)->writeIndex & (1U<<31)) != ((q)->readIndex & (1U<<31))) && (((q)->writeIndex & RPMSG_TXQ_ENTRY_MASK) == ((q)->readIndex & RPMSG_TXQ_ENTRY_MASK))) |
| Checks whether a tx buffer queue is full. | |
| #define | INCR_RPMSG_TXBQ_WR_INDEX(q, n) |
| Increments write pointer. | |
| #define | INCR_RPMSG_TXBQ_RD_INDEX(q, n) |
| Increments read pointer. | |
Enumerations | |
| enum | imu_init_state_t |
| IMU initialization state. More... | |
| enum | imu_msg_type_t |
| RPMSG type. More... | |
| enum | imu_ctrl_msg_subtype_t |
| RPMSG control message subtype. More... | |
Functions | |
| hal_rpmsg_status_t | HAL_ImuAddWlanTxPacket (uint8_t imuLink, uint8_t *txBuf, uint32_t length) |
| Add wlan Tx packet for sending multiple Tx packets within one message. More... | |
| hal_rpmsg_status_t | HAL_ImuInstallCallback (uint8_t imuLink, imu_callback_t callback, uint8_t type) |
| Install wlan callback. More... | |
| hal_rpmsg_status_t | HAL_ImuSendCommand (uint8_t imuLink, uint8_t *cmdBuf, uint32_t length) |
| Send wlan command packet. More... | |
| hal_rpmsg_status_t | HAL_ImuSendTxData (uint8_t imuLink, uint8_t *txBuf, uint32_t length) |
| Add wlan Tx packet for sending one Tx packet within one message. More... | |
| hal_rpmsg_status_t | HAL_ImuSendMultiTxData (uint8_t imuLink) |
| Send multiple Tx packets within one message. More... | |
| hal_rpmsg_status_t | HAL_ImuNoCopySendEvent (uint8_t imuLink, uint8_t *eventBuf) |
| Send wlan event packet. More... | |
| hal_rpmsg_status_t | HAL_ImuNoCopySendCommandResponse (uint8_t imuLink, uint8_t *cmdRspBuf) |
| Send wlan command response packet. More... | |
| hal_rpmsg_status_t | HAL_ImuNoCopySendRxData (uint8_t imuLink, uint8_t *rxBuf) |
| Send wlan Rx packet. More... | |
| hal_rpmsg_status_t | HAL_ImuLinkIsUp (uint8_t imuLink) |
| Check if IMU link is up. More... | |
| hal_rpmsg_status_t | HAL_ImuInit (imu_link_t link) |
| Start IMU link. More... | |
| hal_rpmsg_status_t | HAL_ImuDeinit (imu_link_t link, uint32_t flag) |
| Stop IMU link. More... | |
| hal_rpmsg_status_t | HAL_ImuAddWlanRxPacket (uint8_t imuLink, uint8_t *rxBuf) |
| Add wlan Rx packet for sending multiple Rx packets within one message. More... | |
| hal_rpmsg_status_t | HAL_ImuSendMultiRxData (uint8_t imuLink) |
| Send multiple Rx packets within one message. More... | |
| hal_rpmsg_status_t | HAL_ImuReturnAllTxBuf (imu_link_t link) |
| Return all tx buffer. More... | |
| hal_rpmsg_status_t | HAL_ImuReceive (uint8_t imuLink) |
| Receive IMU message. More... | |
| struct IMU_Hdr_t |
| struct IMU_Msg_t |
| struct IMU_Msg_Wrapper_long_t |
| struct IMU_Msg_Wrapper_short_t |
| struct rpmsg_std_hdr |
| struct rpmsg_std_msg |
Contains the header and the payload.
Data Fields | |
| struct rpmsg_std_hdr | hdr |
| RPMsg message header. | |
| uint32_t | data |
| bytes of message payload data | |
| struct hal_rpmsg_state_t |
| struct hal_rpmsg_ept_buf_t |
| struct IMU_WLAN_TXQ_CTRL_st |
| struct RPMSG_TXQ_CTRL_st |
| struct hal_imu_handle_t |
Data Fields | |
| uint8_t | imuLink |
| Word 0. | |
| bool | cmd_buffer_available |
| Word 1. | |
| uint32_t * | cmd_buffer |
| Word 2. | |
| IMU_WLAN_TXQ_CTRL_st | wlanTxqCtl |
| Word 3. | |
| uint32_t | imuMsgBuf [IMU_PAYLOAD_SIZE] |
| Word 37. | |
| LIST_ELEM_st | eptList |
| Word 45. | |
| RPMSG_TXQ_CTRL_st | rpmsgTxqCtl |
| Word 47. | |
| imu_callback_t | imuHandler [IMU_MSG_MAX] |
| Word 57. | |
| #define IRQ_IMU_CPU13 WL_MCI_WAKEUP0_IRQn |
Remove following definition after RPMSG code integration.
| #define IMU_PAYLOAD_SIZE 8 |
| enum imu_init_state_t |
| enum imu_msg_type_t |
| hal_rpmsg_status_t HAL_ImuAddWlanTxPacket | ( | uint8_t | imuLink, |
| uint8_t * | txBuf, | ||
| uint32_t | length | ||
| ) |
This function is used to add a wlan Tx packet for IMU_MSG_MULTI_TX_DATA.
| imuLink | IMU link ID. |
| txBuf | Tx buffer to be sent. |
| length | Length of Tx data. |
| kStatus_HAL_RpmsgSuccess | or kStatus_HAL_RpmsgError. |
| hal_rpmsg_status_t HAL_ImuInstallCallback | ( | uint8_t | imuLink, |
| imu_callback_t | callback, | ||
| uint8_t | type | ||
| ) |
This function is used to imstall wlan callback
| imuLink | IMU link ID. |
| callback | Callback to be installed. |
| type | Callback type. |
| kStatus_HAL_RpmsgSuccess | or kStatus_HAL_RpmsgError. |
| hal_rpmsg_status_t HAL_ImuSendCommand | ( | uint8_t | imuLink, |
| uint8_t * | cmdBuf, | ||
| uint32_t | length | ||
| ) |
This function is used to send wlan command packet
| imuLink | IMU link ID. |
| cmdBuf | Command buffer to be sent. |
| length | Length of command data. |
| kStatus_HAL_RpmsgSuccess | or kStatus_HAL_RpmsgError. |
| hal_rpmsg_status_t HAL_ImuSendTxData | ( | uint8_t | imuLink, |
| uint8_t * | txBuf, | ||
| uint32_t | length | ||
| ) |
This function is used to send a wlan Tx packet.
| imuLink | IMU link ID. |
| txBuf | Tx buffer to be sent. |
| length | Length of Tx data. |
| kStatus_HAL_RpmsgSuccess | or kStatus_HAL_RpmsgError. |
| hal_rpmsg_status_t HAL_ImuSendMultiTxData | ( | uint8_t | imuLink | ) |
This function is used to send multiple wlan Tx packets within one IMU message, which have been added by HAL_ImuAddWlanTxPacket already.
| imuLink | IMU link ID. |
| kStatus_HAL_RpmsgSuccess | or kStatus_HAL_RpmsgError. |
| hal_rpmsg_status_t HAL_ImuNoCopySendEvent | ( | uint8_t | imuLink, |
| uint8_t * | eventBuf | ||
| ) |
This function is used to send wlan event packet. Event buffer is already in SHMEM, so data copy is not required.
| imuLink | IMU link ID. |
| eventBuf | Command buffer to be sent. |
| kStatus_HAL_RpmsgSuccess | or kStatus_HAL_RpmsgError. |
| hal_rpmsg_status_t HAL_ImuNoCopySendCommandResponse | ( | uint8_t | imuLink, |
| uint8_t * | cmdRspBuf | ||
| ) |
This function is used to send wlan command response packet. Command response buffer is already in SHMEM, so data copy is not required.
| imuLink | IMU link ID. |
| cmdRspBuf | Command response buffer to be sent. |
| kStatus_HAL_RpmsgSuccess | or kStatus_HAL_RpmsgError. |
| hal_rpmsg_status_t HAL_ImuNoCopySendRxData | ( | uint8_t | imuLink, |
| uint8_t * | rxBuf | ||
| ) |
This function is used to send wlan Rx packet. Rx buffer is already in SHMEM, so data copy is not required.
| imuLink | IMU link ID. |
| rxBuf | Rx buffer to be sent. |
| kStatus_HAL_RpmsgSuccess | or kStatus_HAL_RpmsgError. |
| hal_rpmsg_status_t HAL_ImuLinkIsUp | ( | uint8_t | imuLink | ) |
This function is used to check if IMU link is up.
| imuLink | IMU link ID. |
| kStatus_HAL_RpmsgSuccess | for IMU link up or kStatus_HAL_RpmsgError for IMU link not up. |
| hal_rpmsg_status_t HAL_ImuInit | ( | imu_link_t | link | ) |
This function is used to start specified IMU link.
| imuLink | IMU link ID. |
| kStatus_HAL_RpmsgSuccess | or kStatus_HAL_RpmsgError. |
| hal_rpmsg_status_t HAL_ImuDeinit | ( | imu_link_t | link, |
| uint32_t | flag | ||
| ) |
This function is used to stop specified IMU link.
| imuLink | IMU link ID. |
| flag | flag with bits to control. flag bit0: control if need send imu msg to fw (imu tx return /imu shutdown) flag bit1: control if need destroy ImuTask and ImuQFlagsRef |
| kStatus_HAL_RpmsgSuccess | or kStatus_HAL_RpmsgError. |
| hal_rpmsg_status_t HAL_ImuAddWlanRxPacket | ( | uint8_t | imuLink, |
| uint8_t * | rxBuf | ||
| ) |
This function is used to add a wlan Rx packet for IMU_MSG_MULTI_RX_DATA.
| imuLink | IMU link ID. |
| rxBuf | Rx buffer to be sent. |
| kStatus_HAL_RpmsgSuccess | or kStatus_HAL_RpmsgError. |
| hal_rpmsg_status_t HAL_ImuSendMultiRxData | ( | uint8_t | imuLink | ) |
This function is used to send multiple wlan Rx packets within one IMU message, which have been added by HAL_ImuAddWlanRxPacket already.
| imuLink | IMU link ID. |
| kStatus_HAL_RpmsgSuccess | or kStatus_HAL_RpmsgError. |
| hal_rpmsg_status_t HAL_ImuReturnAllTxBuf | ( | imu_link_t | link | ) |
This function is used to return all tx buffer to CPU1.
| imuLink | IMU link ID. |
| kStatus_HAL_RpmsgSuccess | or kStatus_HAL_RpmsgError. |
| hal_rpmsg_status_t HAL_ImuReceive | ( | uint8_t | imuLink | ) |
This function is used to receive and process IMU message
| imuLink | IMU link ID. |
| kStatus_HAL_RpmsgSuccess | or kStatus_HAL_RpmsgError. |