MCUXpresso SDK API Reference Manual  Rev 2.12.1
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages

Overview

The MCUXpresso SDK provides a peripheral driver for the Low Power UART (LPUART) module of MCUXpresso SDK devices.

Typical use case

LPUART Operation

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/lpuart

Data Structures

struct  lpuart_config_t
 LPUART configuration structure. More...
 
struct  lpuart_transfer_t
 LPUART transfer structure. More...
 
struct  lpuart_handle_t
 LPUART handle structure. More...
 

Macros

#define UART_RETRY_TIMES   0U /* Defining to zero means to keep waiting for the flag until it is assert/deassert. */
 Retry times for waiting flag. More...
 

Typedefs

typedef void(* lpuart_transfer_callback_t )(LPUART_Type *base, lpuart_handle_t *handle, status_t status, void *userData)
 LPUART transfer callback function. More...
 

Enumerations

enum  {
  kStatus_LPUART_TxBusy = MAKE_STATUS(kStatusGroup_LPUART, 0),
  kStatus_LPUART_RxBusy = MAKE_STATUS(kStatusGroup_LPUART, 1),
  kStatus_LPUART_TxIdle = MAKE_STATUS(kStatusGroup_LPUART, 2),
  kStatus_LPUART_RxIdle = MAKE_STATUS(kStatusGroup_LPUART, 3),
  kStatus_LPUART_TxWatermarkTooLarge = MAKE_STATUS(kStatusGroup_LPUART, 4),
  kStatus_LPUART_RxWatermarkTooLarge = MAKE_STATUS(kStatusGroup_LPUART, 5),
  kStatus_LPUART_FlagCannotClearManually = MAKE_STATUS(kStatusGroup_LPUART, 6),
  kStatus_LPUART_Error = MAKE_STATUS(kStatusGroup_LPUART, 7),
  kStatus_LPUART_RxRingBufferOverrun,
  kStatus_LPUART_RxHardwareOverrun = MAKE_STATUS(kStatusGroup_LPUART, 9),
  kStatus_LPUART_NoiseError = MAKE_STATUS(kStatusGroup_LPUART, 10),
  kStatus_LPUART_FramingError = MAKE_STATUS(kStatusGroup_LPUART, 11),
  kStatus_LPUART_ParityError = MAKE_STATUS(kStatusGroup_LPUART, 12),
  kStatus_LPUART_BaudrateNotSupport,
  kStatus_LPUART_IdleLineDetected = MAKE_STATUS(kStatusGroup_LPUART, 14),
  kStatus_LPUART_Timeout = MAKE_STATUS(kStatusGroup_LPUART, 15)
}
 Error codes for the LPUART driver. More...
 
enum  lpuart_parity_mode_t {
  kLPUART_ParityDisabled = 0x0U,
  kLPUART_ParityEven = 0x2U,
  kLPUART_ParityOdd = 0x3U
}
 LPUART parity mode. More...
 
enum  lpuart_data_bits_t {
  kLPUART_EightDataBits = 0x0U,
  kLPUART_SevenDataBits = 0x1U
}
 LPUART data bits count. More...
 
enum  lpuart_stop_bit_count_t {
  kLPUART_OneStopBit = 0U,
  kLPUART_TwoStopBit = 1U
}
 LPUART stop bit count. More...
 
enum  lpuart_transmit_cts_source_t {
  kLPUART_CtsSourcePin = 0U,
  kLPUART_CtsSourceMatchResult = 1U
}
 LPUART transmit CTS source. More...
 
enum  lpuart_transmit_cts_config_t {
  kLPUART_CtsSampleAtStart = 0U,
  kLPUART_CtsSampleAtIdle = 1U
}
 LPUART transmit CTS configure. More...
 
enum  lpuart_idle_type_select_t {
  kLPUART_IdleTypeStartBit = 0U,
  kLPUART_IdleTypeStopBit = 1U
}
 LPUART idle flag type defines when the receiver starts counting. More...
 
enum  lpuart_idle_config_t {
  kLPUART_IdleCharacter1 = 0U,
  kLPUART_IdleCharacter2 = 1U,
  kLPUART_IdleCharacter4 = 2U,
  kLPUART_IdleCharacter8 = 3U,
  kLPUART_IdleCharacter16 = 4U,
  kLPUART_IdleCharacter32 = 5U,
  kLPUART_IdleCharacter64 = 6U,
  kLPUART_IdleCharacter128 = 7U
}
 LPUART idle detected configuration. More...
 
enum  _lpuart_interrupt_enable {
  kLPUART_LinBreakInterruptEnable = (LPUART_BAUD_LBKDIE_MASK >> 8U),
  kLPUART_RxActiveEdgeInterruptEnable = (LPUART_BAUD_RXEDGIE_MASK >> 8U),
  kLPUART_TxDataRegEmptyInterruptEnable = (LPUART_CTRL_TIE_MASK),
  kLPUART_TransmissionCompleteInterruptEnable = (LPUART_CTRL_TCIE_MASK),
  kLPUART_RxDataRegFullInterruptEnable = (LPUART_CTRL_RIE_MASK),
  kLPUART_IdleLineInterruptEnable = (LPUART_CTRL_ILIE_MASK),
  kLPUART_RxOverrunInterruptEnable = (LPUART_CTRL_ORIE_MASK),
  kLPUART_NoiseErrorInterruptEnable = (LPUART_CTRL_NEIE_MASK),
  kLPUART_FramingErrorInterruptEnable = (LPUART_CTRL_FEIE_MASK),
  kLPUART_ParityErrorInterruptEnable = (LPUART_CTRL_PEIE_MASK),
  kLPUART_Match1InterruptEnable = (LPUART_CTRL_MA1IE_MASK),
  kLPUART_Match2InterruptEnable = (LPUART_CTRL_MA2IE_MASK),
  kLPUART_TxFifoOverflowInterruptEnable = (LPUART_FIFO_TXOFE_MASK),
  kLPUART_RxFifoUnderflowInterruptEnable = (LPUART_FIFO_RXUFE_MASK)
}
 LPUART interrupt configuration structure, default settings all disabled. More...
 
enum  _lpuart_flags {
  kLPUART_TxDataRegEmptyFlag,
  kLPUART_TransmissionCompleteFlag,
  kLPUART_RxDataRegFullFlag = (LPUART_STAT_RDRF_MASK),
  kLPUART_IdleLineFlag = (LPUART_STAT_IDLE_MASK),
  kLPUART_RxOverrunFlag = (LPUART_STAT_OR_MASK),
  kLPUART_NoiseErrorFlag = (LPUART_STAT_NF_MASK),
  kLPUART_FramingErrorFlag,
  kLPUART_ParityErrorFlag = (LPUART_STAT_PF_MASK),
  kLPUART_LinBreakFlag = (LPUART_STAT_LBKDIF_MASK),
  kLPUART_RxActiveEdgeFlag = (LPUART_STAT_RXEDGIF_MASK),
  kLPUART_RxActiveFlag,
  kLPUART_DataMatch1Flag,
  kLPUART_DataMatch2Flag,
  kLPUART_TxFifoEmptyFlag,
  kLPUART_RxFifoEmptyFlag,
  kLPUART_TxFifoOverflowFlag,
  kLPUART_RxFifoUnderflowFlag
}
 LPUART status flags. More...
 

Driver version

#define FSL_LPUART_DRIVER_VERSION   (MAKE_VERSION(2, 7, 0))
 LPUART driver version. More...
 

Software Reset

static void LPUART_SoftwareReset (LPUART_Type *base)
 Resets the LPUART using software. More...
 

Initialization and deinitialization

status_t LPUART_Init (LPUART_Type *base, const lpuart_config_t *config, uint32_t srcClock_Hz)
 Initializes an LPUART instance with the user configuration structure and the peripheral clock. More...
 
void LPUART_Deinit (LPUART_Type *base)
 Deinitializes a LPUART instance. More...
 
void LPUART_GetDefaultConfig (lpuart_config_t *config)
 Gets the default configuration structure. More...
 

Module configuration

status_t LPUART_SetBaudRate (LPUART_Type *base, uint32_t baudRate_Bps, uint32_t srcClock_Hz)
 Sets the LPUART instance baudrate. More...
 
void LPUART_Enable9bitMode (LPUART_Type *base, bool enable)
 Enable 9-bit data mode for LPUART. More...
 
static void LPUART_SetMatchAddress (LPUART_Type *base, uint16_t address1, uint16_t address2)
 Set the LPUART address. More...
 
static void LPUART_EnableMatchAddress (LPUART_Type *base, bool match1, bool match2)
 Enable the LPUART match address feature. More...
 
static void LPUART_SetRxFifoWatermark (LPUART_Type *base, uint8_t water)
 Sets the rx FIFO watermark. More...
 
static void LPUART_SetTxFifoWatermark (LPUART_Type *base, uint8_t water)
 Sets the tx FIFO watermark. More...
 

Status

uint32_t LPUART_GetStatusFlags (LPUART_Type *base)
 Gets LPUART status flags. More...
 
status_t LPUART_ClearStatusFlags (LPUART_Type *base, uint32_t mask)
 Clears status flags with a provided mask. More...
 

Interrupts

void LPUART_EnableInterrupts (LPUART_Type *base, uint32_t mask)
 Enables LPUART interrupts according to a provided mask. More...
 
void LPUART_DisableInterrupts (LPUART_Type *base, uint32_t mask)
 Disables LPUART interrupts according to a provided mask. More...
 
uint32_t LPUART_GetEnabledInterrupts (LPUART_Type *base)
 Gets enabled LPUART interrupts. More...
 

DMA Configuration

static uint32_t LPUART_GetDataRegisterAddress (LPUART_Type *base)
 Gets the LPUART data register address. More...
 
static void LPUART_EnableTxDMA (LPUART_Type *base, bool enable)
 Enables or disables the LPUART transmitter DMA request. More...
 
static void LPUART_EnableRxDMA (LPUART_Type *base, bool enable)
 Enables or disables the LPUART receiver DMA. More...
 

Bus Operations

uint32_t LPUART_GetInstance (LPUART_Type *base)
 Get the LPUART instance from peripheral base address. More...
 
static void LPUART_EnableTx (LPUART_Type *base, bool enable)
 Enables or disables the LPUART transmitter. More...
 
static void LPUART_EnableRx (LPUART_Type *base, bool enable)
 Enables or disables the LPUART receiver. More...
 
static void LPUART_WriteByte (LPUART_Type *base, uint8_t data)
 Writes to the transmitter register. More...
 
static uint8_t LPUART_ReadByte (LPUART_Type *base)
 Reads the receiver register. More...
 
static uint8_t LPUART_GetRxFifoCount (LPUART_Type *base)
 Gets the rx FIFO data count. More...
 
static uint8_t LPUART_GetTxFifoCount (LPUART_Type *base)
 Gets the tx FIFO data count. More...
 
void LPUART_SendAddress (LPUART_Type *base, uint8_t address)
 Transmit an address frame in 9-bit data mode. More...
 
status_t LPUART_WriteBlocking (LPUART_Type *base, const uint8_t *data, size_t length)
 Writes to the transmitter register using a blocking method. More...
 
status_t LPUART_ReadBlocking (LPUART_Type *base, uint8_t *data, size_t length)
 Reads the receiver data register using a blocking method. More...
 

Transactional

void LPUART_TransferCreateHandle (LPUART_Type *base, lpuart_handle_t *handle, lpuart_transfer_callback_t callback, void *userData)
 Initializes the LPUART handle. More...
 
status_t LPUART_TransferSendNonBlocking (LPUART_Type *base, lpuart_handle_t *handle, lpuart_transfer_t *xfer)
 Transmits a buffer of data using the interrupt method. More...
 
void LPUART_TransferStartRingBuffer (LPUART_Type *base, lpuart_handle_t *handle, uint8_t *ringBuffer, size_t ringBufferSize)
 Sets up the RX ring buffer. More...
 
void LPUART_TransferStopRingBuffer (LPUART_Type *base, lpuart_handle_t *handle)
 Aborts the background transfer and uninstalls the ring buffer. More...
 
size_t LPUART_TransferGetRxRingBufferLength (LPUART_Type *base, lpuart_handle_t *handle)
 Get the length of received data in RX ring buffer. More...
 
void LPUART_TransferAbortSend (LPUART_Type *base, lpuart_handle_t *handle)
 Aborts the interrupt-driven data transmit. More...
 
status_t LPUART_TransferGetSendCount (LPUART_Type *base, lpuart_handle_t *handle, uint32_t *count)
 Gets the number of bytes that have been sent out to bus. More...
 
status_t LPUART_TransferReceiveNonBlocking (LPUART_Type *base, lpuart_handle_t *handle, lpuart_transfer_t *xfer, size_t *receivedBytes)
 Receives a buffer of data using the interrupt method. More...
 
void LPUART_TransferAbortReceive (LPUART_Type *base, lpuart_handle_t *handle)
 Aborts the interrupt-driven data receiving. More...
 
status_t LPUART_TransferGetReceiveCount (LPUART_Type *base, lpuart_handle_t *handle, uint32_t *count)
 Gets the number of bytes that have been received. More...
 
void LPUART_TransferHandleIRQ (LPUART_Type *base, void *irqHandle)
 LPUART IRQ handle function. More...
 
void LPUART_TransferHandleErrorIRQ (LPUART_Type *base, void *irqHandle)
 LPUART Error IRQ handle function. More...
 

Data Structure Documentation

struct lpuart_config_t

Data Fields

uint32_t baudRate_Bps
 LPUART baud rate.
 
lpuart_parity_mode_t parityMode
 Parity mode, disabled (default), even, odd.
 
lpuart_data_bits_t dataBitsCount
 Data bits count, eight (default), seven.
 
bool isMsb
 Data bits order, LSB (default), MSB.
 
lpuart_stop_bit_count_t stopBitCount
 Number of stop bits, 1 stop bit (default) or 2 stop bits.
 
uint8_t txFifoWatermark
 TX FIFO watermark.
 
uint8_t rxFifoWatermark
 RX FIFO watermark.
 
bool enableRxRTS
 RX RTS enable.
 
bool enableTxCTS
 TX CTS enable.
 
lpuart_transmit_cts_source_t txCtsSource
 TX CTS source.
 
lpuart_transmit_cts_config_t txCtsConfig
 TX CTS configure.
 
lpuart_idle_type_select_t rxIdleType
 RX IDLE type. More...
 
lpuart_idle_config_t rxIdleConfig
 RX IDLE configuration. More...
 
bool enableTx
 Enable TX.
 
bool enableRx
 Enable RX.
 

Field Documentation

lpuart_idle_type_select_t lpuart_config_t::rxIdleType
lpuart_idle_config_t lpuart_config_t::rxIdleConfig
struct lpuart_transfer_t

Data Fields

size_t dataSize
 The byte count to be transfer. More...
 
uint8_t * data
 The buffer of data to be transfer. More...
 
uint8_t * rxData
 The buffer to receive data. More...
 
const uint8_t * txData
 The buffer of data to be sent. More...
 

Field Documentation

uint8_t* lpuart_transfer_t::data
uint8_t* lpuart_transfer_t::rxData
const uint8_t* lpuart_transfer_t::txData
size_t lpuart_transfer_t::dataSize
struct _lpuart_handle

Data Fields

const uint8_t *volatile txData
 Address of remaining data to send. More...
 
volatile size_t txDataSize
 Size of the remaining data to send. More...
 
size_t txDataSizeAll
 Size of the data to send out. More...
 
uint8_t *volatile rxData
 Address of remaining data to receive. More...
 
volatile size_t rxDataSize
 Size of the remaining data to receive. More...
 
size_t rxDataSizeAll
 Size of the data to receive. More...
 
uint8_t * rxRingBuffer
 Start address of the receiver ring buffer. More...
 
size_t rxRingBufferSize
 Size of the ring buffer. More...
 
volatile uint16_t rxRingBufferHead
 Index for the driver to store received data into ring buffer. More...
 
volatile uint16_t rxRingBufferTail
 Index for the user to get data from the ring buffer. More...
 
lpuart_transfer_callback_t callback
 Callback function. More...
 
void * userData
 LPUART callback function parameter. More...
 
volatile uint8_t txState
 TX transfer state. More...
 
volatile uint8_t rxState
 RX transfer state. More...
 
bool isSevenDataBits
 Seven data bits flag. More...
 

Field Documentation

const uint8_t* volatile lpuart_handle_t::txData
volatile size_t lpuart_handle_t::txDataSize
size_t lpuart_handle_t::txDataSizeAll
uint8_t* volatile lpuart_handle_t::rxData
volatile size_t lpuart_handle_t::rxDataSize
size_t lpuart_handle_t::rxDataSizeAll
uint8_t* lpuart_handle_t::rxRingBuffer
size_t lpuart_handle_t::rxRingBufferSize
volatile uint16_t lpuart_handle_t::rxRingBufferHead
volatile uint16_t lpuart_handle_t::rxRingBufferTail
lpuart_transfer_callback_t lpuart_handle_t::callback
void* lpuart_handle_t::userData
volatile uint8_t lpuart_handle_t::txState
volatile uint8_t lpuart_handle_t::rxState
bool lpuart_handle_t::isSevenDataBits

Macro Definition Documentation

#define FSL_LPUART_DRIVER_VERSION   (MAKE_VERSION(2, 7, 0))
#define UART_RETRY_TIMES   0U /* Defining to zero means to keep waiting for the flag until it is assert/deassert. */

Typedef Documentation

typedef void(* lpuart_transfer_callback_t)(LPUART_Type *base, lpuart_handle_t *handle, status_t status, void *userData)

Enumeration Type Documentation

anonymous enum
Enumerator
kStatus_LPUART_TxBusy 

TX busy.

kStatus_LPUART_RxBusy 

RX busy.

kStatus_LPUART_TxIdle 

LPUART transmitter is idle.

kStatus_LPUART_RxIdle 

LPUART receiver is idle.

kStatus_LPUART_TxWatermarkTooLarge 

TX FIFO watermark too large.

kStatus_LPUART_RxWatermarkTooLarge 

RX FIFO watermark too large.

kStatus_LPUART_FlagCannotClearManually 

Some flag can't manually clear.

kStatus_LPUART_Error 

Error happens on LPUART.

kStatus_LPUART_RxRingBufferOverrun 

LPUART RX software ring buffer overrun.

kStatus_LPUART_RxHardwareOverrun 

LPUART RX receiver overrun.

kStatus_LPUART_NoiseError 

LPUART noise error.

kStatus_LPUART_FramingError 

LPUART framing error.

kStatus_LPUART_ParityError 

LPUART parity error.

kStatus_LPUART_BaudrateNotSupport 

Baudrate is not support in current clock source.

kStatus_LPUART_IdleLineDetected 

IDLE flag.

kStatus_LPUART_Timeout 

LPUART times out.

Enumerator
kLPUART_ParityDisabled 

Parity disabled.

kLPUART_ParityEven 

Parity enabled, type even, bit setting: PE|PT = 10.

kLPUART_ParityOdd 

Parity enabled, type odd, bit setting: PE|PT = 11.

Enumerator
kLPUART_EightDataBits 

Eight data bit.

kLPUART_SevenDataBits 

Seven data bit.

Enumerator
kLPUART_OneStopBit 

One stop bit.

kLPUART_TwoStopBit 

Two stop bits.

Enumerator
kLPUART_CtsSourcePin 

CTS resource is the LPUART_CTS pin.

kLPUART_CtsSourceMatchResult 

CTS resource is the match result.

Enumerator
kLPUART_CtsSampleAtStart 

CTS input is sampled at the start of each character.

kLPUART_CtsSampleAtIdle 

CTS input is sampled when the transmitter is idle.

Enumerator
kLPUART_IdleTypeStartBit 

Start counting after a valid start bit.

kLPUART_IdleTypeStopBit 

Start counting after a stop bit.

This structure defines the number of idle characters that must be received before the IDLE flag is set.

Enumerator
kLPUART_IdleCharacter1 

the number of idle characters.

kLPUART_IdleCharacter2 

the number of idle characters.

kLPUART_IdleCharacter4 

the number of idle characters.

kLPUART_IdleCharacter8 

the number of idle characters.

kLPUART_IdleCharacter16 

the number of idle characters.

kLPUART_IdleCharacter32 

the number of idle characters.

kLPUART_IdleCharacter64 

the number of idle characters.

kLPUART_IdleCharacter128 

the number of idle characters.

This structure contains the settings for all LPUART interrupt configurations.

Enumerator
kLPUART_LinBreakInterruptEnable 

LIN break detect.

bit 7

kLPUART_RxActiveEdgeInterruptEnable 

Receive Active Edge.

bit 6

kLPUART_TxDataRegEmptyInterruptEnable 

Transmit data register empty.

bit 23

kLPUART_TransmissionCompleteInterruptEnable 

Transmission complete.

bit 22

kLPUART_RxDataRegFullInterruptEnable 

Receiver data register full.

bit 21

kLPUART_IdleLineInterruptEnable 

Idle line.

bit 20

kLPUART_RxOverrunInterruptEnable 

Receiver Overrun.

bit 27

kLPUART_NoiseErrorInterruptEnable 

Noise error flag.

bit 26

kLPUART_FramingErrorInterruptEnable 

Framing error flag.

bit 25

kLPUART_ParityErrorInterruptEnable 

Parity error flag.

bit 24

kLPUART_Match1InterruptEnable 

Parity error flag.

bit 15

kLPUART_Match2InterruptEnable 

Parity error flag.

bit 14

kLPUART_TxFifoOverflowInterruptEnable 

Transmit FIFO Overflow.

bit 9

kLPUART_RxFifoUnderflowInterruptEnable 

Receive FIFO Underflow.

bit 8

This provides constants for the LPUART status flags for use in the LPUART functions.

Enumerator
kLPUART_TxDataRegEmptyFlag 

Transmit data register empty flag, sets when transmit buffer is empty.

bit 23

kLPUART_TransmissionCompleteFlag 

Transmission complete flag, sets when transmission activity complete.

bit 22

kLPUART_RxDataRegFullFlag 

Receive data register full flag, sets when the receive data buffer is full.

bit 21

kLPUART_IdleLineFlag 

Idle line detect flag, sets when idle line detected.

bit 20

kLPUART_RxOverrunFlag 

Receive Overrun, sets when new data is received before data is read from receive register.

bit 19

kLPUART_NoiseErrorFlag 

Receive takes 3 samples of each received bit.

If any of these samples differ, noise flag sets. bit 18

kLPUART_FramingErrorFlag 

Frame error flag, sets if logic 0 was detected where stop bit expected.

bit 17

kLPUART_ParityErrorFlag 

If parity enabled, sets upon parity error detection.

bit 16

kLPUART_LinBreakFlag 

LIN break detect interrupt flag, sets when LIN break char detected and LIN circuit enabled.

bit 31

kLPUART_RxActiveEdgeFlag 

Receive pin active edge interrupt flag, sets when active edge detected.

bit 30

kLPUART_RxActiveFlag 

Receiver Active Flag (RAF), sets at beginning of valid start.

bit 24

kLPUART_DataMatch1Flag 

The next character to be read from LPUART_DATA matches MA1.

bit 15

kLPUART_DataMatch2Flag 

The next character to be read from LPUART_DATA matches MA2.

bit 14

kLPUART_TxFifoEmptyFlag 

TXEMPT bit, sets if transmit buffer is empty.

bit 7

kLPUART_RxFifoEmptyFlag 

RXEMPT bit, sets if receive buffer is empty.

bit 6

kLPUART_TxFifoOverflowFlag 

TXOF bit, sets if transmit buffer overflow occurred.

bit 1

kLPUART_RxFifoUnderflowFlag 

RXUF bit, sets if receive buffer underflow occurred.

bit 0

Function Documentation

static void LPUART_SoftwareReset ( LPUART_Type *  base)
inlinestatic

This function resets all internal logic and registers except the Global Register. Remains set until cleared by software.

Parameters
baseLPUART peripheral base address.
status_t LPUART_Init ( LPUART_Type *  base,
const lpuart_config_t *  config,
uint32_t  srcClock_Hz 
)

This function configures the LPUART module with user-defined settings. Call the LPUART_GetDefaultConfig() function to configure the configuration structure and get the default configuration. The example below shows how to use this API to configure the LPUART.

* lpuart_config_t lpuartConfig;
* lpuartConfig.baudRate_Bps = 115200U;
* lpuartConfig.isMsb = false;
* lpuartConfig.txFifoWatermark = 0;
* lpuartConfig.rxFifoWatermark = 1;
* LPUART_Init(LPUART1, &lpuartConfig, 20000000U);
*
Parameters
baseLPUART peripheral base address.
configPointer to a user-defined configuration structure.
srcClock_HzLPUART clock source frequency in HZ.
Return values
kStatus_LPUART_BaudrateNotSupportBaudrate is not support in current clock source.
kStatus_SuccessLPUART initialize succeed
void LPUART_Deinit ( LPUART_Type *  base)

This function waits for transmit to complete, disables TX and RX, and disables the LPUART clock.

Parameters
baseLPUART peripheral base address.
void LPUART_GetDefaultConfig ( lpuart_config_t *  config)

This function initializes the LPUART configuration structure to a default value. The default values are: lpuartConfig->baudRate_Bps = 115200U; lpuartConfig->parityMode = kLPUART_ParityDisabled; lpuartConfig->dataBitsCount = kLPUART_EightDataBits; lpuartConfig->isMsb = false; lpuartConfig->stopBitCount = kLPUART_OneStopBit; lpuartConfig->txFifoWatermark = 0; lpuartConfig->rxFifoWatermark = 1; lpuartConfig->rxIdleType = kLPUART_IdleTypeStartBit; lpuartConfig->rxIdleConfig = kLPUART_IdleCharacter1; lpuartConfig->enableTx = false; lpuartConfig->enableRx = false;

Parameters
configPointer to a configuration structure.
status_t LPUART_SetBaudRate ( LPUART_Type *  base,
uint32_t  baudRate_Bps,
uint32_t  srcClock_Hz 
)

This function configures the LPUART module baudrate. This function is used to update the LPUART module baudrate after the LPUART module is initialized by the LPUART_Init.

* LPUART_SetBaudRate(LPUART1, 115200U, 20000000U);
*
Parameters
baseLPUART peripheral base address.
baudRate_BpsLPUART baudrate to be set.
srcClock_HzLPUART clock source frequency in HZ.
Return values
kStatus_LPUART_BaudrateNotSupportBaudrate is not supported in the current clock source.
kStatus_SuccessSet baudrate succeeded.
void LPUART_Enable9bitMode ( LPUART_Type *  base,
bool  enable 
)

This function set the 9-bit mode for LPUART module. The 9th bit is not used for parity thus can be modified by user.

Parameters
baseLPUART peripheral base address.
enabletrue to enable, flase to disable.
static void LPUART_SetMatchAddress ( LPUART_Type *  base,
uint16_t  address1,
uint16_t  address2 
)
inlinestatic

This function configures the address for LPUART module that works as slave in 9-bit data mode. One or two address fields can be configured. When the address field's match enable bit is set, the frame it receices with MSB being 1 is considered as an address frame, otherwise it is considered as data frame. Once the address frame matches one of slave's own addresses, this slave is addressed. This address frame and its following data frames are stored in the receive buffer, otherwise the frames will be discarded. To un-address a slave, just send an address frame with unmatched address.

Note
Any LPUART instance joined in the multi-slave system can work as slave. The position of the address mark is the same as the parity bit when parity is enabled for 8 bit and 9 bit data formats.
Parameters
baseLPUART peripheral base address.
address1LPUART slave address1.
address2LPUART slave address2.
static void LPUART_EnableMatchAddress ( LPUART_Type *  base,
bool  match1,
bool  match2 
)
inlinestatic
Parameters
baseLPUART peripheral base address.
match1true to enable match address1, false to disable.
match2true to enable match address2, false to disable.
static void LPUART_SetRxFifoWatermark ( LPUART_Type *  base,
uint8_t  water 
)
inlinestatic
Parameters
baseLPUART peripheral base address.
waterRx FIFO watermark.
static void LPUART_SetTxFifoWatermark ( LPUART_Type *  base,
uint8_t  water 
)
inlinestatic
Parameters
baseLPUART peripheral base address.
waterTx FIFO watermark.
uint32_t LPUART_GetStatusFlags ( LPUART_Type *  base)

This function gets all LPUART status flags. The flags are returned as the logical OR value of the enumerators _lpuart_flags. To check for a specific status, compare the return value with enumerators in the _lpuart_flags. For example, to check whether the TX is empty:

* {
* ...
* }
*
Parameters
baseLPUART peripheral base address.
Returns
LPUART status flags which are ORed by the enumerators in the _lpuart_flags.
status_t LPUART_ClearStatusFlags ( LPUART_Type *  base,
uint32_t  mask 
)

This function clears LPUART status flags with a provided mask. Automatically cleared flags can't be cleared by this function. Flags that can only cleared or set by hardware are: kLPUART_TxDataRegEmptyFlag, kLPUART_TransmissionCompleteFlag, kLPUART_RxDataRegFullFlag, kLPUART_RxActiveFlag, kLPUART_NoiseErrorFlag, kLPUART_ParityErrorFlag, kLPUART_TxFifoEmptyFlag,kLPUART_RxFifoEmptyFlag Note: This API should be called when the Tx/Rx is idle, otherwise it takes no effects.

Parameters
baseLPUART peripheral base address.
maskthe status flags to be cleared. The user can use the enumerators in the _lpuart_status_flag_t to do the OR operation and get the mask.
Returns
0 succeed, others failed.
Return values
kStatus_LPUART_FlagCannotClearManuallyThe flag can't be cleared by this function but it is cleared automatically by hardware.
kStatus_SuccessStatus in the mask are cleared.
void LPUART_EnableInterrupts ( LPUART_Type *  base,
uint32_t  mask 
)

This function enables the LPUART interrupts according to a provided mask. The mask is a logical OR of enumeration members. See the _lpuart_interrupt_enable. This examples shows how to enable TX empty interrupt and RX full interrupt:

Parameters
baseLPUART peripheral base address.
maskThe interrupts to enable. Logical OR of _lpuart_interrupt_enable.
void LPUART_DisableInterrupts ( LPUART_Type *  base,
uint32_t  mask 
)

This function disables the LPUART interrupts according to a provided mask. The mask is a logical OR of enumeration members. See _lpuart_interrupt_enable. This example shows how to disable the TX empty interrupt and RX full interrupt:

Parameters
baseLPUART peripheral base address.
maskThe interrupts to disable. Logical OR of _lpuart_interrupt_enable.
uint32_t LPUART_GetEnabledInterrupts ( LPUART_Type *  base)

This function gets the enabled LPUART interrupts. The enabled interrupts are returned as the logical OR value of the enumerators _lpuart_interrupt_enable. To check a specific interrupt enable status, compare the return value with enumerators in _lpuart_interrupt_enable. For example, to check whether the TX empty interrupt is enabled:

* uint32_t enabledInterrupts = LPUART_GetEnabledInterrupts(LPUART1);
*
* if (kLPUART_TxDataRegEmptyInterruptEnable & enabledInterrupts)
* {
* ...
* }
*
Parameters
baseLPUART peripheral base address.
Returns
LPUART interrupt flags which are logical OR of the enumerators in _lpuart_interrupt_enable.
static uint32_t LPUART_GetDataRegisterAddress ( LPUART_Type *  base)
inlinestatic

This function returns the LPUART data register address, which is mainly used by the DMA/eDMA.

Parameters
baseLPUART peripheral base address.
Returns
LPUART data register addresses which are used both by the transmitter and receiver.
static void LPUART_EnableTxDMA ( LPUART_Type *  base,
bool  enable 
)
inlinestatic

This function enables or disables the transmit data register empty flag, STAT[TDRE], to generate DMA requests.

Parameters
baseLPUART peripheral base address.
enableTrue to enable, false to disable.
static void LPUART_EnableRxDMA ( LPUART_Type *  base,
bool  enable 
)
inlinestatic

This function enables or disables the receiver data register full flag, STAT[RDRF], to generate DMA requests.

Parameters
baseLPUART peripheral base address.
enableTrue to enable, false to disable.
uint32_t LPUART_GetInstance ( LPUART_Type *  base)
Parameters
baseLPUART peripheral base address.
Returns
LPUART instance.
static void LPUART_EnableTx ( LPUART_Type *  base,
bool  enable 
)
inlinestatic

This function enables or disables the LPUART transmitter.

Parameters
baseLPUART peripheral base address.
enableTrue to enable, false to disable.
static void LPUART_EnableRx ( LPUART_Type *  base,
bool  enable 
)
inlinestatic

This function enables or disables the LPUART receiver.

Parameters
baseLPUART peripheral base address.
enableTrue to enable, false to disable.
static void LPUART_WriteByte ( LPUART_Type *  base,
uint8_t  data 
)
inlinestatic

This function writes data to the transmitter register directly. The upper layer must ensure that the TX register is empty or that the TX FIFO has room before calling this function.

Parameters
baseLPUART peripheral base address.
dataData write to the TX register.
static uint8_t LPUART_ReadByte ( LPUART_Type *  base)
inlinestatic

This function reads data from the receiver register directly. The upper layer must ensure that the receiver register is full or that the RX FIFO has data before calling this function.

Parameters
baseLPUART peripheral base address.
Returns
Data read from data register.
static uint8_t LPUART_GetRxFifoCount ( LPUART_Type *  base)
inlinestatic
Parameters
baseLPUART peripheral base address.
Returns
rx FIFO data count.
static uint8_t LPUART_GetTxFifoCount ( LPUART_Type *  base)
inlinestatic
Parameters
baseLPUART peripheral base address.
Returns
tx FIFO data count.
void LPUART_SendAddress ( LPUART_Type *  base,
uint8_t  address 
)
Parameters
baseLPUART peripheral base address.
addressLPUART slave address.
status_t LPUART_WriteBlocking ( LPUART_Type *  base,
const uint8_t *  data,
size_t  length 
)

This function polls the transmitter register, first waits for the register to be empty or TX FIFO to have room, and writes data to the transmitter buffer, then waits for the dat to be sent out to the bus.

Parameters
baseLPUART peripheral base address.
dataStart address of the data to write.
lengthSize of the data to write.
Return values
kStatus_LPUART_TimeoutTransmission timed out and was aborted.
kStatus_SuccessSuccessfully wrote all data.
status_t LPUART_ReadBlocking ( LPUART_Type *  base,
uint8_t *  data,
size_t  length 
)

This function polls the receiver register, waits for the receiver register full or receiver FIFO has data, and reads data from the TX register.

Parameters
baseLPUART peripheral base address.
dataStart address of the buffer to store the received data.
lengthSize of the buffer.
Return values
kStatus_LPUART_RxHardwareOverrunReceiver overrun happened while receiving data.
kStatus_LPUART_NoiseErrorNoise error happened while receiving data.
kStatus_LPUART_FramingErrorFraming error happened while receiving data.
kStatus_LPUART_ParityErrorParity error happened while receiving data.
kStatus_LPUART_TimeoutTransmission timed out and was aborted.
kStatus_SuccessSuccessfully received all data.
void LPUART_TransferCreateHandle ( LPUART_Type *  base,
lpuart_handle_t *  handle,
lpuart_transfer_callback_t  callback,
void *  userData 
)

This function initializes the LPUART handle, which can be used for other LPUART transactional APIs. Usually, for a specified LPUART instance, call this API once to get the initialized handle.

The LPUART driver supports the "background" receiving, which means that user can set up an RX ring buffer optionally. Data received is stored into the ring buffer even when the user doesn't call the LPUART_TransferReceiveNonBlocking() API. If there is already data received in the ring buffer, the user can get the received data from the ring buffer directly. The ring buffer is disabled if passing NULL as ringBuffer.

Parameters
baseLPUART peripheral base address.
handleLPUART handle pointer.
callbackCallback function.
userDataUser data.
status_t LPUART_TransferSendNonBlocking ( LPUART_Type *  base,
lpuart_handle_t *  handle,
lpuart_transfer_t *  xfer 
)

This function send data using an interrupt method. This is a non-blocking function, which returns directly without waiting for all data written to the transmitter register. When all data is written to the TX register in the ISR, the LPUART driver calls the callback function and passes the kStatus_LPUART_TxIdle as status parameter.

Note
The kStatus_LPUART_TxIdle is passed to the upper layer when all data are written to the TX register. However, there is no check to ensure that all the data sent out. Before disabling the TX, check the kLPUART_TransmissionCompleteFlag to ensure that the transmit is finished.
Parameters
baseLPUART peripheral base address.
handleLPUART handle pointer.
xferLPUART transfer structure, see lpuart_transfer_t.
Return values
kStatus_SuccessSuccessfully start the data transmission.
kStatus_LPUART_TxBusyPrevious transmission still not finished, data not all written to the TX register.
kStatus_InvalidArgumentInvalid argument.
void LPUART_TransferStartRingBuffer ( LPUART_Type *  base,
lpuart_handle_t *  handle,
uint8_t *  ringBuffer,
size_t  ringBufferSize 
)

This function sets up the RX ring buffer to a specific UART handle.

When the RX ring buffer is used, data received is stored into the ring buffer even when the user doesn't call the UART_TransferReceiveNonBlocking() API. If there is already data received in the ring buffer, the user can get the received data from the ring buffer directly.

Note
When using RX ring buffer, one byte is reserved for internal use. In other words, if ringBufferSize is 32, then only 31 bytes are used for saving data.
Parameters
baseLPUART peripheral base address.
handleLPUART handle pointer.
ringBufferStart address of ring buffer for background receiving. Pass NULL to disable the ring buffer.
ringBufferSizesize of the ring buffer.
void LPUART_TransferStopRingBuffer ( LPUART_Type *  base,
lpuart_handle_t *  handle 
)

This function aborts the background transfer and uninstalls the ring buffer.

Parameters
baseLPUART peripheral base address.
handleLPUART handle pointer.
size_t LPUART_TransferGetRxRingBufferLength ( LPUART_Type *  base,
lpuart_handle_t *  handle 
)
Parameters
baseLPUART peripheral base address.
handleLPUART handle pointer.
Returns
Length of received data in RX ring buffer.
void LPUART_TransferAbortSend ( LPUART_Type *  base,
lpuart_handle_t *  handle 
)

This function aborts the interrupt driven data sending. The user can get the remainBtyes to find out how many bytes are not sent out.

Parameters
baseLPUART peripheral base address.
handleLPUART handle pointer.
status_t LPUART_TransferGetSendCount ( LPUART_Type *  base,
lpuart_handle_t *  handle,
uint32_t *  count 
)

This function gets the number of bytes that have been sent out to bus by an interrupt method.

Parameters
baseLPUART peripheral base address.
handleLPUART handle pointer.
countSend bytes count.
Return values
kStatus_NoTransferInProgressNo send in progress.
kStatus_InvalidArgumentParameter is invalid.
kStatus_SuccessGet successfully through the parameter count;
status_t LPUART_TransferReceiveNonBlocking ( LPUART_Type *  base,
lpuart_handle_t *  handle,
lpuart_transfer_t *  xfer,
size_t *  receivedBytes 
)

This function receives data using an interrupt method. This is a non-blocking function which returns without waiting to ensure that all data are received. If the RX ring buffer is used and not empty, the data in the ring buffer is copied and the parameter receivedBytes shows how many bytes are copied from the ring buffer. After copying, if the data in the ring buffer is not enough for read, the receive request is saved by the LPUART driver. When the new data arrives, the receive request is serviced first. When all data is received, the LPUART driver notifies the upper layer through a callback function and passes a status parameter kStatus_UART_RxIdle. For example, the upper layer needs 10 bytes but there are only 5 bytes in ring buffer. The 5 bytes are copied to xfer->data, which returns with the parameter receivedBytes set to 5. For the remaining 5 bytes, the newly arrived data is saved from xfer->data[5]. When 5 bytes are received, the LPUART driver notifies the upper layer. If the RX ring buffer is not enabled, this function enables the RX and RX interrupt to receive data to xfer->data. When all data is received, the upper layer is notified.

Parameters
baseLPUART peripheral base address.
handleLPUART handle pointer.
xferLPUART transfer structure, see uart_transfer_t.
receivedBytesBytes received from the ring buffer directly.
Return values
kStatus_SuccessSuccessfully queue the transfer into the transmit queue.
kStatus_LPUART_RxBusyPrevious receive request is not finished.
kStatus_InvalidArgumentInvalid argument.
void LPUART_TransferAbortReceive ( LPUART_Type *  base,
lpuart_handle_t *  handle 
)

This function aborts the interrupt-driven data receiving. The user can get the remainBytes to find out how many bytes not received yet.

Parameters
baseLPUART peripheral base address.
handleLPUART handle pointer.
status_t LPUART_TransferGetReceiveCount ( LPUART_Type *  base,
lpuart_handle_t *  handle,
uint32_t *  count 
)

This function gets the number of bytes that have been received.

Parameters
baseLPUART peripheral base address.
handleLPUART handle pointer.
countReceive bytes count.
Return values
kStatus_NoTransferInProgressNo receive in progress.
kStatus_InvalidArgumentParameter is invalid.
kStatus_SuccessGet successfully through the parameter count;
void LPUART_TransferHandleIRQ ( LPUART_Type *  base,
void *  irqHandle 
)

This function handles the LPUART transmit and receive IRQ request.

Parameters
baseLPUART peripheral base address.
irqHandleLPUART handle pointer.
void LPUART_TransferHandleErrorIRQ ( LPUART_Type *  base,
void *  irqHandle 
)

This function handles the LPUART error IRQ request.

Parameters
baseLPUART peripheral base address.
irqHandleLPUART handle pointer.