![]() |
MCUXpresso SDK API Reference Manual
Rev 2.12.1
NXP Semiconductors
|
The MCUXpresso SDK provides driver for the Trigger Mux (TRGMUX) module of MCUXpresso SDK devices.
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/trgmux
Enumerations | |
| enum | { kStatus_TRGMUX_Locked = MAKE_STATUS(kStatusGroup_TRGMUX, 0) } |
| TRGMUX configure status. More... | |
| enum | trgmux_trigger_input_t { kTRGMUX_TriggerInput0 = TRGMUX_TRGCFG_SEL0_SHIFT, kTRGMUX_TriggerInput1 = TRGMUX_TRGCFG_SEL1_SHIFT, kTRGMUX_TriggerInput2 = TRGMUX_TRGCFG_SEL2_SHIFT, kTRGMUX_TriggerInput3 = TRGMUX_TRGCFG_SEL3_SHIFT } |
| Defines the MUX select for peripheral trigger input. More... | |
Driver version | |
| #define | FSL_TRGMUX_DRIVER_VERSION (MAKE_VERSION(2, 0, 1)) |
| TRGMUX driver version. More... | |
TRGMUX Functional Operation | |
| static void | TRGMUX_LockRegister (TRGMUX_Type *base, uint32_t index) |
| Sets the flag of the register which is used to mark writeable. More... | |
| status_t | TRGMUX_SetTriggerSource (TRGMUX_Type *base, uint32_t index, trgmux_trigger_input_t input, uint32_t trigger_src) |
| Configures the trigger source of the appointed peripheral. More... | |
| #define FSL_TRGMUX_DRIVER_VERSION (MAKE_VERSION(2, 0, 1)) |
|
inlinestatic |
The function sets the flag of the register which is used to mark writeable. Example:
| base | TRGMUX peripheral base address. |
| index | The index of the TRGMUX register, see the enum trgmux_device_t defined in <SOC>.h. |
| status_t TRGMUX_SetTriggerSource | ( | TRGMUX_Type * | base, |
| uint32_t | index, | ||
| trgmux_trigger_input_t | input, | ||
| uint32_t | trigger_src | ||
| ) |
The function configures the trigger source of the appointed peripheral. Example:
| base | TRGMUX peripheral base address. |
| index | The index of the TRGMUX register, see the enum trgmux_device_t defined in <SOC>.h. |
| input | The MUX select for peripheral trigger input |
| trigger_src | The trigger inputs for various peripherals. See the enum trgmux_source_t defined in <SOC>.h. |
| kStatus_Success | Configured successfully. |
| kStatus_TRGMUX_Locked | Configuration failed because the register is locked. |