MCUXpresso SDK API Reference Manual  Rev 2.12.1
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
SPI: Serial Peripheral Interface Driver

Overview

SPI driver includes functional APIs and transactional APIs.

Functional APIs are feature/property target low level APIs. Functional APIs can be used for SPI initialization/configuration/operation for optimization/customization purpose. Using the functional API requires the knowledge of the SPI peripheral and how to organize functional APIs to meet the application requirements. All functional API use the peripheral base address as the first parameter. SPI functional operation groups provide the functional API set.

Transactional APIs are transaction target high level APIs. Transactional APIs can be used to enable the peripheral and in the application if the code size and performance of transactional APIs satisfy the requirements. If the code size and performance are a critical requirement, see the transactional API implementation and write a custom code. All transactional APIs use the spi_handle_t as the first parameter. Initialize the handle by calling the SPI_MasterTransferCreateHandle() or SPI_SlaveTransferCreateHandle() API.

Transactional APIs support asynchronous transfer. This means that the functions SPI_MasterTransferNonBlocking() and SPI_SlaveTransferNonBlocking() set up the interrupt for data transfer. When the transfer completes, the upper layer is notified through a callback function with the kStatus_SPI_Idle status.

Files

file  fsl_spi.h
 

Data Structures

struct  spi_delay_config_t
 SPI delay time configure structure. More...
 
struct  spi_master_config_t
 SPI master user configure structure. More...
 
struct  spi_transfer_t
 SPI transfer structure. More...
 
struct  spi_config_t
 Internal configuration structure used in 'spi' and 'spi_dma' driver. More...
 
struct  spi_master_handle_t
 SPI transfer handle structure. More...
 

Macros

#define SPI_DUMMYDATA   (0xFFU)
 SPI dummy transfer data, the data is sent while txBuff is NULL. More...
 
#define SPI_RETRY_TIMES   0U /* Define to zero means keep waiting until the flag is assert/deassert. */
 Retry times for waiting flag. More...
 

Typedefs

typedef void(* spi_master_callback_t )(SPI_Type *base, spi_master_handle_t *handle, status_t status, void *userData)
 SPI master callback for finished transmit.
 
typedef void(* spi_master_irq_handler_t )(SPI_Type *base, spi_master_handle_t *handle)
 Typedef for master interrupt handler. More...
 

Enumerations

enum  spi_xfer_option_t {
  kSPI_FrameDelay = (SPI_FIFOWR_EOF_MASK),
  kSPI_FrameAssert = (SPI_FIFOWR_EOT_MASK)
}
 SPI transfer option. More...
 
enum  spi_shift_direction_t {
  kSPI_MsbFirst = 0U,
  kSPI_LsbFirst = 1U
}
 SPI data shifter direction options. More...
 
enum  spi_clock_polarity_t {
  kSPI_ClockPolarityActiveHigh = 0x0U,
  kSPI_ClockPolarityActiveLow
}
 SPI clock polarity configuration. More...
 
enum  spi_clock_phase_t {
  kSPI_ClockPhaseFirstEdge = 0x0U,
  kSPI_ClockPhaseSecondEdge
}
 SPI clock phase configuration. More...
 
enum  spi_txfifo_watermark_t {
  kSPI_TxFifo0 = 0,
  kSPI_TxFifo1 = 1,
  kSPI_TxFifo2 = 2,
  kSPI_TxFifo3 = 3,
  kSPI_TxFifo4 = 4,
  kSPI_TxFifo5 = 5,
  kSPI_TxFifo6 = 6,
  kSPI_TxFifo7 = 7
}
 txFIFO watermark values More...
 
enum  spi_rxfifo_watermark_t {
  kSPI_RxFifo1 = 0,
  kSPI_RxFifo2 = 1,
  kSPI_RxFifo3 = 2,
  kSPI_RxFifo4 = 3,
  kSPI_RxFifo5 = 4,
  kSPI_RxFifo6 = 5,
  kSPI_RxFifo7 = 6,
  kSPI_RxFifo8 = 7
}
 rxFIFO watermark values More...
 
enum  spi_data_width_t {
  kSPI_Data8Bits = 7,
  kSPI_Data16Bits = 15
}
 Transfer data width. More...
 
enum  spi_ssel_t { kSPI_Ssel0 = 0 }
 Slave select. More...
 
enum  spi_spol_t
 ssel polarity
 
enum  {
  kStatus_SPI_Busy = MAKE_STATUS(kStatusGroup_LPC_SPI, 0),
  kStatus_SPI_Idle = MAKE_STATUS(kStatusGroup_LPC_SPI, 1),
  kStatus_SPI_Error = MAKE_STATUS(kStatusGroup_LPC_SPI, 2),
  kStatus_SPI_BaudrateNotSupport,
  kStatus_SPI_Timeout = MAKE_STATUS(kStatusGroup_LPC_SPI, 4)
}
 SPI transfer status. More...
 
enum  _spi_interrupt_enable {
  kSPI_RxErrIrq = SPI_FIFOINTENSET_RXERR_MASK,
  kSPI_TxErrIrq = SPI_FIFOINTENSET_TXERR_MASK,
  kSPI_RxLvlIrq = SPI_FIFOINTENSET_RXLVL_MASK,
  kSPI_TxLvlIrq = SPI_FIFOINTENSET_TXLVL_MASK,
  kSPI_SlaveSelectAssertIrq = SPI_INTENSET_SSAEN_MASK << SPI_INTEN_IRQ_SHIFT,
  kSPI_SlaveSelectDeassertIrq = SPI_INTENSET_SSDEN_MASK << SPI_INTEN_IRQ_SHIFT,
  kSPI_MasterIdleIrq = SPI_INTENSET_MSTIDLEEN_MASK << SPI_INTEN_IRQ_SHIFT
}
 SPI interrupt sources. More...
 
enum  _spi_statusflags {
  kSPI_TxEmptyFlag = SPI_FIFOSTAT_TXEMPTY_MASK,
  kSPI_TxNotFullFlag = SPI_FIFOSTAT_TXNOFULL_MASK,
  kSPI_RxNotEmptyFlag = SPI_FIFOSTAT_RXNOTEMPTY_MASK,
  kSPI_RxFullFlag = SPI_FIFOSTAT_RXFULL_MASK
}
 SPI status flags. More...
 

Functions

uint32_t SPI_GetInstance (SPI_Type *base)
 Returns instance number for SPI peripheral base address. More...
 

Variables

volatile uint8_t s_dummyData []
 Global variable for dummy data value setting. More...
 

Driver version

#define FSL_SPI_DRIVER_VERSION   (MAKE_VERSION(2, 1, 0))
 SPI driver version. More...
 

Initialization and deinitialization

void SPI_MasterGetDefaultConfig (spi_master_config_t *config)
 Sets the SPI master configuration structure to default values. More...
 
status_t SPI_MasterInit (SPI_Type *base, const spi_master_config_t *config, uint32_t srcClock_Hz)
 Initializes the SPI with master configuration. More...
 
void SPI_Deinit (SPI_Type *base)
 De-initializes the SPI. More...
 
static void SPI_Enable (SPI_Type *base, bool enable)
 Enable or disable the SPI Master or Slave. More...
 

Status

static uint32_t SPI_GetStatusFlags (SPI_Type *base)
 Gets the status flag. More...
 

Interrupts

static void SPI_EnableInterrupts (SPI_Type *base, uint32_t irqs)
 Enables the interrupt for the SPI. More...
 
static void SPI_DisableInterrupts (SPI_Type *base, uint32_t irqs)
 Disables the interrupt for the SPI. More...
 

DMA Control

void SPI_EnableTxDMA (SPI_Type *base, bool enable)
 Enables the DMA request from SPI txFIFO. More...
 
void SPI_EnableRxDMA (SPI_Type *base, bool enable)
 Enables the DMA request from SPI rxFIFO. More...
 

Bus Operations

void * SPI_GetConfig (SPI_Type *base)
 Returns the configurations. More...
 
status_t SPI_MasterSetBaud (SPI_Type *base, uint32_t baudrate_Bps, uint32_t srcClock_Hz)
 Sets the baud rate for SPI transfer. More...
 
void SPI_WriteData (SPI_Type *base, uint16_t data, uint32_t configFlags)
 Writes a data into the SPI data register. More...
 
static uint32_t SPI_ReadData (SPI_Type *base)
 Gets a data from the SPI data register. More...
 
static void SPI_SetTransferDelay (SPI_Type *base, const spi_delay_config_t *config)
 Set delay time for transfer. More...
 
void SPI_SetDummyData (SPI_Type *base, uint8_t dummyData)
 Set up the dummy data. More...
 

Transactional

status_t SPI_MasterTransferCreateHandle (SPI_Type *base, spi_master_handle_t *handle, spi_master_callback_t callback, void *userData)
 Initializes the SPI master handle. More...
 
status_t SPI_MasterTransferBlocking (SPI_Type *base, spi_transfer_t *xfer)
 Transfers a block of data using a polling method. More...
 
status_t SPI_MasterTransferNonBlocking (SPI_Type *base, spi_master_handle_t *handle, spi_transfer_t *xfer)
 Performs a non-blocking SPI interrupt transfer. More...
 
status_t SPI_MasterTransferGetCount (SPI_Type *base, spi_master_handle_t *handle, size_t *count)
 Gets the master transfer count. More...
 
void SPI_MasterTransferAbort (SPI_Type *base, spi_master_handle_t *handle)
 SPI master aborts a transfer using an interrupt. More...
 
void SPI_MasterTransferHandleIRQ (SPI_Type *base, spi_master_handle_t *handle)
 Interrupts the handler for the SPI. More...
 

Data Structure Documentation

struct spi_delay_config_t

Note: The DLY register controls several programmable delays related to SPI signalling, it stands for how many SPI clock time will be inserted. The maxinun value of these delay time is 15.

Data Fields

uint8_t preDelay
 Delay between SSEL assertion and the beginning of transfer. More...
 
uint8_t postDelay
 Delay between the end of transfer and SSEL deassertion. More...
 
uint8_t frameDelay
 Delay between frame to frame. More...
 
uint8_t transferDelay
 Delay between transfer to transfer. More...
 

Field Documentation

uint8_t spi_delay_config_t::preDelay
uint8_t spi_delay_config_t::postDelay
uint8_t spi_delay_config_t::frameDelay
uint8_t spi_delay_config_t::transferDelay
struct spi_master_config_t

Data Fields

bool enableLoopback
 Enable loopback for test purpose.
 
bool enableMaster
 Enable SPI at initialization time.
 
spi_clock_polarity_t polarity
 Clock polarity.
 
spi_clock_phase_t phase
 Clock phase.
 
spi_shift_direction_t direction
 MSB or LSB.
 
uint32_t baudRate_Bps
 Baud Rate for SPI in Hz.
 
spi_data_width_t dataWidth
 Width of the data.
 
spi_ssel_t sselNum
 Slave select number.
 
spi_spol_t sselPol
 Configure active CS polarity.
 
uint8_t txWatermark
 txFIFO watermark
 
uint8_t rxWatermark
 rxFIFO watermark
 
spi_delay_config_t delayConfig
 Delay configuration. More...
 

Field Documentation

spi_delay_config_t spi_master_config_t::delayConfig
struct spi_transfer_t

Data Fields

uint8_t * txData
 Send buffer.
 
uint8_t * rxData
 Receive buffer.
 
uint32_t configFlags
 Additional option to control transfer, spi_xfer_option_t. More...
 
size_t dataSize
 Transfer bytes.
 

Field Documentation

uint32_t spi_transfer_t::configFlags
struct spi_config_t
struct _spi_master_handle

Master handle type.

Data Fields

uint8_t *volatile txData
 Transfer buffer.
 
uint8_t *volatile rxData
 Receive buffer.
 
volatile size_t txRemainingBytes
 Number of data to be transmitted [in bytes].
 
volatile size_t rxRemainingBytes
 Number of data to be received [in bytes].
 
volatile int8_t toReceiveCount
 The number of data expected to receive in data width. More...
 
size_t totalByteCount
 A number of transfer bytes.
 
volatile uint32_t state
 SPI internal state.
 
spi_master_callback_t callback
 SPI callback.
 
void * userData
 Callback parameter.
 
uint8_t dataWidth
 Width of the data [Valid values: 1 to 16].
 
uint8_t sselNum
 Slave select number to be asserted when transferring data [Valid values: 0 to 3].
 
uint32_t configFlags
 Additional option to control transfer.
 
uint8_t txWatermark
 txFIFO watermark
 
uint8_t rxWatermark
 rxFIFO watermark
 

Field Documentation

volatile int8_t spi_master_handle_t::toReceiveCount

Since the received count and sent count should be the same to complete the transfer, if the sent count is x and the received count is y, toReceiveCount is x-y.

Macro Definition Documentation

#define FSL_SPI_DRIVER_VERSION   (MAKE_VERSION(2, 1, 0))
#define SPI_DUMMYDATA   (0xFFU)
#define SPI_RETRY_TIMES   0U /* Define to zero means keep waiting until the flag is assert/deassert. */

Typedef Documentation

typedef void(* spi_master_irq_handler_t)(SPI_Type *base, spi_master_handle_t *handle)

Enumeration Type Documentation

Enumerator
kSPI_FrameDelay 

A delay may be inserted, defined in the DLY register.

kSPI_FrameAssert 

SSEL will be deasserted at the end of a transfer.

Enumerator
kSPI_MsbFirst 

Data transfers start with most significant bit.

kSPI_LsbFirst 

Data transfers start with least significant bit.

Enumerator
kSPI_ClockPolarityActiveHigh 

Active-high SPI clock (idles low).

kSPI_ClockPolarityActiveLow 

Active-low SPI clock (idles high).

Enumerator
kSPI_ClockPhaseFirstEdge 

First edge on SCK occurs at the middle of the first cycle of a data transfer.

kSPI_ClockPhaseSecondEdge 

First edge on SCK occurs at the start of the first cycle of a data transfer.

Enumerator
kSPI_TxFifo0 

SPI tx watermark is empty.

kSPI_TxFifo1 

SPI tx watermark at 1 item.

kSPI_TxFifo2 

SPI tx watermark at 2 items.

kSPI_TxFifo3 

SPI tx watermark at 3 items.

kSPI_TxFifo4 

SPI tx watermark at 4 items.

kSPI_TxFifo5 

SPI tx watermark at 5 items.

kSPI_TxFifo6 

SPI tx watermark at 6 items.

kSPI_TxFifo7 

SPI tx watermark at 7 items.

Enumerator
kSPI_RxFifo1 

SPI rx watermark at 1 item.

kSPI_RxFifo2 

SPI rx watermark at 2 items.

kSPI_RxFifo3 

SPI rx watermark at 3 items.

kSPI_RxFifo4 

SPI rx watermark at 4 items.

kSPI_RxFifo5 

SPI rx watermark at 5 items.

kSPI_RxFifo6 

SPI rx watermark at 6 items.

kSPI_RxFifo7 

SPI rx watermark at 7 items.

kSPI_RxFifo8 

SPI rx watermark at 8 items.

Enumerator
kSPI_Data8Bits 

8 bits data width (7)

kSPI_Data16Bits 

16 bits data width (15)

enum spi_ssel_t
Enumerator
kSPI_Ssel0 

Slave select 0.

anonymous enum
Enumerator
kStatus_SPI_Busy 

SPI bus is busy.

kStatus_SPI_Idle 

SPI is idle.

kStatus_SPI_Error 

SPI error.

kStatus_SPI_BaudrateNotSupport 

Baudrate is not support in current clock source.

kStatus_SPI_Timeout 

SPI timeout polling status flags.

Enumerator
kSPI_RxErrIrq 

Rx error interrupt.

kSPI_TxErrIrq 

Tx error interrupt.

kSPI_RxLvlIrq 

Rx level interrupt.

kSPI_TxLvlIrq 

Tx level interrupt.

kSPI_SlaveSelectAssertIrq 

Slave select assert.

kSPI_SlaveSelectDeassertIrq 

Slave select deassert.

kSPI_MasterIdleIrq 

Master idle.

Enumerator
kSPI_TxEmptyFlag 

txFifo is empty

kSPI_TxNotFullFlag 

txFifo is not full

kSPI_RxNotEmptyFlag 

rxFIFO is not empty

kSPI_RxFullFlag 

rxFIFO is full

Function Documentation

uint32_t SPI_GetInstance ( SPI_Type *  base)
void SPI_MasterGetDefaultConfig ( spi_master_config_t *  config)

The purpose of this API is to get the configuration structure initialized for use in SPI_MasterInit(). User may use the initialized structure unchanged in SPI_MasterInit(), or modify some fields of the structure before calling SPI_MasterInit(). After calling this API, the master is ready to transfer. Example:

Parameters
configpointer to master config structure
status_t SPI_MasterInit ( SPI_Type *  base,
const spi_master_config_t *  config,
uint32_t  srcClock_Hz 
)

The configuration structure can be filled by user from scratch, or be set with default values by SPI_MasterGetDefaultConfig(). After calling this API, the slave is ready to transfer. Example

.baudRate_Bps = 400000,
...
};
SPI_MasterInit(SPI0, &config);
Parameters
baseSPI base pointer
configpointer to master configuration structure
srcClock_HzSource clock frequency.
void SPI_Deinit ( SPI_Type *  base)

Calling this API resets the SPI module, gates the SPI clock. The SPI module can't work unless calling the SPI_MasterInit/SPI_SlaveInit to initialize module.

Parameters
baseSPI base pointer
static void SPI_Enable ( SPI_Type *  base,
bool  enable 
)
inlinestatic
Parameters
baseSPI base pointer
enableor disable ( true = enable, false = disable)
static uint32_t SPI_GetStatusFlags ( SPI_Type *  base)
inlinestatic
Parameters
baseSPI base pointer
Returns
SPI Status, use status flag to AND _spi_statusflags could get the related status.
static void SPI_EnableInterrupts ( SPI_Type *  base,
uint32_t  irqs 
)
inlinestatic
Parameters
baseSPI base pointer
irqsSPI interrupt source. The parameter can be any combination of the following values:
  • kSPI_RxErrIrq
  • kSPI_TxErrIrq
  • kSPI_RxLvlIrq
  • kSPI_TxLvlIrq
  • kSPI_SlaveSelectAssertIrq
  • kSPI_SlaveSelectDeassertIrq
  • kSPI_MasterIdleIrq
static void SPI_DisableInterrupts ( SPI_Type *  base,
uint32_t  irqs 
)
inlinestatic
Parameters
baseSPI base pointer
irqsSPI interrupt source. The parameter can be any combination of the following values:
  • kSPI_RxErrIrq
  • kSPI_TxErrIrq
  • kSPI_RxLvlIrq
  • kSPI_TxLvlIrq
  • kSPI_SlaveSelectAssertIrq
  • kSPI_SlaveSelectDeassertIrq
  • kSPI_MasterIdleIrq
void SPI_EnableTxDMA ( SPI_Type *  base,
bool  enable 
)
Parameters
baseSPI base pointer
enableTrue means enable DMA, false means disable DMA
void SPI_EnableRxDMA ( SPI_Type *  base,
bool  enable 
)
Parameters
baseSPI base pointer
enableTrue means enable DMA, false means disable DMA
void* SPI_GetConfig ( SPI_Type *  base)
Parameters
baseSPI peripheral address.
Returns
return configurations which contain datawidth and SSEL numbers. return data type is a pointer of spi_config_t.
status_t SPI_MasterSetBaud ( SPI_Type *  base,
uint32_t  baudrate_Bps,
uint32_t  srcClock_Hz 
)

This is only used in master.

Parameters
baseSPI base pointer
baudrate_Bpsbaud rate needed in Hz.
srcClock_HzSPI source clock frequency in Hz.
void SPI_WriteData ( SPI_Type *  base,
uint16_t  data,
uint32_t  configFlags 
)
Parameters
baseSPI base pointer
dataneeds to be write.
configFlagstransfer configuration options spi_xfer_option_t
static uint32_t SPI_ReadData ( SPI_Type *  base)
inlinestatic
Parameters
baseSPI base pointer
Returns
Data in the register.
static void SPI_SetTransferDelay ( SPI_Type *  base,
const spi_delay_config_t *  config 
)
inlinestatic
   the delay uint is SPI clock time, maximum value is 0xF.
Parameters
baseSPI base pointer
configconfiguration for delay option spi_delay_config_t.
void SPI_SetDummyData ( SPI_Type *  base,
uint8_t  dummyData 
)
Parameters
baseSPI peripheral address.
dummyDataData to be transferred when tx buffer is NULL.
status_t SPI_MasterTransferCreateHandle ( SPI_Type *  base,
spi_master_handle_t *  handle,
spi_master_callback_t  callback,
void *  userData 
)

This function initializes the SPI master handle which can be used for other SPI master transactional APIs. Usually, for a specified SPI instance, call this API once to get the initialized handle.

Parameters
baseSPI peripheral base address.
handleSPI handle pointer.
callbackCallback function.
userDataUser data.
status_t SPI_MasterTransferBlocking ( SPI_Type *  base,
spi_transfer_t *  xfer 
)
Parameters
baseSPI base pointer
xferpointer to spi_xfer_config_t structure
Return values
kStatus_SuccessSuccessfully start a transfer.
kStatus_InvalidArgumentInput argument is invalid.
kStatus_SPI_TimeoutThe transfer timed out and was aborted.
status_t SPI_MasterTransferNonBlocking ( SPI_Type *  base,
spi_master_handle_t *  handle,
spi_transfer_t *  xfer 
)
Parameters
baseSPI peripheral base address.
handlepointer to spi_master_handle_t structure which stores the transfer state
xferpointer to spi_xfer_config_t structure
Return values
kStatus_SuccessSuccessfully start a transfer.
kStatus_InvalidArgumentInput argument is invalid.
kStatus_SPI_BusySPI is not idle, is running another transfer.
status_t SPI_MasterTransferGetCount ( SPI_Type *  base,
spi_master_handle_t *  handle,
size_t *  count 
)

This function gets the master transfer count.

Parameters
baseSPI peripheral base address.
handlePointer to the spi_master_handle_t structure which stores the transfer state.
countThe number of bytes transferred by using the non-blocking transaction.
Returns
status of status_t.
void SPI_MasterTransferAbort ( SPI_Type *  base,
spi_master_handle_t *  handle 
)

This function aborts a transfer using an interrupt.

Parameters
baseSPI peripheral base address.
handlePointer to the spi_master_handle_t structure which stores the transfer state.
void SPI_MasterTransferHandleIRQ ( SPI_Type *  base,
spi_master_handle_t *  handle 
)
Parameters
baseSPI peripheral base address.
handlepointer to spi_master_handle_t structure which stores the transfer state.

Variable Documentation

volatile uint8_t s_dummyData[]