MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages

Overview

This section describes the programming interface of the SPI DMA driver.

Files

file  fsl_spi.h
 

Data Structures

struct  spi_master_config_t
 SPI master user configure structure. More...
 
struct  spi_slave_config_t
 SPI slave user configure structure. More...
 
struct  spi_transfer_t
 SPI transfer structure. More...
 
struct  spi_config_t
 Internal configuration structure used in 'spi' and 'spi_dma' driver. More...
 
struct  spi_master_handle_t
 SPI transfer handle structure. More...
 

Typedefs

typedef spi_master_handle_t spi_slave_handle_t
 Slave handle type.
 
typedef void(* spi_master_callback_t )(SPI_Type *base, spi_master_handle_t *handle, status_t status, void *userData)
 SPI master callback for finished transmit.
 
typedef void(* spi_slave_callback_t )(SPI_Type *base, spi_slave_handle_t *handle, status_t status, void *userData)
 SPI slave callback for finished transmit.
 

Enumerations

enum  spi_xfer_option_t {
  kSPI_FrameDelay = (SPI_FIFOWR_EOF_MASK),
  kSPI_FrameAssert = (SPI_FIFOWR_EOT_MASK)
}
 SPI transfer option. More...
 
enum  spi_shift_direction_t {
  kSPI_MsbFirst = 0U,
  kSPI_LsbFirst = 1U
}
 SPI data shifter direction options. More...
 
enum  spi_clock_polarity_t {
  kSPI_ClockPolarityActiveHigh = 0x0U,
  kSPI_ClockPolarityActiveLow
}
 SPI clock polarity configuration. More...
 
enum  spi_clock_phase_t {
  kSPI_ClockPhaseFirstEdge = 0x0U,
  kSPI_ClockPhaseSecondEdge
}
 SPI clock phase configuration. More...
 
enum  spi_txfifo_watermark_t {
  kSPI_TxFifo0 = 0,
  kSPI_TxFifo1 = 1,
  kSPI_TxFifo2 = 2,
  kSPI_TxFifo3 = 3,
  kSPI_TxFifo4 = 4,
  kSPI_TxFifo5 = 5,
  kSPI_TxFifo6 = 6,
  kSPI_TxFifo7 = 7
}
 txFIFO watermark values More...
 
enum  spi_rxfifo_watermark_t {
  kSPI_RxFifo1 = 0,
  kSPI_RxFifo2 = 1,
  kSPI_RxFifo3 = 2,
  kSPI_RxFifo4 = 3,
  kSPI_RxFifo5 = 4,
  kSPI_RxFifo6 = 5,
  kSPI_RxFifo7 = 6,
  kSPI_RxFifo8 = 7
}
 rxFIFO watermark values More...
 
enum  spi_data_width_t {
  kSPI_Data4Bits = 3,
  kSPI_Data5Bits = 4,
  kSPI_Data6Bits = 5,
  kSPI_Data7Bits = 6,
  kSPI_Data8Bits = 7,
  kSPI_Data9Bits = 8,
  kSPI_Data10Bits = 9,
  kSPI_Data11Bits = 10,
  kSPI_Data12Bits = 11,
  kSPI_Data13Bits = 12,
  kSPI_Data14Bits = 13,
  kSPI_Data15Bits = 14,
  kSPI_Data16Bits = 15
}
 Transfer data width. More...
 
enum  spi_ssel_t {
  kSPI_Ssel0 = 0,
  kSPI_Ssel1 = 1,
  kSPI_Ssel2 = 2,
  kSPI_Ssel3 = 3
}
 Slave select. More...
 
enum  spi_spol_t
 ssel polarity
 
enum  _spi_status {
  kStatus_SPI_Busy = MAKE_STATUS(kStatusGroup_LPC_SPI, 0),
  kStatus_SPI_Idle = MAKE_STATUS(kStatusGroup_LPC_SPI, 1),
  kStatus_SPI_Error = MAKE_STATUS(kStatusGroup_LPC_SPI, 2),
  kStatus_SPI_BaudrateNotSupport
}
 SPI transfer status. More...
 
enum  _spi_interrupt_enable {
  kSPI_RxLvlIrq = SPI_FIFOINTENSET_RXLVL_MASK,
  kSPI_TxLvlIrq = SPI_FIFOINTENSET_TXLVL_MASK
}
 SPI interrupt sources. More...
 
enum  _spi_statusflags {
  kSPI_TxEmptyFlag = SPI_FIFOSTAT_TXEMPTY_MASK,
  kSPI_TxNotFullFlag = SPI_FIFOSTAT_TXNOTFULL_MASK,
  kSPI_RxNotEmptyFlag = SPI_FIFOSTAT_RXNOTEMPTY_MASK,
  kSPI_RxFullFlag = SPI_FIFOSTAT_RXFULL_MASK
}
 SPI status flags. More...
 

Functions

uint32_t SPI_GetInstance (SPI_Type *base)
 Returns instance number for SPI peripheral base address. More...
 

Driver version

#define FSL_SPI_DRIVER_VERSION   (MAKE_VERSION(2, 0, 0))
 USART driver version 2.0.0. More...
 

Initialization and deinitialization

void SPI_MasterGetDefaultConfig (spi_master_config_t *config)
 Sets the SPI master configuration structure to default values. More...
 
status_t SPI_MasterInit (SPI_Type *base, const spi_master_config_t *config, uint32_t srcClock_Hz)
 Initializes the SPI with master configuration. More...
 
void SPI_SlaveGetDefaultConfig (spi_slave_config_t *config)
 Sets the SPI slave configuration structure to default values. More...
 
status_t SPI_SlaveInit (SPI_Type *base, const spi_slave_config_t *config)
 Initializes the SPI with slave configuration. More...
 
void SPI_Deinit (SPI_Type *base)
 De-initializes the SPI. More...
 
static void SPI_Enable (SPI_Type *base, bool enable)
 Enable or disable the SPI Master or Slave. More...
 

Status

static uint32_t SPI_GetStatusFlags (SPI_Type *base)
 Gets the status flag. More...
 

Interrupts

static void SPI_EnableInterrupts (SPI_Type *base, uint32_t irqs)
 Enables the interrupt for the SPI. More...
 
static void SPI_DisableInterrupts (SPI_Type *base, uint32_t irqs)
 Disables the interrupt for the SPI. More...
 

DMA Control

void SPI_EnableTxDMA (SPI_Type *base, bool enable)
 Enables the DMA request from SPI txFIFO. More...
 
void SPI_EnableRxDMA (SPI_Type *base, bool enable)
 Enables the DMA request from SPI rxFIFO. More...
 

Bus Operations

status_t SPI_MasterSetBaud (SPI_Type *base, uint32_t baudrate_Bps, uint32_t srcClock_Hz)
 Sets the baud rate for SPI transfer. More...
 
void SPI_WriteData (SPI_Type *base, uint16_t data, uint32_t configFlags)
 Writes a data into the SPI data register. More...
 
static uint32_t SPI_ReadData (SPI_Type *base)
 Gets a data from the SPI data register. More...
 

Transactional

status_t SPI_MasterTransferCreateHandle (SPI_Type *base, spi_master_handle_t *handle, spi_master_callback_t callback, void *userData)
 Initializes the SPI master handle. More...
 
status_t SPI_MasterTransferBlocking (SPI_Type *base, spi_transfer_t *xfer)
 Transfers a block of data using a polling method. More...
 
status_t SPI_MasterTransferNonBlocking (SPI_Type *base, spi_master_handle_t *handle, spi_transfer_t *xfer)
 Performs a non-blocking SPI interrupt transfer. More...
 
status_t SPI_MasterTransferGetCount (SPI_Type *base, spi_master_handle_t *handle, size_t *count)
 Gets the master transfer count. More...
 
void SPI_MasterTransferAbort (SPI_Type *base, spi_master_handle_t *handle)
 SPI master aborts a transfer using an interrupt. More...
 
void SPI_MasterTransferHandleIRQ (SPI_Type *base, spi_master_handle_t *handle)
 Interrupts the handler for the SPI. More...
 
static status_t SPI_SlaveTransferCreateHandle (SPI_Type *base, spi_slave_handle_t *handle, spi_slave_callback_t callback, void *userData)
 Initializes the SPI slave handle. More...
 
static status_t SPI_SlaveTransferNonBlocking (SPI_Type *base, spi_slave_handle_t *handle, spi_transfer_t *xfer)
 Performs a non-blocking SPI slave interrupt transfer. More...
 
static status_t SPI_SlaveTransferGetCount (SPI_Type *base, spi_slave_handle_t *handle, size_t *count)
 Gets the slave transfer count. More...
 
static void SPI_SlaveTransferAbort (SPI_Type *base, spi_slave_handle_t *handle)
 SPI slave aborts a transfer using an interrupt. More...
 
static void SPI_SlaveTransferHandleIRQ (SPI_Type *base, spi_slave_handle_t *handle)
 Interrupts a handler for the SPI slave. More...
 

Data Structure Documentation

struct spi_master_config_t

Data Fields

bool enableLoopback
 Enable loopback for test purpose.
 
bool enableMaster
 Enable SPI at initialization time.
 
spi_clock_polarity_t polarity
 Clock polarity.
 
spi_clock_phase_t phase
 Clock phase.
 
spi_shift_direction_t direction
 MSB or LSB.
 
uint32_t baudRate_Bps
 Baud Rate for SPI in Hz.
 
spi_data_width_t dataWidth
 Width of the data.
 
spi_ssel_t sselNum
 Slave select number.
 
spi_spol_t sselPol
 Configure active CS polarity.
 
spi_txfifo_watermark_t txWatermark
 txFIFO watermark
 
spi_rxfifo_watermark_t rxWatermark
 rxFIFO watermark
 
struct spi_slave_config_t

Data Fields

bool enableSlave
 Enable SPI at initialization time.
 
spi_clock_polarity_t polarity
 Clock polarity.
 
spi_clock_phase_t phase
 Clock phase.
 
spi_shift_direction_t direction
 MSB or LSB.
 
spi_data_width_t dataWidth
 Width of the data.
 
spi_spol_t sselPol
 Configure active CS polarity.
 
spi_txfifo_watermark_t txWatermark
 txFIFO watermark
 
spi_rxfifo_watermark_t rxWatermark
 rxFIFO watermark
 
struct spi_transfer_t

Data Fields

uint8_t * txData
 Send buffer.
 
uint8_t * rxData
 Receive buffer.
 
uint32_t configFlags
 Additional option to control transfer.
 
size_t dataSize
 Transfer bytes.
 
struct spi_config_t
struct _spi_master_handle

Master handle type.

Data Fields

uint8_t *volatile txData
 Transfer buffer.
 
uint8_t *volatile rxData
 Receive buffer.
 
volatile size_t txRemainingBytes
 Number of data to be transmitted [in bytes].
 
volatile size_t rxRemainingBytes
 Number of data to be received [in bytes].
 
volatile size_t toReceiveCount
 Receive data remaining in bytes.
 
size_t totalByteCount
 A number of transfer bytes.
 
volatile uint32_t state
 SPI internal state.
 
spi_master_callback_t callback
 SPI callback.
 
void * userData
 Callback parameter.
 
uint8_t dataWidth
 Width of the data [Valid values: 1 to 16].
 
uint8_t sselNum
 Slave select number to be asserted when transferring data [Valid values: 0 to 3].
 
uint32_t configFlags
 Additional option to control transfer.
 
spi_txfifo_watermark_t txWatermark
 txFIFO watermark
 
spi_rxfifo_watermark_t rxWatermark
 rxFIFO watermark
 

Macro Definition Documentation

#define FSL_SPI_DRIVER_VERSION   (MAKE_VERSION(2, 0, 0))

Enumeration Type Documentation

Enumerator
kSPI_FrameDelay 

Delay chip select.

kSPI_FrameAssert 

When transfer ends, assert chip select.

Enumerator
kSPI_MsbFirst 

Data transfers start with most significant bit.

kSPI_LsbFirst 

Data transfers start with least significant bit.

Enumerator
kSPI_ClockPolarityActiveHigh 

Active-high SPI clock (idles low).

kSPI_ClockPolarityActiveLow 

Active-low SPI clock (idles high).

Enumerator
kSPI_ClockPhaseFirstEdge 

First edge on SCK occurs at the middle of the first cycle of a data transfer.

kSPI_ClockPhaseSecondEdge 

First edge on SCK occurs at the start of the first cycle of a data transfer.

Enumerator
kSPI_TxFifo0 

SPI tx watermark is empty.

kSPI_TxFifo1 

SPI tx watermark at 1 item.

kSPI_TxFifo2 

SPI tx watermark at 2 items.

kSPI_TxFifo3 

SPI tx watermark at 3 items.

kSPI_TxFifo4 

SPI tx watermark at 4 items.

kSPI_TxFifo5 

SPI tx watermark at 5 items.

kSPI_TxFifo6 

SPI tx watermark at 6 items.

kSPI_TxFifo7 

SPI tx watermark at 7 items.

Enumerator
kSPI_RxFifo1 

SPI rx watermark at 1 item.

kSPI_RxFifo2 

SPI rx watermark at 2 items.

kSPI_RxFifo3 

SPI rx watermark at 3 items.

kSPI_RxFifo4 

SPI rx watermark at 4 items.

kSPI_RxFifo5 

SPI rx watermark at 5 items.

kSPI_RxFifo6 

SPI rx watermark at 6 items.

kSPI_RxFifo7 

SPI rx watermark at 7 items.

kSPI_RxFifo8 

SPI rx watermark at 8 items.

Enumerator
kSPI_Data4Bits 

4 bits data width

kSPI_Data5Bits 

5 bits data width

kSPI_Data6Bits 

6 bits data width

kSPI_Data7Bits 

7 bits data width

kSPI_Data8Bits 

8 bits data width

kSPI_Data9Bits 

9 bits data width

kSPI_Data10Bits 

10 bits data width

kSPI_Data11Bits 

11 bits data width

kSPI_Data12Bits 

12 bits data width

kSPI_Data13Bits 

13 bits data width

kSPI_Data14Bits 

14 bits data width

kSPI_Data15Bits 

15 bits data width

kSPI_Data16Bits 

16 bits data width

enum spi_ssel_t
Enumerator
kSPI_Ssel0 

Slave select 0.

kSPI_Ssel1 

Slave select 1.

kSPI_Ssel2 

Slave select 2.

kSPI_Ssel3 

Slave select 3.

Enumerator
kStatus_SPI_Busy 

SPI bus is busy.

kStatus_SPI_Idle 

SPI is idle.

kStatus_SPI_Error 

SPI error.

kStatus_SPI_BaudrateNotSupport 

Baudrate is not support in current clock source.

Enumerator
kSPI_RxLvlIrq 

Rx level interrupt.

kSPI_TxLvlIrq 

Tx level interrupt.

Enumerator
kSPI_TxEmptyFlag 

txFifo is empty

kSPI_TxNotFullFlag 

txFifo is not full

kSPI_RxNotEmptyFlag 

rxFIFO is not empty

kSPI_RxFullFlag 

rxFIFO is full

Function Documentation

uint32_t SPI_GetInstance ( SPI_Type *  base)
void SPI_MasterGetDefaultConfig ( spi_master_config_t *  config)

The purpose of this API is to get the configuration structure initialized for use in SPI_MasterInit(). User may use the initialized structure unchanged in SPI_MasterInit(), or modify some fields of the structure before calling SPI_MasterInit(). After calling this API, the master is ready to transfer. Example:

Parameters
configpointer to master config structure
status_t SPI_MasterInit ( SPI_Type *  base,
const spi_master_config_t *  config,
uint32_t  srcClock_Hz 
)

The configuration structure can be filled by user from scratch, or be set with default values by SPI_MasterGetDefaultConfig(). After calling this API, the slave is ready to transfer. Example

.baudRate_Bps = 400000,
...
};
SPI_MasterInit(SPI0, &config);
Parameters
baseSPI base pointer
configpointer to master configuration structure
srcClock_HzSource clock frequency.
void SPI_SlaveGetDefaultConfig ( spi_slave_config_t *  config)

The purpose of this API is to get the configuration structure initialized for use in SPI_SlaveInit(). Modify some fields of the structure before calling SPI_SlaveInit(). Example:

Parameters
configpointer to slave configuration structure
status_t SPI_SlaveInit ( SPI_Type *  base,
const spi_slave_config_t *  config 
)

The configuration structure can be filled by user from scratch or be set with default values by SPI_SlaveGetDefaultConfig(). After calling this API, the slave is ready to transfer. Example

.polarity = flexSPIClockPolarity_ActiveHigh;
.phase = flexSPIClockPhase_FirstEdge;
.direction = flexSPIMsbFirst;
...
};
SPI_SlaveInit(SPI0, &config);
Parameters
baseSPI base pointer
configpointer to slave configuration structure
void SPI_Deinit ( SPI_Type *  base)

Calling this API resets the SPI module, gates the SPI clock. The SPI module can't work unless calling the SPI_MasterInit/SPI_SlaveInit to initialize module.

Parameters
baseSPI base pointer
static void SPI_Enable ( SPI_Type *  base,
bool  enable 
)
inlinestatic
Parameters
baseSPI base pointer
enableor disable ( true = enable, false = disable)
static uint32_t SPI_GetStatusFlags ( SPI_Type *  base)
inlinestatic
Parameters
baseSPI base pointer
Returns
SPI Status, use status flag to AND _spi_statusflags could get the related status.
static void SPI_EnableInterrupts ( SPI_Type *  base,
uint32_t  irqs 
)
inlinestatic
Parameters
baseSPI base pointer
irqsSPI interrupt source. The parameter can be any combination of the following values:
  • kSPI_RxLvlIrq
  • kSPI_TxLvlIrq
static void SPI_DisableInterrupts ( SPI_Type *  base,
uint32_t  irqs 
)
inlinestatic
Parameters
baseSPI base pointer
irqsSPI interrupt source. The parameter can be any combination of the following values:
  • kSPI_RxLvlIrq
  • kSPI_TxLvlIrq
void SPI_EnableTxDMA ( SPI_Type *  base,
bool  enable 
)
Parameters
baseSPI base pointer
enableTrue means enable DMA, false means disable DMA
void SPI_EnableRxDMA ( SPI_Type *  base,
bool  enable 
)
Parameters
baseSPI base pointer
enableTrue means enable DMA, false means disable DMA
status_t SPI_MasterSetBaud ( SPI_Type *  base,
uint32_t  baudrate_Bps,
uint32_t  srcClock_Hz 
)

This is only used in master.

Parameters
baseSPI base pointer
baudrate_Bpsbaud rate needed in Hz.
srcClock_HzSPI source clock frequency in Hz.
void SPI_WriteData ( SPI_Type *  base,
uint16_t  data,
uint32_t  configFlags 
)
Parameters
baseSPI base pointer
dataneeds to be write.
configFlagstransfer configuration options spi_xfer_option_t
static uint32_t SPI_ReadData ( SPI_Type *  base)
inlinestatic
Parameters
baseSPI base pointer
Returns
Data in the register.
status_t SPI_MasterTransferCreateHandle ( SPI_Type *  base,
spi_master_handle_t *  handle,
spi_master_callback_t  callback,
void *  userData 
)

This function initializes the SPI master handle which can be used for other SPI master transactional APIs. Usually, for a specified SPI instance, call this API once to get the initialized handle.

Parameters
baseSPI peripheral base address.
handleSPI handle pointer.
callbackCallback function.
userDataUser data.
status_t SPI_MasterTransferBlocking ( SPI_Type *  base,
spi_transfer_t *  xfer 
)
Parameters
baseSPI base pointer
xferpointer to spi_xfer_config_t structure
Return values
kStatus_SuccessSuccessfully start a transfer.
kStatus_InvalidArgumentInput argument is invalid.
status_t SPI_MasterTransferNonBlocking ( SPI_Type *  base,
spi_master_handle_t *  handle,
spi_transfer_t *  xfer 
)
Parameters
baseSPI peripheral base address.
handlepointer to spi_master_handle_t structure which stores the transfer state
xferpointer to spi_xfer_config_t structure
Return values
kStatus_SuccessSuccessfully start a transfer.
kStatus_InvalidArgumentInput argument is invalid.
kStatus_SPI_BusySPI is not idle, is running another transfer.
status_t SPI_MasterTransferGetCount ( SPI_Type *  base,
spi_master_handle_t *  handle,
size_t *  count 
)

This function gets the master transfer count.

Parameters
baseSPI peripheral base address.
handlePointer to the spi_master_handle_t structure which stores the transfer state.
countThe number of bytes transferred by using the non-blocking transaction.
Returns
status of status_t.
void SPI_MasterTransferAbort ( SPI_Type *  base,
spi_master_handle_t *  handle 
)

This function aborts a transfer using an interrupt.

Parameters
baseSPI peripheral base address.
handlePointer to the spi_master_handle_t structure which stores the transfer state.
void SPI_MasterTransferHandleIRQ ( SPI_Type *  base,
spi_master_handle_t *  handle 
)
Parameters
baseSPI peripheral base address.
handlepointer to spi_master_handle_t structure which stores the transfer state.
static status_t SPI_SlaveTransferCreateHandle ( SPI_Type *  base,
spi_slave_handle_t *  handle,
spi_slave_callback_t  callback,
void *  userData 
)
inlinestatic

This function initializes the SPI slave handle which can be used for other SPI slave transactional APIs. Usually, for a specified SPI instance, call this API once to get the initialized handle.

Parameters
baseSPI peripheral base address.
handleSPI handle pointer.
callbackCallback function.
userDataUser data.
static status_t SPI_SlaveTransferNonBlocking ( SPI_Type *  base,
spi_slave_handle_t *  handle,
spi_transfer_t *  xfer 
)
inlinestatic
Note
The API returns immediately after the transfer initialization is finished.
Parameters
baseSPI peripheral base address.
handlepointer to spi_master_handle_t structure which stores the transfer state
xferpointer to spi_xfer_config_t structure
Return values
kStatus_SuccessSuccessfully start a transfer.
kStatus_InvalidArgumentInput argument is invalid.
kStatus_SPI_BusySPI is not idle, is running another transfer.
static status_t SPI_SlaveTransferGetCount ( SPI_Type *  base,
spi_slave_handle_t *  handle,
size_t *  count 
)
inlinestatic

This function gets the slave transfer count.

Parameters
baseSPI peripheral base address.
handlePointer to the spi_master_handle_t structure which stores the transfer state.
countThe number of bytes transferred by using the non-blocking transaction.
Returns
status of status_t.
static void SPI_SlaveTransferAbort ( SPI_Type *  base,
spi_slave_handle_t *  handle 
)
inlinestatic

This function aborts a transfer using an interrupt.

Parameters
baseSPI peripheral base address.
handlePointer to the spi_slave_handle_t structure which stores the transfer state.
static void SPI_SlaveTransferHandleIRQ ( SPI_Type *  base,
spi_slave_handle_t *  handle 
)
inlinestatic
Parameters
baseSPI peripheral base address.
handlepointer to spi_slave_handle_t structure which stores the transfer state