MCUXpresso SDK API Reference Manual  Rev 2.13.0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
AFE: Analog Front End Driver

Overview

The MCUXpresso SDK provides a driver for the Analog Front End (AFE) module of MCUXpresso SDK devices.

The Analog Front End or AFE is an integrated module that is comprised of ΣΔADCs, PGA, filtering, and phase compensation blocks. The AFE is responsible for measuring the phase voltage, phase current, and neutral current.

Function groups

Channel configuration structures

The driver uses instances of the channel configuration structures to configuration and initialization AFE channel. This structure holds the settings of the AFE measurement channel. The settings include AFE hardware/software triggering, AFE continuous/Single conversion mode, AFE channel mode, AFE channel analog gain, AFE channel oversampling ration. The AFE channel mode selects whether the bypass mode is enabled or disabled and the external clock selection.

User configuration structures

The AFE driver uses instances of the user configuration structure afe_config_t for the AFE driver configuration. This structure holds the configuration which is common for all AFE channels. The settings include AFE low-power mode, AFE result format, AFE clock divider mode, AFE clock source mode, and AFE start up delay of modulators.

AFE Initialization

To initialize the AFE driver for a typical use case, call the AFE_GetDefaultConfig() function which populates the structure. Then, call the AFE_Init() function and pass the base address of the AFE peripheral and a pointer to the user configuration structure.

To configure the AFE channel, for a typical use case call the AFE_GetDefaultChnConfig() function which populates the structure. Then, call the AFE_SetChnConfig() function and pass the base address of the AFE peripheral and a pointer to the channel configuration structure.

AFE Conversion

The driver contains functions for software triggering, a channel delay after trigger setting, a result (raw or converted to right justified), reading, and waiting functions.

If the software triggering is enabled (hwTriggerEnable parameter in afe_chn_config_t is a false value), call the AFE_SoftTriggerConv() function to start conversion.

Typical use case

AFE Initialization

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/afe

AFE Conversion

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/afe

Data Structures

struct  afe_channel_config_t
 Defines the structure to initialize the AFE channel. More...
 
struct  afe_config_t
 Defines the structure to initialize the AFE module. More...
 

Enumerations

enum  _afe_channel_status_flag {
  kAFE_Channel0OverflowFlag = AFE_SR_OVR0_MASK,
  kAFE_Channel1OverflowFlag = AFE_SR_OVR1_MASK,
  kAFE_Channel2OverflowFlag = AFE_SR_OVR2_MASK,
  kAFE_Channel0ReadyFlag = AFE_SR_RDY0_MASK,
  kAFE_Channel1ReadyFlag = AFE_SR_RDY1_MASK,
  kAFE_Channel2ReadyFlag = AFE_SR_RDY2_MASK,
  kAFE_Channel0ConversionCompleteFlag = AFE_SR_COC0_MASK,
  kAFE_Channel1ConversionCompleteFlag = AFE_SR_COC1_MASK,
  kAFE_Channel2ConversionCompleteFlag = AFE_SR_COC2_MASK,
  kAFE_Channel3OverflowFlag = AFE_SR_OVR3_MASK,
  kAFE_Channel3ReadyFlag = AFE_SR_RDY3_MASK,
  kAFE_Channel3ConversionCompleteFlag = AFE_SR_COC3_MASK
}
 Defines the type of status flags. More...
 
enum  {
  kAFE_Channel0InterruptEnable = AFE_DI_INTEN0_MASK,
  kAFE_Channel1InterruptEnable = AFE_DI_INTEN1_MASK,
  kAFE_Channel2InterruptEnable = AFE_DI_INTEN2_MASK,
  kAFE_Channel3InterruptEnable = AFE_DI_INTEN3_MASK
}
 Defines AFE interrupt enable. More...
 
enum  {
  kAFE_Channel0DMAEnable = AFE_DI_DMAEN0_MASK,
  kAFE_Channel1DMAEnable = AFE_DI_DMAEN1_MASK,
  kAFE_Channel2DMAEnable = AFE_DI_DMAEN2_MASK,
  kAFE_Channel3DMAEnable = AFE_DI_DMAEN3_MASK
}
 Defines AFE DMA enable. More...
 
enum  {
  kAFE_Channel0Trigger = AFE_CR_SOFT_TRG0_MASK,
  kAFE_Channel1Trigger = AFE_CR_SOFT_TRG1_MASK,
  kAFE_Channel2Trigger = AFE_CR_SOFT_TRG2_MASK,
  kAFE_Channel3Trigger = AFE_CR_SOFT_TRG3_MASK
}
 Defines AFE channel trigger flag. More...
 
enum  afe_decimator_oversample_ratio_t {
  kAFE_DecimatorOversampleRatio64 = 0U,
  kAFE_DecimatorOversampleRatio128 = 1U,
  kAFE_DecimatorOversampleRatio256 = 2U,
  kAFE_DecimatorOversampleRatio512 = 3U,
  kAFE_DecimatorOversampleRatio1024 = 4U,
  kAFE_DecimatorOversampleRatio2048 = 5U
}
 AFE OSR modes. More...
 
enum  afe_result_format_t {
  kAFE_ResultFormatLeft = 0U,
  kAFE_ResultFormatRight = 1U
}
 Defines the AFE result format modes. More...
 
enum  afe_clock_divider_t {
  kAFE_ClockDivider1 = 0U,
  kAFE_ClockDivider2 = 1U,
  kAFE_ClockDivider4 = 2U,
  kAFE_ClockDivider8 = 3U,
  kAFE_ClockDivider16 = 4U,
  kAFE_ClockDivider32 = 5U,
  kAFE_ClockDivider64 = 6U,
  kAFE_ClockDivider128 = 7U,
  kAFE_ClockDivider256 = 8U
}
 Defines the AFE clock divider modes. More...
 
enum  afe_clock_source_t {
  kAFE_ClockSource0 = 0U,
  kAFE_ClockSource1 = 1U,
  kAFE_ClockSource2 = 2U,
  kAFE_ClockSource3 = 3U
}
 Defines the AFE clock source modes. More...
 
enum  afe_pga_gain_t {
  kAFE_PgaDisable = 0U,
  kAFE_PgaGain1 = 1U,
  kAFE_PgaGain2 = 2U,
  kAFE_PgaGain4 = 3U,
  kAFE_PgaGain8 = 4U,
  kAFE_PgaGain16 = 5U,
  kAFE_PgaGain32 = 6U
}
 Defines the PGA's values. More...
 
enum  afe_bypass_mode_t {
  kAFE_BypassInternalClockPositiveEdge = 0U,
  kAFE_BypassExternalClockPositiveEdge = 1U,
  kAFE_BypassInternalClockNegativeEdge = 2U,
  kAFE_BypassExternalClockNegativeEdge = 3U,
  kAFE_BypassDisable = 4U
}
 Defines the bypass modes. More...
 

Driver version

#define FSL_AFE_DRIVER_VERSION   (MAKE_VERSION(2, 0, 2))
 Version 2.0.2. More...
 

AFE Initialization

void AFE_Init (AFE_Type *base, const afe_config_t *config)
 Initialization for the AFE module. More...
 
void AFE_Deinit (AFE_Type *base)
 De-Initialization for the AFE module. More...
 
void AFE_GetDefaultConfig (afe_config_t *config)
 Fills the user configure structure. More...
 
static void AFE_SoftwareReset (AFE_Type *base, bool enable)
 Software reset the AFE module. More...
 
static void AFE_Enable (AFE_Type *base, bool enable)
 Enables all configured AFE channels. More...
 

AFE Conversion

void AFE_SetChannelConfig (AFE_Type *base, uint32_t channel, const afe_channel_config_t *config)
 Configure the selected AFE channel. More...
 
void AFE_GetDefaultChannelConfig (afe_channel_config_t *config)
 Fills the channel configuration structure. More...
 
uint32_t AFE_GetChannelConversionValue (AFE_Type *base, uint32_t channel)
 Reads the raw conversion value. More...
 
static void AFE_DoSoftwareTriggerChannel (AFE_Type *base, uint32_t mask)
 Triggers the AFE conversion by software. More...
 
static uint32_t AFE_GetChannelStatusFlags (AFE_Type *base)
 Gets the AFE status flag state. More...
 
void AFE_SetChannelPhaseDelayValue (AFE_Type *base, uint32_t channel, uint32_t value)
 Sets phase delays value. More...
 
static void AFE_SetChannelPhasetDelayOk (AFE_Type *base)
 Asserts the phase delay setting. More...
 
static void AFE_EnableChannelInterrupts (AFE_Type *base, uint32_t mask)
 Enables AFE interrupt. More...
 
static void AFE_DisableChannelInterrupts (AFE_Type *base, uint32_t mask)
 Disables AFE interrupt. More...
 
static uint32_t AFE_GetEnabledChannelInterrupts (AFE_Type *base)
 Returns mask of all enabled AFE interrupts. More...
 
void AFE_EnableChannelDMA (AFE_Type *base, uint32_t mask, bool enable)
 Enables/Disables AFE DMA. More...
 

Data Structure Documentation

struct afe_channel_config_t

This structure keeps the configuration for the AFE channel.

Data Fields

bool enableHardwareTrigger
 Enable triggering by hardware. More...
 
bool enableContinuousConversion
 Enable continuous conversion mode. More...
 
afe_bypass_mode_t channelMode
 Select if channel is in bypassed mode. More...
 
afe_pga_gain_t pgaGainSelect
 Select the analog gain applied to the input signal. More...
 
afe_decimator_oversample_ratio_t decimatorOversampleRatio
 Select the over sampling ration. More...
 

Field Documentation

bool afe_channel_config_t::enableHardwareTrigger
bool afe_channel_config_t::enableContinuousConversion
afe_bypass_mode_t afe_channel_config_t::channelMode
afe_pga_gain_t afe_channel_config_t::pgaGainSelect
afe_decimator_oversample_ratio_t afe_channel_config_t::decimatorOversampleRatio
struct afe_config_t

This structure keeps the configuration for the AFE module.

Data Fields

bool enableLowPower
 Enable low power mode. More...
 
afe_result_format_t resultFormat
 Select the result format. More...
 
afe_clock_divider_t clockDivider
 Select the clock divider ration for the modulator clock. More...
 
afe_clock_source_t clockSource
 Select clock source for modulator clock. More...
 
uint8_t startupCount
 Select the start up delay of modulators. More...
 

Field Documentation

bool afe_config_t::enableLowPower
afe_result_format_t afe_config_t::resultFormat
afe_clock_divider_t afe_config_t::clockDivider
afe_clock_source_t afe_config_t::clockSource
uint8_t afe_config_t::startupCount

Macro Definition Documentation

#define FSL_AFE_DRIVER_VERSION   (MAKE_VERSION(2, 0, 2))

Enumeration Type Documentation

Enumerator
kAFE_Channel0OverflowFlag 

Channel 0 previous conversion result has not been read and new data has already arrived.

kAFE_Channel1OverflowFlag 

Channel 1 previous conversion result has not been read and new data has already arrived.

kAFE_Channel2OverflowFlag 

Channel 2 previous conversion result has not been read and new data has already arrived.

kAFE_Channel0ReadyFlag 

Channel 0 is ready to conversion.

kAFE_Channel1ReadyFlag 

Channel 1 is ready to conversion.

kAFE_Channel2ReadyFlag 

Channel 2 is ready to conversion.

kAFE_Channel0ConversionCompleteFlag 

Channel 0 conversion is complete.

kAFE_Channel1ConversionCompleteFlag 

Channel 1 conversion is complete.

kAFE_Channel2ConversionCompleteFlag 

Channel 2 conversion is complete.

kAFE_Channel3OverflowFlag 

Channel 3 previous conversion result has not been read and new data has already arrived.

kAFE_Channel3ReadyFlag 

Channel 3 is ready to conversion.

kAFE_Channel3ConversionCompleteFlag 

Channel 3 conversion is complete.

anonymous enum
Enumerator
kAFE_Channel0InterruptEnable 

Channel 0 Interrupt.

kAFE_Channel1InterruptEnable 

Channel 1 Interrupt.

kAFE_Channel2InterruptEnable 

Channel 2 Interrupt.

kAFE_Channel3InterruptEnable 

Channel 3 Interrupt.

anonymous enum
Enumerator
kAFE_Channel0DMAEnable 

Channel 0 DMA.

kAFE_Channel1DMAEnable 

Channel 1 DMA.

kAFE_Channel2DMAEnable 

Channel 2 DMA.

kAFE_Channel3DMAEnable 

Channel 3 DMA.

anonymous enum
Enumerator
kAFE_Channel0Trigger 

Channel 0 software trigger.

kAFE_Channel1Trigger 

Channel 1 software trigger.

kAFE_Channel2Trigger 

Channel 2 software trigger.

kAFE_Channel3Trigger 

Channel 3 software trigger.

Enumerator
kAFE_DecimatorOversampleRatio64 

Decimator over sample ratio is 64.

kAFE_DecimatorOversampleRatio128 

Decimator over sample ratio is 128.

kAFE_DecimatorOversampleRatio256 

Decimator over sample ratio is 256.

kAFE_DecimatorOversampleRatio512 

Decimator over sample ratio is 512.

kAFE_DecimatorOversampleRatio1024 

Decimator over sample ratio is 1024.

kAFE_DecimatorOversampleRatio2048 

Decimator over sample ratio is 2048.

Enumerator
kAFE_ResultFormatLeft 

Left justified result format.

kAFE_ResultFormatRight 

Right justified result format.

Enumerator
kAFE_ClockDivider1 

Clock divided by 1.

kAFE_ClockDivider2 

Clock divided by 2.

kAFE_ClockDivider4 

Clock divided by 4.

kAFE_ClockDivider8 

Clock divided by 8.

kAFE_ClockDivider16 

Clock divided by 16.

kAFE_ClockDivider32 

Clock divided by 32.

kAFE_ClockDivider64 

Clock divided by 64.

kAFE_ClockDivider128 

Clock divided by 128.

kAFE_ClockDivider256 

Clock divided by 256.

Enumerator
kAFE_ClockSource0 

Modulator clock source 0.

kAFE_ClockSource1 

Modulator clock source 1.

kAFE_ClockSource2 

Modulator clock source 2.

kAFE_ClockSource3 

Modulator clock source 3.

Enumerator
kAFE_PgaDisable 

PGA disabled.

kAFE_PgaGain1 

Input gained by 1.

kAFE_PgaGain2 

Input gained by 2.

kAFE_PgaGain4 

Input gained by 4.

kAFE_PgaGain8 

Input gained by 8.

kAFE_PgaGain16 

Input gained by 16.

kAFE_PgaGain32 

Input gained by 32.

Enumerator
kAFE_BypassInternalClockPositiveEdge 

Bypassed channel mode - internal clock selected, positive edge for registering data by the decimation filter.

kAFE_BypassExternalClockPositiveEdge 

Bypassed channel mode - external clock selected, positive edge for registering data by the decimation filter.

kAFE_BypassInternalClockNegativeEdge 

Bypassed channel mode - internal clock selected, negative edge for registering data by the decimation filter.

kAFE_BypassExternalClockNegativeEdge 

Bypassed channel mode - external clock selected, negative edge for registering data by the decimation filter.

kAFE_BypassDisable 

Normal channel mode.

Function Documentation

void AFE_Init ( AFE_Type *  base,
const afe_config_t *  config 
)

This function configures the AFE module for the configuration which are shared by all channels.

Parameters
baseAFE peripheral base address.
configPointer to structure of "afe_config_t".
void AFE_Deinit ( AFE_Type *  base)

This function disables clock.

Parameters
baseAFE peripheral base address.
void AFE_GetDefaultConfig ( afe_config_t *  config)

This function fills the afe_config_t structure with default settings. Defaut value are:

* config->enableLowPower = false;
* config->resultFormat = kAFE_ResultFormatRight;
* config->clockDivider = kAFE_ClockDivider2;
* config->clockSource = kAFE_ClockSource1;
* config->startupCount = 2U;
*
Parameters
configPointer to structure of "afe_config_t".
static void AFE_SoftwareReset ( AFE_Type *  base,
bool  enable 
)
inlinestatic

This function is to reset all the ADCs, PGAs, decimation filters and clock configuration bits. When asserted as "false", all ADCs, PGAs and decimation filters are disabled. Clock Configuration bits are reset. When asserted as "true", all ADCs, PGAs and decimation filters are enabled.

Parameters
baseAFE peripheral base address.
enableAssert the reset command.
static void AFE_Enable ( AFE_Type *  base,
bool  enable 
)
inlinestatic

This function enables AFE and filter.

Parameters
baseAFE peripheral base address.
enableEnable the AFE module or not.
void AFE_SetChannelConfig ( AFE_Type *  base,
uint32_t  channel,
const afe_channel_config_t *  config 
)

This function configures the selected AFE channel.

Parameters
baseAFE peripheral base address.
channelAFE channel index.
configPointer to structure of "afe_channel_config_t".
void AFE_GetDefaultChannelConfig ( afe_channel_config_t *  config)

This function fills the afe_channel_config_t structure with default settings. Default value are:

* config->enableHardwareTrigger = false;
* config->enableContinuousConversion = false;
* config->channelMode = kAFE_Normal;
* config->decimatorOversampleRatio = kAFE_DecimatorOversampleRatio64;
* config->pgaGainSelect = kAFE_PgaGain1;
*
Parameters
configPointer to structure of "afe_channel_config_t".
uint32_t AFE_GetChannelConversionValue ( AFE_Type *  base,
uint32_t  channel 
)

This function returns the raw conversion value of the selected channel.

Parameters
baseAFE peripheral base address.
channelAFE channel index.
Returns
Conversion value.
Note
The returned value could be left or right adjusted according to the AFE module configuration.
static void AFE_DoSoftwareTriggerChannel ( AFE_Type *  base,
uint32_t  mask 
)
inlinestatic

This function triggers the AFE conversion by executing a software command. It starts the conversion on selected channels if the software trigger option is selected for the channels.

Parameters
baseAFE peripheral base address.
maskAFE channel mask software trigger. The parameter can be combination of the following source if defined:
  • kAFE_Channel0Trigger
  • kAFE_Channel1Trigger
  • kAFE_Channel2Trigger
  • kAFE_Channel3Trigger
static uint32_t AFE_GetChannelStatusFlags ( AFE_Type *  base)
inlinestatic

This function gets all AFE status.

Parameters
baseAFE peripheral base address.
Returns
the mask of these status flag bits.
void AFE_SetChannelPhaseDelayValue ( AFE_Type *  base,
uint32_t  channel,
uint32_t  value 
)

This function sets the phase delays for channels. This delay is inserted before the trigger response of the decimation filters. The delay is used to provide a phase compensation between AFE channels in step of prescaled modulator clock periods.

Parameters
baseAFE peripheral base address.
channelAFE channel index.
valuedelay time value.
static void AFE_SetChannelPhasetDelayOk ( AFE_Type *  base)
inlinestatic

This function should be called after all desired channel's delay registers are loaded. Values in channel's delay registers are active after calling this function and after the conversation starts.

Parameters
baseAFE peripheral base address.
static void AFE_EnableChannelInterrupts ( AFE_Type *  base,
uint32_t  mask 
)
inlinestatic

This function enables one channel interrupt.

Parameters
baseAFE peripheral base address.
maskAFE channel interrupt mask. The parameter can be combination of the following source if defined:
  • kAFE_Channel0InterruptEnable
  • kAFE_Channel1InterruptEnable
  • kAFE_Channel2InterruptEnable
  • kAFE_Channel3InterruptEnable
static void AFE_DisableChannelInterrupts ( AFE_Type *  base,
uint32_t  mask 
)
inlinestatic

This function disables one channel interrupt.

Parameters
baseAFE peripheral base address.
maskAFE channel interrupt mask. The parameter can be combination of the following source if defined:
  • kAFE_Channel0InterruptEnable
  • kAFE_Channel1InterruptEnable
  • kAFE_Channel2InterruptEnable
  • kAFE_Channel3InterruptEnable
static uint32_t AFE_GetEnabledChannelInterrupts ( AFE_Type *  base)
inlinestatic
Parameters
baseAFE peripheral base address.
Returns
Return the mask of these interrupt enable/disable bits.
void AFE_EnableChannelDMA ( AFE_Type *  base,
uint32_t  mask,
bool  enable 
)

This function enables/disables one channel DMA request.

Parameters
baseAFE peripheral base address.
maskAFE channel dma mask.
enablePass true to enable interrupt, false to disable. The parameter can be combination of the following source if defined:
  • kAFE_Channel0DMAEnable
  • kAFE_Channel1DMAEnable
  • kAFE_Channel2DMAEnable
  • kAFE_Channel3DMAEnable