MCUXpresso SDK API Reference Manual  Rev 2.13.0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages

Overview

SPI driver includes functional APIs and transactional APIs.

Functional APIs are feature/property target low level APIs. Functional APIs can be used for SPI initialization/configuration/operation for optimization/customization purpose. Using the functional API requires the knowledge of the SPI peripheral and how to organize functional APIs to meet the application requirements. All functional API use the peripheral base address as the first parameter. SPI functional operation groups provide the functional API set.

Transactional APIs are transaction target high level APIs. Transactional APIs can be used to enable the peripheral and in the application if the code size and performance of transactional APIs satisfy the requirements. If the code size and performance are a critical requirement, see the transactional API implementation and write a custom code. All transactional APIs use the spi_handle_t as the first parameter. Initialize the handle by calling the SPI_MasterTransferCreateHandle() or SPI_SlaveTransferCreateHandle() API.

Transactional APIs support asynchronous transfer. This means that the functions SPI_MasterTransferNonBlocking() and SPI_SlaveTransferNonBlocking() set up the interrupt for data transfer. When the transfer completes, the upper layer is notified through a callback function with the kStatus_SPI_Idle status.

Typical use case

SPI master transfer using an interrupt method

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/spi

SPI Send/receive using a DMA method

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/spi

Data Structures

struct  spi_master_config_t
 SPI master user configure structure. More...
 
struct  spi_slave_config_t
 SPI slave user configure structure. More...
 
struct  spi_transfer_t
 SPI transfer structure. More...
 
struct  spi_master_handle_t
 SPI transfer handle structure. More...
 

Macros

#define SPI_DUMMYDATA   (0xFFU)
 SPI dummy transfer data, the data is sent while txBuff is NULL. More...
 
#define SPI_RETRY_TIMES   0U /* Define to zero means keep waiting until the flag is assert/deassert. */
 Retry times for waiting flag. More...
 

Typedefs

typedef spi_master_handle_t spi_slave_handle_t
 Slave handle is the same with master handle.
 
typedef void(* spi_master_callback_t )(SPI_Type *base, spi_master_handle_t *handle, status_t status, void *userData)
 SPI master callback for finished transmit.
 
typedef void(* spi_slave_callback_t )(SPI_Type *base, spi_slave_handle_t *handle, status_t status, void *userData)
 SPI master callback for finished transmit.
 

Enumerations

enum  {
  kStatus_SPI_Busy = MAKE_STATUS(kStatusGroup_SPI, 0),
  kStatus_SPI_Idle = MAKE_STATUS(kStatusGroup_SPI, 1),
  kStatus_SPI_Error = MAKE_STATUS(kStatusGroup_SPI, 2),
  kStatus_SPI_Timeout = MAKE_STATUS(kStatusGroup_SPI, 3)
}
 Return status for the SPI driver. More...
 
enum  spi_clock_polarity_t {
  kSPI_ClockPolarityActiveHigh = 0x0U,
  kSPI_ClockPolarityActiveLow
}
 SPI clock polarity configuration. More...
 
enum  spi_clock_phase_t {
  kSPI_ClockPhaseFirstEdge = 0x0U,
  kSPI_ClockPhaseSecondEdge
}
 SPI clock phase configuration. More...
 
enum  spi_shift_direction_t {
  kSPI_MsbFirst = 0x0U,
  kSPI_LsbFirst
}
 SPI data shifter direction options. More...
 
enum  spi_ss_output_mode_t {
  kSPI_SlaveSelectAsGpio = 0x0U,
  kSPI_SlaveSelectFaultInput = 0x2U,
  kSPI_SlaveSelectAutomaticOutput = 0x3U
}
 SPI slave select output mode options. More...
 
enum  spi_pin_mode_t {
  kSPI_PinModeNormal = 0x0U,
  kSPI_PinModeInput = 0x1U,
  kSPI_PinModeOutput = 0x3U
}
 SPI pin mode options. More...
 
enum  spi_data_bitcount_mode_t {
  kSPI_8BitMode = 0x0U,
  kSPI_16BitMode
}
 SPI data length mode options. More...
 
enum  _spi_interrupt_enable {
  kSPI_RxFullAndModfInterruptEnable = 0x1U,
  kSPI_TxEmptyInterruptEnable = 0x2U,
  kSPI_MatchInterruptEnable = 0x4U,
  kSPI_RxFifoNearFullInterruptEnable = 0x8U,
  kSPI_TxFifoNearEmptyInterruptEnable = 0x10U
}
 SPI interrupt sources. More...
 
enum  _spi_flags {
  kSPI_RxBufferFullFlag = SPI_S_SPRF_MASK,
  kSPI_MatchFlag = SPI_S_SPMF_MASK,
  kSPI_TxBufferEmptyFlag = SPI_S_SPTEF_MASK,
  kSPI_ModeFaultFlag = SPI_S_MODF_MASK,
  kSPI_RxFifoNearFullFlag = SPI_S_RNFULLF_MASK,
  kSPI_TxFifoNearEmptyFlag = SPI_S_TNEAREF_MASK,
  kSPI_TxFifoFullFlag = SPI_S_TXFULLF_MASK,
  kSPI_RxFifoEmptyFlag = SPI_S_RFIFOEF_MASK,
  kSPI_TxFifoError = SPI_CI_TXFERR_MASK << 8U,
  kSPI_RxFifoError = SPI_CI_RXFERR_MASK << 8U,
  kSPI_TxOverflow = SPI_CI_TXFOF_MASK << 8U,
  kSPI_RxOverflow = SPI_CI_RXFOF_MASK << 8U
}
 SPI status flags. More...
 
enum  spi_w1c_interrupt_t {
  kSPI_RxFifoFullClearInterrupt = SPI_CI_SPRFCI_MASK,
  kSPI_TxFifoEmptyClearInterrupt = SPI_CI_SPTEFCI_MASK,
  kSPI_RxNearFullClearInterrupt = SPI_CI_RNFULLFCI_MASK,
  kSPI_TxNearEmptyClearInterrupt = SPI_CI_TNEAREFCI_MASK
}
 SPI FIFO write-1-to-clear interrupt flags. More...
 
enum  spi_txfifo_watermark_t {
  kSPI_TxFifoOneFourthEmpty = 0,
  kSPI_TxFifoOneHalfEmpty = 1
}
 SPI TX FIFO watermark settings. More...
 
enum  spi_rxfifo_watermark_t {
  kSPI_RxFifoThreeFourthsFull = 0,
  kSPI_RxFifoOneHalfFull = 1
}
 SPI RX FIFO watermark settings. More...
 
enum  _spi_dma_enable_t {
  kSPI_TxDmaEnable = SPI_C2_TXDMAE_MASK,
  kSPI_RxDmaEnable = SPI_C2_RXDMAE_MASK,
  kSPI_DmaAllEnable = (SPI_C2_TXDMAE_MASK | SPI_C2_RXDMAE_MASK)
}
 SPI DMA source. More...
 

Variables

volatile uint8_t g_spiDummyData []
 Global variable for dummy data value setting. More...
 

Driver version

#define FSL_SPI_DRIVER_VERSION   (MAKE_VERSION(2, 1, 1))
 SPI driver version. More...
 

Initialization and deinitialization

void SPI_MasterGetDefaultConfig (spi_master_config_t *config)
 Sets the SPI master configuration structure to default values. More...
 
void SPI_MasterInit (SPI_Type *base, const spi_master_config_t *config, uint32_t srcClock_Hz)
 Initializes the SPI with master configuration. More...
 
void SPI_SlaveGetDefaultConfig (spi_slave_config_t *config)
 Sets the SPI slave configuration structure to default values. More...
 
void SPI_SlaveInit (SPI_Type *base, const spi_slave_config_t *config)
 Initializes the SPI with slave configuration. More...
 
void SPI_Deinit (SPI_Type *base)
 De-initializes the SPI. More...
 
static void SPI_Enable (SPI_Type *base, bool enable)
 Enables or disables the SPI. More...
 

Status

uint32_t SPI_GetStatusFlags (SPI_Type *base)
 Gets the status flag. More...
 
static void SPI_ClearInterrupt (SPI_Type *base, uint8_t mask)
 Clear the interrupt if enable INCTLR. More...
 

Interrupts

void SPI_EnableInterrupts (SPI_Type *base, uint32_t mask)
 Enables the interrupt for the SPI. More...
 
void SPI_DisableInterrupts (SPI_Type *base, uint32_t mask)
 Disables the interrupt for the SPI. More...
 

DMA Control

static void SPI_EnableDMA (SPI_Type *base, uint8_t mask, bool enable)
 Enables the DMA source for SPI. More...
 
static uint32_t SPI_GetDataRegisterAddress (SPI_Type *base)
 Gets the SPI tx/rx data register address. More...
 

Bus Operations

uint32_t SPI_GetInstance (SPI_Type *base)
 Get the instance for SPI module. More...
 
static void SPI_SetPinMode (SPI_Type *base, spi_pin_mode_t pinMode)
 Sets the pin mode for transfer. More...
 
void SPI_MasterSetBaudRate (SPI_Type *base, uint32_t baudRate_Bps, uint32_t srcClock_Hz)
 Sets the baud rate for SPI transfer. More...
 
static void SPI_SetMatchData (SPI_Type *base, uint32_t matchData)
 Sets the match data for SPI. More...
 
void SPI_EnableFIFO (SPI_Type *base, bool enable)
 Enables or disables the FIFO if there is a FIFO. More...
 
status_t SPI_WriteBlocking (SPI_Type *base, uint8_t *buffer, size_t size)
 Sends a buffer of data bytes using a blocking method. More...
 
void SPI_WriteData (SPI_Type *base, uint16_t data)
 Writes a data into the SPI data register. More...
 
uint16_t SPI_ReadData (SPI_Type *base)
 Gets a data from the SPI data register. More...
 
void SPI_SetDummyData (SPI_Type *base, uint8_t dummyData)
 Set up the dummy data. More...
 

Transactional

void SPI_MasterTransferCreateHandle (SPI_Type *base, spi_master_handle_t *handle, spi_master_callback_t callback, void *userData)
 Initializes the SPI master handle. More...
 
status_t SPI_MasterTransferBlocking (SPI_Type *base, spi_transfer_t *xfer)
 Transfers a block of data using a polling method. More...
 
status_t SPI_MasterTransferNonBlocking (SPI_Type *base, spi_master_handle_t *handle, spi_transfer_t *xfer)
 Performs a non-blocking SPI interrupt transfer. More...
 
status_t SPI_MasterTransferGetCount (SPI_Type *base, spi_master_handle_t *handle, size_t *count)
 Gets the bytes of the SPI interrupt transferred. More...
 
void SPI_MasterTransferAbort (SPI_Type *base, spi_master_handle_t *handle)
 Aborts an SPI transfer using interrupt. More...
 
void SPI_MasterTransferHandleIRQ (SPI_Type *base, spi_master_handle_t *handle)
 Interrupts the handler for the SPI. More...
 
void SPI_SlaveTransferCreateHandle (SPI_Type *base, spi_slave_handle_t *handle, spi_slave_callback_t callback, void *userData)
 Initializes the SPI slave handle. More...
 
status_t SPI_SlaveTransferNonBlocking (SPI_Type *base, spi_slave_handle_t *handle, spi_transfer_t *xfer)
 Performs a non-blocking SPI slave interrupt transfer. More...
 
static status_t SPI_SlaveTransferGetCount (SPI_Type *base, spi_slave_handle_t *handle, size_t *count)
 Gets the bytes of the SPI interrupt transferred. More...
 
static void SPI_SlaveTransferAbort (SPI_Type *base, spi_slave_handle_t *handle)
 Aborts an SPI slave transfer using interrupt. More...
 
void SPI_SlaveTransferHandleIRQ (SPI_Type *base, spi_slave_handle_t *handle)
 Interrupts a handler for the SPI slave. More...
 

Data Structure Documentation

struct spi_master_config_t

Data Fields

bool enableMaster
 Enable SPI at initialization time.
 
bool enableStopInWaitMode
 SPI stop in wait mode.
 
spi_clock_polarity_t polarity
 Clock polarity.
 
spi_clock_phase_t phase
 Clock phase.
 
spi_shift_direction_t direction
 MSB or LSB.
 
spi_data_bitcount_mode_t dataMode
 8bit or 16bit mode
 
spi_txfifo_watermark_t txWatermark
 Tx watermark settings.
 
spi_rxfifo_watermark_t rxWatermark
 Rx watermark settings.
 
spi_ss_output_mode_t outputMode
 SS pin setting.
 
spi_pin_mode_t pinMode
 SPI pin mode select.
 
uint32_t baudRate_Bps
 Baud Rate for SPI in Hz.
 
struct spi_slave_config_t

Data Fields

bool enableSlave
 Enable SPI at initialization time.
 
bool enableStopInWaitMode
 SPI stop in wait mode.
 
spi_clock_polarity_t polarity
 Clock polarity.
 
spi_clock_phase_t phase
 Clock phase.
 
spi_shift_direction_t direction
 MSB or LSB.
 
spi_data_bitcount_mode_t dataMode
 8bit or 16bit mode
 
spi_txfifo_watermark_t txWatermark
 Tx watermark settings.
 
spi_rxfifo_watermark_t rxWatermark
 Rx watermark settings.
 
spi_pin_mode_t pinMode
 SPI pin mode select.
 
struct spi_transfer_t

Data Fields

uint8_t * txData
 Send buffer.
 
uint8_t * rxData
 Receive buffer.
 
size_t dataSize
 Transfer bytes.
 
uint32_t flags
 SPI control flag, useless to SPI. More...
 

Field Documentation

uint32_t spi_transfer_t::flags
struct _spi_master_handle

Data Fields

uint8_t *volatile txData
 Transfer buffer.
 
uint8_t *volatile rxData
 Receive buffer.
 
volatile size_t txRemainingBytes
 Send data remaining in bytes.
 
volatile size_t rxRemainingBytes
 Receive data remaining in bytes.
 
volatile uint32_t state
 SPI internal state.
 
size_t transferSize
 Bytes to be transferred.
 
uint8_t bytePerFrame
 SPI mode, 2bytes or 1byte in a frame.
 
uint8_t watermark
 Watermark value for SPI transfer.
 
spi_master_callback_t callback
 SPI callback.
 
void * userData
 Callback parameter.
 

Macro Definition Documentation

#define FSL_SPI_DRIVER_VERSION   (MAKE_VERSION(2, 1, 1))
#define SPI_DUMMYDATA   (0xFFU)
#define SPI_RETRY_TIMES   0U /* Define to zero means keep waiting until the flag is assert/deassert. */

Enumeration Type Documentation

anonymous enum
Enumerator
kStatus_SPI_Busy 

SPI bus is busy.

kStatus_SPI_Idle 

SPI is idle.

kStatus_SPI_Error 

SPI error.

kStatus_SPI_Timeout 

SPI timeout polling status flags.

Enumerator
kSPI_ClockPolarityActiveHigh 

Active-high SPI clock (idles low).

kSPI_ClockPolarityActiveLow 

Active-low SPI clock (idles high).

Enumerator
kSPI_ClockPhaseFirstEdge 

First edge on SPSCK occurs at the middle of the first cycle of a data transfer.

kSPI_ClockPhaseSecondEdge 

First edge on SPSCK occurs at the start of the first cycle of a data transfer.

Enumerator
kSPI_MsbFirst 

Data transfers start with most significant bit.

kSPI_LsbFirst 

Data transfers start with least significant bit.

Enumerator
kSPI_SlaveSelectAsGpio 

Slave select pin configured as GPIO.

kSPI_SlaveSelectFaultInput 

Slave select pin configured for fault detection.

kSPI_SlaveSelectAutomaticOutput 

Slave select pin configured for automatic SPI output.

Enumerator
kSPI_PinModeNormal 

Pins operate in normal, single-direction mode.

kSPI_PinModeInput 

Bidirectional mode.

Master: MOSI pin is input; Slave: MISO pin is input.

kSPI_PinModeOutput 

Bidirectional mode.

Master: MOSI pin is output; Slave: MISO pin is output.

Enumerator
kSPI_8BitMode 

8-bit data transmission mode

kSPI_16BitMode 

16-bit data transmission mode

Enumerator
kSPI_RxFullAndModfInterruptEnable 

Receive buffer full (SPRF) and mode fault (MODF) interrupt.

kSPI_TxEmptyInterruptEnable 

Transmit buffer empty interrupt.

kSPI_MatchInterruptEnable 

Match interrupt.

kSPI_RxFifoNearFullInterruptEnable 

Receive FIFO nearly full interrupt.

kSPI_TxFifoNearEmptyInterruptEnable 

Transmit FIFO nearly empty interrupt.

enum _spi_flags
Enumerator
kSPI_RxBufferFullFlag 

Read buffer full flag.

kSPI_MatchFlag 

Match flag.

kSPI_TxBufferEmptyFlag 

Transmit buffer empty flag.

kSPI_ModeFaultFlag 

Mode fault flag.

kSPI_RxFifoNearFullFlag 

Rx FIFO near full.

kSPI_TxFifoNearEmptyFlag 

Tx FIFO near empty.

kSPI_TxFifoFullFlag 

Tx FIFO full.

kSPI_RxFifoEmptyFlag 

Rx FIFO empty.

kSPI_TxFifoError 

Tx FIFO error.

kSPI_RxFifoError 

Rx FIFO error.

kSPI_TxOverflow 

Tx FIFO Overflow.

kSPI_RxOverflow 

Rx FIFO Overflow.

Enumerator
kSPI_RxFifoFullClearInterrupt 

Receive FIFO full interrupt.

kSPI_TxFifoEmptyClearInterrupt 

Transmit FIFO empty interrupt.

kSPI_RxNearFullClearInterrupt 

Receive FIFO nearly full interrupt.

kSPI_TxNearEmptyClearInterrupt 

Transmit FIFO nearly empty interrupt.

Enumerator
kSPI_TxFifoOneFourthEmpty 

SPI tx watermark at 1/4 FIFO size.

kSPI_TxFifoOneHalfEmpty 

SPI tx watermark at 1/2 FIFO size.

Enumerator
kSPI_RxFifoThreeFourthsFull 

SPI rx watermark at 3/4 FIFO size.

kSPI_RxFifoOneHalfFull 

SPI rx watermark at 1/2 FIFO size.

Enumerator
kSPI_TxDmaEnable 

Tx DMA request source.

kSPI_RxDmaEnable 

Rx DMA request source.

kSPI_DmaAllEnable 

All DMA request source.

Function Documentation

void SPI_MasterGetDefaultConfig ( spi_master_config_t *  config)

The purpose of this API is to get the configuration structure initialized for use in SPI_MasterInit(). User may use the initialized structure unchanged in SPI_MasterInit(), or modify some fields of the structure before calling SPI_MasterInit(). After calling this API, the master is ready to transfer. Example:

Parameters
configpointer to master config structure
void SPI_MasterInit ( SPI_Type *  base,
const spi_master_config_t *  config,
uint32_t  srcClock_Hz 
)

The configuration structure can be filled by user from scratch, or be set with default values by SPI_MasterGetDefaultConfig(). After calling this API, the slave is ready to transfer. Example

.baudRate_Bps = 400000,
...
};
SPI_MasterInit(SPI0, &config);
Parameters
baseSPI base pointer
configpointer to master configuration structure
srcClock_HzSource clock frequency.
void SPI_SlaveGetDefaultConfig ( spi_slave_config_t *  config)

The purpose of this API is to get the configuration structure initialized for use in SPI_SlaveInit(). Modify some fields of the structure before calling SPI_SlaveInit(). Example:

Parameters
configpointer to slave configuration structure
void SPI_SlaveInit ( SPI_Type *  base,
const spi_slave_config_t *  config 
)

The configuration structure can be filled by user from scratch or be set with default values by SPI_SlaveGetDefaultConfig(). After calling this API, the slave is ready to transfer. Example

.polarity = kSPIClockPolarity_ActiveHigh;
.phase = kSPIClockPhase_FirstEdge;
.direction = kSPIMsbFirst;
...
};
SPI_MasterInit(SPI0, &config);
Parameters
baseSPI base pointer
configpointer to master configuration structure
void SPI_Deinit ( SPI_Type *  base)

Calling this API resets the SPI module, gates the SPI clock. The SPI module can't work unless calling the SPI_MasterInit/SPI_SlaveInit to initialize module.

Parameters
baseSPI base pointer
static void SPI_Enable ( SPI_Type *  base,
bool  enable 
)
inlinestatic
Parameters
baseSPI base pointer
enablepass true to enable module, false to disable module
uint32_t SPI_GetStatusFlags ( SPI_Type *  base)
Parameters
baseSPI base pointer
Returns
SPI Status, use status flag to AND _spi_flags could get the related status.
static void SPI_ClearInterrupt ( SPI_Type *  base,
uint8_t  mask 
)
inlinestatic
Parameters
baseSPI base pointer
maskInterrupt need to be cleared The parameter could be any combination of the following values:
  • kSPI_RxFullAndModfInterruptEnable
  • kSPI_TxEmptyInterruptEnable
  • kSPI_MatchInterruptEnable
  • kSPI_RxFifoNearFullInterruptEnable
  • kSPI_TxFifoNearEmptyInterruptEnable
void SPI_EnableInterrupts ( SPI_Type *  base,
uint32_t  mask 
)
Parameters
baseSPI base pointer
maskSPI interrupt source. The parameter can be any combination of the following values:
  • kSPI_RxFullAndModfInterruptEnable
  • kSPI_TxEmptyInterruptEnable
  • kSPI_MatchInterruptEnable
  • kSPI_RxFifoNearFullInterruptEnable
  • kSPI_TxFifoNearEmptyInterruptEnable
void SPI_DisableInterrupts ( SPI_Type *  base,
uint32_t  mask 
)
Parameters
baseSPI base pointer
maskSPI interrupt source. The parameter can be any combination of the following values:
  • kSPI_RxFullAndModfInterruptEnable
  • kSPI_TxEmptyInterruptEnable
  • kSPI_MatchInterruptEnable
  • kSPI_RxFifoNearFullInterruptEnable
  • kSPI_TxFifoNearEmptyInterruptEnable
static void SPI_EnableDMA ( SPI_Type *  base,
uint8_t  mask,
bool  enable 
)
inlinestatic
Parameters
baseSPI base pointer
maskSPI DMA source.
enableTrue means enable DMA, false means disable DMA
static uint32_t SPI_GetDataRegisterAddress ( SPI_Type *  base)
inlinestatic

This API is used to provide a transfer address for the SPI DMA transfer configuration.

Parameters
baseSPI base pointer
Returns
data register address
uint32_t SPI_GetInstance ( SPI_Type *  base)
Parameters
baseSPI base address
static void SPI_SetPinMode ( SPI_Type *  base,
spi_pin_mode_t  pinMode 
)
inlinestatic
Parameters
baseSPI base pointer
pinModepin mode for transfer AND _spi_pin_mode could get the related configuration.
void SPI_MasterSetBaudRate ( SPI_Type *  base,
uint32_t  baudRate_Bps,
uint32_t  srcClock_Hz 
)

This is only used in master.

Parameters
baseSPI base pointer
baudRate_Bpsbaud rate needed in Hz.
srcClock_HzSPI source clock frequency in Hz.
static void SPI_SetMatchData ( SPI_Type *  base,
uint32_t  matchData 
)
inlinestatic

The match data is a hardware comparison value. When the value received in the SPI receive data buffer equals the hardware comparison value, the SPI Match Flag in the S register (S[SPMF]) sets. This can also generate an interrupt if the enable bit sets.

Parameters
baseSPI base pointer
matchDataMatch data.
void SPI_EnableFIFO ( SPI_Type *  base,
bool  enable 
)
Parameters
baseSPI base pointer
enableTrue means enable FIFO, false means disable FIFO.
status_t SPI_WriteBlocking ( SPI_Type *  base,
uint8_t *  buffer,
size_t  size 
)
Note
This function blocks via polling until all bytes have been sent.
Parameters
baseSPI base pointer
bufferThe data bytes to send
sizeThe number of data bytes to send
Returns
kStatus_SPI_Timeout The transfer timed out and was aborted.
void SPI_WriteData ( SPI_Type *  base,
uint16_t  data 
)
Parameters
baseSPI base pointer
dataneeds to be write.
uint16_t SPI_ReadData ( SPI_Type *  base)
Parameters
baseSPI base pointer
Returns
Data in the register.
void SPI_SetDummyData ( SPI_Type *  base,
uint8_t  dummyData 
)
Parameters
baseSPI peripheral address.
dummyDataData to be transferred when tx buffer is NULL.
void SPI_MasterTransferCreateHandle ( SPI_Type *  base,
spi_master_handle_t *  handle,
spi_master_callback_t  callback,
void *  userData 
)

This function initializes the SPI master handle which can be used for other SPI master transactional APIs. Usually, for a specified SPI instance, call this API once to get the initialized handle.

Parameters
baseSPI peripheral base address.
handleSPI handle pointer.
callbackCallback function.
userDataUser data.
status_t SPI_MasterTransferBlocking ( SPI_Type *  base,
spi_transfer_t *  xfer 
)
Parameters
baseSPI base pointer
xferpointer to spi_xfer_config_t structure
Return values
kStatus_SuccessSuccessfully start a transfer.
kStatus_InvalidArgumentInput argument is invalid.
status_t SPI_MasterTransferNonBlocking ( SPI_Type *  base,
spi_master_handle_t *  handle,
spi_transfer_t *  xfer 
)
Note
The API immediately returns after transfer initialization is finished. Call SPI_GetStatusIRQ() to get the transfer status.
If SPI transfer data frame size is 16 bits, the transfer size cannot be an odd number.
Parameters
baseSPI peripheral base address.
handlepointer to spi_master_handle_t structure which stores the transfer state
xferpointer to spi_xfer_config_t structure
Return values
kStatus_SuccessSuccessfully start a transfer.
kStatus_InvalidArgumentInput argument is invalid.
kStatus_SPI_BusySPI is not idle, is running another transfer.
status_t SPI_MasterTransferGetCount ( SPI_Type *  base,
spi_master_handle_t *  handle,
size_t *  count 
)
Parameters
baseSPI peripheral base address.
handlePointer to SPI transfer handle, this should be a static variable.
countTransferred bytes of SPI master.
Return values
kStatus_SPI_SuccessSucceed get the transfer count.
kStatus_NoTransferInProgressThere is not a non-blocking transaction currently in progress.
void SPI_MasterTransferAbort ( SPI_Type *  base,
spi_master_handle_t *  handle 
)
Parameters
baseSPI peripheral base address.
handlePointer to SPI transfer handle, this should be a static variable.
void SPI_MasterTransferHandleIRQ ( SPI_Type *  base,
spi_master_handle_t *  handle 
)
Parameters
baseSPI peripheral base address.
handlepointer to spi_master_handle_t structure which stores the transfer state.
void SPI_SlaveTransferCreateHandle ( SPI_Type *  base,
spi_slave_handle_t *  handle,
spi_slave_callback_t  callback,
void *  userData 
)

This function initializes the SPI slave handle which can be used for other SPI slave transactional APIs. Usually, for a specified SPI instance, call this API once to get the initialized handle.

Parameters
baseSPI peripheral base address.
handleSPI handle pointer.
callbackCallback function.
userDataUser data.
status_t SPI_SlaveTransferNonBlocking ( SPI_Type *  base,
spi_slave_handle_t *  handle,
spi_transfer_t *  xfer 
)
Note
The API returns immediately after the transfer initialization is finished. Call SPI_GetStatusIRQ() to get the transfer status.
If SPI transfer data frame size is 16 bits, the transfer size cannot be an odd number.
Parameters
baseSPI peripheral base address.
handlepointer to spi_slave_handle_t structure which stores the transfer state
xferpointer to spi_xfer_config_t structure
Return values
kStatus_SuccessSuccessfully start a transfer.
kStatus_InvalidArgumentInput argument is invalid.
kStatus_SPI_BusySPI is not idle, is running another transfer.
static status_t SPI_SlaveTransferGetCount ( SPI_Type *  base,
spi_slave_handle_t *  handle,
size_t *  count 
)
inlinestatic
Parameters
baseSPI peripheral base address.
handlePointer to SPI transfer handle, this should be a static variable.
countTransferred bytes of SPI slave.
Return values
kStatus_SPI_SuccessSucceed get the transfer count.
kStatus_NoTransferInProgressThere is not a non-blocking transaction currently in progress.
static void SPI_SlaveTransferAbort ( SPI_Type *  base,
spi_slave_handle_t *  handle 
)
inlinestatic
Parameters
baseSPI peripheral base address.
handlePointer to SPI transfer handle, this should be a static variable.
void SPI_SlaveTransferHandleIRQ ( SPI_Type *  base,
spi_slave_handle_t *  handle 
)
Parameters
baseSPI peripheral base address.
handlepointer to spi_slave_handle_t structure which stores the transfer state

Variable Documentation

volatile uint8_t g_spiDummyData[]