The MCUXpresso SDK provides a peripheral driver for the CACHE Controller of MCUXpresso SDK devices.
The CACHE driver is created to help the user more easily operate the cache memory. The APIs for basic operations are including the following three levels: 1L. The local cache driver API. This level provides the caches controller drivers.
2L. The unified cache driver API. This level provides many APIs for unified cache driver APIs for combined L1 and L2 cache maintain operations. This is provided for SDK drivers (DMA, ENET, USDHC, etc) which should do the cache maintenance in their transactional APIs. Because in this arch, there is no L2 cache so the unified cache driver API directly calls local driver APIs.
Function groups
CACHE Operation
There are Enable/Disable APIs for cache control and cache maintenance operations as Invalidate/Clean/CleanInvalidate by all and by address range.
Boundary address is the FlexSPI internal address (start from 0) instead of system address (start from FlexSPI AMBA base) to split adjacent regions and must be 1KB aligned. The boundary address itself locates in upper region. Cacheable policy for each region.
| #define CACHE64_LINESIZE_BYTE (FSL_FEATURE_CACHE64_CTRL_LINESIZE_BYTE) |
| #define CACHE64_REGION_NUM (3U) |
| #define CACHE64_REGION_ALIGNMENT (0x400U) |
| Enumerator |
|---|
| kCACHE64_PolicyNonCacheable |
Non-cacheable.
|
| kCACHE64_PolicyWriteThrough |
Write through.
|
| kCACHE64_PolicyWriteBack |
Write back.
|
| uint32_t CACHE64_GetInstance |
( |
CACHE64_POLSEL_Type * |
base | ) |
|
- Parameters
-
| base | The peripheral base address. |
- Returns
- CACHE64_POLSEL instance number starting from 0.
| uint32_t CACHE64_GetInstanceByAddr |
( |
uint32_t |
address | ) |
|
param address The physical memory address.
- Returns
- CACHE64_CTRL instance number starting from 0.
This function configures the CACHE64 module with user-defined settings. Call the CACHE64_GetDefaultConfig() function to configure the configuration structure and get the default configuration.
- Parameters
-
| base | CACHE64_POLSEL peripheral base address. |
| config | Pointer to a user-defined configuration structure. |
- Return values
-
| kStatus_Success | CACHE64 initialize succeed |
This function initializes the CACHE64 configuration structure to a default value. The default values are first region covers whole cacheable area, and policy set to write back.
- Parameters
-
| config | Pointer to a configuration structure. |
| void CACHE64_EnableCache |
( |
CACHE64_CTRL_Type * |
base | ) |
|
- Parameters
-
| base | CACHE64_CTRL peripheral base address. |
| void CACHE64_DisableCache |
( |
CACHE64_CTRL_Type * |
base | ) |
|
- Parameters
-
| base | CACHE64_CTRL peripheral base address. |
| void CACHE64_InvalidateCache |
( |
CACHE64_CTRL_Type * |
base | ) |
|
- Parameters
-
| base | CACHE64_CTRL peripheral base address. |
| void CACHE64_InvalidateCacheByRange |
( |
uint32_t |
address, |
|
|
uint32_t |
size_byte |
|
) |
| |
- Parameters
-
| address | The physical address of cache. |
| size_byte | size of the memory to be invalidated. |
- Note
- Address and size should be aligned to "CACHE64_LINESIZE_BYTE". The startAddr here will be forced to align to CACHE64_LINESIZE_BYTE if startAddr is not aligned. For the size_byte, application should make sure the alignment or make sure the right operation order if the size_byte is not aligned.
| void CACHE64_CleanCache |
( |
CACHE64_CTRL_Type * |
base | ) |
|
- Parameters
-
| base | CACHE64_CTRL peripheral base address. |
| void CACHE64_CleanCacheByRange |
( |
uint32_t |
address, |
|
|
uint32_t |
size_byte |
|
) |
| |
- Parameters
-
| address | The physical address of cache. |
| size_byte | size of the memory to be cleaned. |
- Note
- Address and size should be aligned to "CACHE64_LINESIZE_BYTE". The startAddr here will be forced to align to CACHE64_LINESIZE_BYTE if startAddr is not aligned. For the size_byte, application should make sure the alignment or make sure the right operation order if the size_byte is not aligned.
| void CACHE64_CleanInvalidateCache |
( |
CACHE64_CTRL_Type * |
base | ) |
|
- Parameters
-
| base | CACHE64_CTRL peripheral base address. |
| void CACHE64_CleanInvalidateCacheByRange |
( |
uint32_t |
address, |
|
|
uint32_t |
size_byte |
|
) |
| |
- Parameters
-
| address | The physical address of cache. |
| size_byte | size of the memory to be Cleaned and Invalidated. |
- Note
- Address and size should be aligned to "CACHE64_LINESIZE_BYTE". The startAddr here will be forced to align to CACHE64_LINESIZE_BYTE if startAddr is not aligned. For the size_byte, application should make sure the alignment or make sure the right operation order if the size_byte is not aligned.
| void CACHE64_EnableWriteBuffer |
( |
CACHE64_CTRL_Type * |
base, |
|
|
bool |
enable |
|
) |
| |
- Parameters
-
| base | CACHE64_CTRL peripheral base address. |
| enable | The enable or disable flag. true - enable the write buffer. false - disable the write buffer. |
| static void ICACHE_InvalidateByRange |
( |
uint32_t |
address, |
|
|
uint32_t |
size_byte |
|
) |
| |
|
inlinestatic |
- Parameters
-
| address | The physical address. |
| size_byte | size of the memory to be invalidated. |
- Note
- Address and size should be aligned to CACHE64_LINESIZE_BYTE due to the cache operation unit FSL_FEATURE_CACHE64_CTRL_LINESIZE_BYTE. The startAddr here will be forced to align to the cache line size if startAddr is not aligned. For the size_byte, application should make sure the alignment or make sure the right operation order if the size_byte is not aligned.
| static void DCACHE_InvalidateByRange |
( |
uint32_t |
address, |
|
|
uint32_t |
size_byte |
|
) |
| |
|
inlinestatic |
- Parameters
-
| address | The physical address. |
| size_byte | size of the memory to be invalidated. |
- Note
- Address and size should be aligned to CACHE64_LINESIZE_BYTE due to the cache operation unit FSL_FEATURE_CACHE64_CTRL_LINESIZE_BYTE. The startAddr here will be forced to align to the cache line size if startAddr is not aligned. For the size_byte, application should make sure the alignment or make sure the right operation order if the size_byte is not aligned.
| static void DCACHE_CleanByRange |
( |
uint32_t |
address, |
|
|
uint32_t |
size_byte |
|
) |
| |
|
inlinestatic |
- Parameters
-
| address | The physical address. |
| size_byte | size of the memory to be cleaned. |
- Note
- Address and size should be aligned to CACHE64_LINESIZE_BYTE due to the cache operation unit FSL_FEATURE_CACHE64_CTRL_LINESIZE_BYTE. The startAddr here will be forced to align to the cache line size if startAddr is not aligned. For the size_byte, application should make sure the alignment or make sure the right operation order if the size_byte is not aligned.
| static void DCACHE_CleanInvalidateByRange |
( |
uint32_t |
address, |
|
|
uint32_t |
size_byte |
|
) |
| |
|
inlinestatic |
- Parameters
-
| address | The physical address. |
| size_byte | size of the memory to be Cleaned and Invalidated. |
- Note
- Address and size should be aligned to CACHE64_LINESIZE_BYTE due to the cache operation unit FSL_FEATURE_CACHE64_CTRL_LINESIZE_BYTE. The startAddr here will be forced to align to the cache line size if startAddr is not aligned. For the size_byte, application should make sure the alignment or make sure the right operation order if the size_byte is not aligned.